]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - block/blk-settings.c
am335x: lis33ldlh: Add accelerometer support to AM335X
[sitara-epos/sitara-epos-kernel.git] / block / blk-settings.c
1 /*
2  * Functions related to setting various queue properties from drivers
3  */
4 #include <linux/kernel.h>
5 #include <linux/module.h>
6 #include <linux/init.h>
7 #include <linux/bio.h>
8 #include <linux/blkdev.h>
9 #include <linux/bootmem.h>      /* for max_pfn/max_low_pfn */
10 #include <linux/gcd.h>
11 #include <linux/lcm.h>
12 #include <linux/jiffies.h>
13 #include <linux/gfp.h>
15 #include "blk.h"
17 unsigned long blk_max_low_pfn;
18 EXPORT_SYMBOL(blk_max_low_pfn);
20 unsigned long blk_max_pfn;
22 /**
23  * blk_queue_prep_rq - set a prepare_request function for queue
24  * @q:          queue
25  * @pfn:        prepare_request function
26  *
27  * It's possible for a queue to register a prepare_request callback which
28  * is invoked before the request is handed to the request_fn. The goal of
29  * the function is to prepare a request for I/O, it can be used to build a
30  * cdb from the request data for instance.
31  *
32  */
33 void blk_queue_prep_rq(struct request_queue *q, prep_rq_fn *pfn)
34 {
35         q->prep_rq_fn = pfn;
36 }
37 EXPORT_SYMBOL(blk_queue_prep_rq);
39 /**
40  * blk_queue_unprep_rq - set an unprepare_request function for queue
41  * @q:          queue
42  * @ufn:        unprepare_request function
43  *
44  * It's possible for a queue to register an unprepare_request callback
45  * which is invoked before the request is finally completed. The goal
46  * of the function is to deallocate any data that was allocated in the
47  * prepare_request callback.
48  *
49  */
50 void blk_queue_unprep_rq(struct request_queue *q, unprep_rq_fn *ufn)
51 {
52         q->unprep_rq_fn = ufn;
53 }
54 EXPORT_SYMBOL(blk_queue_unprep_rq);
56 /**
57  * blk_queue_merge_bvec - set a merge_bvec function for queue
58  * @q:          queue
59  * @mbfn:       merge_bvec_fn
60  *
61  * Usually queues have static limitations on the max sectors or segments that
62  * we can put in a request. Stacking drivers may have some settings that
63  * are dynamic, and thus we have to query the queue whether it is ok to
64  * add a new bio_vec to a bio at a given offset or not. If the block device
65  * has such limitations, it needs to register a merge_bvec_fn to control
66  * the size of bio's sent to it. Note that a block device *must* allow a
67  * single page to be added to an empty bio. The block device driver may want
68  * to use the bio_split() function to deal with these bio's. By default
69  * no merge_bvec_fn is defined for a queue, and only the fixed limits are
70  * honored.
71  */
72 void blk_queue_merge_bvec(struct request_queue *q, merge_bvec_fn *mbfn)
73 {
74         q->merge_bvec_fn = mbfn;
75 }
76 EXPORT_SYMBOL(blk_queue_merge_bvec);
78 void blk_queue_softirq_done(struct request_queue *q, softirq_done_fn *fn)
79 {
80         q->softirq_done_fn = fn;
81 }
82 EXPORT_SYMBOL(blk_queue_softirq_done);
84 void blk_queue_rq_timeout(struct request_queue *q, unsigned int timeout)
85 {
86         q->rq_timeout = timeout;
87 }
88 EXPORT_SYMBOL_GPL(blk_queue_rq_timeout);
90 void blk_queue_rq_timed_out(struct request_queue *q, rq_timed_out_fn *fn)
91 {
92         q->rq_timed_out_fn = fn;
93 }
94 EXPORT_SYMBOL_GPL(blk_queue_rq_timed_out);
96 void blk_queue_lld_busy(struct request_queue *q, lld_busy_fn *fn)
97 {
98         q->lld_busy_fn = fn;
99 }
100 EXPORT_SYMBOL_GPL(blk_queue_lld_busy);
102 /**
103  * blk_set_default_limits - reset limits to default values
104  * @lim:  the queue_limits structure to reset
105  *
106  * Description:
107  *   Returns a queue_limit struct to its default state.  Can be used by
108  *   stacking drivers like DM that stage table swaps and reuse an
109  *   existing device queue.
110  */
111 void blk_set_default_limits(struct queue_limits *lim)
113         lim->max_segments = BLK_MAX_SEGMENTS;
114         lim->max_integrity_segments = 0;
115         lim->seg_boundary_mask = BLK_SEG_BOUNDARY_MASK;
116         lim->max_segment_size = BLK_MAX_SEGMENT_SIZE;
117         lim->max_sectors = BLK_DEF_MAX_SECTORS;
118         lim->max_hw_sectors = INT_MAX;
119         lim->max_discard_sectors = 0;
120         lim->discard_granularity = 0;
121         lim->discard_alignment = 0;
122         lim->discard_misaligned = 0;
123         lim->discard_zeroes_data = 1;
124         lim->logical_block_size = lim->physical_block_size = lim->io_min = 512;
125         lim->bounce_pfn = (unsigned long)(BLK_BOUNCE_ANY >> PAGE_SHIFT);
126         lim->alignment_offset = 0;
127         lim->io_opt = 0;
128         lim->misaligned = 0;
129         lim->cluster = 1;
131 EXPORT_SYMBOL(blk_set_default_limits);
133 /**
134  * blk_queue_make_request - define an alternate make_request function for a device
135  * @q:  the request queue for the device to be affected
136  * @mfn: the alternate make_request function
137  *
138  * Description:
139  *    The normal way for &struct bios to be passed to a device
140  *    driver is for them to be collected into requests on a request
141  *    queue, and then to allow the device driver to select requests
142  *    off that queue when it is ready.  This works well for many block
143  *    devices. However some block devices (typically virtual devices
144  *    such as md or lvm) do not benefit from the processing on the
145  *    request queue, and are served best by having the requests passed
146  *    directly to them.  This can be achieved by providing a function
147  *    to blk_queue_make_request().
148  *
149  * Caveat:
150  *    The driver that does this *must* be able to deal appropriately
151  *    with buffers in "highmemory". This can be accomplished by either calling
152  *    __bio_kmap_atomic() to get a temporary kernel mapping, or by calling
153  *    blk_queue_bounce() to create a buffer in normal memory.
154  **/
155 void blk_queue_make_request(struct request_queue *q, make_request_fn *mfn)
157         /*
158          * set defaults
159          */
160         q->nr_requests = BLKDEV_MAX_RQ;
162         q->make_request_fn = mfn;
163         blk_queue_dma_alignment(q, 511);
164         blk_queue_congestion_threshold(q);
165         q->nr_batching = BLK_BATCH_REQ;
167         blk_set_default_limits(&q->limits);
168         blk_queue_max_hw_sectors(q, BLK_SAFE_MAX_SECTORS);
169         q->limits.discard_zeroes_data = 0;
171         /*
172          * by default assume old behaviour and bounce for any highmem page
173          */
174         blk_queue_bounce_limit(q, BLK_BOUNCE_HIGH);
176 EXPORT_SYMBOL(blk_queue_make_request);
178 /**
179  * blk_queue_bounce_limit - set bounce buffer limit for queue
180  * @q: the request queue for the device
181  * @dma_mask: the maximum address the device can handle
182  *
183  * Description:
184  *    Different hardware can have different requirements as to what pages
185  *    it can do I/O directly to. A low level driver can call
186  *    blk_queue_bounce_limit to have lower memory pages allocated as bounce
187  *    buffers for doing I/O to pages residing above @dma_mask.
188  **/
189 void blk_queue_bounce_limit(struct request_queue *q, u64 dma_mask)
191         unsigned long b_pfn = dma_mask >> PAGE_SHIFT;
192         int dma = 0;
194         q->bounce_gfp = GFP_NOIO;
195 #if BITS_PER_LONG == 64
196         /*
197          * Assume anything <= 4GB can be handled by IOMMU.  Actually
198          * some IOMMUs can handle everything, but I don't know of a
199          * way to test this here.
200          */
201         if (b_pfn < (min_t(u64, 0xffffffffUL, BLK_BOUNCE_HIGH) >> PAGE_SHIFT))
202                 dma = 1;
203         q->limits.bounce_pfn = max(max_low_pfn, b_pfn);
204 #else
205         if (b_pfn < blk_max_low_pfn)
206                 dma = 1;
207         q->limits.bounce_pfn = b_pfn;
208 #endif
209         if (dma) {
210                 init_emergency_isa_pool();
211                 q->bounce_gfp = GFP_NOIO | GFP_DMA;
212                 q->limits.bounce_pfn = b_pfn;
213         }
215 EXPORT_SYMBOL(blk_queue_bounce_limit);
217 /**
218  * blk_limits_max_hw_sectors - set hard and soft limit of max sectors for request
219  * @limits: the queue limits
220  * @max_hw_sectors:  max hardware sectors in the usual 512b unit
221  *
222  * Description:
223  *    Enables a low level driver to set a hard upper limit,
224  *    max_hw_sectors, on the size of requests.  max_hw_sectors is set by
225  *    the device driver based upon the combined capabilities of I/O
226  *    controller and storage device.
227  *
228  *    max_sectors is a soft limit imposed by the block layer for
229  *    filesystem type requests.  This value can be overridden on a
230  *    per-device basis in /sys/block/<device>/queue/max_sectors_kb.
231  *    The soft limit can not exceed max_hw_sectors.
232  **/
233 void blk_limits_max_hw_sectors(struct queue_limits *limits, unsigned int max_hw_sectors)
235         if ((max_hw_sectors << 9) < PAGE_CACHE_SIZE) {
236                 max_hw_sectors = 1 << (PAGE_CACHE_SHIFT - 9);
237                 printk(KERN_INFO "%s: set to minimum %d\n",
238                        __func__, max_hw_sectors);
239         }
241         limits->max_hw_sectors = max_hw_sectors;
242         limits->max_sectors = min_t(unsigned int, max_hw_sectors,
243                                     BLK_DEF_MAX_SECTORS);
245 EXPORT_SYMBOL(blk_limits_max_hw_sectors);
247 /**
248  * blk_queue_max_hw_sectors - set max sectors for a request for this queue
249  * @q:  the request queue for the device
250  * @max_hw_sectors:  max hardware sectors in the usual 512b unit
251  *
252  * Description:
253  *    See description for blk_limits_max_hw_sectors().
254  **/
255 void blk_queue_max_hw_sectors(struct request_queue *q, unsigned int max_hw_sectors)
257         blk_limits_max_hw_sectors(&q->limits, max_hw_sectors);
259 EXPORT_SYMBOL(blk_queue_max_hw_sectors);
261 /**
262  * blk_queue_max_discard_sectors - set max sectors for a single discard
263  * @q:  the request queue for the device
264  * @max_discard_sectors: maximum number of sectors to discard
265  **/
266 void blk_queue_max_discard_sectors(struct request_queue *q,
267                 unsigned int max_discard_sectors)
269         q->limits.max_discard_sectors = max_discard_sectors;
271 EXPORT_SYMBOL(blk_queue_max_discard_sectors);
273 /**
274  * blk_queue_max_segments - set max hw segments for a request for this queue
275  * @q:  the request queue for the device
276  * @max_segments:  max number of segments
277  *
278  * Description:
279  *    Enables a low level driver to set an upper limit on the number of
280  *    hw data segments in a request.
281  **/
282 void blk_queue_max_segments(struct request_queue *q, unsigned short max_segments)
284         if (!max_segments) {
285                 max_segments = 1;
286                 printk(KERN_INFO "%s: set to minimum %d\n",
287                        __func__, max_segments);
288         }
290         q->limits.max_segments = max_segments;
292 EXPORT_SYMBOL(blk_queue_max_segments);
294 /**
295  * blk_queue_max_segment_size - set max segment size for blk_rq_map_sg
296  * @q:  the request queue for the device
297  * @max_size:  max size of segment in bytes
298  *
299  * Description:
300  *    Enables a low level driver to set an upper limit on the size of a
301  *    coalesced segment
302  **/
303 void blk_queue_max_segment_size(struct request_queue *q, unsigned int max_size)
305         if (max_size < PAGE_CACHE_SIZE) {
306                 max_size = PAGE_CACHE_SIZE;
307                 printk(KERN_INFO "%s: set to minimum %d\n",
308                        __func__, max_size);
309         }
311         q->limits.max_segment_size = max_size;
313 EXPORT_SYMBOL(blk_queue_max_segment_size);
315 /**
316  * blk_queue_logical_block_size - set logical block size for the queue
317  * @q:  the request queue for the device
318  * @size:  the logical block size, in bytes
319  *
320  * Description:
321  *   This should be set to the lowest possible block size that the
322  *   storage device can address.  The default of 512 covers most
323  *   hardware.
324  **/
325 void blk_queue_logical_block_size(struct request_queue *q, unsigned short size)
327         q->limits.logical_block_size = size;
329         if (q->limits.physical_block_size < size)
330                 q->limits.physical_block_size = size;
332         if (q->limits.io_min < q->limits.physical_block_size)
333                 q->limits.io_min = q->limits.physical_block_size;
335 EXPORT_SYMBOL(blk_queue_logical_block_size);
337 /**
338  * blk_queue_physical_block_size - set physical block size for the queue
339  * @q:  the request queue for the device
340  * @size:  the physical block size, in bytes
341  *
342  * Description:
343  *   This should be set to the lowest possible sector size that the
344  *   hardware can operate on without reverting to read-modify-write
345  *   operations.
346  */
347 void blk_queue_physical_block_size(struct request_queue *q, unsigned int size)
349         q->limits.physical_block_size = size;
351         if (q->limits.physical_block_size < q->limits.logical_block_size)
352                 q->limits.physical_block_size = q->limits.logical_block_size;
354         if (q->limits.io_min < q->limits.physical_block_size)
355                 q->limits.io_min = q->limits.physical_block_size;
357 EXPORT_SYMBOL(blk_queue_physical_block_size);
359 /**
360  * blk_queue_alignment_offset - set physical block alignment offset
361  * @q:  the request queue for the device
362  * @offset: alignment offset in bytes
363  *
364  * Description:
365  *   Some devices are naturally misaligned to compensate for things like
366  *   the legacy DOS partition table 63-sector offset.  Low-level drivers
367  *   should call this function for devices whose first sector is not
368  *   naturally aligned.
369  */
370 void blk_queue_alignment_offset(struct request_queue *q, unsigned int offset)
372         q->limits.alignment_offset =
373                 offset & (q->limits.physical_block_size - 1);
374         q->limits.misaligned = 0;
376 EXPORT_SYMBOL(blk_queue_alignment_offset);
378 /**
379  * blk_limits_io_min - set minimum request size for a device
380  * @limits: the queue limits
381  * @min:  smallest I/O size in bytes
382  *
383  * Description:
384  *   Some devices have an internal block size bigger than the reported
385  *   hardware sector size.  This function can be used to signal the
386  *   smallest I/O the device can perform without incurring a performance
387  *   penalty.
388  */
389 void blk_limits_io_min(struct queue_limits *limits, unsigned int min)
391         limits->io_min = min;
393         if (limits->io_min < limits->logical_block_size)
394                 limits->io_min = limits->logical_block_size;
396         if (limits->io_min < limits->physical_block_size)
397                 limits->io_min = limits->physical_block_size;
399 EXPORT_SYMBOL(blk_limits_io_min);
401 /**
402  * blk_queue_io_min - set minimum request size for the queue
403  * @q:  the request queue for the device
404  * @min:  smallest I/O size in bytes
405  *
406  * Description:
407  *   Storage devices may report a granularity or preferred minimum I/O
408  *   size which is the smallest request the device can perform without
409  *   incurring a performance penalty.  For disk drives this is often the
410  *   physical block size.  For RAID arrays it is often the stripe chunk
411  *   size.  A properly aligned multiple of minimum_io_size is the
412  *   preferred request size for workloads where a high number of I/O
413  *   operations is desired.
414  */
415 void blk_queue_io_min(struct request_queue *q, unsigned int min)
417         blk_limits_io_min(&q->limits, min);
419 EXPORT_SYMBOL(blk_queue_io_min);
421 /**
422  * blk_limits_io_opt - set optimal request size for a device
423  * @limits: the queue limits
424  * @opt:  smallest I/O size in bytes
425  *
426  * Description:
427  *   Storage devices may report an optimal I/O size, which is the
428  *   device's preferred unit for sustained I/O.  This is rarely reported
429  *   for disk drives.  For RAID arrays it is usually the stripe width or
430  *   the internal track size.  A properly aligned multiple of
431  *   optimal_io_size is the preferred request size for workloads where
432  *   sustained throughput is desired.
433  */
434 void blk_limits_io_opt(struct queue_limits *limits, unsigned int opt)
436         limits->io_opt = opt;
438 EXPORT_SYMBOL(blk_limits_io_opt);
440 /**
441  * blk_queue_io_opt - set optimal request size for the queue
442  * @q:  the request queue for the device
443  * @opt:  optimal request size in bytes
444  *
445  * Description:
446  *   Storage devices may report an optimal I/O size, which is the
447  *   device's preferred unit for sustained I/O.  This is rarely reported
448  *   for disk drives.  For RAID arrays it is usually the stripe width or
449  *   the internal track size.  A properly aligned multiple of
450  *   optimal_io_size is the preferred request size for workloads where
451  *   sustained throughput is desired.
452  */
453 void blk_queue_io_opt(struct request_queue *q, unsigned int opt)
455         blk_limits_io_opt(&q->limits, opt);
457 EXPORT_SYMBOL(blk_queue_io_opt);
459 /**
460  * blk_queue_stack_limits - inherit underlying queue limits for stacked drivers
461  * @t:  the stacking driver (top)
462  * @b:  the underlying device (bottom)
463  **/
464 void blk_queue_stack_limits(struct request_queue *t, struct request_queue *b)
466         blk_stack_limits(&t->limits, &b->limits, 0);
468 EXPORT_SYMBOL(blk_queue_stack_limits);
470 /**
471  * blk_stack_limits - adjust queue_limits for stacked devices
472  * @t:  the stacking driver limits (top device)
473  * @b:  the underlying queue limits (bottom, component device)
474  * @start:  first data sector within component device
475  *
476  * Description:
477  *    This function is used by stacking drivers like MD and DM to ensure
478  *    that all component devices have compatible block sizes and
479  *    alignments.  The stacking driver must provide a queue_limits
480  *    struct (top) and then iteratively call the stacking function for
481  *    all component (bottom) devices.  The stacking function will
482  *    attempt to combine the values and ensure proper alignment.
483  *
484  *    Returns 0 if the top and bottom queue_limits are compatible.  The
485  *    top device's block sizes and alignment offsets may be adjusted to
486  *    ensure alignment with the bottom device. If no compatible sizes
487  *    and alignments exist, -1 is returned and the resulting top
488  *    queue_limits will have the misaligned flag set to indicate that
489  *    the alignment_offset is undefined.
490  */
491 int blk_stack_limits(struct queue_limits *t, struct queue_limits *b,
492                      sector_t start)
494         unsigned int top, bottom, alignment, ret = 0;
496         t->max_sectors = min_not_zero(t->max_sectors, b->max_sectors);
497         t->max_hw_sectors = min_not_zero(t->max_hw_sectors, b->max_hw_sectors);
498         t->bounce_pfn = min_not_zero(t->bounce_pfn, b->bounce_pfn);
500         t->seg_boundary_mask = min_not_zero(t->seg_boundary_mask,
501                                             b->seg_boundary_mask);
503         t->max_segments = min_not_zero(t->max_segments, b->max_segments);
504         t->max_integrity_segments = min_not_zero(t->max_integrity_segments,
505                                                  b->max_integrity_segments);
507         t->max_segment_size = min_not_zero(t->max_segment_size,
508                                            b->max_segment_size);
510         t->misaligned |= b->misaligned;
512         alignment = queue_limit_alignment_offset(b, start);
514         /* Bottom device has different alignment.  Check that it is
515          * compatible with the current top alignment.
516          */
517         if (t->alignment_offset != alignment) {
519                 top = max(t->physical_block_size, t->io_min)
520                         + t->alignment_offset;
521                 bottom = max(b->physical_block_size, b->io_min) + alignment;
523                 /* Verify that top and bottom intervals line up */
524                 if (max(top, bottom) & (min(top, bottom) - 1)) {
525                         t->misaligned = 1;
526                         ret = -1;
527                 }
528         }
530         t->logical_block_size = max(t->logical_block_size,
531                                     b->logical_block_size);
533         t->physical_block_size = max(t->physical_block_size,
534                                      b->physical_block_size);
536         t->io_min = max(t->io_min, b->io_min);
537         t->io_opt = lcm(t->io_opt, b->io_opt);
539         t->cluster &= b->cluster;
540         t->discard_zeroes_data &= b->discard_zeroes_data;
542         /* Physical block size a multiple of the logical block size? */
543         if (t->physical_block_size & (t->logical_block_size - 1)) {
544                 t->physical_block_size = t->logical_block_size;
545                 t->misaligned = 1;
546                 ret = -1;
547         }
549         /* Minimum I/O a multiple of the physical block size? */
550         if (t->io_min & (t->physical_block_size - 1)) {
551                 t->io_min = t->physical_block_size;
552                 t->misaligned = 1;
553                 ret = -1;
554         }
556         /* Optimal I/O a multiple of the physical block size? */
557         if (t->io_opt & (t->physical_block_size - 1)) {
558                 t->io_opt = 0;
559                 t->misaligned = 1;
560                 ret = -1;
561         }
563         /* Find lowest common alignment_offset */
564         t->alignment_offset = lcm(t->alignment_offset, alignment)
565                 & (max(t->physical_block_size, t->io_min) - 1);
567         /* Verify that new alignment_offset is on a logical block boundary */
568         if (t->alignment_offset & (t->logical_block_size - 1)) {
569                 t->misaligned = 1;
570                 ret = -1;
571         }
573         /* Discard alignment and granularity */
574         if (b->discard_granularity) {
575                 alignment = queue_limit_discard_alignment(b, start);
577                 if (t->discard_granularity != 0 &&
578                     t->discard_alignment != alignment) {
579                         top = t->discard_granularity + t->discard_alignment;
580                         bottom = b->discard_granularity + alignment;
582                         /* Verify that top and bottom intervals line up */
583                         if (max(top, bottom) & (min(top, bottom) - 1))
584                                 t->discard_misaligned = 1;
585                 }
587                 t->max_discard_sectors = min_not_zero(t->max_discard_sectors,
588                                                       b->max_discard_sectors);
589                 t->discard_granularity = max(t->discard_granularity,
590                                              b->discard_granularity);
591                 t->discard_alignment = lcm(t->discard_alignment, alignment) &
592                         (t->discard_granularity - 1);
593         }
595         return ret;
597 EXPORT_SYMBOL(blk_stack_limits);
599 /**
600  * bdev_stack_limits - adjust queue limits for stacked drivers
601  * @t:  the stacking driver limits (top device)
602  * @bdev:  the component block_device (bottom)
603  * @start:  first data sector within component device
604  *
605  * Description:
606  *    Merges queue limits for a top device and a block_device.  Returns
607  *    0 if alignment didn't change.  Returns -1 if adding the bottom
608  *    device caused misalignment.
609  */
610 int bdev_stack_limits(struct queue_limits *t, struct block_device *bdev,
611                       sector_t start)
613         struct request_queue *bq = bdev_get_queue(bdev);
615         start += get_start_sect(bdev);
617         return blk_stack_limits(t, &bq->limits, start);
619 EXPORT_SYMBOL(bdev_stack_limits);
621 /**
622  * disk_stack_limits - adjust queue limits for stacked drivers
623  * @disk:  MD/DM gendisk (top)
624  * @bdev:  the underlying block device (bottom)
625  * @offset:  offset to beginning of data within component device
626  *
627  * Description:
628  *    Merges the limits for a top level gendisk and a bottom level
629  *    block_device.
630  */
631 void disk_stack_limits(struct gendisk *disk, struct block_device *bdev,
632                        sector_t offset)
634         struct request_queue *t = disk->queue;
636         if (bdev_stack_limits(&t->limits, bdev, offset >> 9) < 0) {
637                 char top[BDEVNAME_SIZE], bottom[BDEVNAME_SIZE];
639                 disk_name(disk, 0, top);
640                 bdevname(bdev, bottom);
642                 printk(KERN_NOTICE "%s: Warning: Device %s is misaligned\n",
643                        top, bottom);
644         }
646 EXPORT_SYMBOL(disk_stack_limits);
648 /**
649  * blk_queue_dma_pad - set pad mask
650  * @q:     the request queue for the device
651  * @mask:  pad mask
652  *
653  * Set dma pad mask.
654  *
655  * Appending pad buffer to a request modifies the last entry of a
656  * scatter list such that it includes the pad buffer.
657  **/
658 void blk_queue_dma_pad(struct request_queue *q, unsigned int mask)
660         q->dma_pad_mask = mask;
662 EXPORT_SYMBOL(blk_queue_dma_pad);
664 /**
665  * blk_queue_update_dma_pad - update pad mask
666  * @q:     the request queue for the device
667  * @mask:  pad mask
668  *
669  * Update dma pad mask.
670  *
671  * Appending pad buffer to a request modifies the last entry of a
672  * scatter list such that it includes the pad buffer.
673  **/
674 void blk_queue_update_dma_pad(struct request_queue *q, unsigned int mask)
676         if (mask > q->dma_pad_mask)
677                 q->dma_pad_mask = mask;
679 EXPORT_SYMBOL(blk_queue_update_dma_pad);
681 /**
682  * blk_queue_dma_drain - Set up a drain buffer for excess dma.
683  * @q:  the request queue for the device
684  * @dma_drain_needed: fn which returns non-zero if drain is necessary
685  * @buf:        physically contiguous buffer
686  * @size:       size of the buffer in bytes
687  *
688  * Some devices have excess DMA problems and can't simply discard (or
689  * zero fill) the unwanted piece of the transfer.  They have to have a
690  * real area of memory to transfer it into.  The use case for this is
691  * ATAPI devices in DMA mode.  If the packet command causes a transfer
692  * bigger than the transfer size some HBAs will lock up if there
693  * aren't DMA elements to contain the excess transfer.  What this API
694  * does is adjust the queue so that the buf is always appended
695  * silently to the scatterlist.
696  *
697  * Note: This routine adjusts max_hw_segments to make room for appending
698  * the drain buffer.  If you call blk_queue_max_segments() after calling
699  * this routine, you must set the limit to one fewer than your device
700  * can support otherwise there won't be room for the drain buffer.
701  */
702 int blk_queue_dma_drain(struct request_queue *q,
703                                dma_drain_needed_fn *dma_drain_needed,
704                                void *buf, unsigned int size)
706         if (queue_max_segments(q) < 2)
707                 return -EINVAL;
708         /* make room for appending the drain */
709         blk_queue_max_segments(q, queue_max_segments(q) - 1);
710         q->dma_drain_needed = dma_drain_needed;
711         q->dma_drain_buffer = buf;
712         q->dma_drain_size = size;
714         return 0;
716 EXPORT_SYMBOL_GPL(blk_queue_dma_drain);
718 /**
719  * blk_queue_segment_boundary - set boundary rules for segment merging
720  * @q:  the request queue for the device
721  * @mask:  the memory boundary mask
722  **/
723 void blk_queue_segment_boundary(struct request_queue *q, unsigned long mask)
725         if (mask < PAGE_CACHE_SIZE - 1) {
726                 mask = PAGE_CACHE_SIZE - 1;
727                 printk(KERN_INFO "%s: set to minimum %lx\n",
728                        __func__, mask);
729         }
731         q->limits.seg_boundary_mask = mask;
733 EXPORT_SYMBOL(blk_queue_segment_boundary);
735 /**
736  * blk_queue_dma_alignment - set dma length and memory alignment
737  * @q:     the request queue for the device
738  * @mask:  alignment mask
739  *
740  * description:
741  *    set required memory and length alignment for direct dma transactions.
742  *    this is used when building direct io requests for the queue.
743  *
744  **/
745 void blk_queue_dma_alignment(struct request_queue *q, int mask)
747         q->dma_alignment = mask;
749 EXPORT_SYMBOL(blk_queue_dma_alignment);
751 /**
752  * blk_queue_update_dma_alignment - update dma length and memory alignment
753  * @q:     the request queue for the device
754  * @mask:  alignment mask
755  *
756  * description:
757  *    update required memory and length alignment for direct dma transactions.
758  *    If the requested alignment is larger than the current alignment, then
759  *    the current queue alignment is updated to the new value, otherwise it
760  *    is left alone.  The design of this is to allow multiple objects
761  *    (driver, device, transport etc) to set their respective
762  *    alignments without having them interfere.
763  *
764  **/
765 void blk_queue_update_dma_alignment(struct request_queue *q, int mask)
767         BUG_ON(mask > PAGE_SIZE);
769         if (mask > q->dma_alignment)
770                 q->dma_alignment = mask;
772 EXPORT_SYMBOL(blk_queue_update_dma_alignment);
774 /**
775  * blk_queue_flush - configure queue's cache flush capability
776  * @q:          the request queue for the device
777  * @flush:      0, REQ_FLUSH or REQ_FLUSH | REQ_FUA
778  *
779  * Tell block layer cache flush capability of @q.  If it supports
780  * flushing, REQ_FLUSH should be set.  If it supports bypassing
781  * write cache for individual writes, REQ_FUA should be set.
782  */
783 void blk_queue_flush(struct request_queue *q, unsigned int flush)
785         WARN_ON_ONCE(flush & ~(REQ_FLUSH | REQ_FUA));
787         if (WARN_ON_ONCE(!(flush & REQ_FLUSH) && (flush & REQ_FUA)))
788                 flush &= ~REQ_FUA;
790         q->flush_flags = flush & (REQ_FLUSH | REQ_FUA);
792 EXPORT_SYMBOL_GPL(blk_queue_flush);
794 void blk_queue_flush_queueable(struct request_queue *q, bool queueable)
796         q->flush_not_queueable = !queueable;
798 EXPORT_SYMBOL_GPL(blk_queue_flush_queueable);
800 static int __init blk_settings_init(void)
802         blk_max_low_pfn = max_low_pfn - 1;
803         blk_max_pfn = max_pfn - 1;
804         return 0;
806 subsys_initcall(blk_settings_init);