1 #
2 # TI device configuration
3 #
5 config NET_VENDOR_TI
6 bool "Texas Instruments (TI) devices"
7 default y
8 depends on PCI || EISA || AR7 || (ARM && (ARCH_DAVINCI || ARCH_OMAP3))
9 ---help---
10 If you have a network (Ethernet) card belonging to this class, say Y
11 and read the Ethernet-HOWTO, available from
12 <http://www.tldp.org/docs.html#howto>.
14 Note that the answer to this question doesn't directly affect the
15 kernel: saying N will just cause the configurator to skip all
16 the questions about TI devices. If you say Y, you will be asked for
17 your specific card in the following questions.
19 if NET_VENDOR_TI
21 config TI_DAVINCI_EMAC
22 tristate "TI DaVinci EMAC Support"
23 depends on ARM && ( ARCH_DAVINCI || ARCH_OMAP3 )
24 select TI_DAVINCI_MDIO
25 select TI_DAVINCI_CPDMA
26 select PHYLIB
27 ---help---
28 This driver supports TI's DaVinci Ethernet .
30 To compile this driver as a module, choose M here: the module
31 will be called davinci_emac_driver. This is recommended.
33 config TI_DAVINCI_MDIO
34 tristate "TI DaVinci MDIO Support"
35 depends on ARM && ( ARCH_DAVINCI || ARCH_OMAP3 )
36 select PHYLIB
37 ---help---
38 This driver supports TI's DaVinci MDIO module.
40 To compile this driver as a module, choose M here: the module
41 will be called davinci_mdio. This is recommended.
43 config TI_DAVINCI_CPDMA
44 tristate "TI DaVinci CPDMA Support"
45 depends on ARM && ( ARCH_DAVINCI || ARCH_OMAP3 )
46 ---help---
47 This driver supports TI's DaVinci CPDMA dma engine.
49 To compile this driver as a module, choose M here: the module
50 will be called davinci_cpdma. This is recommended.
52 config TI_CPSW
53 tristate "TI CPSW Switch Support"
54 depends on ARM && (ARCH_DAVINCI || SOC_OMAPAM33XX)
55 select TI_DAVINCI_CPDMA
56 select TI_DAVINCI_MDIO
57 ---help---
58 This driver supports TI's CPSW Ethernet Switch.
60 To compile this driver as a module, choose M here: the module
61 will be called cpsw.
63 config TI_CPSW_DUAL_EMAC
64 bool "TI CPSW Switch as Dual EMAC"
65 depends on TI_CPSW
66 help
67 This driver makes TI's CPSW Ethernet Switch as Dual EMAC. Switch
68 features will not be available in this mode, Dual Emac default
69 VLAN ids should not be used in VLAN configuration
71 config TLAN
72 tristate "TI ThunderLAN support"
73 depends on (PCI || EISA)
74 ---help---
75 If you have a PCI Ethernet network card based on the ThunderLAN chip
76 which is supported by this driver, say Y and read the
77 Ethernet-HOWTO, available from
78 <http://www.tldp.org/docs.html#howto>.
80 Devices currently supported by this driver are Compaq Netelligent,
81 Compaq NetFlex and Olicom cards. Please read the file
82 <file:Documentation/networking/tlan.txt> for more details.
84 To compile this driver as a module, choose M here. The module
85 will be called tlan.
87 Please email feedback to <torben.mathiasen@compaq.com>.
89 config CPMAC
90 tristate "TI AR7 CPMAC Ethernet support (EXPERIMENTAL)"
91 depends on EXPERIMENTAL && AR7
92 select PHYLIB
93 ---help---
94 TI AR7 CPMAC Ethernet support
96 endif # NET_VENDOR_TI