1 #
2 # RTC class/drivers configuration
3 #
5 config RTC_LIB
6 bool
8 menuconfig RTC_CLASS
9 bool "Real Time Clock"
10 default n
11 depends on !S390 && !UML
12 select RTC_LIB
13 help
14 Generic RTC class support. If you say yes here, you will
15 be allowed to plug one or more RTCs to your system. You will
16 probably want to enable one or more of the interfaces below.
18 if RTC_CLASS
20 config RTC_HCTOSYS
21 bool "Set system time from RTC on startup and resume"
22 depends on RTC_CLASS = y
23 default y
24 help
25 If you say yes here, the system time (wall clock) will be set using
26 the value read from a specified RTC device. This is useful to avoid
27 unnecessary fsck runs at boot time, and to network better.
29 config RTC_HCTOSYS_DEVICE
30 string "RTC used to set the system time"
31 depends on RTC_HCTOSYS = y
32 default "rtc0"
33 help
34 The RTC device that will be used to (re)initialize the system
35 clock, usually rtc0. Initialization is done when the system
36 starts up, and when it resumes from a low power state. This
37 device should record time in UTC, since the kernel won't do
38 timezone correction.
40 The driver for this RTC device must be loaded before late_initcall
41 functions run, so it must usually be statically linked.
43 This clock should be battery-backed, so that it reads the correct
44 time when the system boots from a power-off state. Otherwise, your
45 system will need an external clock source (like an NTP server).
47 If the clock you specify here is not battery backed, it may still
48 be useful to reinitialize system time when resuming from system
49 sleep states. Do not specify an RTC here unless it stays powered
50 during all this system's supported sleep states.
52 config RTC_DEBUG
53 bool "RTC debug support"
54 depends on RTC_CLASS = y
55 help
56 Say yes here to enable debugging support in the RTC framework
57 and individual RTC drivers.
59 comment "RTC interfaces"
61 config RTC_INTF_SYSFS
62 boolean "/sys/class/rtc/rtcN (sysfs)"
63 depends on SYSFS
64 default RTC_CLASS
65 help
66 Say yes here if you want to use your RTCs using sysfs interfaces,
67 /sys/class/rtc/rtc0 through /sys/.../rtcN.
69 If unsure, say Y.
71 config RTC_INTF_PROC
72 boolean "/proc/driver/rtc (procfs for rtc0)"
73 depends on PROC_FS
74 default RTC_CLASS
75 help
76 Say yes here if you want to use your first RTC through the proc
77 interface, /proc/driver/rtc. Other RTCs will not be available
78 through that API.
80 If unsure, say Y.
82 config RTC_INTF_DEV
83 boolean "/dev/rtcN (character devices)"
84 default RTC_CLASS
85 help
86 Say yes here if you want to use your RTCs using the /dev
87 interfaces, which "udev" sets up as /dev/rtc0 through
88 /dev/rtcN.
90 You may want to set up a symbolic link so one of these
91 can be accessed as /dev/rtc, which is a name
92 expected by "hwclock" and some other programs. Recent
93 versions of "udev" are known to set up the symlink for you.
95 If unsure, say Y.
97 config RTC_INTF_DEV_UIE_EMUL
98 bool "RTC UIE emulation on dev interface"
99 depends on RTC_INTF_DEV
100 help
101 Provides an emulation for RTC_UIE if the underlying rtc chip
102 driver does not expose RTC_UIE ioctls. Those requests generate
103 once-per-second update interrupts, used for synchronization.
105 The emulation code will read the time from the hardware
106 clock several times per second, please enable this option
107 only if you know that you really need it.
109 config RTC_DRV_TEST
110 tristate "Test driver/device"
111 help
112 If you say yes here you get support for the
113 RTC test driver. It's a software RTC which can be
114 used to test the RTC subsystem APIs. It gets
115 the time from the system clock.
116 You want this driver only if you are doing development
117 on the RTC subsystem. Please read the source code
118 for further details.
120 This driver can also be built as a module. If so, the module
121 will be called rtc-test.
123 comment "I2C RTC drivers"
124 depends on I2C
126 if I2C
128 config RTC_DRV_88PM860X
129 tristate "Marvell 88PM860x"
130 depends on RTC_CLASS && I2C && MFD_88PM860X
131 help
132 If you say yes here you get support for RTC function in Marvell
133 88PM860x chips.
135 This driver can also be built as a module. If so, the module
136 will be called rtc-88pm860x.
138 config RTC_DRV_DS1307
139 tristate "Dallas/Maxim DS1307/37/38/39/40, ST M41T00, EPSON RX-8025"
140 help
141 If you say yes here you get support for various compatible RTC
142 chips (often with battery backup) connected with I2C. This driver
143 should handle DS1307, DS1337, DS1338, DS1339, DS1340, ST M41T00,
144 EPSON RX-8025 and probably other chips. In some cases the RTC
145 must already have been initialized (by manufacturing or a
146 bootloader).
148 The first seven registers on these chips hold an RTC, and other
149 registers may add features such as NVRAM, a trickle charger for
150 the RTC/NVRAM backup power, and alarms. NVRAM is visible in
151 sysfs, but other chip features may not be available.
153 This driver can also be built as a module. If so, the module
154 will be called rtc-ds1307.
156 config RTC_DRV_DS1374
157 tristate "Dallas/Maxim DS1374"
158 depends on RTC_CLASS && I2C
159 help
160 If you say yes here you get support for Dallas Semiconductor
161 DS1374 real-time clock chips. If an interrupt is associated
162 with the device, the alarm functionality is supported.
164 This driver can also be built as a module. If so, the module
165 will be called rtc-ds1374.
167 config RTC_DRV_DS1672
168 tristate "Dallas/Maxim DS1672"
169 help
170 If you say yes here you get support for the
171 Dallas/Maxim DS1672 timekeeping chip.
173 This driver can also be built as a module. If so, the module
174 will be called rtc-ds1672.
176 config RTC_DRV_DS3232
177 tristate "Dallas/Maxim DS3232"
178 depends on RTC_CLASS && I2C
179 help
180 If you say yes here you get support for Dallas Semiconductor
181 DS3232 real-time clock chips. If an interrupt is associated
182 with the device, the alarm functionality is supported.
184 This driver can also be built as a module. If so, the module
185 will be called rtc-ds3232.
187 config RTC_DRV_MAX6900
188 tristate "Maxim MAX6900"
189 help
190 If you say yes here you will get support for the
191 Maxim MAX6900 I2C RTC chip.
193 This driver can also be built as a module. If so, the module
194 will be called rtc-max6900.
196 config RTC_DRV_MAX8925
197 tristate "Maxim MAX8925"
198 depends on MFD_MAX8925
199 help
200 If you say yes here you will get support for the
201 RTC of Maxim MAX8925 PMIC.
203 This driver can also be built as a module. If so, the module
204 will be called rtc-max8925.
206 config RTC_DRV_MAX8998
207 tristate "Maxim MAX8998"
208 depends on MFD_MAX8998
209 help
210 If you say yes here you will get support for the
211 RTC of Maxim MAX8998 PMIC.
213 This driver can also be built as a module. If so, the module
214 will be called rtc-max8998.
216 config RTC_DRV_RS5C372
217 tristate "Ricoh R2025S/D, RS5C372A/B, RV5C386, RV5C387A"
218 help
219 If you say yes here you get support for the
220 Ricoh R2025S/D, RS5C372A, RS5C372B, RV5C386, and RV5C387A RTC chips.
222 This driver can also be built as a module. If so, the module
223 will be called rtc-rs5c372.
225 config RTC_DRV_ISL1208
226 tristate "Intersil ISL1208"
227 help
228 If you say yes here you get support for the
229 Intersil ISL1208 RTC chip.
231 This driver can also be built as a module. If so, the module
232 will be called rtc-isl1208.
234 config RTC_DRV_ISL12022
235 tristate "Intersil ISL12022"
236 help
237 If you say yes here you get support for the
238 Intersil ISL12022 RTC chip.
240 This driver can also be built as a module. If so, the module
241 will be called rtc-isl12022.
243 config RTC_DRV_X1205
244 tristate "Xicor/Intersil X1205"
245 help
246 If you say yes here you get support for the
247 Xicor/Intersil X1205 RTC chip.
249 This driver can also be built as a module. If so, the module
250 will be called rtc-x1205.
252 config RTC_DRV_PCF8563
253 tristate "Philips PCF8563/Epson RTC8564"
254 help
255 If you say yes here you get support for the
256 Philips PCF8563 RTC chip. The Epson RTC8564
257 should work as well.
259 This driver can also be built as a module. If so, the module
260 will be called rtc-pcf8563.
262 config RTC_DRV_PCF8583
263 tristate "Philips PCF8583"
264 help
265 If you say yes here you get support for the Philips PCF8583
266 RTC chip found on Acorn RiscPCs. This driver supports the
267 platform specific method of retrieving the current year from
268 the RTC's SRAM. It will work on other platforms with the same
269 chip, but the year will probably have to be tweaked.
271 This driver can also be built as a module. If so, the module
272 will be called rtc-pcf8583.
274 config RTC_DRV_M41T80
275 tristate "ST M41T62/65/M41T80/81/82/83/84/85/87"
276 help
277 If you say Y here you will get support for the ST M41T60
278 and M41T80 RTC chips series. Currently, the following chips are
279 supported: M41T62, M41T65, M41T80, M41T81, M41T82, M41T83, M41ST84,
280 M41ST85, and M41ST87.
282 This driver can also be built as a module. If so, the module
283 will be called rtc-m41t80.
285 config RTC_DRV_M41T80_WDT
286 bool "ST M41T65/M41T80 series RTC watchdog timer"
287 depends on RTC_DRV_M41T80
288 help
289 If you say Y here you will get support for the
290 watchdog timer in the ST M41T60 and M41T80 RTC chips series.
292 config RTC_DRV_BQ32K
293 tristate "TI BQ32000"
294 help
295 If you say Y here you will get support for the TI
296 BQ32000 I2C RTC chip.
298 This driver can also be built as a module. If so, the module
299 will be called rtc-bq32k.
301 config RTC_DRV_DM355EVM
302 tristate "TI DaVinci DM355 EVM RTC"
303 depends on MFD_DM355EVM_MSP
304 help
305 Supports the RTC firmware in the MSP430 on the DM355 EVM.
307 config RTC_DRV_TWL92330
308 boolean "TI TWL92330/Menelaus"
309 depends on MENELAUS
310 help
311 If you say yes here you get support for the RTC on the
312 TWL92330 "Menelaus" power management chip, used with OMAP2
313 platforms. The support is integrated with the rest of
314 the Menelaus driver; it's not separate module.
316 config RTC_DRV_TWL4030
317 tristate "TI TWL4030/TWL5030/TWL6030/TPS659x0"
318 depends on RTC_CLASS && TWL4030_CORE
319 help
320 If you say yes here you get support for the RTC on the
321 TWL4030/TWL5030/TWL6030 family chips, used mostly with OMAP3 platforms.
323 This driver can also be built as a module. If so, the module
324 will be called rtc-twl.
326 config RTC_DRV_S35390A
327 tristate "Seiko Instruments S-35390A"
328 select BITREVERSE
329 help
330 If you say yes here you will get support for the Seiko
331 Instruments S-35390A.
333 This driver can also be built as a module. If so the module
334 will be called rtc-s35390a.
336 config RTC_DRV_FM3130
337 tristate "Ramtron FM3130"
338 help
339 If you say Y here you will get support for the
340 Ramtron FM3130 RTC chips.
341 Ramtron FM3130 is a chip with two separate devices inside,
342 RTC clock and FRAM. This driver provides only RTC functionality.
344 This driver can also be built as a module. If so the module
345 will be called rtc-fm3130.
347 config RTC_DRV_RX8581
348 tristate "Epson RX-8581"
349 help
350 If you say yes here you will get support for the Epson RX-8581.
352 This driver can also be built as a module. If so the module
353 will be called rtc-rx8581.
355 config RTC_DRV_RX8025
356 tristate "Epson RX-8025SA/NB"
357 help
358 If you say yes here you get support for the Epson
359 RX-8025SA/NB RTC chips.
361 This driver can also be built as a module. If so, the module
362 will be called rtc-rx8025.
364 config RTC_DRV_EM3027
365 tristate "EM Microelectronic EM3027"
366 help
367 If you say yes here you get support for the EM
368 Microelectronic EM3027 RTC chips.
370 This driver can also be built as a module. If so, the module
371 will be called rtc-em3027.
373 config RTC_DRV_RV3029C2
374 tristate "Micro Crystal RTC"
375 help
376 If you say yes here you get support for the Micro Crystal
377 RV3029-C2 RTC chips.
379 This driver can also be built as a module. If so, the module
380 will be called rtc-rv3029c2.
382 endif # I2C
384 comment "SPI RTC drivers"
386 if SPI_MASTER
388 config RTC_DRV_M41T93
389 tristate "ST M41T93"
390 help
391 If you say yes here you will get support for the
392 ST M41T93 SPI RTC chip.
394 This driver can also be built as a module. If so, the module
395 will be called rtc-m41t93.
397 config RTC_DRV_M41T94
398 tristate "ST M41T94"
399 help
400 If you say yes here you will get support for the
401 ST M41T94 SPI RTC chip.
403 This driver can also be built as a module. If so, the module
404 will be called rtc-m41t94.
406 config RTC_DRV_DS1305
407 tristate "Dallas/Maxim DS1305/DS1306"
408 help
409 Select this driver to get support for the Dallas/Maxim DS1305
410 and DS1306 real time clock chips. These support a trickle
411 charger, alarms, and NVRAM in addition to the clock.
413 This driver can also be built as a module. If so, the module
414 will be called rtc-ds1305.
416 config RTC_DRV_DS1390
417 tristate "Dallas/Maxim DS1390/93/94"
418 help
419 If you say yes here you get support for the
420 Dallas/Maxim DS1390/93/94 chips.
422 This driver only supports the RTC feature, and not other chip
423 features such as alarms and trickle charging.
425 This driver can also be built as a module. If so, the module
426 will be called rtc-ds1390.
428 config RTC_DRV_MAX6902
429 tristate "Maxim MAX6902"
430 help
431 If you say yes here you will get support for the
432 Maxim MAX6902 SPI RTC chip.
434 This driver can also be built as a module. If so, the module
435 will be called rtc-max6902.
437 config RTC_DRV_R9701
438 tristate "Epson RTC-9701JE"
439 help
440 If you say yes here you will get support for the
441 Epson RTC-9701JE SPI RTC chip.
443 This driver can also be built as a module. If so, the module
444 will be called rtc-r9701.
446 config RTC_DRV_RS5C348
447 tristate "Ricoh RS5C348A/B"
448 help
449 If you say yes here you get support for the
450 Ricoh RS5C348A and RS5C348B RTC chips.
452 This driver can also be built as a module. If so, the module
453 will be called rtc-rs5c348.
455 config RTC_DRV_DS3234
456 tristate "Maxim/Dallas DS3234"
457 help
458 If you say yes here you get support for the
459 Maxim/Dallas DS3234 SPI RTC chip.
461 This driver can also be built as a module. If so, the module
462 will be called rtc-ds3234.
464 config RTC_DRV_PCF2123
465 tristate "NXP PCF2123"
466 help
467 If you say yes here you get support for the NXP PCF2123
468 RTC chip.
470 This driver can also be built as a module. If so, the module
471 will be called rtc-pcf2123.
473 endif # SPI_MASTER
475 comment "Platform RTC drivers"
477 # this 'CMOS' RTC driver is arch dependent because <asm-generic/rtc.h>
478 # requires <asm/mc146818rtc.h> defining CMOS_READ/CMOS_WRITE, and a
479 # global rtc_lock ... it's not yet just another platform_device.
481 config RTC_DRV_CMOS
482 tristate "PC-style 'CMOS'"
483 depends on X86 || ALPHA || ARM || M32R || ATARI || PPC || MIPS || SPARC64
484 default y if X86
485 help
486 Say "yes" here to get direct support for the real time clock
487 found in every PC or ACPI-based system, and some other boards.
488 Specifically the original MC146818, compatibles like those in
489 PC south bridges, the DS12887 or M48T86, some multifunction
490 or LPC bus chips, and so on.
492 Your system will need to define the platform device used by
493 this driver, otherwise it won't be accessible. This means
494 you can safely enable this driver if you don't know whether
495 or not your board has this kind of hardware.
497 This driver can also be built as a module. If so, the module
498 will be called rtc-cmos.
500 config RTC_DRV_VRTC
501 tristate "Virtual RTC for Moorestown platforms"
502 depends on X86_MRST
503 default y if X86_MRST
505 help
506 Say "yes" here to get direct support for the real time clock
507 found on Moorestown platforms. The VRTC is a emulated RTC that
508 derives its clock source from a real RTC in the PMIC. The MC146818
509 style programming interface is mostly conserved, but any
510 updates are done via IPC calls to the system controller FW.
512 config RTC_DRV_DS1216
513 tristate "Dallas DS1216"
514 depends on SNI_RM
515 help
516 If you say yes here you get support for the Dallas DS1216 RTC chips.
518 config RTC_DRV_DS1286
519 tristate "Dallas DS1286"
520 help
521 If you say yes here you get support for the Dallas DS1286 RTC chips.
523 config RTC_DRV_DS1302
524 tristate "Dallas DS1302"
525 depends on SH_SECUREEDGE5410
526 help
527 If you say yes here you get support for the Dallas DS1302 RTC chips.
529 config RTC_DRV_DS1511
530 tristate "Dallas DS1511"
531 depends on RTC_CLASS
532 help
533 If you say yes here you get support for the
534 Dallas DS1511 timekeeping/watchdog chip.
536 This driver can also be built as a module. If so, the module
537 will be called rtc-ds1511.
539 config RTC_DRV_DS1553
540 tristate "Maxim/Dallas DS1553"
541 help
542 If you say yes here you get support for the
543 Maxim/Dallas DS1553 timekeeping chip.
545 This driver can also be built as a module. If so, the module
546 will be called rtc-ds1553.
548 config RTC_DRV_DS1742
549 tristate "Maxim/Dallas DS1742/1743"
550 help
551 If you say yes here you get support for the
552 Maxim/Dallas DS1742/1743 timekeeping chip.
554 This driver can also be built as a module. If so, the module
555 will be called rtc-ds1742.
557 config RTC_DRV_EFI
558 tristate "EFI RTC"
559 depends on IA64
560 help
561 If you say yes here you will get support for the EFI
562 Real Time Clock.
564 This driver can also be built as a module. If so, the module
565 will be called rtc-efi.
567 config RTC_DRV_STK17TA8
568 tristate "Simtek STK17TA8"
569 depends on RTC_CLASS
570 help
571 If you say yes here you get support for the
572 Simtek STK17TA8 timekeeping chip.
574 This driver can also be built as a module. If so, the module
575 will be called rtc-stk17ta8.
577 config RTC_DRV_M48T86
578 tristate "ST M48T86/Dallas DS12887"
579 help
580 If you say Y here you will get support for the
581 ST M48T86 and Dallas DS12887 RTC chips.
583 This driver can also be built as a module. If so, the module
584 will be called rtc-m48t86.
586 config RTC_DRV_M48T35
587 tristate "ST M48T35"
588 help
589 If you say Y here you will get support for the
590 ST M48T35 RTC chip.
592 This driver can also be built as a module, if so, the module
593 will be called "rtc-m48t35".
595 config RTC_DRV_M48T59
596 tristate "ST M48T59/M48T08/M48T02"
597 help
598 If you say Y here you will get support for the
599 ST M48T59 RTC chip and compatible ST M48T08 and M48T02.
601 These chips are usually found in Sun SPARC and UltraSPARC
602 workstations.
604 This driver can also be built as a module, if so, the module
605 will be called "rtc-m48t59".
607 config RTC_DRV_MSM6242
608 tristate "Oki MSM6242"
609 help
610 If you say yes here you get support for the Oki MSM6242
611 timekeeping chip. It is used in some Amiga models (e.g. A2000).
613 This driver can also be built as a module. If so, the module
614 will be called rtc-msm6242.
616 config RTC_DRV_IMXDI
617 tristate "Freescale IMX DryIce Real Time Clock"
618 depends on ARCH_MX25
619 depends on RTC_CLASS
620 help
621 Support for Freescale IMX DryIce RTC
623 This driver can also be built as a module, if so, the module
624 will be called "rtc-imxdi".
626 config RTC_MXC
627 tristate "Freescale MXC Real Time Clock"
628 depends on ARCH_MXC
629 depends on RTC_CLASS
630 help
631 If you say yes here you get support for the Freescale MXC
632 RTC module.
634 This driver can also be built as a module, if so, the module
635 will be called "rtc-mxc".
637 config RTC_DRV_BQ4802
638 tristate "TI BQ4802"
639 help
640 If you say Y here you will get support for the TI
641 BQ4802 RTC chip.
643 This driver can also be built as a module. If so, the module
644 will be called rtc-bq4802.
646 config RTC_DRV_RP5C01
647 tristate "Ricoh RP5C01"
648 help
649 If you say yes here you get support for the Ricoh RP5C01
650 timekeeping chip. It is used in some Amiga models (e.g. A3000
651 and A4000).
653 This driver can also be built as a module. If so, the module
654 will be called rtc-rp5c01.
656 config RTC_DRV_V3020
657 tristate "EM Microelectronic V3020"
658 help
659 If you say yes here you will get support for the
660 EM Microelectronic v3020 RTC chip.
662 This driver can also be built as a module. If so, the module
663 will be called rtc-v3020.
665 config RTC_DRV_WM831X
666 tristate "Wolfson Microelectronics WM831x RTC"
667 depends on MFD_WM831X
668 help
669 If you say yes here you will get support for the RTC subsystem
670 of the Wolfson Microelectronics WM831X series PMICs.
672 This driver can also be built as a module. If so, the module
673 will be called "rtc-wm831x".
675 config RTC_DRV_WM8350
676 tristate "Wolfson Microelectronics WM8350 RTC"
677 depends on MFD_WM8350
678 help
679 If you say yes here you will get support for the RTC subsystem
680 of the Wolfson Microelectronics WM8350.
682 This driver can also be built as a module. If so, the module
683 will be called "rtc-wm8350".
685 config RTC_DRV_SPEAR
686 tristate "SPEAR ST RTC"
687 depends on PLAT_SPEAR
688 default y
689 help
690 If you say Y here you will get support for the RTC found on
691 spear
693 config RTC_DRV_PCF50633
694 depends on MFD_PCF50633
695 tristate "NXP PCF50633 RTC"
696 help
697 If you say yes here you get support for the RTC subsystem of the
698 NXP PCF50633 used in embedded systems.
700 config RTC_DRV_AB3100
701 tristate "ST-Ericsson AB3100 RTC"
702 depends on AB3100_CORE
703 default y if AB3100_CORE
704 help
705 Select this to enable the ST-Ericsson AB3100 Mixed Signal IC RTC
706 support. This chip contains a battery- and capacitor-backed RTC.
708 config RTC_DRV_AB8500
709 tristate "ST-Ericsson AB8500 RTC"
710 depends on AB8500_CORE
711 help
712 Select this to enable the ST-Ericsson AB8500 power management IC RTC
713 support. This chip contains a battery- and capacitor-backed RTC.
715 config RTC_DRV_NUC900
716 tristate "NUC910/NUC920 RTC driver"
717 depends on RTC_CLASS && ARCH_W90X900
718 help
719 If you say yes here you get support for the RTC subsystem of the
720 NUC910/NUC920 used in embedded systems.
722 comment "on-CPU RTC drivers"
724 config RTC_DRV_DAVINCI
725 tristate "TI DaVinci RTC"
726 depends on ARCH_DAVINCI_DM365
727 help
728 If you say yes here you get support for the RTC on the
729 DaVinci platforms (DM365).
731 This driver can also be built as a module. If so, the module
732 will be called rtc-davinci.
734 config RTC_DRV_OMAP
735 tristate "TI OMAP1"
736 depends on ARCH_OMAP15XX || ARCH_OMAP16XX || ARCH_OMAP730 || ARCH_DAVINCI_DA8XX
737 help
738 Say "yes" here to support the real time clock on TI OMAP1 and
739 DA8xx/OMAP-L13x chips. This driver can also be built as a
740 module called rtc-omap.
742 config HAVE_S3C_RTC
743 bool
744 help
745 This will include RTC support for Samsung SoCs. If
746 you want to include RTC support for any machine, kindly
747 select this in the respective mach-XXXX/Kconfig file.
749 config RTC_DRV_S3C
750 tristate "Samsung S3C series SoC RTC"
751 depends on ARCH_S3C2410 || ARCH_S3C64XX || HAVE_S3C_RTC
752 help
753 RTC (Realtime Clock) driver for the clock inbuilt into the
754 Samsung S3C24XX series of SoCs. This can provide periodic
755 interrupt rates from 1Hz to 64Hz for user programs, and
756 wakeup from Alarm.
758 The driver currently supports the common features on all the
759 S3C24XX range, such as the S3C2410, S3C2412, S3C2413, S3C2440
760 and S3C2442.
762 This driver can also be build as a module. If so, the module
763 will be called rtc-s3c.
765 config RTC_DRV_EP93XX
766 tristate "Cirrus Logic EP93XX"
767 depends on ARCH_EP93XX
768 help
769 If you say yes here you get support for the
770 RTC embedded in the Cirrus Logic EP93XX processors.
772 This driver can also be built as a module. If so, the module
773 will be called rtc-ep93xx.
775 config RTC_DRV_SA1100
776 tristate "SA11x0/PXA2xx"
777 depends on ARCH_SA1100 || ARCH_PXA
778 help
779 If you say Y here you will get access to the real time clock
780 built into your SA11x0 or PXA2xx CPU.
782 To compile this driver as a module, choose M here: the
783 module will be called rtc-sa1100.
785 config RTC_DRV_SH
786 tristate "SuperH On-Chip RTC"
787 depends on RTC_CLASS && SUPERH && HAVE_CLK
788 help
789 Say Y here to enable support for the on-chip RTC found in
790 most SuperH processors.
792 To compile this driver as a module, choose M here: the
793 module will be called rtc-sh.
795 config RTC_DRV_VR41XX
796 tristate "NEC VR41XX"
797 depends on CPU_VR41XX
798 help
799 If you say Y here you will get access to the real time clock
800 built into your NEC VR41XX CPU.
802 To compile this driver as a module, choose M here: the
803 module will be called rtc-vr41xx.
805 config RTC_DRV_PL030
806 tristate "ARM AMBA PL030 RTC"
807 depends on ARM_AMBA
808 help
809 If you say Y here you will get access to ARM AMBA
810 PrimeCell PL030 RTC found on certain ARM SOCs.
812 To compile this driver as a module, choose M here: the
813 module will be called rtc-pl030.
815 config RTC_DRV_PL031
816 tristate "ARM AMBA PL031 RTC"
817 depends on ARM_AMBA
818 help
819 If you say Y here you will get access to ARM AMBA
820 PrimeCell PL031 RTC found on certain ARM SOCs.
822 To compile this driver as a module, choose M here: the
823 module will be called rtc-pl031.
825 config RTC_DRV_AT32AP700X
826 tristate "AT32AP700X series RTC"
827 depends on PLATFORM_AT32AP
828 help
829 Driver for the internal RTC (Realtime Clock) on Atmel AVR32
830 AT32AP700x family processors.
832 config RTC_DRV_AT91RM9200
833 tristate "AT91RM9200 or some AT91SAM9 RTC"
834 depends on ARCH_AT91RM9200 || ARCH_AT91SAM9RL || ARCH_AT91SAM9G45
835 help
836 Driver for the internal RTC (Realtime Clock) module found on
837 Atmel AT91RM9200's and some AT91SAM9 chips. On AT91SAM9 chips
838 this is powered by the backup power supply.
840 config RTC_DRV_AT91SAM9
841 tristate "AT91SAM9x/AT91CAP9 RTT as RTC"
842 depends on ARCH_AT91 && !(ARCH_AT91RM9200 || ARCH_AT91X40)
843 help
844 RTC driver for the Atmel AT91SAM9x and AT91CAP9 internal RTT
845 (Real Time Timer). These timers are powered by the backup power
846 supply (such as a small coin cell battery), but do not need to
847 be used as RTCs.
849 (On AT91SAM9rl and AT91SAM9G45 chips you probably want to use the
850 dedicated RTC module and leave the RTT available for other uses.)
852 config RTC_DRV_AT91SAM9_RTT
853 int
854 range 0 1
855 default 0
856 prompt "RTT module Number" if ARCH_AT91SAM9263
857 depends on RTC_DRV_AT91SAM9
858 help
859 More than one RTT module is available. You can choose which
860 one will be used as an RTC. The default of zero is normally
861 OK to use, though some systems use that for non-RTC purposes.
863 config RTC_DRV_AT91SAM9_GPBR
864 int
865 range 0 3 if !ARCH_AT91SAM9263
866 range 0 15 if ARCH_AT91SAM9263
867 default 0
868 prompt "Backup Register Number"
869 depends on RTC_DRV_AT91SAM9
870 help
871 The RTC driver needs to use one of the General Purpose Backup
872 Registers (GPBRs) as well as the RTT. You can choose which one
873 will be used. The default of zero is normally OK to use, but
874 on some systems other software needs to use that register.
876 config RTC_DRV_AU1XXX
877 tristate "Au1xxx Counter0 RTC support"
878 depends on MIPS_ALCHEMY
879 help
880 This is a driver for the Au1xxx on-chip Counter0 (Time-Of-Year
881 counter) to be used as a RTC.
883 This driver can also be built as a module. If so, the module
884 will be called rtc-au1xxx.
886 config RTC_DRV_BFIN
887 tristate "Blackfin On-Chip RTC"
888 depends on BLACKFIN && !BF561
889 help
890 If you say yes here you will get support for the
891 Blackfin On-Chip Real Time Clock.
893 This driver can also be built as a module. If so, the module
894 will be called rtc-bfin.
896 config RTC_DRV_RS5C313
897 tristate "Ricoh RS5C313"
898 depends on SH_LANDISK
899 help
900 If you say yes here you get support for the Ricoh RS5C313 RTC chips.
902 config RTC_DRV_GENERIC
903 tristate "Generic RTC support"
904 # Please consider writing a new RTC driver instead of using the generic
905 # RTC abstraction
906 depends on PARISC || M68K || PPC || SUPERH32
907 help
908 Say Y or M here to enable RTC support on systems using the generic
909 RTC abstraction. If you do not know what you are doing, you should
910 just say Y.
912 config RTC_DRV_PXA
913 tristate "PXA27x/PXA3xx"
914 depends on ARCH_PXA
915 help
916 If you say Y here you will get access to the real time clock
917 built into your PXA27x or PXA3xx CPU.
919 This RTC driver uses PXA RTC registers available since pxa27x
920 series (RDxR, RYxR) instead of legacy RCNR, RTAR.
922 config RTC_DRV_VT8500
923 tristate "VIA/WonderMedia 85xx SoC RTC"
924 depends on ARCH_VT8500
925 help
926 If you say Y here you will get access to the real time clock
927 built into your VIA VT8500 SoC or its relatives.
930 config RTC_DRV_SUN4V
931 bool "SUN4V Hypervisor RTC"
932 depends on SPARC64
933 help
934 If you say Y here you will get support for the Hypervisor
935 based RTC on SUN4V systems.
937 config RTC_DRV_STARFIRE
938 bool "Starfire RTC"
939 depends on SPARC64
940 help
941 If you say Y here you will get support for the RTC found on
942 Starfire systems.
944 config RTC_DRV_TX4939
945 tristate "TX4939 SoC"
946 depends on SOC_TX4939
947 help
948 Driver for the internal RTC (Realtime Clock) module found on
949 Toshiba TX4939 SoC.
951 config RTC_DRV_MV
952 tristate "Marvell SoC RTC"
953 depends on ARCH_KIRKWOOD || ARCH_DOVE
954 help
955 If you say yes here you will get support for the in-chip RTC
956 that can be found in some of Marvell's SoC devices, such as
957 the Kirkwood 88F6281 and 88F6192.
959 This driver can also be built as a module. If so, the module
960 will be called rtc-mv.
962 config RTC_DRV_PS3
963 tristate "PS3 RTC"
964 depends on PPC_PS3
965 help
966 If you say yes here you will get support for the RTC on PS3.
968 This driver can also be built as a module. If so, the module
969 will be called rtc-ps3.
971 config RTC_DRV_COH901331
972 tristate "ST-Ericsson COH 901 331 RTC"
973 depends on ARCH_U300
974 help
975 If you say Y here you will get access to ST-Ericsson
976 COH 901 331 RTC clock found in some ST-Ericsson Mobile
977 Platforms.
979 This driver can also be built as a module. If so, the module
980 will be called "rtc-coh901331".
983 config RTC_DRV_STMP
984 tristate "Freescale STMP3xxx/i.MX23/i.MX28 RTC"
985 depends on ARCH_MXS
986 help
987 If you say yes here you will get support for the onboard
988 STMP3xxx/i.MX23/i.MX28 RTC.
990 This driver can also be built as a module. If so, the module
991 will be called rtc-stmp3xxx.
993 config RTC_DRV_PCAP
994 tristate "PCAP RTC"
995 depends on EZX_PCAP
996 help
997 If you say Y here you will get support for the RTC found on
998 the PCAP2 ASIC used on some Motorola phones.
1000 config RTC_DRV_MC13XXX
1001 depends on MFD_MC13XXX
1002 tristate "Freescale MC13xxx RTC"
1003 help
1004 This enables support for the RTCs found on Freescale's PMICs
1005 MC13783 and MC13892.
1007 config RTC_DRV_MPC5121
1008 tristate "Freescale MPC5121 built-in RTC"
1009 depends on PPC_MPC512x || PPC_MPC52xx
1010 help
1011 If you say yes here you will get support for the
1012 built-in RTC on MPC5121 or on MPC5200.
1014 This driver can also be built as a module. If so, the module
1015 will be called rtc-mpc5121.
1017 config RTC_DRV_JZ4740
1018 tristate "Ingenic JZ4740 SoC"
1019 depends on RTC_CLASS
1020 depends on MACH_JZ4740
1021 help
1022 If you say yes here you get support for the Ingenic JZ4740 SoC RTC
1023 controller.
1025 This driver can also be buillt as a module. If so, the module
1026 will be called rtc-jz4740.
1028 config RTC_DRV_LPC32XX
1029 depends on ARCH_LPC32XX
1030 tristate "NXP LPC32XX RTC"
1031 help
1032 This enables support for the NXP RTC in the LPC32XX
1034 This driver can also be buillt as a module. If so, the module
1035 will be called rtc-lpc32xx.
1037 config RTC_DRV_PM8XXX
1038 tristate "Qualcomm PMIC8XXX RTC"
1039 depends on MFD_PM8XXX
1040 help
1041 If you say yes here you get support for the
1042 Qualcomm PMIC8XXX RTC.
1044 To compile this driver as a module, choose M here: the
1045 module will be called rtc-pm8xxx.
1047 config RTC_DRV_TEGRA
1048 tristate "NVIDIA Tegra Internal RTC driver"
1049 depends on RTC_CLASS && ARCH_TEGRA
1050 help
1051 If you say yes here you get support for the
1052 Tegra 200 series internal RTC module.
1054 This drive can also be built as a module. If so, the module
1055 will be called rtc-tegra.
1057 config RTC_DRV_TILE
1058 tristate "Tilera hypervisor RTC support"
1059 depends on TILE
1060 help
1061 Enable support for the Linux driver side of the Tilera
1062 hypervisor's real-time clock interface.
1064 config RTC_DRV_PUV3
1065 tristate "PKUnity v3 RTC support"
1066 depends on ARCH_PUV3
1067 help
1068 This enables support for the RTC in the PKUnity-v3 SoCs.
1070 This drive can also be built as a module. If so, the module
1071 will be called rtc-puv3.
1073 endif # RTC_CLASS