]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - drivers/rtc/Kconfig
Merge branch 'master' of git://git.kernel.org/pub/scm/linux/kernel/git/linville/wirel...
[sitara-epos/sitara-epos-kernel.git] / drivers / rtc / Kconfig
1 #
2 # RTC class/drivers configuration
3 #
5 config RTC_LIB
6         bool
8 menuconfig RTC_CLASS
9         bool "Real Time Clock"
10         default n
11         depends on !S390 && !UML
12         select RTC_LIB
13         help
14           Generic RTC class support. If you say yes here, you will
15           be allowed to plug one or more RTCs to your system. You will
16           probably want to enable one or more of the interfaces below.
18 if RTC_CLASS
20 config RTC_HCTOSYS
21         bool "Set system time from RTC on startup and resume"
22         depends on RTC_CLASS = y
23         default y
24         help
25           If you say yes here, the system time (wall clock) will be set using
26           the value read from a specified RTC device. This is useful to avoid
27           unnecessary fsck runs at boot time, and to network better.
29 config RTC_HCTOSYS_DEVICE
30         string "RTC used to set the system time"
31         depends on RTC_HCTOSYS = y
32         default "rtc0"
33         help
34           The RTC device that will be used to (re)initialize the system
35           clock, usually rtc0. Initialization is done when the system
36           starts up, and when it resumes from a low power state. This
37           device should record time in UTC, since the kernel won't do
38           timezone correction.
40           The driver for this RTC device must be loaded before late_initcall
41           functions run, so it must usually be statically linked.
43           This clock should be battery-backed, so that it reads the correct
44           time when the system boots from a power-off state. Otherwise, your
45           system will need an external clock source (like an NTP server).
47           If the clock you specify here is not battery backed, it may still
48           be useful to reinitialize system time when resuming from system
49           sleep states. Do not specify an RTC here unless it stays powered
50           during all this system's supported sleep states.
52 config RTC_DEBUG
53         bool "RTC debug support"
54         depends on RTC_CLASS = y
55         help
56           Say yes here to enable debugging support in the RTC framework
57           and individual RTC drivers.
59 comment "RTC interfaces"
61 config RTC_INTF_SYSFS
62         boolean "/sys/class/rtc/rtcN (sysfs)"
63         depends on SYSFS
64         default RTC_CLASS
65         help
66           Say yes here if you want to use your RTCs using sysfs interfaces,
67           /sys/class/rtc/rtc0 through /sys/.../rtcN.
69           If unsure, say Y.
71 config RTC_INTF_PROC
72         boolean "/proc/driver/rtc (procfs for rtc0)"
73         depends on PROC_FS
74         default RTC_CLASS
75         help
76           Say yes here if you want to use your first RTC through the proc
77           interface, /proc/driver/rtc. Other RTCs will not be available
78           through that API.
80           If unsure, say Y.
82 config RTC_INTF_DEV
83         boolean "/dev/rtcN (character devices)"
84         default RTC_CLASS
85         help
86           Say yes here if you want to use your RTCs using the /dev
87           interfaces, which "udev" sets up as /dev/rtc0 through
88           /dev/rtcN.
90           You may want to set up a symbolic link so one of these
91           can be accessed as /dev/rtc, which is a name
92           expected by "hwclock" and some other programs. Recent
93           versions of "udev" are known to set up the symlink for you.
95           If unsure, say Y.
97 config RTC_INTF_DEV_UIE_EMUL
98         bool "RTC UIE emulation on dev interface"
99         depends on RTC_INTF_DEV
100         help
101           Provides an emulation for RTC_UIE if the underlying rtc chip
102           driver does not expose RTC_UIE ioctls. Those requests generate
103           once-per-second update interrupts, used for synchronization.
105           The emulation code will read the time from the hardware
106           clock several times per second, please enable this option
107           only if you know that you really need it.
109 config RTC_DRV_TEST
110         tristate "Test driver/device"
111         help
112           If you say yes here you get support for the
113           RTC test driver. It's a software RTC which can be
114           used to test the RTC subsystem APIs. It gets
115           the time from the system clock.
116           You want this driver only if you are doing development
117           on the RTC subsystem. Please read the source code
118           for further details.
120           This driver can also be built as a module. If so, the module
121           will be called rtc-test.
123 comment "I2C RTC drivers"
124         depends on I2C
126 if I2C
128 config RTC_DRV_88PM860X
129         tristate "Marvell 88PM860x"
130         depends on RTC_CLASS && I2C && MFD_88PM860X
131         help
132           If you say yes here you get support for RTC function in Marvell
133           88PM860x chips.
135           This driver can also be built as a module. If so, the module
136           will be called rtc-88pm860x.
138 config RTC_DRV_DS1307
139         tristate "Dallas/Maxim DS1307/37/38/39/40, ST M41T00, EPSON RX-8025"
140         help
141           If you say yes here you get support for various compatible RTC
142           chips (often with battery backup) connected with I2C. This driver
143           should handle DS1307, DS1337, DS1338, DS1339, DS1340, ST M41T00,
144           EPSON RX-8025 and probably other chips. In some cases the RTC
145           must already have been initialized (by manufacturing or a
146           bootloader).
148           The first seven registers on these chips hold an RTC, and other
149           registers may add features such as NVRAM, a trickle charger for
150           the RTC/NVRAM backup power, and alarms. NVRAM is visible in
151           sysfs, but other chip features may not be available.
153           This driver can also be built as a module. If so, the module
154           will be called rtc-ds1307.
156 config RTC_DRV_DS1374
157         tristate "Dallas/Maxim DS1374"
158         depends on RTC_CLASS && I2C
159         help
160           If you say yes here you get support for Dallas Semiconductor
161           DS1374 real-time clock chips. If an interrupt is associated
162           with the device, the alarm functionality is supported.
164           This driver can also be built as a module. If so, the module
165           will be called rtc-ds1374.
167 config RTC_DRV_DS1672
168         tristate "Dallas/Maxim DS1672"
169         help
170           If you say yes here you get support for the
171           Dallas/Maxim DS1672 timekeeping chip.
173           This driver can also be built as a module. If so, the module
174           will be called rtc-ds1672.
176 config RTC_DRV_DS3232
177         tristate "Dallas/Maxim DS3232"
178         depends on RTC_CLASS && I2C
179         help
180           If you say yes here you get support for Dallas Semiconductor
181           DS3232 real-time clock chips. If an interrupt is associated
182           with the device, the alarm functionality is supported.
184           This driver can also be built as a module.  If so, the module
185           will be called rtc-ds3232.
187 config RTC_DRV_MAX6900
188         tristate "Maxim MAX6900"
189         help
190           If you say yes here you will get support for the
191           Maxim MAX6900 I2C RTC chip.
193           This driver can also be built as a module. If so, the module
194           will be called rtc-max6900.
196 config RTC_DRV_MAX8925
197         tristate "Maxim MAX8925"
198         depends on MFD_MAX8925
199         help
200           If you say yes here you will get support for the
201           RTC of Maxim MAX8925 PMIC.
203           This driver can also be built as a module. If so, the module
204           will be called rtc-max8925.
206 config RTC_DRV_MAX8998
207         tristate "Maxim MAX8998"
208         depends on MFD_MAX8998
209         help
210           If you say yes here you will get support for the
211           RTC of Maxim MAX8998 PMIC.
213           This driver can also be built as a module. If so, the module
214           will be called rtc-max8998.
216 config RTC_DRV_RS5C372
217         tristate "Ricoh R2025S/D, RS5C372A/B, RV5C386, RV5C387A"
218         help
219           If you say yes here you get support for the
220           Ricoh R2025S/D, RS5C372A, RS5C372B, RV5C386, and RV5C387A RTC chips.
222           This driver can also be built as a module. If so, the module
223           will be called rtc-rs5c372.
225 config RTC_DRV_ISL1208
226         tristate "Intersil ISL1208"
227         help
228           If you say yes here you get support for the
229           Intersil ISL1208 RTC chip.
231           This driver can also be built as a module. If so, the module
232           will be called rtc-isl1208.
234 config RTC_DRV_ISL12022
235         tristate "Intersil ISL12022"
236         help
237           If you say yes here you get support for the
238           Intersil ISL12022 RTC chip.
240           This driver can also be built as a module. If so, the module
241           will be called rtc-isl12022.
243 config RTC_DRV_X1205
244         tristate "Xicor/Intersil X1205"
245         help
246           If you say yes here you get support for the
247           Xicor/Intersil X1205 RTC chip.
249           This driver can also be built as a module. If so, the module
250           will be called rtc-x1205.
252 config RTC_DRV_PCF8563
253         tristate "Philips PCF8563/Epson RTC8564"
254         help
255           If you say yes here you get support for the
256           Philips PCF8563 RTC chip. The Epson RTC8564
257           should work as well.
259           This driver can also be built as a module. If so, the module
260           will be called rtc-pcf8563.
262 config RTC_DRV_PCF8583
263         tristate "Philips PCF8583"
264         help
265           If you say yes here you get support for the Philips PCF8583
266           RTC chip found on Acorn RiscPCs. This driver supports the
267           platform specific method of retrieving the current year from
268           the RTC's SRAM. It will work on other platforms with the same
269           chip, but the year will probably have to be tweaked.
271           This driver can also be built as a module. If so, the module
272           will be called rtc-pcf8583.
274 config RTC_DRV_M41T80
275         tristate "ST M41T62/65/M41T80/81/82/83/84/85/87"
276         help
277           If you say Y here you will get support for the ST M41T60
278           and M41T80 RTC chips series. Currently, the following chips are
279           supported: M41T62, M41T65, M41T80, M41T81, M41T82, M41T83, M41ST84,
280           M41ST85, and M41ST87.
282           This driver can also be built as a module. If so, the module
283           will be called rtc-m41t80.
285 config RTC_DRV_M41T80_WDT
286         bool "ST M41T65/M41T80 series RTC watchdog timer"
287         depends on RTC_DRV_M41T80
288         help
289           If you say Y here you will get support for the
290           watchdog timer in the ST M41T60 and M41T80 RTC chips series.
292 config RTC_DRV_BQ32K
293         tristate "TI BQ32000"
294         help
295           If you say Y here you will get support for the TI
296           BQ32000 I2C RTC chip.
298           This driver can also be built as a module. If so, the module
299           will be called rtc-bq32k.
301 config RTC_DRV_DM355EVM
302         tristate "TI DaVinci DM355 EVM RTC"
303         depends on MFD_DM355EVM_MSP
304         help
305           Supports the RTC firmware in the MSP430 on the DM355 EVM.
307 config RTC_DRV_TWL92330
308         boolean "TI TWL92330/Menelaus"
309         depends on MENELAUS
310         help
311           If you say yes here you get support for the RTC on the
312           TWL92330 "Menelaus" power management chip, used with OMAP2
313           platforms. The support is integrated with the rest of
314           the Menelaus driver; it's not separate module.
316 config RTC_DRV_TWL4030
317         tristate "TI TWL4030/TWL5030/TWL6030/TPS659x0"
318         depends on RTC_CLASS && TWL4030_CORE
319         help
320           If you say yes here you get support for the RTC on the
321           TWL4030/TWL5030/TWL6030 family chips, used mostly with OMAP3 platforms.
323           This driver can also be built as a module. If so, the module
324           will be called rtc-twl.
326 config RTC_DRV_S35390A
327         tristate "Seiko Instruments S-35390A"
328         select BITREVERSE
329         help
330           If you say yes here you will get support for the Seiko
331           Instruments S-35390A.
333           This driver can also be built as a module. If so the module
334           will be called rtc-s35390a.
336 config RTC_DRV_FM3130
337         tristate "Ramtron FM3130"
338         help
339           If you say Y here you will get support for the
340           Ramtron FM3130 RTC chips.
341           Ramtron FM3130 is a chip with two separate devices inside,
342           RTC clock and FRAM. This driver provides only RTC functionality.
344           This driver can also be built as a module. If so the module
345           will be called rtc-fm3130.
347 config RTC_DRV_RX8581
348         tristate "Epson RX-8581"
349         help
350           If you say yes here you will get support for the Epson RX-8581.
352           This driver can also be built as a module. If so the module
353           will be called rtc-rx8581.
355 config RTC_DRV_RX8025
356         tristate "Epson RX-8025SA/NB"
357         help
358           If you say yes here you get support for the Epson
359           RX-8025SA/NB RTC chips.
361           This driver can also be built as a module. If so, the module
362           will be called rtc-rx8025.
364 config RTC_DRV_EM3027
365         tristate "EM Microelectronic EM3027"
366         help
367           If you say yes here you get support for the EM
368           Microelectronic EM3027 RTC chips.
370           This driver can also be built as a module. If so, the module
371           will be called rtc-em3027.
373 config RTC_DRV_RV3029C2
374         tristate "Micro Crystal RTC"
375         help
376           If you say yes here you get support for the Micro Crystal
377           RV3029-C2 RTC chips.
379           This driver can also be built as a module. If so, the module
380           will be called rtc-rv3029c2.
382 endif # I2C
384 comment "SPI RTC drivers"
386 if SPI_MASTER
388 config RTC_DRV_M41T93
389         tristate "ST M41T93"
390         help
391           If you say yes here you will get support for the
392           ST M41T93 SPI RTC chip.
394           This driver can also be built as a module. If so, the module
395           will be called rtc-m41t93.
397 config RTC_DRV_M41T94
398         tristate "ST M41T94"
399         help
400           If you say yes here you will get support for the
401           ST M41T94 SPI RTC chip.
403           This driver can also be built as a module. If so, the module
404           will be called rtc-m41t94.
406 config RTC_DRV_DS1305
407         tristate "Dallas/Maxim DS1305/DS1306"
408         help
409           Select this driver to get support for the Dallas/Maxim DS1305
410           and DS1306 real time clock chips. These support a trickle
411           charger, alarms, and NVRAM in addition to the clock.
413           This driver can also be built as a module. If so, the module
414           will be called rtc-ds1305.
416 config RTC_DRV_DS1390
417         tristate "Dallas/Maxim DS1390/93/94"
418         help
419           If you say yes here you get support for the
420           Dallas/Maxim DS1390/93/94 chips.
422           This driver only supports the RTC feature, and not other chip
423           features such as alarms and trickle charging.
425           This driver can also be built as a module. If so, the module
426           will be called rtc-ds1390.
428 config RTC_DRV_MAX6902
429         tristate "Maxim MAX6902"
430         help
431           If you say yes here you will get support for the
432           Maxim MAX6902 SPI RTC chip.
434           This driver can also be built as a module. If so, the module
435           will be called rtc-max6902.
437 config RTC_DRV_R9701
438         tristate "Epson RTC-9701JE"
439         help
440           If you say yes here you will get support for the
441           Epson RTC-9701JE SPI RTC chip.
443           This driver can also be built as a module. If so, the module
444           will be called rtc-r9701.
446 config RTC_DRV_RS5C348
447         tristate "Ricoh RS5C348A/B"
448         help
449           If you say yes here you get support for the
450           Ricoh RS5C348A and RS5C348B RTC chips.
452           This driver can also be built as a module. If so, the module
453           will be called rtc-rs5c348.
455 config RTC_DRV_DS3234
456         tristate "Maxim/Dallas DS3234"
457         help
458           If you say yes here you get support for the
459           Maxim/Dallas DS3234 SPI RTC chip.
461           This driver can also be built as a module. If so, the module
462           will be called rtc-ds3234.
464 config RTC_DRV_PCF2123
465         tristate "NXP PCF2123"
466         help
467           If you say yes here you get support for the NXP PCF2123
468           RTC chip.
470           This driver can also be built as a module. If so, the module
471           will be called rtc-pcf2123.
473 endif # SPI_MASTER
475 comment "Platform RTC drivers"
477 # this 'CMOS' RTC driver is arch dependent because <asm-generic/rtc.h>
478 # requires <asm/mc146818rtc.h> defining CMOS_READ/CMOS_WRITE, and a
479 # global rtc_lock ... it's not yet just another platform_device.
481 config RTC_DRV_CMOS
482         tristate "PC-style 'CMOS'"
483         depends on X86 || ALPHA || ARM || M32R || ATARI || PPC || MIPS || SPARC64
484         default y if X86
485         help
486           Say "yes" here to get direct support for the real time clock
487           found in every PC or ACPI-based system, and some other boards.
488           Specifically the original MC146818, compatibles like those in
489           PC south bridges, the DS12887 or M48T86, some multifunction
490           or LPC bus chips, and so on.
492           Your system will need to define the platform device used by
493           this driver, otherwise it won't be accessible. This means
494           you can safely enable this driver if you don't know whether
495           or not your board has this kind of hardware.
497           This driver can also be built as a module. If so, the module
498           will be called rtc-cmos.
500 config RTC_DRV_VRTC
501         tristate "Virtual RTC for Moorestown platforms"
502         depends on X86_MRST
503         default y if X86_MRST
505         help
506         Say "yes" here to get direct support for the real time clock
507         found on Moorestown platforms. The VRTC is a emulated RTC that
508         derives its clock source from a real RTC in the PMIC. The MC146818
509         style programming interface is mostly conserved, but any
510         updates are done via IPC calls to the system controller FW.
512 config RTC_DRV_DS1216
513         tristate "Dallas DS1216"
514         depends on SNI_RM
515         help
516           If you say yes here you get support for the Dallas DS1216 RTC chips.
518 config RTC_DRV_DS1286
519         tristate "Dallas DS1286"
520         help
521           If you say yes here you get support for the Dallas DS1286 RTC chips.
523 config RTC_DRV_DS1302
524         tristate "Dallas DS1302"
525         depends on SH_SECUREEDGE5410
526         help
527           If you say yes here you get support for the Dallas DS1302 RTC chips.
529 config RTC_DRV_DS1511
530         tristate "Dallas DS1511"
531         depends on RTC_CLASS
532         help
533           If you say yes here you get support for the
534           Dallas DS1511 timekeeping/watchdog chip.
536           This driver can also be built as a module. If so, the module
537           will be called rtc-ds1511.
539 config RTC_DRV_DS1553
540         tristate "Maxim/Dallas DS1553"
541         help
542           If you say yes here you get support for the
543           Maxim/Dallas DS1553 timekeeping chip.
545           This driver can also be built as a module. If so, the module
546           will be called rtc-ds1553.
548 config RTC_DRV_DS1742
549         tristate "Maxim/Dallas DS1742/1743"
550         help
551           If you say yes here you get support for the
552           Maxim/Dallas DS1742/1743 timekeeping chip.
554           This driver can also be built as a module. If so, the module
555           will be called rtc-ds1742.
557 config RTC_DRV_EFI
558         tristate "EFI RTC"
559         depends on IA64
560         help
561           If you say yes here you will get support for the EFI
562           Real Time Clock.
564           This driver can also be built as a module. If so, the module
565           will be called rtc-efi.
567 config RTC_DRV_STK17TA8
568         tristate "Simtek STK17TA8"
569         depends on RTC_CLASS
570         help
571           If you say yes here you get support for the
572           Simtek STK17TA8 timekeeping chip.
574           This driver can also be built as a module. If so, the module
575           will be called rtc-stk17ta8.
577 config RTC_DRV_M48T86
578         tristate "ST M48T86/Dallas DS12887"
579         help
580           If you say Y here you will get support for the
581           ST M48T86 and Dallas DS12887 RTC chips.
583           This driver can also be built as a module. If so, the module
584           will be called rtc-m48t86.
586 config RTC_DRV_M48T35
587         tristate "ST M48T35"
588         help
589           If you say Y here you will get support for the
590           ST M48T35 RTC chip.
592           This driver can also be built as a module, if so, the module
593           will be called "rtc-m48t35".
595 config RTC_DRV_M48T59
596         tristate "ST M48T59/M48T08/M48T02"
597         help
598           If you say Y here you will get support for the
599           ST M48T59 RTC chip and compatible ST M48T08 and M48T02.
601           These chips are usually found in Sun SPARC and UltraSPARC
602           workstations.
604           This driver can also be built as a module, if so, the module
605           will be called "rtc-m48t59".
607 config RTC_DRV_MSM6242
608         tristate "Oki MSM6242"
609         help
610           If you say yes here you get support for the Oki MSM6242
611           timekeeping chip. It is used in some Amiga models (e.g. A2000).
613           This driver can also be built as a module. If so, the module
614           will be called rtc-msm6242.
616 config RTC_DRV_IMXDI
617         tristate "Freescale IMX DryIce Real Time Clock"
618         depends on ARCH_MX25
619         depends on RTC_CLASS
620         help
621            Support for Freescale IMX DryIce RTC
623            This driver can also be built as a module, if so, the module
624            will be called "rtc-imxdi".
626 config RTC_MXC
627         tristate "Freescale MXC Real Time Clock"
628         depends on ARCH_MXC
629         depends on RTC_CLASS
630         help
631            If you say yes here you get support for the Freescale MXC
632            RTC module.
634            This driver can also be built as a module, if so, the module
635            will be called "rtc-mxc".
637 config RTC_DRV_BQ4802
638         tristate "TI BQ4802"
639         help
640           If you say Y here you will get support for the TI
641           BQ4802 RTC chip.
643           This driver can also be built as a module. If so, the module
644           will be called rtc-bq4802.
646 config RTC_DRV_RP5C01
647         tristate "Ricoh RP5C01"
648         help
649           If you say yes here you get support for the Ricoh RP5C01
650           timekeeping chip. It is used in some Amiga models (e.g. A3000
651           and A4000).
653           This driver can also be built as a module. If so, the module
654           will be called rtc-rp5c01.
656 config RTC_DRV_V3020
657         tristate "EM Microelectronic V3020"
658         help
659           If you say yes here you will get support for the
660           EM Microelectronic v3020 RTC chip.
662           This driver can also be built as a module. If so, the module
663           will be called rtc-v3020.
665 config RTC_DRV_WM831X
666         tristate "Wolfson Microelectronics WM831x RTC"
667         depends on MFD_WM831X
668         help
669           If you say yes here you will get support for the RTC subsystem
670           of the Wolfson Microelectronics WM831X series PMICs.
672           This driver can also be built as a module. If so, the module
673           will be called "rtc-wm831x".
675 config RTC_DRV_WM8350
676         tristate "Wolfson Microelectronics WM8350 RTC"
677         depends on MFD_WM8350
678         help
679           If you say yes here you will get support for the RTC subsystem
680           of the Wolfson Microelectronics WM8350.
682           This driver can also be built as a module. If so, the module
683           will be called "rtc-wm8350".
685 config RTC_DRV_SPEAR
686         tristate "SPEAR ST RTC"
687         depends on PLAT_SPEAR
688         default y
689         help
690          If you say Y here you will get support for the RTC found on
691          spear
693 config RTC_DRV_PCF50633
694         depends on MFD_PCF50633
695         tristate "NXP PCF50633 RTC"
696         help
697           If you say yes here you get support for the RTC subsystem of the
698           NXP PCF50633 used in embedded systems.
700 config RTC_DRV_AB3100
701         tristate "ST-Ericsson AB3100 RTC"
702         depends on AB3100_CORE
703         default y if AB3100_CORE
704         help
705           Select this to enable the ST-Ericsson AB3100 Mixed Signal IC RTC
706           support. This chip contains a battery- and capacitor-backed RTC.
708 config RTC_DRV_AB8500
709         tristate "ST-Ericsson AB8500 RTC"
710         depends on AB8500_CORE
711         help
712           Select this to enable the ST-Ericsson AB8500 power management IC RTC
713           support. This chip contains a battery- and capacitor-backed RTC.
715 config RTC_DRV_NUC900
716         tristate "NUC910/NUC920 RTC driver"
717         depends on RTC_CLASS && ARCH_W90X900
718         help
719           If you say yes here you get support for the RTC subsystem of the
720           NUC910/NUC920 used in embedded systems.
722 comment "on-CPU RTC drivers"
724 config RTC_DRV_DAVINCI
725         tristate "TI DaVinci RTC"
726         depends on ARCH_DAVINCI_DM365
727         help
728           If you say yes here you get support for the RTC on the
729           DaVinci platforms (DM365).
731           This driver can also be built as a module. If so, the module
732           will be called rtc-davinci.
734 config RTC_DRV_OMAP
735         tristate "TI OMAP1"
736         depends on ARCH_OMAP15XX || ARCH_OMAP16XX || ARCH_OMAP730 || ARCH_DAVINCI_DA8XX
737         help
738           Say "yes" here to support the real time clock on TI OMAP1 and
739           DA8xx/OMAP-L13x chips.  This driver can also be built as a
740           module called rtc-omap.
742 config HAVE_S3C_RTC
743         bool
744         help
745           This will include RTC support for Samsung SoCs. If
746           you want to include RTC support for any machine, kindly
747           select this in the respective mach-XXXX/Kconfig file.
749 config RTC_DRV_S3C
750         tristate "Samsung S3C series SoC RTC"
751         depends on ARCH_S3C2410 || ARCH_S3C64XX || HAVE_S3C_RTC
752         help
753           RTC (Realtime Clock) driver for the clock inbuilt into the
754           Samsung S3C24XX series of SoCs. This can provide periodic
755           interrupt rates from 1Hz to 64Hz for user programs, and
756           wakeup from Alarm.
758           The driver currently supports the common features on all the
759           S3C24XX range, such as the S3C2410, S3C2412, S3C2413, S3C2440
760           and S3C2442.
762           This driver can also be build as a module. If so, the module
763           will be called rtc-s3c.
765 config RTC_DRV_EP93XX
766         tristate "Cirrus Logic EP93XX"
767         depends on ARCH_EP93XX
768         help
769           If you say yes here you get support for the
770           RTC embedded in the Cirrus Logic EP93XX processors.
772           This driver can also be built as a module. If so, the module
773           will be called rtc-ep93xx.
775 config RTC_DRV_SA1100
776         tristate "SA11x0/PXA2xx"
777         depends on ARCH_SA1100 || ARCH_PXA
778         help
779           If you say Y here you will get access to the real time clock
780           built into your SA11x0 or PXA2xx CPU.
782           To compile this driver as a module, choose M here: the
783           module will be called rtc-sa1100.
785 config RTC_DRV_SH
786         tristate "SuperH On-Chip RTC"
787         depends on RTC_CLASS && SUPERH && HAVE_CLK
788         help
789           Say Y here to enable support for the on-chip RTC found in
790           most SuperH processors.
792           To compile this driver as a module, choose M here: the
793           module will be called rtc-sh.
795 config RTC_DRV_VR41XX
796         tristate "NEC VR41XX"
797         depends on CPU_VR41XX
798         help
799           If you say Y here you will get access to the real time clock
800           built into your NEC VR41XX CPU.
802           To compile this driver as a module, choose M here: the
803           module will be called rtc-vr41xx.
805 config RTC_DRV_PL030
806         tristate "ARM AMBA PL030 RTC"
807         depends on ARM_AMBA
808         help
809           If you say Y here you will get access to ARM AMBA
810           PrimeCell PL030 RTC found on certain ARM SOCs.
812           To compile this driver as a module, choose M here: the
813           module will be called rtc-pl030.
815 config RTC_DRV_PL031
816         tristate "ARM AMBA PL031 RTC"
817         depends on ARM_AMBA
818         help
819           If you say Y here you will get access to ARM AMBA
820           PrimeCell PL031 RTC found on certain ARM SOCs.
822           To compile this driver as a module, choose M here: the
823           module will be called rtc-pl031.
825 config RTC_DRV_AT32AP700X
826         tristate "AT32AP700X series RTC"
827         depends on PLATFORM_AT32AP
828         help
829           Driver for the internal RTC (Realtime Clock) on Atmel AVR32
830           AT32AP700x family processors.
832 config RTC_DRV_AT91RM9200
833         tristate "AT91RM9200 or some AT91SAM9 RTC"
834         depends on ARCH_AT91RM9200 || ARCH_AT91SAM9RL || ARCH_AT91SAM9G45
835         help
836           Driver for the internal RTC (Realtime Clock) module found on
837           Atmel AT91RM9200's and some  AT91SAM9 chips. On AT91SAM9 chips
838           this is powered by the backup power supply.
840 config RTC_DRV_AT91SAM9
841         tristate "AT91SAM9x/AT91CAP9 RTT as RTC"
842         depends on ARCH_AT91 && !(ARCH_AT91RM9200 || ARCH_AT91X40)
843         help
844           RTC driver for the Atmel AT91SAM9x and AT91CAP9 internal RTT
845           (Real Time Timer). These timers are powered by the backup power
846           supply (such as a small coin cell battery), but do not need to
847           be used as RTCs.
849           (On AT91SAM9rl and AT91SAM9G45 chips you probably want to use the
850           dedicated RTC module and leave the RTT available for other uses.)
852 config RTC_DRV_AT91SAM9_RTT
853         int
854         range 0 1
855         default 0
856         prompt "RTT module Number" if ARCH_AT91SAM9263
857         depends on RTC_DRV_AT91SAM9
858         help
859           More than one RTT module is available. You can choose which
860           one will be used as an RTC. The default of zero is normally
861           OK to use, though some systems use that for non-RTC purposes.
863 config RTC_DRV_AT91SAM9_GPBR
864         int
865         range 0 3 if !ARCH_AT91SAM9263
866         range 0 15 if ARCH_AT91SAM9263
867         default 0
868         prompt "Backup Register Number"
869         depends on RTC_DRV_AT91SAM9
870         help
871           The RTC driver needs to use one of the General Purpose Backup
872           Registers (GPBRs) as well as the RTT. You can choose which one
873           will be used. The default of zero is normally OK to use, but
874           on some systems other software needs to use that register.
876 config RTC_DRV_AU1XXX
877         tristate "Au1xxx Counter0 RTC support"
878         depends on MIPS_ALCHEMY
879         help
880           This is a driver for the Au1xxx on-chip Counter0 (Time-Of-Year
881           counter) to be used as a RTC.
883           This driver can also be built as a module. If so, the module
884           will be called rtc-au1xxx.
886 config RTC_DRV_BFIN
887         tristate "Blackfin On-Chip RTC"
888         depends on BLACKFIN && !BF561
889         help
890           If you say yes here you will get support for the
891           Blackfin On-Chip Real Time Clock.
893           This driver can also be built as a module. If so, the module
894           will be called rtc-bfin.
896 config RTC_DRV_RS5C313
897         tristate "Ricoh RS5C313"
898         depends on SH_LANDISK
899         help
900           If you say yes here you get support for the Ricoh RS5C313 RTC chips.
902 config RTC_DRV_GENERIC
903         tristate "Generic RTC support"
904         # Please consider writing a new RTC driver instead of using the generic
905         # RTC abstraction
906         depends on PARISC || M68K || PPC || SUPERH32
907         help
908           Say Y or M here to enable RTC support on systems using the generic
909           RTC abstraction. If you do not know what you are doing, you should
910           just say Y.
912 config RTC_DRV_PXA
913        tristate "PXA27x/PXA3xx"
914        depends on ARCH_PXA
915        help
916          If you say Y here you will get access to the real time clock
917          built into your PXA27x or PXA3xx CPU.
919          This RTC driver uses PXA RTC registers available since pxa27x
920          series (RDxR, RYxR) instead of legacy RCNR, RTAR.
922 config RTC_DRV_VT8500
923         tristate "VIA/WonderMedia 85xx SoC RTC"
924         depends on ARCH_VT8500
925         help
926           If you say Y here you will get access to the real time clock
927           built into your VIA VT8500 SoC or its relatives.
930 config RTC_DRV_SUN4V
931         bool "SUN4V Hypervisor RTC"
932         depends on SPARC64
933         help
934           If you say Y here you will get support for the Hypervisor
935           based RTC on SUN4V systems.
937 config RTC_DRV_STARFIRE
938         bool "Starfire RTC"
939         depends on SPARC64
940         help
941           If you say Y here you will get support for the RTC found on
942           Starfire systems.
944 config RTC_DRV_TX4939
945         tristate "TX4939 SoC"
946         depends on SOC_TX4939
947         help
948           Driver for the internal RTC (Realtime Clock) module found on
949           Toshiba TX4939 SoC.
951 config RTC_DRV_MV
952         tristate "Marvell SoC RTC"
953         depends on ARCH_KIRKWOOD || ARCH_DOVE
954         help
955           If you say yes here you will get support for the in-chip RTC
956           that can be found in some of Marvell's SoC devices, such as
957           the Kirkwood 88F6281 and 88F6192.
959           This driver can also be built as a module. If so, the module
960           will be called rtc-mv.
962 config RTC_DRV_PS3
963         tristate "PS3 RTC"
964         depends on PPC_PS3
965         help
966           If you say yes here you will get support for the RTC on PS3.
968           This driver can also be built as a module. If so, the module
969           will be called rtc-ps3.
971 config RTC_DRV_COH901331
972         tristate "ST-Ericsson COH 901 331 RTC"
973         depends on ARCH_U300
974         help
975           If you say Y here you will get access to ST-Ericsson
976           COH 901 331 RTC clock found in some ST-Ericsson Mobile
977           Platforms.
979           This driver can also be built as a module. If so, the module
980           will be called "rtc-coh901331".
983 config RTC_DRV_STMP
984         tristate "Freescale STMP3xxx/i.MX23/i.MX28 RTC"
985         depends on ARCH_MXS
986         help
987           If you say yes here you will get support for the onboard
988           STMP3xxx/i.MX23/i.MX28 RTC.
990           This driver can also be built as a module. If so, the module
991           will be called rtc-stmp3xxx.
993 config RTC_DRV_PCAP
994         tristate "PCAP RTC"
995         depends on EZX_PCAP
996         help
997           If you say Y here you will get support for the RTC found on
998           the PCAP2 ASIC used on some Motorola phones.
1000 config RTC_DRV_MC13XXX
1001         depends on MFD_MC13XXX
1002         tristate "Freescale MC13xxx RTC"
1003         help
1004           This enables support for the RTCs found on Freescale's PMICs
1005           MC13783 and MC13892.
1007 config RTC_DRV_MPC5121
1008         tristate "Freescale MPC5121 built-in RTC"
1009         depends on PPC_MPC512x || PPC_MPC52xx
1010         help
1011           If you say yes here you will get support for the
1012           built-in RTC on MPC5121 or on MPC5200.
1014           This driver can also be built as a module. If so, the module
1015           will be called rtc-mpc5121.
1017 config RTC_DRV_JZ4740
1018         tristate "Ingenic JZ4740 SoC"
1019         depends on RTC_CLASS
1020         depends on MACH_JZ4740
1021         help
1022           If you say yes here you get support for the Ingenic JZ4740 SoC RTC
1023           controller.
1025           This driver can also be buillt as a module. If so, the module
1026           will be called rtc-jz4740.
1028 config RTC_DRV_LPC32XX
1029         depends on ARCH_LPC32XX
1030         tristate "NXP LPC32XX RTC"
1031         help
1032           This enables support for the NXP RTC in the LPC32XX
1034           This driver can also be buillt as a module. If so, the module
1035           will be called rtc-lpc32xx.
1037 config RTC_DRV_PM8XXX
1038         tristate "Qualcomm PMIC8XXX RTC"
1039         depends on MFD_PM8XXX
1040         help
1041           If you say yes here you get support for the
1042           Qualcomm PMIC8XXX RTC.
1044           To compile this driver as a module, choose M here: the
1045           module will be called rtc-pm8xxx.
1047 config RTC_DRV_TEGRA
1048         tristate "NVIDIA Tegra Internal RTC driver"
1049         depends on RTC_CLASS && ARCH_TEGRA
1050         help
1051           If you say yes here you get support for the
1052           Tegra 200 series internal RTC module.
1054           This drive can also be built as a module. If so, the module
1055           will be called rtc-tegra.
1057 config RTC_DRV_TILE
1058         tristate "Tilera hypervisor RTC support"
1059         depends on TILE
1060         help
1061           Enable support for the Linux driver side of the Tilera
1062           hypervisor's real-time clock interface.
1064 config RTC_DRV_PUV3
1065         tristate "PKUnity v3 RTC support"
1066         depends on ARCH_PUV3
1067         help
1068           This enables support for the RTC in the PKUnity-v3 SoCs.
1070           This drive can also be built as a module. If so, the module
1071           will be called rtc-puv3.
1073 endif # RTC_CLASS