1 /*
2 * Texas Instruments AM35x "glue layer"
3 *
4 * Copyright (c) 2010, by Texas Instruments
5 *
6 * Based on the DA8xx "glue layer" code.
7 * Copyright (c) 2008-2009, MontaVista Software, Inc. <source@mvista.com>
8 *
9 * This file is part of the Inventra Controller Driver for Linux.
10 *
11 * The Inventra Controller Driver for Linux is free software; you
12 * can redistribute it and/or modify it under the terms of the GNU
13 * General Public License version 2 as published by the Free Software
14 * Foundation.
15 *
16 * The Inventra Controller Driver for Linux is distributed in
17 * the hope that it will be useful, but WITHOUT ANY WARRANTY;
18 * without even the implied warranty of MERCHANTABILITY or
19 * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public
20 * License for more details.
21 *
22 * You should have received a copy of the GNU General Public License
23 * along with The Inventra Controller Driver for Linux ; if not,
24 * write to the Free Software Foundation, Inc., 59 Temple Place,
25 * Suite 330, Boston, MA 02111-1307 USA
26 *
27 */
29 #include <linux/init.h>
30 #include <linux/module.h>
31 #include <linux/clk.h>
32 #include <linux/io.h>
33 #include <linux/platform_device.h>
34 #include <linux/dma-mapping.h>
36 #include <plat/usb.h>
38 #include "musb_core.h"
40 /*
41 * AM35x specific definitions
42 */
43 /* USB 2.0 OTG module registers */
44 #define USB_REVISION_REG 0x00
45 #define USB_CTRL_REG 0x04
46 #define USB_STAT_REG 0x08
47 #define USB_EMULATION_REG 0x0c
48 /* 0x10 Reserved */
49 #define USB_AUTOREQ_REG 0x14
50 #define USB_SRP_FIX_TIME_REG 0x18
51 #define USB_TEARDOWN_REG 0x1c
52 #define EP_INTR_SRC_REG 0x20
53 #define EP_INTR_SRC_SET_REG 0x24
54 #define EP_INTR_SRC_CLEAR_REG 0x28
55 #define EP_INTR_MASK_REG 0x2c
56 #define EP_INTR_MASK_SET_REG 0x30
57 #define EP_INTR_MASK_CLEAR_REG 0x34
58 #define EP_INTR_SRC_MASKED_REG 0x38
59 #define CORE_INTR_SRC_REG 0x40
60 #define CORE_INTR_SRC_SET_REG 0x44
61 #define CORE_INTR_SRC_CLEAR_REG 0x48
62 #define CORE_INTR_MASK_REG 0x4c
63 #define CORE_INTR_MASK_SET_REG 0x50
64 #define CORE_INTR_MASK_CLEAR_REG 0x54
65 #define CORE_INTR_SRC_MASKED_REG 0x58
66 /* 0x5c Reserved */
67 #define USB_END_OF_INTR_REG 0x60
69 /* Control register bits */
70 #define AM35X_SOFT_RESET_MASK 1
72 /* USB interrupt register bits */
73 #define AM35X_INTR_USB_SHIFT 16
74 #define AM35X_INTR_USB_MASK (0x1ff << AM35X_INTR_USB_SHIFT)
75 #define AM35X_INTR_DRVVBUS 0x100
76 #define AM35X_INTR_RX_SHIFT 16
77 #define AM35X_INTR_TX_SHIFT 0
78 #define AM35X_TX_EP_MASK 0xffff /* EP0 + 15 Tx EPs */
79 #define AM35X_RX_EP_MASK 0xfffe /* 15 Rx EPs */
80 #define AM35X_TX_INTR_MASK (AM35X_TX_EP_MASK << AM35X_INTR_TX_SHIFT)
81 #define AM35X_RX_INTR_MASK (AM35X_RX_EP_MASK << AM35X_INTR_RX_SHIFT)
83 #define USB_MENTOR_CORE_OFFSET 0x400
85 struct am35x_glue {
86 struct device *dev;
87 struct platform_device *musb;
88 struct clk *phy_clk;
89 struct clk *clk;
90 };
91 #define glue_to_musb(g) platform_get_drvdata(g->musb)
93 /*
94 * am35x_musb_enable - enable interrupts
95 */
96 static void am35x_musb_enable(struct musb *musb)
97 {
98 void __iomem *reg_base = musb->ctrl_base;
99 u32 epmask;
101 /* Workaround: setup IRQs through both register sets. */
102 epmask = ((musb->epmask & AM35X_TX_EP_MASK) << AM35X_INTR_TX_SHIFT) |
103 ((musb->epmask & AM35X_RX_EP_MASK) << AM35X_INTR_RX_SHIFT);
105 musb_writel(reg_base, EP_INTR_MASK_SET_REG, epmask);
106 musb_writel(reg_base, CORE_INTR_MASK_SET_REG, AM35X_INTR_USB_MASK);
108 /* Force the DRVVBUS IRQ so we can start polling for ID change. */
109 if (is_otg_enabled(musb))
110 musb_writel(reg_base, CORE_INTR_SRC_SET_REG,
111 AM35X_INTR_DRVVBUS << AM35X_INTR_USB_SHIFT);
112 }
114 /*
115 * am35x_musb_disable - disable HDRC and flush interrupts
116 */
117 static void am35x_musb_disable(struct musb *musb)
118 {
119 void __iomem *reg_base = musb->ctrl_base;
121 musb_writel(reg_base, CORE_INTR_MASK_CLEAR_REG, AM35X_INTR_USB_MASK);
122 musb_writel(reg_base, EP_INTR_MASK_CLEAR_REG,
123 AM35X_TX_INTR_MASK | AM35X_RX_INTR_MASK);
124 musb_writeb(musb->mregs, MUSB_DEVCTL, 0);
125 musb_writel(reg_base, USB_END_OF_INTR_REG, 0);
126 }
128 #define portstate(stmt) stmt
130 static void am35x_musb_set_vbus(struct musb *musb, int is_on)
131 {
132 WARN_ON(is_on && is_peripheral_active(musb));
133 }
135 #define POLL_SECONDS 2
137 static struct timer_list otg_workaround;
139 static void otg_timer(unsigned long _musb)
140 {
141 struct musb *musb = (void *)_musb;
142 void __iomem *mregs = musb->mregs;
143 u8 devctl;
144 unsigned long flags;
146 /*
147 * We poll because AM35x's won't expose several OTG-critical
148 * status change events (from the transceiver) otherwise.
149 */
150 devctl = musb_readb(mregs, MUSB_DEVCTL);
151 dev_dbg(musb->controller, "Poll devctl %02x (%s)\n", devctl,
152 otg_state_string(musb->xceiv->state));
154 spin_lock_irqsave(&musb->lock, flags);
155 switch (musb->xceiv->state) {
156 case OTG_STATE_A_WAIT_BCON:
157 devctl &= ~MUSB_DEVCTL_SESSION;
158 musb_writeb(musb->mregs, MUSB_DEVCTL, devctl);
160 devctl = musb_readb(musb->mregs, MUSB_DEVCTL);
161 if (devctl & MUSB_DEVCTL_BDEVICE) {
162 musb->xceiv->state = OTG_STATE_B_IDLE;
163 MUSB_DEV_MODE(musb);
164 } else {
165 musb->xceiv->state = OTG_STATE_A_IDLE;
166 MUSB_HST_MODE(musb);
167 }
168 break;
169 case OTG_STATE_A_WAIT_VFALL:
170 musb->xceiv->state = OTG_STATE_A_WAIT_VRISE;
171 musb_writel(musb->ctrl_base, CORE_INTR_SRC_SET_REG,
172 MUSB_INTR_VBUSERROR << AM35X_INTR_USB_SHIFT);
173 break;
174 case OTG_STATE_B_IDLE:
175 if (!is_peripheral_enabled(musb))
176 break;
178 devctl = musb_readb(mregs, MUSB_DEVCTL);
179 if (devctl & MUSB_DEVCTL_BDEVICE)
180 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
181 else
182 musb->xceiv->state = OTG_STATE_A_IDLE;
183 break;
184 default:
185 break;
186 }
187 spin_unlock_irqrestore(&musb->lock, flags);
188 }
190 static void am35x_musb_try_idle(struct musb *musb, unsigned long timeout)
191 {
192 static unsigned long last_timer;
194 if (!is_otg_enabled(musb))
195 return;
197 if (timeout == 0)
198 timeout = jiffies + msecs_to_jiffies(3);
200 /* Never idle if active, or when VBUS timeout is not set as host */
201 if (musb->is_active || (musb->a_wait_bcon == 0 &&
202 musb->xceiv->state == OTG_STATE_A_WAIT_BCON)) {
203 dev_dbg(musb->controller, "%s active, deleting timer\n",
204 otg_state_string(musb->xceiv->state));
205 del_timer(&otg_workaround);
206 last_timer = jiffies;
207 return;
208 }
210 if (time_after(last_timer, timeout) && timer_pending(&otg_workaround)) {
211 dev_dbg(musb->controller, "Longer idle timer already pending, ignoring...\n");
212 return;
213 }
214 last_timer = timeout;
216 dev_dbg(musb->controller, "%s inactive, starting idle timer for %u ms\n",
217 otg_state_string(musb->xceiv->state),
218 jiffies_to_msecs(timeout - jiffies));
219 mod_timer(&otg_workaround, timeout);
220 }
222 static irqreturn_t am35x_musb_interrupt(int irq, void *hci)
223 {
224 struct musb *musb = hci;
225 void __iomem *reg_base = musb->ctrl_base;
226 struct device *dev = musb->controller;
227 struct musb_hdrc_platform_data *plat = dev->platform_data;
228 struct omap_musb_board_data *data = plat->board_data;
229 unsigned long flags;
230 irqreturn_t ret = IRQ_NONE;
231 u32 epintr, usbintr;
233 spin_lock_irqsave(&musb->lock, flags);
235 /* Get endpoint interrupts */
236 epintr = musb_readl(reg_base, EP_INTR_SRC_MASKED_REG);
238 if (epintr) {
239 musb_writel(reg_base, EP_INTR_SRC_CLEAR_REG, epintr);
241 musb->int_rx =
242 (epintr & AM35X_RX_INTR_MASK) >> AM35X_INTR_RX_SHIFT;
243 musb->int_tx =
244 (epintr & AM35X_TX_INTR_MASK) >> AM35X_INTR_TX_SHIFT;
245 }
247 /* Get usb core interrupts */
248 usbintr = musb_readl(reg_base, CORE_INTR_SRC_MASKED_REG);
249 if (!usbintr && !epintr)
250 goto eoi;
252 if (usbintr) {
253 musb_writel(reg_base, CORE_INTR_SRC_CLEAR_REG, usbintr);
255 musb->int_usb =
256 (usbintr & AM35X_INTR_USB_MASK) >> AM35X_INTR_USB_SHIFT;
257 }
258 /*
259 * DRVVBUS IRQs are the only proxy we have (a very poor one!) for
260 * AM35x's missing ID change IRQ. We need an ID change IRQ to
261 * switch appropriately between halves of the OTG state machine.
262 * Managing DEVCTL.SESSION per Mentor docs requires that we know its
263 * value but DEVCTL.BDEVICE is invalid without DEVCTL.SESSION set.
264 * Also, DRVVBUS pulses for SRP (but not at 5V) ...
265 */
266 if (usbintr & (AM35X_INTR_DRVVBUS << AM35X_INTR_USB_SHIFT)) {
267 int drvvbus = musb_readl(reg_base, USB_STAT_REG);
268 void __iomem *mregs = musb->mregs;
269 u8 devctl = musb_readb(mregs, MUSB_DEVCTL);
270 int err;
272 err = is_host_enabled(musb) && (musb->int_usb &
273 MUSB_INTR_VBUSERROR);
274 if (err) {
275 /*
276 * The Mentor core doesn't debounce VBUS as needed
277 * to cope with device connect current spikes. This
278 * means it's not uncommon for bus-powered devices
279 * to get VBUS errors during enumeration.
280 *
281 * This is a workaround, but newer RTL from Mentor
282 * seems to allow a better one: "re"-starting sessions
283 * without waiting for VBUS to stop registering in
284 * devctl.
285 */
286 musb->int_usb &= ~MUSB_INTR_VBUSERROR;
287 musb->xceiv->state = OTG_STATE_A_WAIT_VFALL;
288 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
289 WARNING("VBUS error workaround (delay coming)\n");
290 } else if (is_host_enabled(musb) && drvvbus) {
291 MUSB_HST_MODE(musb);
292 musb->xceiv->default_a = 1;
293 musb->xceiv->state = OTG_STATE_A_WAIT_VRISE;
294 portstate(musb->port1_status |= USB_PORT_STAT_POWER);
295 del_timer(&otg_workaround);
296 } else {
297 musb->is_active = 0;
298 MUSB_DEV_MODE(musb);
299 musb->xceiv->default_a = 0;
300 musb->xceiv->state = OTG_STATE_B_IDLE;
301 portstate(musb->port1_status &= ~USB_PORT_STAT_POWER);
302 }
304 /* NOTE: this must complete power-on within 100 ms. */
305 dev_dbg(musb->controller, "VBUS %s (%s)%s, devctl %02x\n",
306 drvvbus ? "on" : "off",
307 otg_state_string(musb->xceiv->state),
308 err ? " ERROR" : "",
309 devctl);
310 ret = IRQ_HANDLED;
311 }
313 if (musb->int_tx || musb->int_rx || musb->int_usb)
314 ret |= musb_interrupt(musb);
316 eoi:
317 /* EOI needs to be written for the IRQ to be re-asserted. */
318 if (ret == IRQ_HANDLED || epintr || usbintr) {
319 /* clear level interrupt */
320 if (data->clear_irq)
321 data->clear_irq();
322 /* write EOI */
323 musb_writel(reg_base, USB_END_OF_INTR_REG, 0);
324 }
326 /* Poll for ID change */
327 if (is_otg_enabled(musb) && musb->xceiv->state == OTG_STATE_B_IDLE)
328 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
330 spin_unlock_irqrestore(&musb->lock, flags);
332 return ret;
333 }
335 static int am35x_musb_set_mode(struct musb *musb, u8 musb_mode)
336 {
337 struct device *dev = musb->controller;
338 struct musb_hdrc_platform_data *plat = dev->platform_data;
339 struct omap_musb_board_data *data = plat->board_data;
340 int retval = 0;
342 if (data->set_mode)
343 data->set_mode(musb_mode);
344 else
345 retval = -EIO;
347 return retval;
348 }
350 static int am35x_musb_init(struct musb *musb)
351 {
352 struct device *dev = musb->controller;
353 struct musb_hdrc_platform_data *plat = dev->platform_data;
354 struct omap_musb_board_data *data = plat->board_data;
355 void __iomem *reg_base = musb->ctrl_base;
356 u32 rev;
358 musb->mregs += USB_MENTOR_CORE_OFFSET;
360 /* Returns zero if e.g. not clocked */
361 rev = musb_readl(reg_base, USB_REVISION_REG);
362 if (!rev)
363 return -ENODEV;
365 usb_nop_xceiv_register();
366 musb->xceiv = otg_get_transceiver();
367 if (!musb->xceiv)
368 return -ENODEV;
370 if (is_host_enabled(musb))
371 setup_timer(&otg_workaround, otg_timer, (unsigned long) musb);
373 /* Reset the musb */
374 if (data->reset)
375 data->reset();
377 /* Reset the controller */
378 musb_writel(reg_base, USB_CTRL_REG, AM35X_SOFT_RESET_MASK);
380 /* Start the on-chip PHY and its PLL. */
381 if (data->set_phy_power)
382 data->set_phy_power(1);
384 msleep(5);
386 musb->isr = am35x_musb_interrupt;
388 /* clear level interrupt */
389 if (data->clear_irq)
390 data->clear_irq();
392 return 0;
393 }
395 static int am35x_musb_exit(struct musb *musb)
396 {
397 struct device *dev = musb->controller;
398 struct musb_hdrc_platform_data *plat = dev->platform_data;
399 struct omap_musb_board_data *data = plat->board_data;
401 if (is_host_enabled(musb))
402 del_timer_sync(&otg_workaround);
404 /* Shutdown the on-chip PHY and its PLL. */
405 if (data->set_phy_power)
406 data->set_phy_power(0);
408 otg_put_transceiver(musb->xceiv);
409 usb_nop_xceiv_unregister();
411 return 0;
412 }
414 /* AM35x supports only 32bit read operation */
415 static void am35x_musb_read_fifo(struct musb_hw_ep *hw_ep, u16 len, u8 *dst)
416 {
417 void __iomem *fifo = hw_ep->fifo;
418 u32 val;
419 int i;
421 /* Read for 32bit-aligned destination address */
422 if (likely((0x03 & (unsigned long) dst) == 0) && len >= 4) {
423 readsl(fifo, dst, len >> 2);
424 dst += len & ~0x03;
425 len &= 0x03;
426 }
427 /*
428 * Now read the remaining 1 to 3 byte or complete length if
429 * unaligned address.
430 */
431 if (len > 4) {
432 for (i = 0; i < (len >> 2); i++) {
433 *(u32 *) dst = musb_readl(fifo, 0);
434 dst += 4;
435 }
436 len &= 0x03;
437 }
438 if (len > 0) {
439 val = musb_readl(fifo, 0);
440 memcpy(dst, &val, len);
441 }
442 }
444 static const struct musb_platform_ops am35x_ops = {
445 .fifo_mode = 4,
446 .flags = MUSB_GLUE_EP_ADDR_FLAT_MAPPING,
447 .init = am35x_musb_init,
448 .exit = am35x_musb_exit,
450 .enable = am35x_musb_enable,
451 .disable = am35x_musb_disable,
453 .set_mode = am35x_musb_set_mode,
454 .try_idle = am35x_musb_try_idle,
456 .set_vbus = am35x_musb_set_vbus,
458 .read_fifo = am35x_musb_read_fifo,
459 .write_fifo = musb_write_fifo,
460 };
462 static u64 am35x_dmamask = DMA_BIT_MASK(32);
464 static int __init am35x_probe(struct platform_device *pdev)
465 {
466 struct musb_hdrc_platform_data *pdata = pdev->dev.platform_data;
467 struct platform_device *musb;
468 struct am35x_glue *glue;
470 struct clk *phy_clk;
471 struct clk *clk;
473 int ret = -ENOMEM;
475 glue = kzalloc(sizeof(*glue), GFP_KERNEL);
476 if (!glue) {
477 dev_err(&pdev->dev, "failed to allocate glue context\n");
478 goto err0;
479 }
481 musb = platform_device_alloc("musb-hdrc", -1);
482 if (!musb) {
483 dev_err(&pdev->dev, "failed to allocate musb device\n");
484 goto err1;
485 }
487 phy_clk = clk_get(&pdev->dev, "fck");
488 if (IS_ERR(phy_clk)) {
489 dev_err(&pdev->dev, "failed to get PHY clock\n");
490 ret = PTR_ERR(phy_clk);
491 goto err2;
492 }
494 clk = clk_get(&pdev->dev, "ick");
495 if (IS_ERR(clk)) {
496 dev_err(&pdev->dev, "failed to get clock\n");
497 ret = PTR_ERR(clk);
498 goto err3;
499 }
501 ret = clk_enable(phy_clk);
502 if (ret) {
503 dev_err(&pdev->dev, "failed to enable PHY clock\n");
504 goto err4;
505 }
507 ret = clk_enable(clk);
508 if (ret) {
509 dev_err(&pdev->dev, "failed to enable clock\n");
510 goto err5;
511 }
513 musb->dev.parent = &pdev->dev;
514 musb->dev.dma_mask = &am35x_dmamask;
515 musb->dev.coherent_dma_mask = am35x_dmamask;
517 glue->dev = &pdev->dev;
518 glue->musb = musb;
519 glue->phy_clk = phy_clk;
520 glue->clk = clk;
522 pdata->platform_ops = &am35x_ops;
524 platform_set_drvdata(pdev, glue);
526 ret = platform_device_add_resources(musb, pdev->resource,
527 pdev->num_resources);
528 if (ret) {
529 dev_err(&pdev->dev, "failed to add resources\n");
530 goto err6;
531 }
533 ret = platform_device_add_data(musb, pdata, sizeof(*pdata));
534 if (ret) {
535 dev_err(&pdev->dev, "failed to add platform_data\n");
536 goto err6;
537 }
539 ret = platform_device_add(musb);
540 if (ret) {
541 dev_err(&pdev->dev, "failed to register musb device\n");
542 goto err6;
543 }
545 return 0;
547 err6:
548 clk_disable(clk);
550 err5:
551 clk_disable(phy_clk);
553 err4:
554 clk_put(clk);
556 err3:
557 clk_put(phy_clk);
559 err2:
560 platform_device_put(musb);
562 err1:
563 kfree(glue);
565 err0:
566 return ret;
567 }
569 static int __exit am35x_remove(struct platform_device *pdev)
570 {
571 struct am35x_glue *glue = platform_get_drvdata(pdev);
573 platform_device_del(glue->musb);
574 platform_device_put(glue->musb);
575 clk_disable(glue->clk);
576 clk_disable(glue->phy_clk);
577 clk_put(glue->clk);
578 clk_put(glue->phy_clk);
579 kfree(glue);
581 return 0;
582 }
584 #ifdef CONFIG_PM
585 static int am35x_suspend(struct device *dev)
586 {
587 struct am35x_glue *glue = dev_get_drvdata(dev);
588 struct musb_hdrc_platform_data *plat = dev->platform_data;
589 struct omap_musb_board_data *data = plat->board_data;
591 /* Shutdown the on-chip PHY and its PLL. */
592 if (data->set_phy_power)
593 data->set_phy_power(0);
595 clk_disable(glue->phy_clk);
596 clk_disable(glue->clk);
598 return 0;
599 }
601 static int am35x_resume(struct device *dev)
602 {
603 struct am35x_glue *glue = dev_get_drvdata(dev);
604 struct musb_hdrc_platform_data *plat = dev->platform_data;
605 struct omap_musb_board_data *data = plat->board_data;
606 int ret;
608 /* Start the on-chip PHY and its PLL. */
609 if (data->set_phy_power)
610 data->set_phy_power(1);
612 ret = clk_enable(glue->phy_clk);
613 if (ret) {
614 dev_err(dev, "failed to enable PHY clock\n");
615 return ret;
616 }
618 ret = clk_enable(glue->clk);
619 if (ret) {
620 dev_err(dev, "failed to enable clock\n");
621 return ret;
622 }
624 return 0;
625 }
627 static struct dev_pm_ops am35x_pm_ops = {
628 .suspend = am35x_suspend,
629 .resume = am35x_resume,
630 };
632 #define DEV_PM_OPS &am35x_pm_ops
633 #else
634 #define DEV_PM_OPS NULL
635 #endif
637 static struct platform_driver am35x_driver = {
638 .remove = __exit_p(am35x_remove),
639 .driver = {
640 .name = "musb-am35x",
641 .pm = DEV_PM_OPS,
642 },
643 };
645 MODULE_DESCRIPTION("AM35x MUSB Glue Layer");
646 MODULE_AUTHOR("Ajay Kumar Gupta <ajay.gupta@ti.com>");
647 MODULE_LICENSE("GPL v2");
649 static int __init am35x_init(void)
650 {
651 return platform_driver_probe(&am35x_driver, am35x_probe);
652 }
653 subsys_initcall(am35x_init);
655 static void __exit am35x_exit(void)
656 {
657 platform_driver_unregister(&am35x_driver);
658 }
659 module_exit(am35x_exit);