]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - drivers/usb/musb/cppi41.c
musb: adding support for am335x
[sitara-epos/sitara-epos-kernel.git] / drivers / usb / musb / cppi41.c
1 /*
2  * CPPI 4.1 support
3  *
4  * Copyright (C) 2008-2009 MontaVista Software, Inc. <source@mvista.com>
5  *
6  * Based on the PAL CPPI 4.1 implementation
7  * Copyright (C) 1998-2006 Texas Instruments Incorporated
8  *
9  * This file contains the main implementation for CPPI 4.1 common peripherals,
10  * including the DMA Controllers and the Queue Managers.
11  *
12  * This program is free software; you can distribute it and/or modify it
13  * under the terms of the GNU General Public License (Version 2) as
14  * published by the Free Software Foundation.
15  *
16  * This program is distributed in the hope it will be useful, but WITHOUT
17  * ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or
18  * FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License
19  * for more details.
20  *
21  * You should have received a copy of the GNU General Public License along
22  * with this program; if not, write to the Free Software Foundation, Inc.,
23  * 59 Temple Place - Suite 330, Boston MA 02111-1307, USA.
24  *
25  */
27 #include <linux/io.h>
28 #include <linux/init.h>
29 #include <linux/slab.h>
30 #include <linux/module.h>
31 #include <linux/dma-mapping.h>
33 #include "cppi41.h"
35 #undef  CPPI41_DEBUG
37 #ifdef  CPPI41_DEBUG
38 #define DBG(format, args...) printk(format, ##args)
39 #else
40 #define DBG(format, args...)
41 #endif
43 static struct {
44         void *virt_addr;
45         dma_addr_t phys_addr;
46         u32     size;
47 } linking_ram[CPPI41_NUM_QUEUE_MGR];
49 static u32 *allocated_queues[CPPI41_NUM_QUEUE_MGR];
51 /* First 32 packet descriptors are reserved for unallocated memory regions. */
52 static u32 next_desc_index[CPPI41_NUM_QUEUE_MGR] = { 1 << 5 };
53 static u8  next_mem_rgn[CPPI41_NUM_QUEUE_MGR];
55 static struct {
56         size_t rgn_size;
57         void *virt_addr;
58         dma_addr_t phys_addr;
59         struct cppi41_queue_obj queue_obj;
60         u8 mem_rgn;
61         u16 q_mgr;
62         u16 q_num;
63         u32 num_desc;
64 } dma_teardown[CPPI41_NUM_DMA_BLOCK];
66 struct cppi41_dma_sched_tbl_t {
67         u8      pos;
68         u8      dma_ch;
69         u8      is_tx;
70         u8      enb;
71 };
73 struct cppi41_dma_sched_tbl_t dma_sched_tbl[MAX_SCHED_TBL_ENTRY] = {
74         /*pos  dma_ch#  is_tx  enb/dis*/
75         { 0,    0,      0,      1},
76         { 1,    0,      1,      1},
77         { 2,    1,      0,      1},
78         { 3,    1,      1,      1},
79         { 4,    2,      0,      1},
80         { 5,    2,      1,      1},
81         { 6,    3,      0,      1},
82         { 7,    3,      1,      1}
83 };
85 struct cppi41_queue_mgr cppi41_queue_mgr[CPPI41_NUM_QUEUE_MGR];
86 EXPORT_SYMBOL(cppi41_queue_mgr);
88 struct cppi41_dma_block cppi41_dma_block[CPPI41_NUM_DMA_BLOCK];
89 EXPORT_SYMBOL(cppi41_dma_block);
90 /******************** CPPI 4.1 Functions (External Interface) *****************/
92 int cppi41_queue_mgr_init(u8 q_mgr, dma_addr_t rgn0_base, u16 rgn0_size)
93 {
94         void __iomem *q_mgr_regs;
95         void *ptr;
97         if (q_mgr >= cppi41_num_queue_mgr)
98                 return -EINVAL;
100         q_mgr_regs = cppi41_queue_mgr[q_mgr].q_mgr_rgn_base;
101         ptr = dma_alloc_coherent(NULL, rgn0_size * 4,
102                                  &linking_ram[q_mgr].phys_addr,
103                                  GFP_KERNEL | GFP_DMA);
104         if (ptr == NULL) {
105                 printk(KERN_ERR "ERROR: %s: Unable to allocate "
106                        "linking RAM.\n", __func__);
107                 return -ENOMEM;
108         }
109         linking_ram[q_mgr].virt_addr = ptr;
110         linking_ram[q_mgr].size = rgn0_size * 4;
112         __raw_writel(linking_ram[q_mgr].phys_addr,
113                         q_mgr_regs + QMGR_LINKING_RAM_RGN0_BASE_REG);
114         DBG("Linking RAM region 0 base @ %p, value: %x\n",
115             q_mgr_regs + QMGR_LINKING_RAM_RGN0_BASE_REG,
116             __raw_readl(q_mgr_regs + QMGR_LINKING_RAM_RGN0_BASE_REG));
118         __raw_writel(rgn0_size, q_mgr_regs + QMGR_LINKING_RAM_RGN0_SIZE_REG);
119         DBG("Linking RAM region 0 size @ %p, value: %x\n",
120             q_mgr_regs + QMGR_LINKING_RAM_RGN0_SIZE_REG,
121             __raw_readl(q_mgr_regs + QMGR_LINKING_RAM_RGN0_SIZE_REG));
123         ptr = kzalloc(BITS_TO_LONGS(cppi41_queue_mgr[q_mgr].num_queue),
124                       GFP_KERNEL);
125         if (ptr == NULL) {
126                 printk(KERN_ERR "ERROR: %s: Unable to allocate queue bitmap.\n",
127                        __func__);
128                 dma_free_coherent(NULL, rgn0_size * 4,
129                                   linking_ram[q_mgr].virt_addr,
130                                   linking_ram[q_mgr].phys_addr);
131                 return -ENOMEM;
132         }
133         allocated_queues[q_mgr] = ptr;
135         return 0;
137 EXPORT_SYMBOL(cppi41_queue_mgr_init);
139 int cppi41_queue_mgr_uninit(u8 q_mgr)
141         void __iomem *q_mgr_regs;
143         if (q_mgr >= cppi41_num_queue_mgr)
144                 return -EINVAL;
146         q_mgr_regs = cppi41_queue_mgr[q_mgr].q_mgr_rgn_base;
148         /* free the Queue Mgr linking ram space */
149         __raw_writel(0, q_mgr_regs + QMGR_LINKING_RAM_RGN0_BASE_REG);
150         __raw_writel(0, q_mgr_regs + QMGR_LINKING_RAM_RGN0_SIZE_REG);
151         dma_free_coherent(NULL, linking_ram[q_mgr].size,
152                         linking_ram[q_mgr].virt_addr,
153                         linking_ram[q_mgr].phys_addr);
155         /* free the allocated queues */
156         kfree(allocated_queues[q_mgr]);
157         return 0;
159 EXPORT_SYMBOL(cppi41_queue_mgr_uninit);
161 int cppi41_dma_sched_tbl_init(u8 dma_num, u8 q_mgr,
162                         u32 *sched_tbl, u8 tbl_size)
164         struct cppi41_dma_block *dma_block;
165         int num_reg, k, i, val = 0;
167         dma_block = (struct cppi41_dma_block *)&cppi41_dma_block[dma_num];
169         num_reg = (tbl_size + 3) / 4;
170         for (k = i = 0; i < num_reg; i++) {
171 #if 0
172                 for (val = j = 0; j < 4; j++, k++) {
173                         val >>= 8;
174                         if (k < tbl_size)
175                                 val |= sched_tbl[k] << 24;
176                 }
177 #endif
178                 val = sched_tbl[i];
179                 __raw_writel(val, dma_block->sched_table_base +
180                         DMA_SCHED_TABLE_WORD_REG(i));
181                 DBG("DMA scheduler table @ %p, value written: %x\n",
182                 dma_block->sched_table_base + DMA_SCHED_TABLE_WORD_REG(i),
183                         val);
184         }
185         return 0;
187 EXPORT_SYMBOL(cppi41_dma_sched_tbl_init);
189 int cppi41_schedtbl_add_dma_ch(u8 dmanum, u8 qmgr, u8 dma_ch, u8 is_tx)
191         struct cppi41_dma_block *dma_block;
192         int num_ch, i, tbl_index = 0, j = 0, found = 0;
193         u32 val;
195         dma_block = (struct cppi41_dma_block *)&cppi41_dma_block[dmanum];
197         val = 0;
198         for (num_ch = 0, i = 0; i < MAX_SCHED_TBL_ENTRY; i++) {
199                 if (!found && dma_sched_tbl[i].dma_ch == dma_ch &&
200                         dma_sched_tbl[i].is_tx == is_tx &&
201                         dma_sched_tbl[i].enb == 0) {
202                         dma_sched_tbl[i].enb = 1;
203                         found = 1;
204                 }
206                 if (dma_sched_tbl[i].enb) {
207                         val |= ((dma_sched_tbl[i].dma_ch |
208                                 (dma_sched_tbl[i].is_tx ? 0 : (1<<7))) << j*8);
209                         num_ch++;
210                         j++;
211                 }
212                 if (num_ch % 4 == 0) {
213                         __raw_writel(val, dma_block->sched_table_base +
214                                 DMA_SCHED_TABLE_WORD_REG(tbl_index));
215                         tbl_index++;
216                         val = j = 0;
217                 }
218         }
220         if (num_ch % 4) {
221                 __raw_writel(val, dma_block->sched_table_base +
222                         DMA_SCHED_TABLE_WORD_REG(tbl_index));
223         }
224         return num_ch;
226 EXPORT_SYMBOL(cppi41_schedtbl_add_dma_ch);
228 int cppi41_schedtbl_remove_dma_ch(u8 dmanum, u8 qmgr, u8 dma_ch, u8 is_tx)
230         struct cppi41_dma_block *dma_block;
231         int num_ch, i, tbl_index = 0, j = 0, found = 0;
232         u32 val;
234         dma_block = (struct cppi41_dma_block *)&cppi41_dma_block[dmanum];
236         val = 0;
237         for (num_ch = 0, i = 0; i < MAX_SCHED_TBL_ENTRY; i++) {
238                 if (!found && dma_sched_tbl[i].dma_ch == dma_ch &&
239                         dma_sched_tbl[i].is_tx == is_tx &&
240                         dma_sched_tbl[i].enb == 1) {
241                         dma_sched_tbl[i].enb = 0;
242                 }
244                 if (dma_sched_tbl[i].enb) {
245                         val |= ((dma_sched_tbl[i].dma_ch |
246                                 (dma_sched_tbl[i].is_tx ? 0 : (1<<7))) << j*8);
247                         num_ch++;
248                         j++;
249                 }
250                 if (num_ch % 4 == 0) {
251                         __raw_writel(val, dma_block->sched_table_base +
252                                 DMA_SCHED_TABLE_WORD_REG(tbl_index));
253                         tbl_index++;
254                         val = j = 0;
255                 }
256         }
258         if (num_ch % 4) {
259                 __raw_writel(val, dma_block->sched_table_base +
260                         DMA_SCHED_TABLE_WORD_REG(tbl_index));
261         }
262         return num_ch;
264 EXPORT_SYMBOL(cppi41_schedtbl_remove_dma_ch);
266 int cppi41_dma_block_init(u8 dma_num, u8 q_mgr, u8 num_order,
267                                  u32 *sched_tbl, u8 tbl_size)
269         const struct cppi41_dma_block *dma_block;
270         struct cppi41_teardown_desc *curr_td;
271         dma_addr_t td_addr;
272         unsigned num_desc, num_reg;
273         void *ptr;
274         int error, i;
275         u16 q_num;
276         u32 val;
278         if (dma_num >= cppi41_num_dma_block ||
279             q_mgr >= cppi41_num_queue_mgr ||
280             !tbl_size || sched_tbl == NULL)
281                 return -EINVAL;
283         error = cppi41_queue_alloc(CPPI41_FREE_DESC_QUEUE |
284                                    CPPI41_UNASSIGNED_QUEUE, q_mgr, &q_num);
285         if (error) {
286                 printk(KERN_ERR "ERROR: %s: Unable to allocate teardown "
287                        "descriptor queue.\n", __func__);
288                 return error;
289         }
290         DBG("Teardown descriptor queue %d in queue manager 0 "
291             "allocated\n", q_num);
293         /*
294          * Tell the hardware about the Teardown descriptor
295          * queue manager and queue number.
296          */
297         dma_block = &cppi41_dma_block[dma_num];
298         __raw_writel((q_mgr << DMA_TD_DESC_QMGR_SHIFT) |
299                      (q_num << DMA_TD_DESC_QNUM_SHIFT),
300                      dma_block->global_ctrl_base +
301                      DMA_TEARDOWN_FREE_DESC_CTRL_REG);
302         DBG("Teardown free descriptor control @ %p, value: %x\n",
303             dma_block->global_ctrl_base + DMA_TEARDOWN_FREE_DESC_CTRL_REG,
304             __raw_readl(dma_block->global_ctrl_base +
305                         DMA_TEARDOWN_FREE_DESC_CTRL_REG));
307         num_desc = 1 << num_order;
308         dma_teardown[dma_num].rgn_size = num_desc *
309                                          sizeof(struct cppi41_teardown_desc);
311         /* Pre-allocate teardown descriptors. */
312         ptr = dma_alloc_coherent(NULL, dma_teardown[dma_num].rgn_size,
313                                  &dma_teardown[dma_num].phys_addr,
314                                  GFP_KERNEL | GFP_DMA);
315         if (ptr == NULL) {
316                 printk(KERN_ERR "ERROR: %s: Unable to allocate teardown "
317                        "descriptors.\n", __func__);
318                 error = -ENOMEM;
319                 goto free_queue;
320         }
321         dma_teardown[dma_num].virt_addr = ptr;
323         error = cppi41_mem_rgn_alloc(q_mgr, dma_teardown[dma_num].phys_addr, 5,
324                                      num_order, &dma_teardown[dma_num].mem_rgn);
325         if (error) {
326                 printk(KERN_ERR "ERROR: %s: Unable to allocate queue manager "
327                        "memory region for teardown descriptors.\n", __func__);
328                 goto free_mem;
329         }
331         error = cppi41_queue_init(&dma_teardown[dma_num].queue_obj, 0, q_num);
332         if (error) {
333                 printk(KERN_ERR "ERROR: %s: Unable to initialize teardown "
334                        "free descriptor queue.\n", __func__);
335                 goto free_rgn;
336         }
338         dma_teardown[dma_num].q_num = q_num;
339         dma_teardown[dma_num].q_mgr = q_mgr;
340         /*
341          * Push all teardown descriptors to the free teardown queue
342          * for the CPPI 4.1 system.
343          */
344         curr_td = dma_teardown[dma_num].virt_addr;
345         td_addr = dma_teardown[dma_num].phys_addr;
347         for (i = 0; i < num_desc; i++) {
348                 cppi41_queue_push(&dma_teardown[dma_num].queue_obj, td_addr,
349                                   sizeof(*curr_td), 0);
350                 td_addr += sizeof(*curr_td);
351         }
352         dma_teardown[dma_num].num_desc = num_desc;
354         /* Initialize the DMA scheduler. */
355         num_reg = (tbl_size + 3) / 4;
356         for (i = 0; i < num_reg; i++) {
357                 val = sched_tbl[i];
358                 __raw_writel(val, dma_block->sched_table_base +
359                              DMA_SCHED_TABLE_WORD_REG(i));
360                 DBG("DMA scheduler table @ %p, value written: %x\n",
361                     dma_block->sched_table_base + DMA_SCHED_TABLE_WORD_REG(i),
362                     val);
363         }
365         __raw_writel((tbl_size - 1) << DMA_SCHED_LAST_ENTRY_SHIFT |
366                      DMA_SCHED_ENABLE_MASK,
367                      dma_block->sched_ctrl_base + DMA_SCHED_CTRL_REG);
368         DBG("DMA scheduler control @ %p, value: %x\n",
369             dma_block->sched_ctrl_base + DMA_SCHED_CTRL_REG,
370             __raw_readl(dma_block->sched_ctrl_base + DMA_SCHED_CTRL_REG));
372         return 0;
374 free_rgn:
375         cppi41_mem_rgn_free(q_mgr, dma_teardown[dma_num].mem_rgn);
376 free_mem:
377         dma_free_coherent(NULL, dma_teardown[dma_num].rgn_size,
378                           dma_teardown[dma_num].virt_addr,
379                           dma_teardown[dma_num].phys_addr);
380 free_queue:
381         cppi41_queue_free(q_mgr, q_num);
382         return error;
384 EXPORT_SYMBOL(cppi41_dma_block_init);
386 int cppi41_dma_block_uninit(u8 dma_num, u8 q_mgr, u8 num_order,
387                                  u32 *sched_tbl, u8 tbl_size)
389         const struct cppi41_dma_block *dma_block;
390         unsigned num_reg;
391         int i;
393         /* popout all teardown descriptors */
394         cppi41_free_teardown_queue(dma_num);
396         /* free queue mgr region */
397         cppi41_mem_rgn_free(q_mgr, dma_teardown[dma_num].mem_rgn);
398         /* free the allocated teardown descriptors */
399         dma_free_coherent(NULL, dma_teardown[dma_num].rgn_size,
400                         dma_teardown[dma_num].virt_addr,
401                         dma_teardown[dma_num].phys_addr);
403         /* free the teardown queue*/
404         cppi41_queue_free(dma_teardown[dma_num].q_mgr,
405                         dma_teardown[dma_num].q_num);
407         dma_block = (struct cppi41_dma_block *)&cppi41_dma_block[dma_num];
408         /* disable the dma schedular */
409         num_reg = (tbl_size + 3) / 4;
410         for (i = 0; i < num_reg; i++) {
411                 __raw_writel(0, dma_block->sched_table_base +
412                              DMA_SCHED_TABLE_WORD_REG(i));
413                 DBG("DMA scheduler table @ %p, value written: %x\n",
414                     dma_block->sched_table_base + DMA_SCHED_TABLE_WORD_REG(i),
415                     0);
416         }
418         __raw_writel(0, dma_block->sched_ctrl_base + DMA_SCHED_CTRL_REG);
420         return 0;
422 EXPORT_SYMBOL(cppi41_dma_block_uninit);
423 /*
424  * cppi41_mem_rgn_alloc - allocate a memory region within the queue manager
425  */
426 int cppi41_mem_rgn_alloc(u8 q_mgr, dma_addr_t rgn_addr, u8 size_order,
427                          u8 num_order, u8 *mem_rgn)
429         void __iomem *desc_mem_regs;
430         u32 num_desc = 1 << num_order, index, ctrl;
431         int rgn;
433         DBG("%s called with rgn_addr = %08x, size_order = %d, num_order = %d\n",
434             __func__, rgn_addr, size_order, num_order);
436         if (q_mgr >= cppi41_num_queue_mgr ||
437             size_order < 5 || size_order > 13 ||
438             num_order  < 5 || num_order  > 12 ||
439             (rgn_addr & ((1 << size_order) - 1)))
440                 return -EINVAL;
442         rgn = next_mem_rgn[q_mgr];
443         index = next_desc_index[q_mgr];
444         if (rgn >= CPPI41_MAX_MEM_RGN || index + num_desc > 0x4000)
445                 return -ENOSPC;
447         next_mem_rgn[q_mgr] = rgn + 1;
448         next_desc_index[q_mgr] = index + num_desc;
450         desc_mem_regs = cppi41_queue_mgr[q_mgr].desc_mem_rgn_base;
452         /* Write the base register */
453         __raw_writel(rgn_addr, desc_mem_regs + QMGR_MEM_RGN_BASE_REG(rgn));
454         DBG("Descriptor region base @ %p, value: %x\n",
455             desc_mem_regs + QMGR_MEM_RGN_BASE_REG(rgn),
456             __raw_readl(desc_mem_regs + QMGR_MEM_RGN_BASE_REG(rgn)));
458         /* Write the control register */
459         ctrl = ((index << QMGR_MEM_RGN_INDEX_SHIFT) &
460                 QMGR_MEM_RGN_INDEX_MASK) |
461                (((size_order - 5) << QMGR_MEM_RGN_DESC_SIZE_SHIFT) &
462                 QMGR_MEM_RGN_DESC_SIZE_MASK) |
463                (((num_order - 5) << QMGR_MEM_RGN_SIZE_SHIFT) &
464                 QMGR_MEM_RGN_SIZE_MASK);
465         __raw_writel(ctrl, desc_mem_regs + QMGR_MEM_RGN_CTRL_REG(rgn));
466         DBG("Descriptor region control @ %p, value: %x\n",
467             desc_mem_regs + QMGR_MEM_RGN_CTRL_REG(rgn),
468             __raw_readl(desc_mem_regs + QMGR_MEM_RGN_CTRL_REG(rgn)));
470         *mem_rgn = rgn;
471         return 0;
473 EXPORT_SYMBOL(cppi41_mem_rgn_alloc);
475 /*
476  * cppi41_mem_rgn_free - free the memory region within the queue manager
477  */
478 int cppi41_mem_rgn_free(u8 q_mgr, u8 mem_rgn)
480         void __iomem *desc_mem_regs;
482         DBG("%s called.\n", __func__);
484         if (q_mgr >= cppi41_num_queue_mgr || mem_rgn >= next_mem_rgn[q_mgr])
485                 return -EINVAL;
487         desc_mem_regs = cppi41_queue_mgr[q_mgr].desc_mem_rgn_base;
489         if (__raw_readl(desc_mem_regs + QMGR_MEM_RGN_BASE_REG(mem_rgn)) == 0)
490                 return -ENOENT;
492         __raw_writel(0, desc_mem_regs + QMGR_MEM_RGN_BASE_REG(mem_rgn));
493         __raw_writel(0, desc_mem_regs + QMGR_MEM_RGN_CTRL_REG(mem_rgn));
495         return 0;
497 EXPORT_SYMBOL(cppi41_mem_rgn_free);
499 /*
500  * cppi41_tx_ch_init - initialize a CPPI 4.1 Tx channel object
501  *
502  * Verify the channel info (range checking, etc.) and store the channel
503  * information within the object structure.
504  */
505 int cppi41_tx_ch_init(struct cppi41_dma_ch_obj *tx_ch_obj,
506                       u8 dma_num, u8 ch_num)
508         if (dma_num >= cppi41_num_dma_block ||
509             ch_num  >= cppi41_dma_block[dma_num].num_tx_ch)
510                 return -EINVAL;
512         /* Populate the channel object structure */
513         tx_ch_obj->base_addr  = cppi41_dma_block[dma_num].ch_ctrl_stat_base +
514                                 DMA_CH_TX_GLOBAL_CFG_REG(ch_num);
515         tx_ch_obj->global_cfg = __raw_readl(tx_ch_obj->base_addr);
516         return 0;
518 EXPORT_SYMBOL(cppi41_tx_ch_init);
520 /*
521  * cppi41_rx_ch_init - initialize a CPPI 4.1 Rx channel object
522  *
523  * Verify the channel info (range checking, etc.) and store the channel
524  * information within the object structure.
525  */
526 int cppi41_rx_ch_init(struct cppi41_dma_ch_obj *rx_ch_obj,
527                       u8 dma_num, u8 ch_num)
529         if (dma_num >= cppi41_num_dma_block ||
530             ch_num  >= cppi41_dma_block[dma_num].num_rx_ch)
531                 return -EINVAL;
533         /* Populate the channel object structure */
534         rx_ch_obj->base_addr  = cppi41_dma_block[dma_num].ch_ctrl_stat_base +
535                                 DMA_CH_RX_GLOBAL_CFG_REG(ch_num);
536         rx_ch_obj->global_cfg = __raw_readl(rx_ch_obj->base_addr);
537         return 0;
539 EXPORT_SYMBOL(cppi41_rx_ch_init);
541 /*
542  * We have to cache the last written Rx/Tx channel global configration register
543  * value due to its bits other than enable/teardown being write-only. Yet there
544  * is a caveat related to caching the enable bit: this bit may be automatically
545  * cleared as a result of teardown, so we can't trust its cached value!
546  * When modifying the write only register fields, we're making use of the fact
547  * that they read back as zeros, and not clearing them explicitly...
548  */
550 /*
551  * cppi41_dma_ch_default_queue - set CPPI 4.1 channel default completion queue
552  */
553 void cppi41_dma_ch_default_queue(struct cppi41_dma_ch_obj *dma_ch_obj,
554                                  u8 q_mgr, u16 q_num)
556         u32 val = dma_ch_obj->global_cfg;
558         /* Clear the fields to be modified. */
559         val &= ~(DMA_CH_TX_DEFAULT_QMGR_MASK | DMA_CH_TX_DEFAULT_QNUM_MASK |
560                  DMA_CH_TX_ENABLE_MASK);
562         /* Set the default completion queue. */
563         val |= ((q_mgr << DMA_CH_TX_DEFAULT_QMGR_SHIFT) &
564                 DMA_CH_TX_DEFAULT_QMGR_MASK) |
565                ((q_num << DMA_CH_TX_DEFAULT_QNUM_SHIFT) &
566                 DMA_CH_TX_DEFAULT_QNUM_MASK);
568         /* Get the current state of the enable bit. */
569         dma_ch_obj->global_cfg = val |= __raw_readl(dma_ch_obj->base_addr);
570         __raw_writel(val, dma_ch_obj->base_addr);
571         DBG("Channel global configuration @ %p, value written: %x, "
572             "value read: %x\n", dma_ch_obj->base_addr, val,
573             __raw_readl(dma_ch_obj->base_addr));
576 EXPORT_SYMBOL(cppi41_dma_ch_default_queue);
578 /*
579  * cppi41_rx_ch_configure - configure CPPI 4.1 Rx channel
580  */
581 void cppi41_rx_ch_configure(struct cppi41_dma_ch_obj *rx_ch_obj,
582                             struct cppi41_rx_ch_cfg  *cfg)
584         void __iomem *base = rx_ch_obj->base_addr;
585         u32 val = __raw_readl(rx_ch_obj->base_addr);
587         val |= ((cfg->sop_offset << DMA_CH_RX_SOP_OFFSET_SHIFT) &
588                 DMA_CH_RX_SOP_OFFSET_MASK) |
589                ((cfg->default_desc_type << DMA_CH_RX_DEFAULT_DESC_TYPE_SHIFT) &
590                 DMA_CH_RX_DEFAULT_DESC_TYPE_MASK) |
591                ((cfg->retry_starved << DMA_CH_RX_ERROR_HANDLING_SHIFT) &
592                 DMA_CH_RX_ERROR_HANDLING_MASK) |
593                ((cfg->rx_queue.q_mgr << DMA_CH_RX_DEFAULT_RQ_QMGR_SHIFT) &
594                 DMA_CH_RX_DEFAULT_RQ_QMGR_MASK) |
595                ((cfg->rx_queue.q_num << DMA_CH_RX_DEFAULT_RQ_QNUM_SHIFT) &
596                 DMA_CH_RX_DEFAULT_RQ_QNUM_MASK);
598         val &= ~(0x7 << DMA_CH_RX_MAX_BUF_CNT_SHIFT);
599         val |= (cfg->rx_max_buf_cnt << DMA_CH_RX_MAX_BUF_CNT_SHIFT);
601         rx_ch_obj->global_cfg = val;
602         __raw_writel(val, base);
603         DBG("Rx channel global configuration @ %p, value written: %x, "
604             "value read: %x\n", base, val, __raw_readl(base));
606         base -= DMA_CH_RX_GLOBAL_CFG_REG(0);
608         /*
609          * Set up the packet configuration register
610          * based on the descriptor type...
611          */
612         switch (cfg->default_desc_type) {
613         case DMA_CH_RX_DEFAULT_DESC_EMBED:
614                 val = ((cfg->cfg.embed_pkt.fd_queue.q_mgr <<
615                         DMA_CH_RX_EMBED_FDQ_QMGR_SHIFT) &
616                        DMA_CH_RX_EMBED_FDQ_QMGR_MASK) |
617                       ((cfg->cfg.embed_pkt.fd_queue.q_num <<
618                         DMA_CH_RX_EMBED_FDQ_QNUM_SHIFT) &
619                        DMA_CH_RX_EMBED_FDQ_QNUM_MASK) |
620                       ((cfg->cfg.embed_pkt.num_buf_slot <<
621                         DMA_CH_RX_EMBED_NUM_SLOT_SHIFT) &
622                        DMA_CH_RX_EMBED_NUM_SLOT_MASK) |
623                       ((cfg->cfg.embed_pkt.sop_slot_num <<
624                         DMA_CH_RX_EMBED_SOP_SLOT_SHIFT) &
625                        DMA_CH_RX_EMBED_SOP_SLOT_MASK);
627                 __raw_writel(val, base + DMA_CH_RX_EMBED_PKT_CFG_REG_B(0));
628                 DBG("Rx channel embedded packet configuration B @ %p, "
629                     "value written: %x\n",
630                     base + DMA_CH_RX_EMBED_PKT_CFG_REG_B(0), val);
632                 val = ((cfg->cfg.embed_pkt.free_buf_pool[0].b_pool <<
633                         DMA_CH_RX_EMBED_FBP_PNUM_SHIFT(0)) &
634                        DMA_CH_RX_EMBED_FBP_PNUM_MASK(0)) |
635                       ((cfg->cfg.embed_pkt.free_buf_pool[0].b_mgr <<
636                         DMA_CH_RX_EMBED_FBP_BMGR_SHIFT(0)) &
637                        DMA_CH_RX_EMBED_FBP_BMGR_MASK(0)) |
638                       ((cfg->cfg.embed_pkt.free_buf_pool[1].b_pool <<
639                         DMA_CH_RX_EMBED_FBP_PNUM_SHIFT(1)) &
640                        DMA_CH_RX_EMBED_FBP_PNUM_MASK(1)) |
641                       ((cfg->cfg.embed_pkt.free_buf_pool[1].b_mgr <<
642                         DMA_CH_RX_EMBED_FBP_BMGR_SHIFT(1)) &
643                        DMA_CH_RX_EMBED_FBP_BMGR_MASK(1)) |
644                       ((cfg->cfg.embed_pkt.free_buf_pool[2].b_pool <<
645                         DMA_CH_RX_EMBED_FBP_PNUM_SHIFT(2)) &
646                        DMA_CH_RX_EMBED_FBP_PNUM_MASK(2)) |
647                       ((cfg->cfg.embed_pkt.free_buf_pool[2].b_mgr <<
648                         DMA_CH_RX_EMBED_FBP_BMGR_SHIFT(2)) &
649                        DMA_CH_RX_EMBED_FBP_BMGR_MASK(2)) |
650                       ((cfg->cfg.embed_pkt.free_buf_pool[3].b_pool <<
651                         DMA_CH_RX_EMBED_FBP_PNUM_SHIFT(3)) &
652                        DMA_CH_RX_EMBED_FBP_PNUM_MASK(3)) |
653                       ((cfg->cfg.embed_pkt.free_buf_pool[3].b_mgr <<
654                         DMA_CH_RX_EMBED_FBP_BMGR_SHIFT(3)) &
655                        DMA_CH_RX_EMBED_FBP_BMGR_MASK(3));
657                 __raw_writel(val, base + DMA_CH_RX_EMBED_PKT_CFG_REG_A(0));
658                 DBG("Rx channel embedded packet configuration A @ %p, "
659                     "value written: %x\n",
660                     base + DMA_CH_RX_EMBED_PKT_CFG_REG_A(0), val);
661                 break;
662         case DMA_CH_RX_DEFAULT_DESC_HOST:
663                 val = ((cfg->cfg.host_pkt.fdb_queue[0].q_num <<
664                         DMA_CH_RX_HOST_FDQ_QNUM_SHIFT(0)) &
665                        DMA_CH_RX_HOST_FDQ_QNUM_MASK(0)) |
666                       ((cfg->cfg.host_pkt.fdb_queue[0].q_mgr <<
667                         DMA_CH_RX_HOST_FDQ_QMGR_SHIFT(0)) &
668                        DMA_CH_RX_HOST_FDQ_QMGR_MASK(0)) |
669                       ((cfg->cfg.host_pkt.fdb_queue[1].q_num <<
670                         DMA_CH_RX_HOST_FDQ_QNUM_SHIFT(1)) &
671                        DMA_CH_RX_HOST_FDQ_QNUM_MASK(1)) |
672                       ((cfg->cfg.host_pkt.fdb_queue[1].q_mgr <<
673                         DMA_CH_RX_HOST_FDQ_QMGR_SHIFT(1)) &
674                        DMA_CH_RX_HOST_FDQ_QMGR_MASK(1));
676                 __raw_writel(val, base + DMA_CH_RX_HOST_PKT_CFG_REG_A(0));
677                 DBG("Rx channel host packet configuration A @ %p, "
678                     "value written: %x\n",
679                     base + DMA_CH_RX_HOST_PKT_CFG_REG_A(0), val);
681                 val = ((cfg->cfg.host_pkt.fdb_queue[2].q_num <<
682                         DMA_CH_RX_HOST_FDQ_QNUM_SHIFT(2)) &
683                        DMA_CH_RX_HOST_FDQ_QNUM_MASK(2)) |
684                       ((cfg->cfg.host_pkt.fdb_queue[2].q_mgr <<
685                         DMA_CH_RX_HOST_FDQ_QMGR_SHIFT(2)) &
686                        DMA_CH_RX_HOST_FDQ_QMGR_MASK(2)) |
687                       ((cfg->cfg.host_pkt.fdb_queue[3].q_num <<
688                        DMA_CH_RX_HOST_FDQ_QNUM_SHIFT(3)) &
689                        DMA_CH_RX_HOST_FDQ_QNUM_MASK(3)) |
690                       ((cfg->cfg.host_pkt.fdb_queue[3].q_mgr <<
691                         DMA_CH_RX_HOST_FDQ_QMGR_SHIFT(3)) &
692                        DMA_CH_RX_HOST_FDQ_QMGR_MASK(3));
694                 __raw_writel(val, base + DMA_CH_RX_HOST_PKT_CFG_REG_B(0));
695                 DBG("Rx channel host packet configuration B @ %p, "
696                     "value written: %x\n",
697                     base + DMA_CH_RX_HOST_PKT_CFG_REG_B(0), val);
698                 break;
699         case DMA_CH_RX_DEFAULT_DESC_MONO:
700                 val = ((cfg->cfg.mono_pkt.fd_queue.q_num <<
701                         DMA_CH_RX_MONO_FDQ_QNUM_SHIFT) &
702                        DMA_CH_RX_MONO_FDQ_QNUM_MASK) |
703                       ((cfg->cfg.mono_pkt.fd_queue.q_mgr <<
704                         DMA_CH_RX_MONO_FDQ_QMGR_SHIFT) &
705                        DMA_CH_RX_MONO_FDQ_QMGR_MASK) |
706                       ((cfg->cfg.mono_pkt.sop_offset <<
707                         DMA_CH_RX_MONO_SOP_OFFSET_SHIFT) &
708                        DMA_CH_RX_MONO_SOP_OFFSET_MASK);
710                 __raw_writel(val, base + DMA_CH_RX_MONO_PKT_CFG_REG(0));
711                 DBG("Rx channel monolithic packet configuration @ %p, "
712                     "value written: %x\n",
713                     base + DMA_CH_RX_MONO_PKT_CFG_REG(0), val);
714                 break;
715         }
717 EXPORT_SYMBOL(cppi41_rx_ch_configure);
719 void cppi41_rx_ch_set_maxbufcnt(struct cppi41_dma_ch_obj *rx_ch_obj,
720                             u8 rx_max_buf_cnt)
722         void __iomem *base = rx_ch_obj->base_addr;
723         u32 val = __raw_readl(rx_ch_obj->base_addr);
725         val = rx_ch_obj->global_cfg;
726         val &= ~(0x7 << DMA_CH_RX_MAX_BUF_CNT_SHIFT);
727         val |= (rx_max_buf_cnt << DMA_CH_RX_MAX_BUF_CNT_SHIFT);
729         rx_ch_obj->global_cfg = val;
730         __raw_writel(val, base);
732         DBG("%s: rx-global-cfg @ %p, value written: %x, "
733             "value read: %x\n", __func__, base, val, __raw_readl(base));
736 EXPORT_SYMBOL(cppi41_rx_ch_set_maxbufcnt);
737 /*
738  * cppi41_dma_ch_teardown - teardown a given Tx/Rx channel
739  */
740 void cppi41_dma_ch_teardown(struct cppi41_dma_ch_obj *dma_ch_obj)
742         u32 val = __raw_readl(dma_ch_obj->base_addr);
744         /* Initiate channel teardown. */
745         val |= dma_ch_obj->global_cfg & ~DMA_CH_TX_ENABLE_MASK;
746         dma_ch_obj->global_cfg = val |= DMA_CH_TX_TEARDOWN_MASK;
747         __raw_writel(val, dma_ch_obj->base_addr);
748         DBG("Tear down channel @ %p, value written: %x, value read: %x\n",
749             dma_ch_obj->base_addr, val, __raw_readl(dma_ch_obj->base_addr));
751 EXPORT_SYMBOL(cppi41_dma_ch_teardown);
753 /*
754  * cppi41_dma_ch_enable - enable Tx/Rx DMA channel in hardware
755  *
756  * Makes the channel ready for data transmission/reception.
757  */
758 void cppi41_dma_ch_enable(struct cppi41_dma_ch_obj *dma_ch_obj)
760         u32 val = dma_ch_obj->global_cfg | DMA_CH_TX_ENABLE_MASK;
762         /* Teardown bit remains set after completion, so clear it now... */
763         dma_ch_obj->global_cfg = val &= ~DMA_CH_TX_TEARDOWN_MASK;
764         __raw_writel(val, dma_ch_obj->base_addr);
765         DBG("Enable channel @ %p, value written: %x, value read: %x\n",
766             dma_ch_obj->base_addr, val, __raw_readl(dma_ch_obj->base_addr));
768 EXPORT_SYMBOL(cppi41_dma_ch_enable);
770 /*
771  * cppi41_dma_ch_disable - disable Tx/Rx DMA channel in hardware
772  */
773 void cppi41_dma_ch_disable(struct cppi41_dma_ch_obj *dma_ch_obj)
775         dma_ch_obj->global_cfg &= ~DMA_CH_TX_ENABLE_MASK;
776         __raw_writel(dma_ch_obj->global_cfg, dma_ch_obj->base_addr);
777         DBG("Disable channel @ %p, value written: %x, value read: %x\n",
778             dma_ch_obj->base_addr, dma_ch_obj->global_cfg,
779             __raw_readl(dma_ch_obj->base_addr));
781 EXPORT_SYMBOL(cppi41_dma_ch_disable);
783 void cppi41_free_teardown_queue(int dma_num)
785         unsigned long td_addr;
786         u32 num_desc = dma_teardown[dma_num].num_desc;
788         while (num_desc--) {
789                 td_addr = cppi41_queue_pop(&dma_teardown[dma_num].queue_obj);
791                 if (td_addr == 0)
792                         break;
793         }
795 EXPORT_SYMBOL(cppi41_free_teardown_queue);
797 /**
798  * alloc_queue - allocate a queue in the given range
799  * @allocated:  pointer to the bitmap of the allocated queues
800  * @excluded:   pointer to the bitmap of the queues excluded from allocation
801  *              (optional)
802  * @start:      starting queue number
803  * @count:      number of queues available
804  *
805  * Returns queue number on success, -ENOSPC otherwise.
806  */
807 static int alloc_queue(u32 *allocated, const u32 *excluded, unsigned start,
808                        unsigned count)
810         u32 bit, mask = 0;
811         int index = -1;
813         /*
814          * We're starting the loop as if we've just wrapped around 32 bits
815          * in order to save on preloading the bitmasks.
816          */
817         for (bit = 0; count--; start++, bit <<= 1) {
818                 /* Have we just wrapped around 32 bits? */
819                 if (!bit) {
820                         /* Start over with the next bitmask word */
821                         bit = 1;
822                         index++;
823                         /* Have we just entered the loop? */
824                         if (!index) {
825                                 /* Calculate the starting values */
826                                 bit <<= start & 0x1f;
827                                 index = start >> 5;
828                         }
829                         /*
830                          * Load the next word of the allocated bitmask OR'ing
831                          * it with the excluded bitmask if it's been passed.
832                          */
833                         mask = allocated[index];
834                         if (excluded != NULL)
835                                 mask |= excluded[index];
836                 }
837                 /*
838                  * If the bit in the combined bitmask is zero,
839                  * we've just found a free queue.
840                  */
841                 if (!(mask & bit)) {
842                         allocated[index] |= bit;
843                         return start;
844                 }
845         }
846         return -ENOSPC;
849 /*
850  * cppi41_queue_alloc - allocate a queue of a given type in the queue manager
851  */
852 int cppi41_queue_alloc(u8 type, u8 q_mgr, u16 *q_num)
854         int res = -ENOSPC;
856         if (q_mgr >= cppi41_num_queue_mgr)
857                 return -EINVAL;
859         /* Mask out the unsupported queue types */
860         type &= cppi41_queue_mgr[q_mgr].queue_types;
861         /* First see if a free descriptor queue was requested... */
862         if (type & CPPI41_FREE_DESC_QUEUE)
863                 res = alloc_queue(allocated_queues[q_mgr], NULL,
864                                   cppi41_queue_mgr[q_mgr].base_fdq_num,  16);
866         /* Then see if a free descriptor/buffer queue was requested... */
867         if (res < 0 && (type & CPPI41_FREE_DESC_BUF_QUEUE))
868                 res = alloc_queue(allocated_queues[q_mgr], NULL,
869                                   cppi41_queue_mgr[q_mgr].base_fdbq_num, 16);
871         /* Last see if an unassigned queue was requested... */
872         if (res < 0 && (type & CPPI41_UNASSIGNED_QUEUE))
873                 res = alloc_queue(allocated_queues[q_mgr],
874                                   cppi41_queue_mgr[q_mgr].assigned, 0,
875                                   cppi41_queue_mgr[q_mgr].num_queue);
877         /* See if any queue was allocated... */
878         if (res < 0)
879                 return res;
881         /* Return the queue allocated */
882         *q_num = res;
883         return 0;
885 EXPORT_SYMBOL(cppi41_queue_alloc);
887 /*
888  * cppi41_queue_free - free the given queue in the queue manager
889  */
890 int cppi41_queue_free(u8 q_mgr, u16 q_num)
892         int index = q_num >> 5, bit = 1 << (q_num & 0x1f);
894         if (allocated_queues[q_mgr] != NULL) {
895                 if (q_mgr >= cppi41_num_queue_mgr ||
896                     q_num >= cppi41_queue_mgr[q_mgr].num_queue ||
897                     !(allocated_queues[q_mgr][index] & bit))
898                         return -EINVAL;
899                 allocated_queues[q_mgr][index] &= ~bit;
900         }
901         return 0;
903 EXPORT_SYMBOL(cppi41_queue_free);
905 /*
906  * cppi41_queue_init - initialize a CPPI 4.1 queue object
907  */
908 int cppi41_queue_init(struct cppi41_queue_obj *queue_obj, u8 q_mgr, u16 q_num)
910         if (q_mgr >= cppi41_num_queue_mgr ||
911             q_num >= cppi41_queue_mgr[q_mgr].num_queue)
912                 return -EINVAL;
914         queue_obj->base_addr = cppi41_queue_mgr[q_mgr].q_mgmt_rgn_base +
915                                QMGR_QUEUE_STATUS_REG_A(q_num);
917         return 0;
919 EXPORT_SYMBOL(cppi41_queue_init);
921 /*
922  * cppi41_queue_push - push a descriptor into the given queue
923  */
924 void cppi41_queue_push(const struct cppi41_queue_obj *queue_obj, u32 desc_addr,
925                        u32 desc_size, u32 pkt_size)
927         u32 val;
929         /*
930          * Write to the tail of the queue.
931          * TODO: Can't think of a reason why a queue to head may be required.
932          * If it is, the API may have to be extended.
933          */
934 #if 0
935         /*
936          * Also, can't understand why packet size is required to queue up a
937          * descriptor. The spec says packet size *must* be written prior to
938          * the packet write operation.
939          */
940         if (pkt_size)
941                 val = (pkt_size << QMGR_QUEUE_PKT_SIZE_SHIFT) &
942                       QMGR_QUEUE_PKT_SIZE_MASK;
943         __raw_writel(val, queue_obj->base_addr + QMGR_QUEUE_REG_C(0));
944 #endif
946         val = (((desc_size - 24) >> (2 - QMGR_QUEUE_DESC_SIZE_SHIFT)) &
947                QMGR_QUEUE_DESC_SIZE_MASK) |
948               (desc_addr & QMGR_QUEUE_DESC_PTR_MASK);
950         DBG("Pushing value %x to queue @ %p\n", val, queue_obj->base_addr);
952         __raw_writel(val, queue_obj->base_addr + QMGR_QUEUE_REG_D(0));
954 EXPORT_SYMBOL(cppi41_queue_push);
956 /*
957  * cppi41_queue_pop - pop a descriptor from a given queue
958  */
959 unsigned long cppi41_queue_pop(const struct cppi41_queue_obj *queue_obj)
961         u32 val = __raw_readl(queue_obj->base_addr + QMGR_QUEUE_REG_D(0));
963         DBG("Popping value %x from queue @ %p\n", val, queue_obj->base_addr);
965         return val & QMGR_QUEUE_DESC_PTR_MASK;
967 EXPORT_SYMBOL(cppi41_queue_pop);
969 /*
970  * cppi41_get_teardown_info - extract information from a teardown descriptor
971  */
972 int cppi41_get_teardown_info(unsigned long addr, u32 *info)
974         struct cppi41_teardown_desc *desc;
975         int dma_num;
977         for (dma_num = 0; dma_num < cppi41_num_dma_block; dma_num++)
978                 if (addr >= dma_teardown[dma_num].phys_addr &&
979                     addr <  dma_teardown[dma_num].phys_addr +
980                             dma_teardown[dma_num].rgn_size)
981                         break;
983         if (dma_num == cppi41_num_dma_block)
984                 return -EINVAL;
986         desc = addr - dma_teardown[dma_num].phys_addr +
987                dma_teardown[dma_num].virt_addr;
989         if ((desc->teardown_info & CPPI41_DESC_TYPE_MASK) !=
990             (CPPI41_DESC_TYPE_TEARDOWN << CPPI41_DESC_TYPE_SHIFT))
991                 return -EINVAL;
993         *info = desc->teardown_info;
994 #if 1
995         /* Hardware is not giving the current DMA number as of now. :-/ */
996         *info |= (dma_num << CPPI41_TEARDOWN_DMA_NUM_SHIFT) &
997                  CPPI41_TEARDOWN_DMA_NUM_MASK;
998 #else
999         dma_num = (desc->teardown_info & CPPI41_TEARDOWN_DMA_NUM_MASK) >>
1000                  CPPI41_TEARDOWN_DMA_NUM_SHIFT;
1001 #endif
1003         cppi41_queue_push(&dma_teardown[dma_num].queue_obj, addr,
1004                           sizeof(struct cppi41_teardown_desc), 0);
1006         return 0;
1008 EXPORT_SYMBOL(cppi41_get_teardown_info);
1010 MODULE_DESCRIPTION("TI CPPI 4.1 support");
1011 MODULE_AUTHOR("MontaVista Software");
1012 MODULE_LICENSE("GPL");