1284f8875d7acc405dbc0b5788c14251b0d6d73e
1 /*
2 * Texas Instruments DA8xx/OMAP-L1x "glue layer"
3 *
4 * Copyright (c) 2008-2009 MontaVista Software, Inc. <source@mvista.com>
5 *
6 * Based on the DaVinci "glue layer" code.
7 * Copyright (C) 2005-2006 by Texas Instruments
8 *
9 * This file is part of the Inventra Controller Driver for Linux.
10 *
11 * The Inventra Controller Driver for Linux is free software; you
12 * can redistribute it and/or modify it under the terms of the GNU
13 * General Public License version 2 as published by the Free Software
14 * Foundation.
15 *
16 * The Inventra Controller Driver for Linux is distributed in
17 * the hope that it will be useful, but WITHOUT ANY WARRANTY;
18 * without even the implied warranty of MERCHANTABILITY or
19 * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public
20 * License for more details.
21 *
22 * You should have received a copy of the GNU General Public License
23 * along with The Inventra Controller Driver for Linux ; if not,
24 * write to the Free Software Foundation, Inc., 59 Temple Place,
25 * Suite 330, Boston, MA 02111-1307 USA
26 *
27 */
29 #include <linux/init.h>
30 #include <linux/module.h>
31 #include <linux/clk.h>
32 #include <linux/io.h>
33 #include <linux/platform_device.h>
34 #include <linux/dma-mapping.h>
36 #include <mach/da8xx.h>
37 #include <mach/usb.h>
39 #include "musb_core.h"
41 /*
42 * DA8XX specific definitions
43 */
45 /* USB 2.0 OTG module registers */
46 #define DA8XX_USB_REVISION_REG 0x00
47 #define DA8XX_USB_CTRL_REG 0x04
48 #define DA8XX_USB_STAT_REG 0x08
49 #define DA8XX_USB_EMULATION_REG 0x0c
50 #define DA8XX_USB_MODE_REG 0x10 /* Transparent, CDC, [Generic] RNDIS */
51 #define DA8XX_USB_AUTOREQ_REG 0x14
52 #define DA8XX_USB_SRP_FIX_TIME_REG 0x18
53 #define DA8XX_USB_TEARDOWN_REG 0x1c
54 #define DA8XX_USB_INTR_SRC_REG 0x20
55 #define DA8XX_USB_INTR_SRC_SET_REG 0x24
56 #define DA8XX_USB_INTR_SRC_CLEAR_REG 0x28
57 #define DA8XX_USB_INTR_MASK_REG 0x2c
58 #define DA8XX_USB_INTR_MASK_SET_REG 0x30
59 #define DA8XX_USB_INTR_MASK_CLEAR_REG 0x34
60 #define DA8XX_USB_INTR_SRC_MASKED_REG 0x38
61 #define DA8XX_USB_END_OF_INTR_REG 0x3c
62 #define DA8XX_USB_GENERIC_RNDIS_EP_SIZE_REG(n) (0x50 + (((n) - 1) << 2))
64 /* Control register bits */
65 #define DA8XX_SOFT_RESET_MASK 1
67 #define DA8XX_USB_TX_EP_MASK 0x1f /* EP0 + 4 Tx EPs */
68 #define DA8XX_USB_RX_EP_MASK 0x1e /* 4 Rx EPs */
70 /* USB interrupt register bits */
71 #define DA8XX_INTR_USB_SHIFT 16
72 #define DA8XX_INTR_USB_MASK (0x1ff << DA8XX_INTR_USB_SHIFT) /* 8 Mentor */
73 /* interrupts and DRVVBUS interrupt */
74 #define DA8XX_INTR_DRVVBUS 0x100
75 #define DA8XX_INTR_RX_SHIFT 8
76 #define DA8XX_INTR_RX_MASK (DA8XX_USB_RX_EP_MASK << DA8XX_INTR_RX_SHIFT)
77 #define DA8XX_INTR_TX_SHIFT 0
78 #define DA8XX_INTR_TX_MASK (DA8XX_USB_TX_EP_MASK << DA8XX_INTR_TX_SHIFT)
80 #define DA8XX_MENTOR_CORE_OFFSET 0x400
82 #define CFGCHIP2 IO_ADDRESS(DA8XX_SYSCFG0_BASE + DA8XX_CFGCHIP2_REG)
84 struct da8xx_glue {
85 struct device *dev;
86 struct platform_device *musb;
87 struct clk *clk;
88 };
90 /*
91 * REVISIT (PM): we should be able to keep the PHY in low power mode most
92 * of the time (24 MHz oscillator and PLL off, etc.) by setting POWER.D0
93 * and, when in host mode, autosuspending idle root ports... PHY_PLLON
94 * (overriding SUSPENDM?) then likely needs to stay off.
95 */
97 static inline void phy_on(void)
98 {
99 u32 cfgchip2 = __raw_readl(CFGCHIP2);
101 /*
102 * Start the on-chip PHY and its PLL.
103 */
104 cfgchip2 &= ~(CFGCHIP2_RESET | CFGCHIP2_PHYPWRDN | CFGCHIP2_OTGPWRDN);
105 cfgchip2 |= CFGCHIP2_PHY_PLLON;
106 __raw_writel(cfgchip2, CFGCHIP2);
108 pr_info("Waiting for USB PHY clock good...\n");
109 while (!(__raw_readl(CFGCHIP2) & CFGCHIP2_PHYCLKGD))
110 cpu_relax();
111 }
113 static inline void phy_off(void)
114 {
115 u32 cfgchip2 = __raw_readl(CFGCHIP2);
117 /*
118 * Ensure that USB 1.1 reference clock is not being sourced from
119 * USB 2.0 PHY. Otherwise do not power down the PHY.
120 */
121 if (!(cfgchip2 & CFGCHIP2_USB1PHYCLKMUX) &&
122 (cfgchip2 & CFGCHIP2_USB1SUSPENDM)) {
123 pr_warning("USB 1.1 clocked from USB 2.0 PHY -- "
124 "can't power it down\n");
125 return;
126 }
128 /*
129 * Power down the on-chip PHY.
130 */
131 cfgchip2 |= CFGCHIP2_PHYPWRDN | CFGCHIP2_OTGPWRDN;
132 __raw_writel(cfgchip2, CFGCHIP2);
133 }
135 /*
136 * Because we don't set CTRL.UINT, it's "important" to:
137 * - not read/write INTRUSB/INTRUSBE (except during
138 * initial setup, as a workaround);
139 * - use INTSET/INTCLR instead.
140 */
142 /**
143 * da8xx_musb_enable - enable interrupts
144 */
145 static void da8xx_musb_enable(struct musb *musb)
146 {
147 void __iomem *reg_base = musb->ctrl_base;
148 u32 mask;
150 /* Workaround: setup IRQs through both register sets. */
151 mask = ((musb->epmask & DA8XX_USB_TX_EP_MASK) << DA8XX_INTR_TX_SHIFT) |
152 ((musb->epmask & DA8XX_USB_RX_EP_MASK) << DA8XX_INTR_RX_SHIFT) |
153 DA8XX_INTR_USB_MASK;
154 musb_writel(reg_base, DA8XX_USB_INTR_MASK_SET_REG, mask);
156 /* Force the DRVVBUS IRQ so we can start polling for ID change. */
157 if (is_otg_enabled(musb))
158 musb_writel(reg_base, DA8XX_USB_INTR_SRC_SET_REG,
159 DA8XX_INTR_DRVVBUS << DA8XX_INTR_USB_SHIFT);
160 }
162 /**
163 * da8xx_musb_disable - disable HDRC and flush interrupts
164 */
165 static void da8xx_musb_disable(struct musb *musb)
166 {
167 void __iomem *reg_base = musb->ctrl_base;
169 musb_writel(reg_base, DA8XX_USB_INTR_MASK_CLEAR_REG,
170 DA8XX_INTR_USB_MASK |
171 DA8XX_INTR_TX_MASK | DA8XX_INTR_RX_MASK);
172 musb_writeb(musb->mregs, MUSB_DEVCTL, 0);
173 musb_writel(reg_base, DA8XX_USB_END_OF_INTR_REG, 0);
174 }
176 #define portstate(stmt) stmt
178 static void da8xx_musb_set_vbus(struct musb *musb, int is_on)
179 {
180 WARN_ON(is_on && is_peripheral_active(musb));
181 }
183 #define POLL_SECONDS 2
185 static struct timer_list otg_workaround;
187 static void otg_timer(unsigned long _musb)
188 {
189 struct musb *musb = (void *)_musb;
190 void __iomem *mregs = musb->mregs;
191 u8 devctl;
192 unsigned long flags;
194 /*
195 * We poll because DaVinci's won't expose several OTG-critical
196 * status change events (from the transceiver) otherwise.
197 */
198 devctl = musb_readb(mregs, MUSB_DEVCTL);
199 dev_dbg(musb->controller, "Poll devctl %02x (%s)\n", devctl,
200 otg_state_string(musb->xceiv->state));
202 spin_lock_irqsave(&musb->lock, flags);
203 switch (musb->xceiv->state) {
204 case OTG_STATE_A_WAIT_BCON:
205 devctl &= ~MUSB_DEVCTL_SESSION;
206 musb_writeb(musb->mregs, MUSB_DEVCTL, devctl);
208 devctl = musb_readb(musb->mregs, MUSB_DEVCTL);
209 if (devctl & MUSB_DEVCTL_BDEVICE) {
210 musb->xceiv->state = OTG_STATE_B_IDLE;
211 MUSB_DEV_MODE(musb);
212 } else {
213 musb->xceiv->state = OTG_STATE_A_IDLE;
214 MUSB_HST_MODE(musb);
215 }
216 break;
217 case OTG_STATE_A_WAIT_VFALL:
218 /*
219 * Wait till VBUS falls below SessionEnd (~0.2 V); the 1.3
220 * RTL seems to mis-handle session "start" otherwise (or in
221 * our case "recover"), in routine "VBUS was valid by the time
222 * VBUSERR got reported during enumeration" cases.
223 */
224 if (devctl & MUSB_DEVCTL_VBUS) {
225 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
226 break;
227 }
228 musb->xceiv->state = OTG_STATE_A_WAIT_VRISE;
229 musb_writel(musb->ctrl_base, DA8XX_USB_INTR_SRC_SET_REG,
230 MUSB_INTR_VBUSERROR << DA8XX_INTR_USB_SHIFT);
231 break;
232 case OTG_STATE_B_IDLE:
233 if (!is_peripheral_enabled(musb))
234 break;
236 /*
237 * There's no ID-changed IRQ, so we have no good way to tell
238 * when to switch to the A-Default state machine (by setting
239 * the DEVCTL.Session bit).
240 *
241 * Workaround: whenever we're in B_IDLE, try setting the
242 * session flag every few seconds. If it works, ID was
243 * grounded and we're now in the A-Default state machine.
244 *
245 * NOTE: setting the session flag is _supposed_ to trigger
246 * SRP but clearly it doesn't.
247 */
248 musb_writeb(mregs, MUSB_DEVCTL, devctl | MUSB_DEVCTL_SESSION);
249 devctl = musb_readb(mregs, MUSB_DEVCTL);
250 if (devctl & MUSB_DEVCTL_BDEVICE)
251 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
252 else
253 musb->xceiv->state = OTG_STATE_A_IDLE;
254 break;
255 default:
256 break;
257 }
258 spin_unlock_irqrestore(&musb->lock, flags);
259 }
261 static void da8xx_musb_try_idle(struct musb *musb, unsigned long timeout)
262 {
263 static unsigned long last_timer;
265 if (!is_otg_enabled(musb))
266 return;
268 if (timeout == 0)
269 timeout = jiffies + msecs_to_jiffies(3);
271 /* Never idle if active, or when VBUS timeout is not set as host */
272 if (musb->is_active || (musb->a_wait_bcon == 0 &&
273 musb->xceiv->state == OTG_STATE_A_WAIT_BCON)) {
274 dev_dbg(musb->controller, "%s active, deleting timer\n",
275 otg_state_string(musb->xceiv->state));
276 del_timer(&otg_workaround);
277 last_timer = jiffies;
278 return;
279 }
281 if (time_after(last_timer, timeout) && timer_pending(&otg_workaround)) {
282 dev_dbg(musb->controller, "Longer idle timer already pending, ignoring...\n");
283 return;
284 }
285 last_timer = timeout;
287 dev_dbg(musb->controller, "%s inactive, starting idle timer for %u ms\n",
288 otg_state_string(musb->xceiv->state),
289 jiffies_to_msecs(timeout - jiffies));
290 mod_timer(&otg_workaround, timeout);
291 }
293 static irqreturn_t da8xx_musb_interrupt(int irq, void *hci)
294 {
295 struct musb *musb = hci;
296 void __iomem *reg_base = musb->ctrl_base;
297 unsigned long flags;
298 irqreturn_t ret = IRQ_NONE;
299 u32 status;
301 spin_lock_irqsave(&musb->lock, flags);
303 /*
304 * NOTE: DA8XX shadows the Mentor IRQs. Don't manage them through
305 * the Mentor registers (except for setup), use the TI ones and EOI.
306 */
308 /* Acknowledge and handle non-CPPI interrupts */
309 status = musb_readl(reg_base, DA8XX_USB_INTR_SRC_MASKED_REG);
310 if (!status)
311 goto eoi;
313 musb_writel(reg_base, DA8XX_USB_INTR_SRC_CLEAR_REG, status);
314 dev_dbg(musb->controller, "USB IRQ %08x\n", status);
316 musb->int_rx = (status & DA8XX_INTR_RX_MASK) >> DA8XX_INTR_RX_SHIFT;
317 musb->int_tx = (status & DA8XX_INTR_TX_MASK) >> DA8XX_INTR_TX_SHIFT;
318 musb->int_usb = (status & DA8XX_INTR_USB_MASK) >> DA8XX_INTR_USB_SHIFT;
320 /*
321 * DRVVBUS IRQs are the only proxy we have (a very poor one!) for
322 * DA8xx's missing ID change IRQ. We need an ID change IRQ to
323 * switch appropriately between halves of the OTG state machine.
324 * Managing DEVCTL.Session per Mentor docs requires that we know its
325 * value but DEVCTL.BDevice is invalid without DEVCTL.Session set.
326 * Also, DRVVBUS pulses for SRP (but not at 5 V)...
327 */
328 if (status & (DA8XX_INTR_DRVVBUS << DA8XX_INTR_USB_SHIFT)) {
329 int drvvbus = musb_readl(reg_base, DA8XX_USB_STAT_REG);
330 void __iomem *mregs = musb->mregs;
331 u8 devctl = musb_readb(mregs, MUSB_DEVCTL);
332 int err;
334 err = is_host_enabled(musb) && (musb->int_usb &
335 MUSB_INTR_VBUSERROR);
336 if (err) {
337 /*
338 * The Mentor core doesn't debounce VBUS as needed
339 * to cope with device connect current spikes. This
340 * means it's not uncommon for bus-powered devices
341 * to get VBUS errors during enumeration.
342 *
343 * This is a workaround, but newer RTL from Mentor
344 * seems to allow a better one: "re"-starting sessions
345 * without waiting for VBUS to stop registering in
346 * devctl.
347 */
348 musb->int_usb &= ~MUSB_INTR_VBUSERROR;
349 musb->xceiv->state = OTG_STATE_A_WAIT_VFALL;
350 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
351 WARNING("VBUS error workaround (delay coming)\n");
352 } else if (is_host_enabled(musb) && drvvbus) {
353 MUSB_HST_MODE(musb);
354 musb->xceiv->default_a = 1;
355 musb->xceiv->state = OTG_STATE_A_WAIT_VRISE;
356 portstate(musb->port1_status |= USB_PORT_STAT_POWER);
357 del_timer(&otg_workaround);
358 } else {
359 musb->is_active = 0;
360 MUSB_DEV_MODE(musb);
361 musb->xceiv->default_a = 0;
362 musb->xceiv->state = OTG_STATE_B_IDLE;
363 portstate(musb->port1_status &= ~USB_PORT_STAT_POWER);
364 }
366 dev_dbg(musb->controller, "VBUS %s (%s)%s, devctl %02x\n",
367 drvvbus ? "on" : "off",
368 otg_state_string(musb->xceiv->state),
369 err ? " ERROR" : "",
370 devctl);
371 ret = IRQ_HANDLED;
372 }
374 if (musb->int_tx || musb->int_rx || musb->int_usb)
375 ret |= musb_interrupt(musb);
377 eoi:
378 /* EOI needs to be written for the IRQ to be re-asserted. */
379 if (ret == IRQ_HANDLED || status)
380 musb_writel(reg_base, DA8XX_USB_END_OF_INTR_REG, 0);
382 /* Poll for ID change */
383 if (is_otg_enabled(musb) && musb->xceiv->state == OTG_STATE_B_IDLE)
384 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
386 spin_unlock_irqrestore(&musb->lock, flags);
388 return ret;
389 }
391 static int da8xx_musb_set_mode(struct musb *musb, u8 musb_mode)
392 {
393 u32 cfgchip2 = __raw_readl(CFGCHIP2);
395 cfgchip2 &= ~CFGCHIP2_OTGMODE;
396 switch (musb_mode) {
397 case MUSB_HOST: /* Force VBUS valid, ID = 0 */
398 cfgchip2 |= CFGCHIP2_FORCE_HOST;
399 break;
400 case MUSB_PERIPHERAL: /* Force VBUS valid, ID = 1 */
401 cfgchip2 |= CFGCHIP2_FORCE_DEVICE;
402 break;
403 case MUSB_OTG: /* Don't override the VBUS/ID comparators */
404 cfgchip2 |= CFGCHIP2_NO_OVERRIDE;
405 break;
406 default:
407 dev_dbg(musb->controller, "Trying to set unsupported mode %u\n", musb_mode);
408 }
410 __raw_writel(cfgchip2, CFGCHIP2);
411 return 0;
412 }
414 static int da8xx_musb_init(struct musb *musb)
415 {
416 void __iomem *reg_base = musb->ctrl_base;
417 u32 rev;
419 musb->mregs += DA8XX_MENTOR_CORE_OFFSET;
421 /* Returns zero if e.g. not clocked */
422 rev = musb_readl(reg_base, DA8XX_USB_REVISION_REG);
423 if (!rev)
424 goto fail;
426 usb_nop_xceiv_register();
427 musb->xceiv = otg_get_transceiver();
428 if (!musb->xceiv)
429 goto fail;
431 if (is_host_enabled(musb))
432 setup_timer(&otg_workaround, otg_timer, (unsigned long)musb);
434 /* Reset the controller */
435 musb_writel(reg_base, DA8XX_USB_CTRL_REG, DA8XX_SOFT_RESET_MASK);
437 /* Start the on-chip PHY and its PLL. */
438 phy_on();
440 msleep(5);
442 /* NOTE: IRQs are in mixed mode, not bypass to pure MUSB */
443 pr_debug("DA8xx OTG revision %08x, PHY %03x, control %02x\n",
444 rev, __raw_readl(CFGCHIP2),
445 musb_readb(reg_base, DA8XX_USB_CTRL_REG));
447 musb->isr = da8xx_musb_interrupt;
448 return 0;
449 fail:
450 return -ENODEV;
451 }
453 static int da8xx_musb_exit(struct musb *musb)
454 {
455 if (is_host_enabled(musb))
456 del_timer_sync(&otg_workaround);
458 phy_off();
460 otg_put_transceiver(musb->xceiv);
461 usb_nop_xceiv_unregister();
463 return 0;
464 }
466 static const struct musb_platform_ops da8xx_ops = {
467 .fifo_mode = 2,
468 .init = da8xx_musb_init,
469 .exit = da8xx_musb_exit,
471 .enable = da8xx_musb_enable,
472 .disable = da8xx_musb_disable,
474 .set_mode = da8xx_musb_set_mode,
475 .try_idle = da8xx_musb_try_idle,
477 .set_vbus = da8xx_musb_set_vbus,
479 .read_fifo = musb_read_fifo,
480 .write_fifo = musb_write_fifo,
481 };
483 static u64 da8xx_dmamask = DMA_BIT_MASK(32);
485 static int __init da8xx_probe(struct platform_device *pdev)
486 {
487 struct musb_hdrc_platform_data *pdata = pdev->dev.platform_data;
488 struct platform_device *musb;
489 struct da8xx_glue *glue;
491 struct clk *clk;
493 int ret = -ENOMEM;
495 glue = kzalloc(sizeof(*glue), GFP_KERNEL);
496 if (!glue) {
497 dev_err(&pdev->dev, "failed to allocate glue context\n");
498 goto err0;
499 }
501 musb = platform_device_alloc("musb-hdrc", -1);
502 if (!musb) {
503 dev_err(&pdev->dev, "failed to allocate musb device\n");
504 goto err1;
505 }
507 clk = clk_get(&pdev->dev, "usb20");
508 if (IS_ERR(clk)) {
509 dev_err(&pdev->dev, "failed to get clock\n");
510 ret = PTR_ERR(clk);
511 goto err2;
512 }
514 ret = clk_enable(clk);
515 if (ret) {
516 dev_err(&pdev->dev, "failed to enable clock\n");
517 goto err3;
518 }
520 musb->dev.parent = &pdev->dev;
521 musb->dev.dma_mask = &da8xx_dmamask;
522 musb->dev.coherent_dma_mask = da8xx_dmamask;
524 glue->dev = &pdev->dev;
525 glue->musb = musb;
526 glue->clk = clk;
528 pdata->platform_ops = &da8xx_ops;
530 platform_set_drvdata(pdev, glue);
532 ret = platform_device_add_resources(musb, pdev->resource,
533 pdev->num_resources);
534 if (ret) {
535 dev_err(&pdev->dev, "failed to add resources\n");
536 goto err4;
537 }
539 ret = platform_device_add_data(musb, pdata, sizeof(*pdata));
540 if (ret) {
541 dev_err(&pdev->dev, "failed to add platform_data\n");
542 goto err4;
543 }
545 ret = platform_device_add(musb);
546 if (ret) {
547 dev_err(&pdev->dev, "failed to register musb device\n");
548 goto err4;
549 }
551 return 0;
553 err4:
554 clk_disable(clk);
556 err3:
557 clk_put(clk);
559 err2:
560 platform_device_put(musb);
562 err1:
563 kfree(glue);
565 err0:
566 return ret;
567 }
569 static int __exit da8xx_remove(struct platform_device *pdev)
570 {
571 struct da8xx_glue *glue = platform_get_drvdata(pdev);
573 platform_device_del(glue->musb);
574 platform_device_put(glue->musb);
575 clk_disable(glue->clk);
576 clk_put(glue->clk);
577 kfree(glue);
579 return 0;
580 }
582 static struct platform_driver da8xx_driver = {
583 .remove = __exit_p(da8xx_remove),
584 .driver = {
585 .name = "musb-da8xx",
586 },
587 };
589 MODULE_DESCRIPTION("DA8xx/OMAP-L1x MUSB Glue Layer");
590 MODULE_AUTHOR("Sergei Shtylyov <sshtylyov@ru.mvista.com>");
591 MODULE_LICENSE("GPL v2");
593 static int __init da8xx_init(void)
594 {
595 return platform_driver_probe(&da8xx_driver, da8xx_probe);
596 }
597 subsys_initcall(da8xx_init);
599 static void __exit da8xx_exit(void)
600 {
601 platform_driver_unregister(&da8xx_driver);
602 }
603 module_exit(da8xx_exit);