]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - drivers/usb/musb/da8xx.c
usb: musb: same MUSB_OFFSET/musb_ep_select for all controller
[sitara-epos/sitara-epos-kernel.git] / drivers / usb / musb / da8xx.c
1 /*
2  * Texas Instruments DA8xx/OMAP-L1x "glue layer"
3  *
4  * Copyright (c) 2008-2009 MontaVista Software, Inc. <source@mvista.com>
5  *
6  * Based on the DaVinci "glue layer" code.
7  * Copyright (C) 2005-2006 by Texas Instruments
8  *
9  * This file is part of the Inventra Controller Driver for Linux.
10  *
11  * The Inventra Controller Driver for Linux is free software; you
12  * can redistribute it and/or modify it under the terms of the GNU
13  * General Public License version 2 as published by the Free Software
14  * Foundation.
15  *
16  * The Inventra Controller Driver for Linux is distributed in
17  * the hope that it will be useful, but WITHOUT ANY WARRANTY;
18  * without even the implied warranty of MERCHANTABILITY or
19  * FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public
20  * License for more details.
21  *
22  * You should have received a copy of the GNU General Public License
23  * along with The Inventra Controller Driver for Linux ; if not,
24  * write to the Free Software Foundation, Inc., 59 Temple Place,
25  * Suite 330, Boston, MA  02111-1307  USA
26  *
27  */
29 #include <linux/init.h>
30 #include <linux/module.h>
31 #include <linux/clk.h>
32 #include <linux/io.h>
33 #include <linux/platform_device.h>
34 #include <linux/dma-mapping.h>
36 #include <mach/da8xx.h>
37 #include <mach/usb.h>
39 #include "musb_core.h"
41 /*
42  * DA8XX specific definitions
43  */
45 /* USB 2.0 OTG module registers */
46 #define DA8XX_USB_REVISION_REG  0x00
47 #define DA8XX_USB_CTRL_REG      0x04
48 #define DA8XX_USB_STAT_REG      0x08
49 #define DA8XX_USB_EMULATION_REG 0x0c
50 #define DA8XX_USB_MODE_REG      0x10    /* Transparent, CDC, [Generic] RNDIS */
51 #define DA8XX_USB_AUTOREQ_REG   0x14
52 #define DA8XX_USB_SRP_FIX_TIME_REG 0x18
53 #define DA8XX_USB_TEARDOWN_REG  0x1c
54 #define DA8XX_USB_INTR_SRC_REG  0x20
55 #define DA8XX_USB_INTR_SRC_SET_REG 0x24
56 #define DA8XX_USB_INTR_SRC_CLEAR_REG 0x28
57 #define DA8XX_USB_INTR_MASK_REG 0x2c
58 #define DA8XX_USB_INTR_MASK_SET_REG 0x30
59 #define DA8XX_USB_INTR_MASK_CLEAR_REG 0x34
60 #define DA8XX_USB_INTR_SRC_MASKED_REG 0x38
61 #define DA8XX_USB_END_OF_INTR_REG 0x3c
62 #define DA8XX_USB_GENERIC_RNDIS_EP_SIZE_REG(n) (0x50 + (((n) - 1) << 2))
64 /* Control register bits */
65 #define DA8XX_SOFT_RESET_MASK   1
67 #define DA8XX_USB_TX_EP_MASK    0x1f            /* EP0 + 4 Tx EPs */
68 #define DA8XX_USB_RX_EP_MASK    0x1e            /* 4 Rx EPs */
70 /* USB interrupt register bits */
71 #define DA8XX_INTR_USB_SHIFT    16
72 #define DA8XX_INTR_USB_MASK     (0x1ff << DA8XX_INTR_USB_SHIFT) /* 8 Mentor */
73                                         /* interrupts and DRVVBUS interrupt */
74 #define DA8XX_INTR_DRVVBUS      0x100
75 #define DA8XX_INTR_RX_SHIFT     8
76 #define DA8XX_INTR_RX_MASK      (DA8XX_USB_RX_EP_MASK << DA8XX_INTR_RX_SHIFT)
77 #define DA8XX_INTR_TX_SHIFT     0
78 #define DA8XX_INTR_TX_MASK      (DA8XX_USB_TX_EP_MASK << DA8XX_INTR_TX_SHIFT)
80 #define DA8XX_MENTOR_CORE_OFFSET 0x400
82 #define CFGCHIP2        IO_ADDRESS(DA8XX_SYSCFG0_BASE + DA8XX_CFGCHIP2_REG)
84 struct da8xx_glue {
85         struct device           *dev;
86         struct platform_device  *musb;
87         struct clk              *clk;
88 };
90 /*
91  * REVISIT (PM): we should be able to keep the PHY in low power mode most
92  * of the time (24 MHz oscillator and PLL off, etc.) by setting POWER.D0
93  * and, when in host mode, autosuspending idle root ports... PHY_PLLON
94  * (overriding SUSPENDM?) then likely needs to stay off.
95  */
97 static inline void phy_on(void)
98 {
99         u32 cfgchip2 = __raw_readl(CFGCHIP2);
101         /*
102          * Start the on-chip PHY and its PLL.
103          */
104         cfgchip2 &= ~(CFGCHIP2_RESET | CFGCHIP2_PHYPWRDN | CFGCHIP2_OTGPWRDN);
105         cfgchip2 |= CFGCHIP2_PHY_PLLON;
106         __raw_writel(cfgchip2, CFGCHIP2);
108         pr_info("Waiting for USB PHY clock good...\n");
109         while (!(__raw_readl(CFGCHIP2) & CFGCHIP2_PHYCLKGD))
110                 cpu_relax();
113 static inline void phy_off(void)
115         u32 cfgchip2 = __raw_readl(CFGCHIP2);
117         /*
118          * Ensure that USB 1.1 reference clock is not being sourced from
119          * USB 2.0 PHY.  Otherwise do not power down the PHY.
120          */
121         if (!(cfgchip2 & CFGCHIP2_USB1PHYCLKMUX) &&
122              (cfgchip2 & CFGCHIP2_USB1SUSPENDM)) {
123                 pr_warning("USB 1.1 clocked from USB 2.0 PHY -- "
124                            "can't power it down\n");
125                 return;
126         }
128         /*
129          * Power down the on-chip PHY.
130          */
131         cfgchip2 |= CFGCHIP2_PHYPWRDN | CFGCHIP2_OTGPWRDN;
132         __raw_writel(cfgchip2, CFGCHIP2);
135 /*
136  * Because we don't set CTRL.UINT, it's "important" to:
137  *      - not read/write INTRUSB/INTRUSBE (except during
138  *        initial setup, as a workaround);
139  *      - use INTSET/INTCLR instead.
140  */
142 /**
143  * da8xx_musb_enable - enable interrupts
144  */
145 static void da8xx_musb_enable(struct musb *musb)
147         void __iomem *reg_base = musb->ctrl_base;
148         u32 mask;
150         /* Workaround: setup IRQs through both register sets. */
151         mask = ((musb->epmask & DA8XX_USB_TX_EP_MASK) << DA8XX_INTR_TX_SHIFT) |
152                ((musb->epmask & DA8XX_USB_RX_EP_MASK) << DA8XX_INTR_RX_SHIFT) |
153                DA8XX_INTR_USB_MASK;
154         musb_writel(reg_base, DA8XX_USB_INTR_MASK_SET_REG, mask);
156         /* Force the DRVVBUS IRQ so we can start polling for ID change. */
157         if (is_otg_enabled(musb))
158                 musb_writel(reg_base, DA8XX_USB_INTR_SRC_SET_REG,
159                             DA8XX_INTR_DRVVBUS << DA8XX_INTR_USB_SHIFT);
162 /**
163  * da8xx_musb_disable - disable HDRC and flush interrupts
164  */
165 static void da8xx_musb_disable(struct musb *musb)
167         void __iomem *reg_base = musb->ctrl_base;
169         musb_writel(reg_base, DA8XX_USB_INTR_MASK_CLEAR_REG,
170                     DA8XX_INTR_USB_MASK |
171                     DA8XX_INTR_TX_MASK | DA8XX_INTR_RX_MASK);
172         musb_writeb(musb->mregs, MUSB_DEVCTL, 0);
173         musb_writel(reg_base, DA8XX_USB_END_OF_INTR_REG, 0);
176 #define portstate(stmt)         stmt
178 static void da8xx_musb_set_vbus(struct musb *musb, int is_on)
180         WARN_ON(is_on && is_peripheral_active(musb));
183 #define POLL_SECONDS    2
185 static struct timer_list otg_workaround;
187 static void otg_timer(unsigned long _musb)
189         struct musb             *musb = (void *)_musb;
190         void __iomem            *mregs = musb->mregs;
191         u8                      devctl;
192         unsigned long           flags;
194         /*
195          * We poll because DaVinci's won't expose several OTG-critical
196          * status change events (from the transceiver) otherwise.
197          */
198         devctl = musb_readb(mregs, MUSB_DEVCTL);
199         dev_dbg(musb->controller, "Poll devctl %02x (%s)\n", devctl,
200                 otg_state_string(musb->xceiv->state));
202         spin_lock_irqsave(&musb->lock, flags);
203         switch (musb->xceiv->state) {
204         case OTG_STATE_A_WAIT_BCON:
205                 devctl &= ~MUSB_DEVCTL_SESSION;
206                 musb_writeb(musb->mregs, MUSB_DEVCTL, devctl);
208                 devctl = musb_readb(musb->mregs, MUSB_DEVCTL);
209                 if (devctl & MUSB_DEVCTL_BDEVICE) {
210                         musb->xceiv->state = OTG_STATE_B_IDLE;
211                         MUSB_DEV_MODE(musb);
212                 } else {
213                         musb->xceiv->state = OTG_STATE_A_IDLE;
214                         MUSB_HST_MODE(musb);
215                 }
216                 break;
217         case OTG_STATE_A_WAIT_VFALL:
218                 /*
219                  * Wait till VBUS falls below SessionEnd (~0.2 V); the 1.3
220                  * RTL seems to mis-handle session "start" otherwise (or in
221                  * our case "recover"), in routine "VBUS was valid by the time
222                  * VBUSERR got reported during enumeration" cases.
223                  */
224                 if (devctl & MUSB_DEVCTL_VBUS) {
225                         mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
226                         break;
227                 }
228                 musb->xceiv->state = OTG_STATE_A_WAIT_VRISE;
229                 musb_writel(musb->ctrl_base, DA8XX_USB_INTR_SRC_SET_REG,
230                             MUSB_INTR_VBUSERROR << DA8XX_INTR_USB_SHIFT);
231                 break;
232         case OTG_STATE_B_IDLE:
233                 if (!is_peripheral_enabled(musb))
234                         break;
236                 /*
237                  * There's no ID-changed IRQ, so we have no good way to tell
238                  * when to switch to the A-Default state machine (by setting
239                  * the DEVCTL.Session bit).
240                  *
241                  * Workaround:  whenever we're in B_IDLE, try setting the
242                  * session flag every few seconds.  If it works, ID was
243                  * grounded and we're now in the A-Default state machine.
244                  *
245                  * NOTE: setting the session flag is _supposed_ to trigger
246                  * SRP but clearly it doesn't.
247                  */
248                 musb_writeb(mregs, MUSB_DEVCTL, devctl | MUSB_DEVCTL_SESSION);
249                 devctl = musb_readb(mregs, MUSB_DEVCTL);
250                 if (devctl & MUSB_DEVCTL_BDEVICE)
251                         mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
252                 else
253                         musb->xceiv->state = OTG_STATE_A_IDLE;
254                 break;
255         default:
256                 break;
257         }
258         spin_unlock_irqrestore(&musb->lock, flags);
261 static void da8xx_musb_try_idle(struct musb *musb, unsigned long timeout)
263         static unsigned long last_timer;
265         if (!is_otg_enabled(musb))
266                 return;
268         if (timeout == 0)
269                 timeout = jiffies + msecs_to_jiffies(3);
271         /* Never idle if active, or when VBUS timeout is not set as host */
272         if (musb->is_active || (musb->a_wait_bcon == 0 &&
273                                 musb->xceiv->state == OTG_STATE_A_WAIT_BCON)) {
274                 dev_dbg(musb->controller, "%s active, deleting timer\n",
275                         otg_state_string(musb->xceiv->state));
276                 del_timer(&otg_workaround);
277                 last_timer = jiffies;
278                 return;
279         }
281         if (time_after(last_timer, timeout) && timer_pending(&otg_workaround)) {
282                 dev_dbg(musb->controller, "Longer idle timer already pending, ignoring...\n");
283                 return;
284         }
285         last_timer = timeout;
287         dev_dbg(musb->controller, "%s inactive, starting idle timer for %u ms\n",
288                 otg_state_string(musb->xceiv->state),
289                 jiffies_to_msecs(timeout - jiffies));
290         mod_timer(&otg_workaround, timeout);
293 static irqreturn_t da8xx_musb_interrupt(int irq, void *hci)
295         struct musb             *musb = hci;
296         void __iomem            *reg_base = musb->ctrl_base;
297         unsigned long           flags;
298         irqreturn_t             ret = IRQ_NONE;
299         u32                     status;
301         spin_lock_irqsave(&musb->lock, flags);
303         /*
304          * NOTE: DA8XX shadows the Mentor IRQs.  Don't manage them through
305          * the Mentor registers (except for setup), use the TI ones and EOI.
306          */
308         /* Acknowledge and handle non-CPPI interrupts */
309         status = musb_readl(reg_base, DA8XX_USB_INTR_SRC_MASKED_REG);
310         if (!status)
311                 goto eoi;
313         musb_writel(reg_base, DA8XX_USB_INTR_SRC_CLEAR_REG, status);
314         dev_dbg(musb->controller, "USB IRQ %08x\n", status);
316         musb->int_rx = (status & DA8XX_INTR_RX_MASK) >> DA8XX_INTR_RX_SHIFT;
317         musb->int_tx = (status & DA8XX_INTR_TX_MASK) >> DA8XX_INTR_TX_SHIFT;
318         musb->int_usb = (status & DA8XX_INTR_USB_MASK) >> DA8XX_INTR_USB_SHIFT;
320         /*
321          * DRVVBUS IRQs are the only proxy we have (a very poor one!) for
322          * DA8xx's missing ID change IRQ.  We need an ID change IRQ to
323          * switch appropriately between halves of the OTG state machine.
324          * Managing DEVCTL.Session per Mentor docs requires that we know its
325          * value but DEVCTL.BDevice is invalid without DEVCTL.Session set.
326          * Also, DRVVBUS pulses for SRP (but not at 5 V)...
327          */
328         if (status & (DA8XX_INTR_DRVVBUS << DA8XX_INTR_USB_SHIFT)) {
329                 int drvvbus = musb_readl(reg_base, DA8XX_USB_STAT_REG);
330                 void __iomem *mregs = musb->mregs;
331                 u8 devctl = musb_readb(mregs, MUSB_DEVCTL);
332                 int err;
334                 err = is_host_enabled(musb) && (musb->int_usb &
335                                                 MUSB_INTR_VBUSERROR);
336                 if (err) {
337                         /*
338                          * The Mentor core doesn't debounce VBUS as needed
339                          * to cope with device connect current spikes. This
340                          * means it's not uncommon for bus-powered devices
341                          * to get VBUS errors during enumeration.
342                          *
343                          * This is a workaround, but newer RTL from Mentor
344                          * seems to allow a better one: "re"-starting sessions
345                          * without waiting for VBUS to stop registering in
346                          * devctl.
347                          */
348                         musb->int_usb &= ~MUSB_INTR_VBUSERROR;
349                         musb->xceiv->state = OTG_STATE_A_WAIT_VFALL;
350                         mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
351                         WARNING("VBUS error workaround (delay coming)\n");
352                 } else if (is_host_enabled(musb) && drvvbus) {
353                         MUSB_HST_MODE(musb);
354                         musb->xceiv->default_a = 1;
355                         musb->xceiv->state = OTG_STATE_A_WAIT_VRISE;
356                         portstate(musb->port1_status |= USB_PORT_STAT_POWER);
357                         del_timer(&otg_workaround);
358                 } else {
359                         musb->is_active = 0;
360                         MUSB_DEV_MODE(musb);
361                         musb->xceiv->default_a = 0;
362                         musb->xceiv->state = OTG_STATE_B_IDLE;
363                         portstate(musb->port1_status &= ~USB_PORT_STAT_POWER);
364                 }
366                 dev_dbg(musb->controller, "VBUS %s (%s)%s, devctl %02x\n",
367                                 drvvbus ? "on" : "off",
368                                 otg_state_string(musb->xceiv->state),
369                                 err ? " ERROR" : "",
370                                 devctl);
371                 ret = IRQ_HANDLED;
372         }
374         if (musb->int_tx || musb->int_rx || musb->int_usb)
375                 ret |= musb_interrupt(musb);
377  eoi:
378         /* EOI needs to be written for the IRQ to be re-asserted. */
379         if (ret == IRQ_HANDLED || status)
380                 musb_writel(reg_base, DA8XX_USB_END_OF_INTR_REG, 0);
382         /* Poll for ID change */
383         if (is_otg_enabled(musb) && musb->xceiv->state == OTG_STATE_B_IDLE)
384                 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
386         spin_unlock_irqrestore(&musb->lock, flags);
388         return ret;
391 static int da8xx_musb_set_mode(struct musb *musb, u8 musb_mode)
393         u32 cfgchip2 = __raw_readl(CFGCHIP2);
395         cfgchip2 &= ~CFGCHIP2_OTGMODE;
396         switch (musb_mode) {
397         case MUSB_HOST:         /* Force VBUS valid, ID = 0 */
398                 cfgchip2 |= CFGCHIP2_FORCE_HOST;
399                 break;
400         case MUSB_PERIPHERAL:   /* Force VBUS valid, ID = 1 */
401                 cfgchip2 |= CFGCHIP2_FORCE_DEVICE;
402                 break;
403         case MUSB_OTG:          /* Don't override the VBUS/ID comparators */
404                 cfgchip2 |= CFGCHIP2_NO_OVERRIDE;
405                 break;
406         default:
407                 dev_dbg(musb->controller, "Trying to set unsupported mode %u\n", musb_mode);
408         }
410         __raw_writel(cfgchip2, CFGCHIP2);
411         return 0;
414 static int da8xx_musb_init(struct musb *musb)
416         void __iomem *reg_base = musb->ctrl_base;
417         u32 rev;
419         musb->mregs += DA8XX_MENTOR_CORE_OFFSET;
421         /* Returns zero if e.g. not clocked */
422         rev = musb_readl(reg_base, DA8XX_USB_REVISION_REG);
423         if (!rev)
424                 goto fail;
426         usb_nop_xceiv_register();
427         musb->xceiv = otg_get_transceiver();
428         if (!musb->xceiv)
429                 goto fail;
431         if (is_host_enabled(musb))
432                 setup_timer(&otg_workaround, otg_timer, (unsigned long)musb);
434         /* Reset the controller */
435         musb_writel(reg_base, DA8XX_USB_CTRL_REG, DA8XX_SOFT_RESET_MASK);
437         /* Start the on-chip PHY and its PLL. */
438         phy_on();
440         msleep(5);
442         /* NOTE: IRQs are in mixed mode, not bypass to pure MUSB */
443         pr_debug("DA8xx OTG revision %08x, PHY %03x, control %02x\n",
444                  rev, __raw_readl(CFGCHIP2),
445                  musb_readb(reg_base, DA8XX_USB_CTRL_REG));
447         musb->isr = da8xx_musb_interrupt;
448         return 0;
449 fail:
450         return -ENODEV;
453 static int da8xx_musb_exit(struct musb *musb)
455         if (is_host_enabled(musb))
456                 del_timer_sync(&otg_workaround);
458         phy_off();
460         otg_put_transceiver(musb->xceiv);
461         usb_nop_xceiv_unregister();
463         return 0;
466 static const struct musb_platform_ops da8xx_ops = {
467         .fifo_mode      = 2,
468         .flags          = MUSB_GLUE_EP_ADDR_FLAT_MAPPING,
469         .init           = da8xx_musb_init,
470         .exit           = da8xx_musb_exit,
472         .enable         = da8xx_musb_enable,
473         .disable        = da8xx_musb_disable,
475         .set_mode       = da8xx_musb_set_mode,
476         .try_idle       = da8xx_musb_try_idle,
478         .set_vbus       = da8xx_musb_set_vbus,
480         .read_fifo      = musb_read_fifo,
481         .write_fifo     = musb_write_fifo,
482 };
484 static u64 da8xx_dmamask = DMA_BIT_MASK(32);
486 static int __init da8xx_probe(struct platform_device *pdev)
488         struct musb_hdrc_platform_data  *pdata = pdev->dev.platform_data;
489         struct platform_device          *musb;
490         struct da8xx_glue               *glue;
492         struct clk                      *clk;
494         int                             ret = -ENOMEM;
496         glue = kzalloc(sizeof(*glue), GFP_KERNEL);
497         if (!glue) {
498                 dev_err(&pdev->dev, "failed to allocate glue context\n");
499                 goto err0;
500         }
502         musb = platform_device_alloc("musb-hdrc", -1);
503         if (!musb) {
504                 dev_err(&pdev->dev, "failed to allocate musb device\n");
505                 goto err1;
506         }
508         clk = clk_get(&pdev->dev, "usb20");
509         if (IS_ERR(clk)) {
510                 dev_err(&pdev->dev, "failed to get clock\n");
511                 ret = PTR_ERR(clk);
512                 goto err2;
513         }
515         ret = clk_enable(clk);
516         if (ret) {
517                 dev_err(&pdev->dev, "failed to enable clock\n");
518                 goto err3;
519         }
521         musb->dev.parent                = &pdev->dev;
522         musb->dev.dma_mask              = &da8xx_dmamask;
523         musb->dev.coherent_dma_mask     = da8xx_dmamask;
525         glue->dev                       = &pdev->dev;
526         glue->musb                      = musb;
527         glue->clk                       = clk;
529         pdata->platform_ops             = &da8xx_ops;
531         platform_set_drvdata(pdev, glue);
533         ret = platform_device_add_resources(musb, pdev->resource,
534                         pdev->num_resources);
535         if (ret) {
536                 dev_err(&pdev->dev, "failed to add resources\n");
537                 goto err4;
538         }
540         ret = platform_device_add_data(musb, pdata, sizeof(*pdata));
541         if (ret) {
542                 dev_err(&pdev->dev, "failed to add platform_data\n");
543                 goto err4;
544         }
546         ret = platform_device_add(musb);
547         if (ret) {
548                 dev_err(&pdev->dev, "failed to register musb device\n");
549                 goto err4;
550         }
552         return 0;
554 err4:
555         clk_disable(clk);
557 err3:
558         clk_put(clk);
560 err2:
561         platform_device_put(musb);
563 err1:
564         kfree(glue);
566 err0:
567         return ret;
570 static int __exit da8xx_remove(struct platform_device *pdev)
572         struct da8xx_glue               *glue = platform_get_drvdata(pdev);
574         platform_device_del(glue->musb);
575         platform_device_put(glue->musb);
576         clk_disable(glue->clk);
577         clk_put(glue->clk);
578         kfree(glue);
580         return 0;
583 static struct platform_driver da8xx_driver = {
584         .remove         = __exit_p(da8xx_remove),
585         .driver         = {
586                 .name   = "musb-da8xx",
587         },
588 };
590 MODULE_DESCRIPTION("DA8xx/OMAP-L1x MUSB Glue Layer");
591 MODULE_AUTHOR("Sergei Shtylyov <sshtylyov@ru.mvista.com>");
592 MODULE_LICENSE("GPL v2");
594 static int __init da8xx_init(void)
596         return platform_driver_probe(&da8xx_driver, da8xx_probe);
598 subsys_initcall(da8xx_init);
600 static void __exit da8xx_exit(void)
602         platform_driver_unregister(&da8xx_driver);
604 module_exit(da8xx_exit);