4e0b21a4cbb9b8c1291f8db61ae5f7aa5be615c4
1 /*
2 * Copyright (C) 2005-2006 by Texas Instruments
3 *
4 * This file is part of the Inventra Controller Driver for Linux.
5 *
6 * The Inventra Controller Driver for Linux is free software; you
7 * can redistribute it and/or modify it under the terms of the GNU
8 * General Public License version 2 as published by the Free Software
9 * Foundation.
10 *
11 * The Inventra Controller Driver for Linux is distributed in
12 * the hope that it will be useful, but WITHOUT ANY WARRANTY;
13 * without even the implied warranty of MERCHANTABILITY or
14 * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public
15 * License for more details.
16 *
17 * You should have received a copy of the GNU General Public License
18 * along with The Inventra Controller Driver for Linux ; if not,
19 * write to the Free Software Foundation, Inc., 59 Temple Place,
20 * Suite 330, Boston, MA 02111-1307 USA
21 *
22 */
24 #include <linux/module.h>
25 #include <linux/kernel.h>
26 #include <linux/sched.h>
27 #include <linux/init.h>
28 #include <linux/list.h>
29 #include <linux/delay.h>
30 #include <linux/clk.h>
31 #include <linux/io.h>
32 #include <linux/gpio.h>
33 #include <linux/platform_device.h>
34 #include <linux/dma-mapping.h>
36 #include <mach/hardware.h>
37 #include <mach/memory.h>
38 #include <asm/gpio.h>
39 #include <mach/cputype.h>
41 #include <asm/mach-types.h>
43 #include "musb_core.h"
45 #ifdef CONFIG_MACH_DAVINCI_EVM
46 #define GPIO_nVBUS_DRV 160
47 #endif
49 #include "davinci.h"
50 #include "cppi_dma.h"
53 #define USB_PHY_CTRL IO_ADDRESS(USBPHY_CTL_PADDR)
54 #define DM355_DEEPSLEEP IO_ADDRESS(DM355_DEEPSLEEP_PADDR)
56 struct davinci_glue {
57 struct device *dev;
58 struct platform_device *musb;
59 struct clk *clk;
60 };
62 /* REVISIT (PM) we should be able to keep the PHY in low power mode most
63 * of the time (24 MHZ oscillator and PLL off, etc) by setting POWER.D0
64 * and, when in host mode, autosuspending idle root ports... PHYPLLON
65 * (overriding SUSPENDM?) then likely needs to stay off.
66 */
68 static inline void phy_on(void)
69 {
70 u32 phy_ctrl = __raw_readl(USB_PHY_CTRL);
72 /* power everything up; start the on-chip PHY and its PLL */
73 phy_ctrl &= ~(USBPHY_OSCPDWN | USBPHY_OTGPDWN | USBPHY_PHYPDWN);
74 phy_ctrl |= USBPHY_SESNDEN | USBPHY_VBDTCTEN | USBPHY_PHYPLLON;
75 __raw_writel(phy_ctrl, USB_PHY_CTRL);
77 /* wait for PLL to lock before proceeding */
78 while ((__raw_readl(USB_PHY_CTRL) & USBPHY_PHYCLKGD) == 0)
79 cpu_relax();
80 }
82 static inline void phy_off(void)
83 {
84 u32 phy_ctrl = __raw_readl(USB_PHY_CTRL);
86 /* powerdown the on-chip PHY, its PLL, and the OTG block */
87 phy_ctrl &= ~(USBPHY_SESNDEN | USBPHY_VBDTCTEN | USBPHY_PHYPLLON);
88 phy_ctrl |= USBPHY_OSCPDWN | USBPHY_OTGPDWN | USBPHY_PHYPDWN;
89 __raw_writel(phy_ctrl, USB_PHY_CTRL);
90 }
92 static int dma_off = 1;
94 static void davinci_musb_enable(struct musb *musb)
95 {
96 u32 tmp, old, val;
98 /* workaround: setup irqs through both register sets */
99 tmp = (musb->epmask & DAVINCI_USB_TX_ENDPTS_MASK)
100 << DAVINCI_USB_TXINT_SHIFT;
101 musb_writel(musb->ctrl_base, DAVINCI_USB_INT_MASK_SET_REG, tmp);
102 old = tmp;
103 tmp = (musb->epmask & (0xfffe & DAVINCI_USB_RX_ENDPTS_MASK))
104 << DAVINCI_USB_RXINT_SHIFT;
105 musb_writel(musb->ctrl_base, DAVINCI_USB_INT_MASK_SET_REG, tmp);
106 tmp |= old;
108 val = ~MUSB_INTR_SOF;
109 tmp |= ((val & 0x01ff) << DAVINCI_USB_USBINT_SHIFT);
110 musb_writel(musb->ctrl_base, DAVINCI_USB_INT_MASK_SET_REG, tmp);
112 if (is_dma_capable() && !dma_off)
113 printk(KERN_WARNING "%s %s: dma not reactivated\n",
114 __FILE__, __func__);
115 else
116 dma_off = 0;
118 /* force a DRVVBUS irq so we can start polling for ID change */
119 if (is_otg_enabled(musb))
120 musb_writel(musb->ctrl_base, DAVINCI_USB_INT_SET_REG,
121 DAVINCI_INTR_DRVVBUS << DAVINCI_USB_USBINT_SHIFT);
122 }
124 /*
125 * Disable the HDRC and flush interrupts
126 */
127 static void davinci_musb_disable(struct musb *musb)
128 {
129 /* because we don't set CTRLR.UINT, "important" to:
130 * - not read/write INTRUSB/INTRUSBE
131 * - (except during initial setup, as workaround)
132 * - use INTSETR/INTCLRR instead
133 */
134 musb_writel(musb->ctrl_base, DAVINCI_USB_INT_MASK_CLR_REG,
135 DAVINCI_USB_USBINT_MASK
136 | DAVINCI_USB_TXINT_MASK
137 | DAVINCI_USB_RXINT_MASK);
138 musb_writeb(musb->mregs, MUSB_DEVCTL, 0);
139 musb_writel(musb->ctrl_base, DAVINCI_USB_EOI_REG, 0);
141 if (is_dma_capable() && !dma_off)
142 WARNING("dma still active\n");
143 }
146 #define portstate(stmt) stmt
148 /*
149 * VBUS SWITCHING IS BOARD-SPECIFIC ... at least for the DM6446 EVM,
150 * which doesn't wire DRVVBUS to the FET that switches it. Unclear
151 * if that's a problem with the DM6446 chip or just with that board.
152 *
153 * In either case, the DM355 EVM automates DRVVBUS the normal way,
154 * when J10 is out, and TI documents it as handling OTG.
155 */
157 #ifdef CONFIG_MACH_DAVINCI_EVM
159 static int vbus_state = -1;
161 /* I2C operations are always synchronous, and require a task context.
162 * With unloaded systems, using the shared workqueue seems to suffice
163 * to satisfy the 100msec A_WAIT_VRISE timeout...
164 */
165 static void evm_deferred_drvvbus(struct work_struct *ignored)
166 {
167 gpio_set_value_cansleep(GPIO_nVBUS_DRV, vbus_state);
168 vbus_state = !vbus_state;
169 }
171 #endif /* EVM */
173 static void davinci_musb_source_power(struct musb *musb, int is_on, int immediate)
174 {
175 #ifdef CONFIG_MACH_DAVINCI_EVM
176 if (is_on)
177 is_on = 1;
179 if (vbus_state == is_on)
180 return;
181 vbus_state = !is_on; /* 0/1 vs "-1 == unknown/init" */
183 if (machine_is_davinci_evm()) {
184 static DECLARE_WORK(evm_vbus_work, evm_deferred_drvvbus);
186 if (immediate)
187 gpio_set_value_cansleep(GPIO_nVBUS_DRV, vbus_state);
188 else
189 schedule_work(&evm_vbus_work);
190 }
191 if (immediate)
192 vbus_state = is_on;
193 #endif
194 }
196 static void davinci_musb_set_vbus(struct musb *musb, int is_on)
197 {
198 WARN_ON(is_on && is_peripheral_active(musb));
199 davinci_musb_source_power(musb, is_on, 0);
200 }
203 #define POLL_SECONDS 2
205 static struct timer_list otg_workaround;
207 static void otg_timer(unsigned long _musb)
208 {
209 struct musb *musb = (void *)_musb;
210 void __iomem *mregs = musb->mregs;
211 u8 devctl;
212 unsigned long flags;
214 /* We poll because DaVinci's won't expose several OTG-critical
215 * status change events (from the transceiver) otherwise.
216 */
217 devctl = musb_readb(mregs, MUSB_DEVCTL);
218 dev_dbg(musb->controller, "poll devctl %02x (%s)\n", devctl,
219 otg_state_string(musb->xceiv->state));
221 spin_lock_irqsave(&musb->lock, flags);
222 switch (musb->xceiv->state) {
223 case OTG_STATE_A_WAIT_VFALL:
224 /* Wait till VBUS falls below SessionEnd (~0.2V); the 1.3 RTL
225 * seems to mis-handle session "start" otherwise (or in our
226 * case "recover"), in routine "VBUS was valid by the time
227 * VBUSERR got reported during enumeration" cases.
228 */
229 if (devctl & MUSB_DEVCTL_VBUS) {
230 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
231 break;
232 }
233 musb->xceiv->state = OTG_STATE_A_WAIT_VRISE;
234 musb_writel(musb->ctrl_base, DAVINCI_USB_INT_SET_REG,
235 MUSB_INTR_VBUSERROR << DAVINCI_USB_USBINT_SHIFT);
236 break;
237 case OTG_STATE_B_IDLE:
238 if (!is_peripheral_enabled(musb))
239 break;
241 /* There's no ID-changed IRQ, so we have no good way to tell
242 * when to switch to the A-Default state machine (by setting
243 * the DEVCTL.SESSION flag).
244 *
245 * Workaround: whenever we're in B_IDLE, try setting the
246 * session flag every few seconds. If it works, ID was
247 * grounded and we're now in the A-Default state machine.
248 *
249 * NOTE setting the session flag is _supposed_ to trigger
250 * SRP, but clearly it doesn't.
251 */
252 musb_writeb(mregs, MUSB_DEVCTL,
253 devctl | MUSB_DEVCTL_SESSION);
254 devctl = musb_readb(mregs, MUSB_DEVCTL);
255 if (devctl & MUSB_DEVCTL_BDEVICE)
256 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
257 else
258 musb->xceiv->state = OTG_STATE_A_IDLE;
259 break;
260 default:
261 break;
262 }
263 spin_unlock_irqrestore(&musb->lock, flags);
264 }
266 static irqreturn_t davinci_musb_interrupt(int irq, void *__hci)
267 {
268 unsigned long flags;
269 irqreturn_t retval = IRQ_NONE;
270 struct musb *musb = __hci;
271 void __iomem *tibase = musb->ctrl_base;
272 struct cppi *cppi;
273 u32 tmp;
275 spin_lock_irqsave(&musb->lock, flags);
277 /* NOTE: DaVinci shadows the Mentor IRQs. Don't manage them through
278 * the Mentor registers (except for setup), use the TI ones and EOI.
279 *
280 * Docs describe irq "vector" registers associated with the CPPI and
281 * USB EOI registers. These hold a bitmask corresponding to the
282 * current IRQ, not an irq handler address. Would using those bits
283 * resolve some of the races observed in this dispatch code??
284 */
286 /* CPPI interrupts share the same IRQ line, but have their own
287 * mask, state, "vector", and EOI registers.
288 */
289 cppi = container_of(musb->dma_controller, struct cppi, controller);
290 if (is_cppi_enabled() && musb->dma_controller && !cppi->irq)
291 retval = cppi_interrupt(irq, __hci);
293 /* ack and handle non-CPPI interrupts */
294 tmp = musb_readl(tibase, DAVINCI_USB_INT_SRC_MASKED_REG);
295 musb_writel(tibase, DAVINCI_USB_INT_SRC_CLR_REG, tmp);
296 dev_dbg(musb->controller, "IRQ %08x\n", tmp);
298 musb->int_rx = (tmp & DAVINCI_USB_RXINT_MASK)
299 >> DAVINCI_USB_RXINT_SHIFT;
300 musb->int_tx = (tmp & DAVINCI_USB_TXINT_MASK)
301 >> DAVINCI_USB_TXINT_SHIFT;
302 musb->int_usb = (tmp & DAVINCI_USB_USBINT_MASK)
303 >> DAVINCI_USB_USBINT_SHIFT;
305 /* DRVVBUS irqs are the only proxy we have (a very poor one!) for
306 * DaVinci's missing ID change IRQ. We need an ID change IRQ to
307 * switch appropriately between halves of the OTG state machine.
308 * Managing DEVCTL.SESSION per Mentor docs requires we know its
309 * value, but DEVCTL.BDEVICE is invalid without DEVCTL.SESSION set.
310 * Also, DRVVBUS pulses for SRP (but not at 5V) ...
311 */
312 if (tmp & (DAVINCI_INTR_DRVVBUS << DAVINCI_USB_USBINT_SHIFT)) {
313 int drvvbus = musb_readl(tibase, DAVINCI_USB_STAT_REG);
314 void __iomem *mregs = musb->mregs;
315 u8 devctl = musb_readb(mregs, MUSB_DEVCTL);
316 int err = musb->int_usb & MUSB_INTR_VBUSERROR;
318 err = is_host_enabled(musb)
319 && (musb->int_usb & MUSB_INTR_VBUSERROR);
320 if (err) {
321 /* The Mentor core doesn't debounce VBUS as needed
322 * to cope with device connect current spikes. This
323 * means it's not uncommon for bus-powered devices
324 * to get VBUS errors during enumeration.
325 *
326 * This is a workaround, but newer RTL from Mentor
327 * seems to allow a better one: "re"starting sessions
328 * without waiting (on EVM, a **long** time) for VBUS
329 * to stop registering in devctl.
330 */
331 musb->int_usb &= ~MUSB_INTR_VBUSERROR;
332 musb->xceiv->state = OTG_STATE_A_WAIT_VFALL;
333 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
334 WARNING("VBUS error workaround (delay coming)\n");
335 } else if (is_host_enabled(musb) && drvvbus) {
336 MUSB_HST_MODE(musb);
337 musb->xceiv->default_a = 1;
338 musb->xceiv->state = OTG_STATE_A_WAIT_VRISE;
339 portstate(musb->port1_status |= USB_PORT_STAT_POWER);
340 del_timer(&otg_workaround);
341 } else {
342 musb->is_active = 0;
343 MUSB_DEV_MODE(musb);
344 musb->xceiv->default_a = 0;
345 musb->xceiv->state = OTG_STATE_B_IDLE;
346 portstate(musb->port1_status &= ~USB_PORT_STAT_POWER);
347 }
349 /* NOTE: this must complete poweron within 100 msec
350 * (OTG_TIME_A_WAIT_VRISE) but we don't check for that.
351 */
352 davinci_musb_source_power(musb, drvvbus, 0);
353 dev_dbg(musb->controller, "VBUS %s (%s)%s, devctl %02x\n",
354 drvvbus ? "on" : "off",
355 otg_state_string(musb->xceiv->state),
356 err ? " ERROR" : "",
357 devctl);
358 retval = IRQ_HANDLED;
359 }
361 if (musb->int_tx || musb->int_rx || musb->int_usb)
362 retval |= musb_interrupt(musb);
364 /* irq stays asserted until EOI is written */
365 musb_writel(tibase, DAVINCI_USB_EOI_REG, 0);
367 /* poll for ID change */
368 if (is_otg_enabled(musb)
369 && musb->xceiv->state == OTG_STATE_B_IDLE)
370 mod_timer(&otg_workaround, jiffies + POLL_SECONDS * HZ);
372 spin_unlock_irqrestore(&musb->lock, flags);
374 return retval;
375 }
377 static int davinci_musb_set_mode(struct musb *musb, u8 mode)
378 {
379 /* EVM can't do this (right?) */
380 return -EIO;
381 }
383 static int davinci_musb_init(struct musb *musb)
384 {
385 void __iomem *tibase = musb->ctrl_base;
386 u32 revision;
388 usb_nop_xceiv_register();
389 musb->xceiv = otg_get_transceiver();
390 if (!musb->xceiv)
391 return -ENODEV;
393 musb->mregs += DAVINCI_BASE_OFFSET;
395 /* returns zero if e.g. not clocked */
396 revision = musb_readl(tibase, DAVINCI_USB_VERSION_REG);
397 if (revision == 0)
398 goto fail;
400 if (is_host_enabled(musb))
401 setup_timer(&otg_workaround, otg_timer, (unsigned long) musb);
403 davinci_musb_source_power(musb, 0, 1);
405 /* dm355 EVM swaps D+/D- for signal integrity, and
406 * is clocked from the main 24 MHz crystal.
407 */
408 if (machine_is_davinci_dm355_evm()) {
409 u32 phy_ctrl = __raw_readl(USB_PHY_CTRL);
411 phy_ctrl &= ~(3 << 9);
412 phy_ctrl |= USBPHY_DATAPOL;
413 __raw_writel(phy_ctrl, USB_PHY_CTRL);
414 }
416 /* On dm355, the default-A state machine needs DRVVBUS control.
417 * If we won't be a host, there's no need to turn it on.
418 */
419 if (cpu_is_davinci_dm355()) {
420 u32 deepsleep = __raw_readl(DM355_DEEPSLEEP);
422 if (is_host_enabled(musb)) {
423 deepsleep &= ~DRVVBUS_OVERRIDE;
424 } else {
425 deepsleep &= ~DRVVBUS_FORCE;
426 deepsleep |= DRVVBUS_OVERRIDE;
427 }
428 __raw_writel(deepsleep, DM355_DEEPSLEEP);
429 }
431 /* reset the controller */
432 musb_writel(tibase, DAVINCI_USB_CTRL_REG, 0x1);
434 /* start the on-chip PHY and its PLL */
435 phy_on();
437 msleep(5);
439 /* NOTE: irqs are in mixed mode, not bypass to pure-musb */
440 pr_debug("DaVinci OTG revision %08x phy %03x control %02x\n",
441 revision, __raw_readl(USB_PHY_CTRL),
442 musb_readb(tibase, DAVINCI_USB_CTRL_REG));
444 musb->isr = davinci_musb_interrupt;
445 return 0;
447 fail:
448 otg_put_transceiver(musb->xceiv);
449 usb_nop_xceiv_unregister();
450 return -ENODEV;
451 }
453 static int davinci_musb_exit(struct musb *musb)
454 {
455 if (is_host_enabled(musb))
456 del_timer_sync(&otg_workaround);
458 /* force VBUS off */
459 if (cpu_is_davinci_dm355()) {
460 u32 deepsleep = __raw_readl(DM355_DEEPSLEEP);
462 deepsleep &= ~DRVVBUS_FORCE;
463 deepsleep |= DRVVBUS_OVERRIDE;
464 __raw_writel(deepsleep, DM355_DEEPSLEEP);
465 }
467 davinci_musb_source_power(musb, 0 /*off*/, 1);
469 /* delay, to avoid problems with module reload */
470 if (is_host_enabled(musb) && musb->xceiv->default_a) {
471 int maxdelay = 30;
472 u8 devctl, warn = 0;
474 /* if there's no peripheral connected, this can take a
475 * long time to fall, especially on EVM with huge C133.
476 */
477 do {
478 devctl = musb_readb(musb->mregs, MUSB_DEVCTL);
479 if (!(devctl & MUSB_DEVCTL_VBUS))
480 break;
481 if ((devctl & MUSB_DEVCTL_VBUS) != warn) {
482 warn = devctl & MUSB_DEVCTL_VBUS;
483 dev_dbg(musb->controller, "VBUS %d\n",
484 warn >> MUSB_DEVCTL_VBUS_SHIFT);
485 }
486 msleep(1000);
487 maxdelay--;
488 } while (maxdelay > 0);
490 /* in OTG mode, another host might be connected */
491 if (devctl & MUSB_DEVCTL_VBUS)
492 dev_dbg(musb->controller, "VBUS off timeout (devctl %02x)\n", devctl);
493 }
495 phy_off();
497 otg_put_transceiver(musb->xceiv);
498 usb_nop_xceiv_unregister();
500 return 0;
501 }
503 static const struct musb_platform_ops davinci_ops = {
504 .fifo_mode = 2,
505 .init = davinci_musb_init,
506 .exit = davinci_musb_exit,
508 .enable = davinci_musb_enable,
509 .disable = davinci_musb_disable,
511 .set_mode = davinci_musb_set_mode,
513 .set_vbus = davinci_musb_set_vbus,
515 .read_fifo = musb_read_fifo,
516 .write_fifo = musb_write_fifo,
517 };
519 static u64 davinci_dmamask = DMA_BIT_MASK(32);
521 static int __init davinci_probe(struct platform_device *pdev)
522 {
523 struct musb_hdrc_platform_data *pdata = pdev->dev.platform_data;
524 struct platform_device *musb;
525 struct davinci_glue *glue;
526 struct clk *clk;
528 int ret = -ENOMEM;
530 glue = kzalloc(sizeof(*glue), GFP_KERNEL);
531 if (!glue) {
532 dev_err(&pdev->dev, "failed to allocate glue context\n");
533 goto err0;
534 }
536 musb = platform_device_alloc("musb-hdrc", -1);
537 if (!musb) {
538 dev_err(&pdev->dev, "failed to allocate musb device\n");
539 goto err1;
540 }
542 clk = clk_get(&pdev->dev, "usb");
543 if (IS_ERR(clk)) {
544 dev_err(&pdev->dev, "failed to get clock\n");
545 ret = PTR_ERR(clk);
546 goto err2;
547 }
549 ret = clk_enable(clk);
550 if (ret) {
551 dev_err(&pdev->dev, "failed to enable clock\n");
552 goto err3;
553 }
555 musb->dev.parent = &pdev->dev;
556 musb->dev.dma_mask = &davinci_dmamask;
557 musb->dev.coherent_dma_mask = davinci_dmamask;
559 glue->dev = &pdev->dev;
560 glue->musb = musb;
561 glue->clk = clk;
563 pdata->platform_ops = &davinci_ops;
565 platform_set_drvdata(pdev, glue);
567 ret = platform_device_add_resources(musb, pdev->resource,
568 pdev->num_resources);
569 if (ret) {
570 dev_err(&pdev->dev, "failed to add resources\n");
571 goto err4;
572 }
574 ret = platform_device_add_data(musb, pdata, sizeof(*pdata));
575 if (ret) {
576 dev_err(&pdev->dev, "failed to add platform_data\n");
577 goto err4;
578 }
580 ret = platform_device_add(musb);
581 if (ret) {
582 dev_err(&pdev->dev, "failed to register musb device\n");
583 goto err4;
584 }
586 return 0;
588 err4:
589 clk_disable(clk);
591 err3:
592 clk_put(clk);
594 err2:
595 platform_device_put(musb);
597 err1:
598 kfree(glue);
600 err0:
601 return ret;
602 }
604 static int __exit davinci_remove(struct platform_device *pdev)
605 {
606 struct davinci_glue *glue = platform_get_drvdata(pdev);
608 platform_device_del(glue->musb);
609 platform_device_put(glue->musb);
610 clk_disable(glue->clk);
611 clk_put(glue->clk);
612 kfree(glue);
614 return 0;
615 }
617 static struct platform_driver davinci_driver = {
618 .remove = __exit_p(davinci_remove),
619 .driver = {
620 .name = "musb-davinci",
621 },
622 };
624 MODULE_DESCRIPTION("DaVinci MUSB Glue Layer");
625 MODULE_AUTHOR("Felipe Balbi <balbi@ti.com>");
626 MODULE_LICENSE("GPL v2");
628 static int __init davinci_init(void)
629 {
630 return platform_driver_probe(&davinci_driver, davinci_probe);
631 }
632 subsys_initcall(davinci_init);
634 static void __exit davinci_exit(void)
635 {
636 platform_driver_unregister(&davinci_driver);
637 }
638 module_exit(davinci_exit);