]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - drivers/video/backlight/Kconfig
backlight: Add TLC59108 backlight control driver
[sitara-epos/sitara-epos-kernel.git] / drivers / video / backlight / Kconfig
1 #
2 # Backlight & LCD drivers configuration
3 #
5 menuconfig BACKLIGHT_LCD_SUPPORT
6         bool "Backlight & LCD device support"
7         help
8           Enable this to be able to choose the drivers for controlling the
9           backlight and the LCD panel on some platforms, for example on PDAs.
11 if BACKLIGHT_LCD_SUPPORT
13 #
14 # LCD
15 #
16 config LCD_CLASS_DEVICE
17         tristate "Lowlevel LCD controls"
18         default m
19         help
20           This framework adds support for low-level control of LCD.
21           Some framebuffer devices connect to platform-specific LCD modules
22           in order to have a platform-specific way to control the flat panel
23           (contrast and applying power to the LCD (not to the backlight!)).
25           To have support for your specific LCD panel you will have to
26           select the proper drivers which depend on this option.
28 if LCD_CLASS_DEVICE
30 config LCD_CORGI
31         tristate "LCD Panel support for SHARP corgi/spitz model"
32         depends on SPI_MASTER && PXA_SHARPSL
33         help
34           Say y here to support the LCD panels usually found on SHARP
35           corgi (C7x0) and spitz (Cxx00) models.
37 config LCD_L4F00242T03
38         tristate "Epson L4F00242T03 LCD"
39         depends on SPI_MASTER && GENERIC_GPIO
40         help
41           SPI driver for Epson L4F00242T03. This provides basic support
42           for init and powering the LCD up/down through a sysfs interface.
44 config LCD_LMS283GF05
45         tristate "Samsung LMS283GF05 LCD"
46         depends on SPI_MASTER && GENERIC_GPIO
47         help
48           SPI driver for Samsung LMS283GF05. This provides basic support
49           for powering the LCD up/down through a sysfs interface.
51 config LCD_LTV350QV
52         tristate "Samsung LTV350QV LCD Panel"
53         depends on SPI_MASTER
54         help
55           If you have a Samsung LTV350QV LCD panel, say y to include a
56           power control driver for it.  The panel starts up in power
57           off state, so you need this driver in order to see any
58           output.
60           The LTV350QV panel is present on all ATSTK1000 boards.
62 config LCD_ILI9320
63         tristate
64         help
65           If you have a panel based on the ILI9320 controller chip
66           then say y to include a power driver for it.
68 config LCD_TDO24M
69         tristate "Toppoly TDO24M  and TDO35S LCD Panels support"
70         depends on SPI_MASTER
71         help
72           If you have a Toppoly TDO24M/TDO35S series LCD panel, say y here to
73           include the support for it.
75 config LCD_VGG2432A4
76         tristate "VGG2432A4 LCM device support"
77         depends on SPI_MASTER
78         select LCD_ILI9320
79         help
80           If you have a VGG2432A4 panel based on the ILI9320 controller chip
81           then say y to include a power driver for it.
83 config LCD_PLATFORM
84         tristate "Platform LCD controls"
85         help
86           This driver provides a platform-device registered LCD power
87           control interface.
89 config LCD_TOSA
90         tristate "Sharp SL-6000 LCD Driver"
91         depends on SPI && MACH_TOSA
92         help
93           If you have an Sharp SL-6000 Zaurus say Y to enable a driver
94           for its LCD.
96 config LCD_HP700
97         tristate "HP Jornada 700 series LCD Driver"
98         depends on SA1100_JORNADA720_SSP && !PREEMPT
99         default y
100         help
101           If you have an HP Jornada 700 series handheld (710/720/728)
102           say Y to enable LCD control driver.
104 config LCD_S6E63M0
105         tristate "S6E63M0 AMOLED LCD Driver"
106         depends on SPI && BACKLIGHT_CLASS_DEVICE
107         default n
108         help
109           If you have an S6E63M0 LCD Panel, say Y to enable its
110           LCD control driver.
112 config LCD_LD9040
113         tristate "LD9040 AMOLED LCD Driver"
114         depends on SPI && BACKLIGHT_CLASS_DEVICE
115         default n
116         help
117           If you have an LD9040 Panel, say Y to enable its
118           control driver.
120 config LCD_AMS369FG06
121         tristate "AMS369FG06 AMOLED LCD Driver"
122         depends on SPI && BACKLIGHT_CLASS_DEVICE
123         default n
124         help
125           If you have an AMS369FG06 AMOLED Panel, say Y to enable its
126           LCD control driver.
128 endif # LCD_CLASS_DEVICE
131 # Backlight
133 config BACKLIGHT_CLASS_DEVICE
134         tristate "Lowlevel Backlight controls"
135         default m
136         help
137           This framework adds support for low-level control of the LCD
138           backlight. This includes support for brightness and power.
140           To have support for your specific LCD panel you will have to
141           select the proper drivers which depend on this option.
143 if BACKLIGHT_CLASS_DEVICE
145 config BACKLIGHT_ATMEL_LCDC
146         bool "Atmel LCDC Contrast-as-Backlight control"
147         depends on FB_ATMEL
148         default y if MACH_SAM9261EK || MACH_SAM9G10EK || MACH_SAM9263EK
149         help
150           This provides a backlight control internal to the Atmel LCDC
151           driver.  If the LCD "contrast control" on your board is wired
152           so it controls the backlight brightness, select this option to
153           export this as a PWM-based backlight control.
155           If in doubt, it's safe to enable this option; it doesn't kick
156           in unless the board's description says it's wired that way.
158 config BACKLIGHT_ATMEL_PWM
159         tristate "Atmel PWM backlight control"
160         depends on ATMEL_PWM
161         help
162           Say Y here if you want to use the PWM peripheral in Atmel AT91 and
163           AVR32 devices. This driver will need additional platform data to know
164           which PWM instance to use and how to configure it.
166           To compile this driver as a module, choose M here: the module will be
167           called atmel-pwm-bl.
169 config BACKLIGHT_EP93XX
170         tristate "Cirrus EP93xx Backlight Driver"
171         depends on FB_EP93XX
172         help
173           If you have a LCD backlight connected to the BRIGHT output of
174           the EP93xx, say Y here to enable this driver.
176           To compile this driver as a module, choose M here: the module will
177           be called ep93xx_bl.
179 config BACKLIGHT_GENERIC
180         tristate "Generic (aka Sharp Corgi) Backlight Driver"
181         default y
182         help
183           Say y to enable the generic platform backlight driver previously
184           known as the Corgi backlight driver. If you have a Sharp Zaurus
185           SL-C7xx, SL-Cxx00 or SL-6000x say y.
187 config BACKLIGHT_LOCOMO
188         tristate "Sharp LOCOMO LCD/Backlight Driver"
189         depends on SHARP_LOCOMO
190         default y
191         help
192           If you have a Sharp Zaurus SL-5500 (Collie) or SL-5600 (Poodle) say y to
193           enable the LCD/backlight driver.
195 config BACKLIGHT_OMAP1
196         tristate "OMAP1 PWL-based LCD Backlight"
197         depends on ARCH_OMAP1
198         default y
199         help
200           This driver controls the LCD backlight level and power for
201           the PWL module of OMAP1 processors.  Say Y if your board
202           uses this hardware.
204 config BACKLIGHT_HP680
205         tristate "HP Jornada 680 Backlight Driver"
206         depends on SH_HP6XX
207         default y
208         help
209           If you have a HP Jornada 680, say y to enable the
210           backlight driver.
212 config BACKLIGHT_HP700
213         tristate "HP Jornada 700 series Backlight Driver"
214         depends on SA1100_JORNADA720_SSP && !PREEMPT
215         default y
216         help
217           If you have an HP Jornada 700 series,
218           say Y to include backlight control driver.
220 config BACKLIGHT_PROGEAR
221         tristate "Frontpath ProGear Backlight Driver"
222         depends on PCI && X86
223         help
224           If you have a Frontpath ProGear say Y to enable the
225           backlight driver.
227 config BACKLIGHT_CARILLO_RANCH
228         tristate "Intel Carillo Ranch Backlight Driver"
229         depends on LCD_CLASS_DEVICE && PCI && X86 && FB_LE80578
230         help
231           If you have a Intel LE80578 (Carillo Ranch) say Y to enable the
232           backlight driver.
234 config BACKLIGHT_PWM
235         tristate "Generic PWM based Backlight Driver"
236         depends on HAVE_PWM
237         help
238           If you have a LCD backlight adjustable by PWM, say Y to enable
239           this driver.
241 config BACKLIGHT_DA903X
242         tristate "Backlight Driver for DA9030/DA9034 using WLED"
243         depends on PMIC_DA903X
244         help
245           If you have a LCD backlight connected to the WLED output of DA9030
246           or DA9034 WLED output, say Y here to enable this driver.
248 config BACKLIGHT_MAX8925
249         tristate "Backlight driver for MAX8925"
250         depends on MFD_MAX8925
251         help
252           If you have a LCD backlight connected to the WLED output of MAX8925
253           WLED output, say Y here to enable this driver.
255 config BACKLIGHT_APPLE
256        tristate "Apple Backlight Driver"
257        depends on X86 && ACPI
258        help
259          If you have an Intel-based Apple say Y to enable a driver for its
260          backlight.
262 config BACKLIGHT_TOSA
263         tristate "Sharp SL-6000 Backlight Driver"
264         depends on I2C && MACH_TOSA && LCD_TOSA
265         help
266           If you have an Sharp SL-6000 Zaurus say Y to enable a driver
267           for its backlight
269 config BACKLIGHT_SAHARA
270         tristate "Tabletkiosk Sahara Touch-iT Backlight Driver"
271         depends on X86
272         help
273           If you have a Tabletkiosk Sahara Touch-iT, say y to enable the
274           backlight driver.
276 config BACKLIGHT_WM831X
277         tristate "WM831x PMIC Backlight Driver"
278         depends on MFD_WM831X
279         help
280           If you have a backlight driven by the ISINK and DCDC of a
281           WM831x PMIC say y to enable the backlight driver for it.
283 config BACKLIGHT_ADX
284         tristate "Avionic Design Xanthos Backlight Driver"
285         depends on ARCH_PXA_ADX
286         default y
287         help
288           Say Y to enable the backlight driver on Avionic Design Xanthos-based
289           boards.
291 config BACKLIGHT_ADP5520
292         tristate "Backlight Driver for ADP5520/ADP5501 using WLED"
293         depends on PMIC_ADP5520
294         help
295           If you have a LCD backlight connected to the BST/BL_SNK output of
296           ADP5520 or ADP5501, say Y here to enable this driver.
298           To compile this driver as a module, choose M here: the module will
299           be called adp5520_bl.
301 config BACKLIGHT_ADP8860
302         tristate "Backlight Driver for ADP8860/ADP8861/ADP8863 using WLED"
303         depends on BACKLIGHT_CLASS_DEVICE && I2C
304         select NEW_LEDS
305         select LEDS_CLASS
306         help
307           If you have a LCD backlight connected to the ADP8860, ADP8861 or
308           ADP8863 say Y here to enable this driver.
310           To compile this driver as a module, choose M here: the module will
311           be called adp8860_bl.
313 config BACKLIGHT_ADP8870
314         tristate "Backlight Driver for ADP8870 using WLED"
315         depends on BACKLIGHT_CLASS_DEVICE && I2C
316         select NEW_LEDS
317         select LEDS_CLASS
318         help
319           If you have a LCD backlight connected to the ADP8870,
320           say Y here to enable this driver.
322           To compile this driver as a module, choose M here: the module will
323           be called adp8870_bl.
325 config BACKLIGHT_88PM860X
326         tristate "Backlight Driver for 88PM8606 using WLED"
327         depends on MFD_88PM860X
328         help
329           Say Y to enable the backlight driver for Marvell 88PM8606.
331 config BACKLIGHT_PCF50633
332         tristate "Backlight driver for NXP PCF50633 MFD"
333         depends on BACKLIGHT_CLASS_DEVICE && MFD_PCF50633
334         help
335           If you have a backlight driven by a NXP PCF50633 MFD, say Y here to
336           enable its driver.
338 config BACKLIGHT_AAT2870
339         tristate "AnalogicTech AAT2870 Backlight"
340         depends on BACKLIGHT_CLASS_DEVICE && MFD_AAT2870_CORE
341         help
342           If you have a AnalogicTech AAT2870 say Y to enable the
343           backlight driver.
345 config BACKLIGHT_TLC59108
346         tristate "TLC59108 LCD Backlight Driver"
347         depends on I2C && BACKLIGHT_CLASS_DEVICE
348         default n
349         help
350           If you have an LCD Panel with backlight control via TLC59108,
351           say Y to enable its LCD control driver.
353 endif # BACKLIGHT_CLASS_DEVICE
355 endif # BACKLIGHT_LCD_SUPPORT