1 /*
2 * fs/anon_inodes.c
3 *
4 * Copyright (C) 2007 Davide Libenzi <davidel@xmailserver.org>
5 *
6 * Thanks to Arnd Bergmann for code review and suggestions.
7 * More changes for Thomas Gleixner suggestions.
8 *
9 */
11 #include <linux/cred.h>
12 #include <linux/file.h>
13 #include <linux/poll.h>
14 #include <linux/sched.h>
15 #include <linux/init.h>
16 #include <linux/fs.h>
17 #include <linux/mount.h>
18 #include <linux/module.h>
19 #include <linux/kernel.h>
20 #include <linux/magic.h>
21 #include <linux/anon_inodes.h>
23 #include <asm/uaccess.h>
25 static struct vfsmount *anon_inode_mnt __read_mostly;
26 static struct inode *anon_inode_inode;
27 static const struct file_operations anon_inode_fops;
29 /*
30 * anon_inodefs_dname() is called from d_path().
31 */
32 static char *anon_inodefs_dname(struct dentry *dentry, char *buffer, int buflen)
33 {
34 return dynamic_dname(dentry, buffer, buflen, "anon_inode:%s",
35 dentry->d_name.name);
36 }
38 static const struct dentry_operations anon_inodefs_dentry_operations = {
39 .d_dname = anon_inodefs_dname,
40 };
42 static struct dentry *anon_inodefs_mount(struct file_system_type *fs_type,
43 int flags, const char *dev_name, void *data)
44 {
45 return mount_pseudo(fs_type, "anon_inode:", NULL,
46 &anon_inodefs_dentry_operations, ANON_INODE_FS_MAGIC);
47 }
49 static struct file_system_type anon_inode_fs_type = {
50 .name = "anon_inodefs",
51 .mount = anon_inodefs_mount,
52 .kill_sb = kill_anon_super,
53 };
55 /*
56 * nop .set_page_dirty method so that people can use .page_mkwrite on
57 * anon inodes.
58 */
59 static int anon_set_page_dirty(struct page *page)
60 {
61 return 0;
62 };
64 static const struct address_space_operations anon_aops = {
65 .set_page_dirty = anon_set_page_dirty,
66 };
68 /**
69 * anon_inode_getfile - creates a new file instance by hooking it up to an
70 * anonymous inode, and a dentry that describe the "class"
71 * of the file
72 *
73 * @name: [in] name of the "class" of the new file
74 * @fops: [in] file operations for the new file
75 * @priv: [in] private data for the new file (will be file's private_data)
76 * @flags: [in] flags
77 *
78 * Creates a new file by hooking it on a single inode. This is useful for files
79 * that do not need to have a full-fledged inode in order to operate correctly.
80 * All the files created with anon_inode_getfile() will share a single inode,
81 * hence saving memory and avoiding code duplication for the file/inode/dentry
82 * setup. Returns the newly created file* or an error pointer.
83 */
84 struct file *anon_inode_getfile(const char *name,
85 const struct file_operations *fops,
86 void *priv, int flags)
87 {
88 struct qstr this;
89 struct path path;
90 struct file *file;
91 int error;
93 if (IS_ERR(anon_inode_inode))
94 return ERR_PTR(-ENODEV);
96 if (fops->owner && !try_module_get(fops->owner))
97 return ERR_PTR(-ENOENT);
99 /*
100 * Link the inode to a directory entry by creating a unique name
101 * using the inode sequence number.
102 */
103 error = -ENOMEM;
104 this.name = name;
105 this.len = strlen(name);
106 this.hash = 0;
107 path.dentry = d_alloc_pseudo(anon_inode_mnt->mnt_sb, &this);
108 if (!path.dentry)
109 goto err_module;
111 path.mnt = mntget(anon_inode_mnt);
112 /*
113 * We know the anon_inode inode count is always greater than zero,
114 * so ihold() is safe.
115 */
116 ihold(anon_inode_inode);
118 d_instantiate(path.dentry, anon_inode_inode);
120 error = -ENFILE;
121 file = alloc_file(&path, OPEN_FMODE(flags), fops);
122 if (!file)
123 goto err_dput;
124 file->f_mapping = anon_inode_inode->i_mapping;
126 file->f_pos = 0;
127 file->f_flags = flags & (O_ACCMODE | O_NONBLOCK);
128 file->f_version = 0;
129 file->private_data = priv;
131 return file;
133 err_dput:
134 path_put(&path);
135 err_module:
136 module_put(fops->owner);
137 return ERR_PTR(error);
138 }
139 EXPORT_SYMBOL_GPL(anon_inode_getfile);
141 /**
142 * anon_inode_getfd - creates a new file instance by hooking it up to an
143 * anonymous inode, and a dentry that describe the "class"
144 * of the file
145 *
146 * @name: [in] name of the "class" of the new file
147 * @fops: [in] file operations for the new file
148 * @priv: [in] private data for the new file (will be file's private_data)
149 * @flags: [in] flags
150 *
151 * Creates a new file by hooking it on a single inode. This is useful for files
152 * that do not need to have a full-fledged inode in order to operate correctly.
153 * All the files created with anon_inode_getfd() will share a single inode,
154 * hence saving memory and avoiding code duplication for the file/inode/dentry
155 * setup. Returns new descriptor or an error code.
156 */
157 int anon_inode_getfd(const char *name, const struct file_operations *fops,
158 void *priv, int flags)
159 {
160 int error, fd;
161 struct file *file;
163 error = get_unused_fd_flags(flags);
164 if (error < 0)
165 return error;
166 fd = error;
168 file = anon_inode_getfile(name, fops, priv, flags);
169 if (IS_ERR(file)) {
170 error = PTR_ERR(file);
171 goto err_put_unused_fd;
172 }
173 fd_install(fd, file);
175 return fd;
177 err_put_unused_fd:
178 put_unused_fd(fd);
179 return error;
180 }
181 EXPORT_SYMBOL_GPL(anon_inode_getfd);
183 /*
184 * A single inode exists for all anon_inode files. Contrary to pipes,
185 * anon_inode inodes have no associated per-instance data, so we need
186 * only allocate one of them.
187 */
188 static struct inode *anon_inode_mkinode(void)
189 {
190 struct inode *inode = new_inode_pseudo(anon_inode_mnt->mnt_sb);
192 if (!inode)
193 return ERR_PTR(-ENOMEM);
195 inode->i_ino = get_next_ino();
196 inode->i_fop = &anon_inode_fops;
198 inode->i_mapping->a_ops = &anon_aops;
200 /*
201 * Mark the inode dirty from the very beginning,
202 * that way it will never be moved to the dirty
203 * list because mark_inode_dirty() will think
204 * that it already _is_ on the dirty list.
205 */
206 inode->i_state = I_DIRTY;
207 inode->i_mode = S_IRUSR | S_IWUSR;
208 inode->i_uid = current_fsuid();
209 inode->i_gid = current_fsgid();
210 inode->i_flags |= S_PRIVATE;
211 inode->i_atime = inode->i_mtime = inode->i_ctime = CURRENT_TIME;
212 return inode;
213 }
215 static int __init anon_inode_init(void)
216 {
217 int error;
219 error = register_filesystem(&anon_inode_fs_type);
220 if (error)
221 goto err_exit;
222 anon_inode_mnt = kern_mount(&anon_inode_fs_type);
223 if (IS_ERR(anon_inode_mnt)) {
224 error = PTR_ERR(anon_inode_mnt);
225 goto err_unregister_filesystem;
226 }
227 anon_inode_inode = anon_inode_mkinode();
228 if (IS_ERR(anon_inode_inode)) {
229 error = PTR_ERR(anon_inode_inode);
230 goto err_mntput;
231 }
233 return 0;
235 err_mntput:
236 kern_unmount(anon_inode_mnt);
237 err_unregister_filesystem:
238 unregister_filesystem(&anon_inode_fs_type);
239 err_exit:
240 panic(KERN_ERR "anon_inode_init() failed (%d)\n", error);
241 }
243 fs_initcall(anon_inode_init);