1 /*
2 * fs/eventpoll.c (Efficient event retrieval implementation)
3 * Copyright (C) 2001,...,2009 Davide Libenzi
4 *
5 * This program is free software; you can redistribute it and/or modify
6 * it under the terms of the GNU General Public License as published by
7 * the Free Software Foundation; either version 2 of the License, or
8 * (at your option) any later version.
9 *
10 * Davide Libenzi <davidel@xmailserver.org>
11 *
12 */
14 #include <linux/init.h>
15 #include <linux/kernel.h>
16 #include <linux/sched.h>
17 #include <linux/fs.h>
18 #include <linux/file.h>
19 #include <linux/signal.h>
20 #include <linux/errno.h>
21 #include <linux/mm.h>
22 #include <linux/slab.h>
23 #include <linux/poll.h>
24 #include <linux/string.h>
25 #include <linux/list.h>
26 #include <linux/hash.h>
27 #include <linux/spinlock.h>
28 #include <linux/syscalls.h>
29 #include <linux/rbtree.h>
30 #include <linux/wait.h>
31 #include <linux/eventpoll.h>
32 #include <linux/mount.h>
33 #include <linux/bitops.h>
34 #include <linux/mutex.h>
35 #include <linux/anon_inodes.h>
36 #include <asm/uaccess.h>
37 #include <asm/system.h>
38 #include <asm/io.h>
39 #include <asm/mman.h>
40 #include <linux/atomic.h>
42 /*
43 * LOCKING:
44 * There are three level of locking required by epoll :
45 *
46 * 1) epmutex (mutex)
47 * 2) ep->mtx (mutex)
48 * 3) ep->lock (spinlock)
49 *
50 * The acquire order is the one listed above, from 1 to 3.
51 * We need a spinlock (ep->lock) because we manipulate objects
52 * from inside the poll callback, that might be triggered from
53 * a wake_up() that in turn might be called from IRQ context.
54 * So we can't sleep inside the poll callback and hence we need
55 * a spinlock. During the event transfer loop (from kernel to
56 * user space) we could end up sleeping due a copy_to_user(), so
57 * we need a lock that will allow us to sleep. This lock is a
58 * mutex (ep->mtx). It is acquired during the event transfer loop,
59 * during epoll_ctl(EPOLL_CTL_DEL) and during eventpoll_release_file().
60 * Then we also need a global mutex to serialize eventpoll_release_file()
61 * and ep_free().
62 * This mutex is acquired by ep_free() during the epoll file
63 * cleanup path and it is also acquired by eventpoll_release_file()
64 * if a file has been pushed inside an epoll set and it is then
65 * close()d without a previous call to epoll_ctl(EPOLL_CTL_DEL).
66 * It is also acquired when inserting an epoll fd onto another epoll
67 * fd. We do this so that we walk the epoll tree and ensure that this
68 * insertion does not create a cycle of epoll file descriptors, which
69 * could lead to deadlock. We need a global mutex to prevent two
70 * simultaneous inserts (A into B and B into A) from racing and
71 * constructing a cycle without either insert observing that it is
72 * going to.
73 * It is necessary to acquire multiple "ep->mtx"es at once in the
74 * case when one epoll fd is added to another. In this case, we
75 * always acquire the locks in the order of nesting (i.e. after
76 * epoll_ctl(e1, EPOLL_CTL_ADD, e2), e1->mtx will always be acquired
77 * before e2->mtx). Since we disallow cycles of epoll file
78 * descriptors, this ensures that the mutexes are well-ordered. In
79 * order to communicate this nesting to lockdep, when walking a tree
80 * of epoll file descriptors, we use the current recursion depth as
81 * the lockdep subkey.
82 * It is possible to drop the "ep->mtx" and to use the global
83 * mutex "epmutex" (together with "ep->lock") to have it working,
84 * but having "ep->mtx" will make the interface more scalable.
85 * Events that require holding "epmutex" are very rare, while for
86 * normal operations the epoll private "ep->mtx" will guarantee
87 * a better scalability.
88 */
90 /* Epoll private bits inside the event mask */
91 #define EP_PRIVATE_BITS (EPOLLONESHOT | EPOLLET)
93 /* Maximum number of nesting allowed inside epoll sets */
94 #define EP_MAX_NESTS 4
96 #define EP_MAX_EVENTS (INT_MAX / sizeof(struct epoll_event))
98 #define EP_UNACTIVE_PTR ((void *) -1L)
100 #define EP_ITEM_COST (sizeof(struct epitem) + sizeof(struct eppoll_entry))
102 struct epoll_filefd {
103 struct file *file;
104 int fd;
105 };
107 /*
108 * Structure used to track possible nested calls, for too deep recursions
109 * and loop cycles.
110 */
111 struct nested_call_node {
112 struct list_head llink;
113 void *cookie;
114 void *ctx;
115 };
117 /*
118 * This structure is used as collector for nested calls, to check for
119 * maximum recursion dept and loop cycles.
120 */
121 struct nested_calls {
122 struct list_head tasks_call_list;
123 spinlock_t lock;
124 };
126 /*
127 * Each file descriptor added to the eventpoll interface will
128 * have an entry of this type linked to the "rbr" RB tree.
129 */
130 struct epitem {
131 /* RB tree node used to link this structure to the eventpoll RB tree */
132 struct rb_node rbn;
134 /* List header used to link this structure to the eventpoll ready list */
135 struct list_head rdllink;
137 /*
138 * Works together "struct eventpoll"->ovflist in keeping the
139 * single linked chain of items.
140 */
141 struct epitem *next;
143 /* The file descriptor information this item refers to */
144 struct epoll_filefd ffd;
146 /* Number of active wait queue attached to poll operations */
147 int nwait;
149 /* List containing poll wait queues */
150 struct list_head pwqlist;
152 /* The "container" of this item */
153 struct eventpoll *ep;
155 /* List header used to link this item to the "struct file" items list */
156 struct list_head fllink;
158 /* The structure that describe the interested events and the source fd */
159 struct epoll_event event;
160 };
162 /*
163 * This structure is stored inside the "private_data" member of the file
164 * structure and represents the main data structure for the eventpoll
165 * interface.
166 */
167 struct eventpoll {
168 /* Protect the access to this structure */
169 spinlock_t lock;
171 /*
172 * This mutex is used to ensure that files are not removed
173 * while epoll is using them. This is held during the event
174 * collection loop, the file cleanup path, the epoll file exit
175 * code and the ctl operations.
176 */
177 struct mutex mtx;
179 /* Wait queue used by sys_epoll_wait() */
180 wait_queue_head_t wq;
182 /* Wait queue used by file->poll() */
183 wait_queue_head_t poll_wait;
185 /* List of ready file descriptors */
186 struct list_head rdllist;
188 /* RB tree root used to store monitored fd structs */
189 struct rb_root rbr;
191 /*
192 * This is a single linked list that chains all the "struct epitem" that
193 * happened while transferring ready events to userspace w/out
194 * holding ->lock.
195 */
196 struct epitem *ovflist;
198 /* The user that created the eventpoll descriptor */
199 struct user_struct *user;
200 };
202 /* Wait structure used by the poll hooks */
203 struct eppoll_entry {
204 /* List header used to link this structure to the "struct epitem" */
205 struct list_head llink;
207 /* The "base" pointer is set to the container "struct epitem" */
208 struct epitem *base;
210 /*
211 * Wait queue item that will be linked to the target file wait
212 * queue head.
213 */
214 wait_queue_t wait;
216 /* The wait queue head that linked the "wait" wait queue item */
217 wait_queue_head_t *whead;
218 };
220 /* Wrapper struct used by poll queueing */
221 struct ep_pqueue {
222 poll_table pt;
223 struct epitem *epi;
224 };
226 /* Used by the ep_send_events() function as callback private data */
227 struct ep_send_events_data {
228 int maxevents;
229 struct epoll_event __user *events;
230 };
232 /*
233 * Configuration options available inside /proc/sys/fs/epoll/
234 */
235 /* Maximum number of epoll watched descriptors, per user */
236 static long max_user_watches __read_mostly;
238 /*
239 * This mutex is used to serialize ep_free() and eventpoll_release_file().
240 */
241 static DEFINE_MUTEX(epmutex);
243 /* Used to check for epoll file descriptor inclusion loops */
244 static struct nested_calls poll_loop_ncalls;
246 /* Used for safe wake up implementation */
247 static struct nested_calls poll_safewake_ncalls;
249 /* Used to call file's f_op->poll() under the nested calls boundaries */
250 static struct nested_calls poll_readywalk_ncalls;
252 /* Slab cache used to allocate "struct epitem" */
253 static struct kmem_cache *epi_cache __read_mostly;
255 /* Slab cache used to allocate "struct eppoll_entry" */
256 static struct kmem_cache *pwq_cache __read_mostly;
258 #ifdef CONFIG_SYSCTL
260 #include <linux/sysctl.h>
262 static long zero;
263 static long long_max = LONG_MAX;
265 ctl_table epoll_table[] = {
266 {
267 .procname = "max_user_watches",
268 .data = &max_user_watches,
269 .maxlen = sizeof(max_user_watches),
270 .mode = 0644,
271 .proc_handler = proc_doulongvec_minmax,
272 .extra1 = &zero,
273 .extra2 = &long_max,
274 },
275 { }
276 };
277 #endif /* CONFIG_SYSCTL */
280 /* Setup the structure that is used as key for the RB tree */
281 static inline void ep_set_ffd(struct epoll_filefd *ffd,
282 struct file *file, int fd)
283 {
284 ffd->file = file;
285 ffd->fd = fd;
286 }
288 /* Compare RB tree keys */
289 static inline int ep_cmp_ffd(struct epoll_filefd *p1,
290 struct epoll_filefd *p2)
291 {
292 return (p1->file > p2->file ? +1:
293 (p1->file < p2->file ? -1 : p1->fd - p2->fd));
294 }
296 /* Tells us if the item is currently linked */
297 static inline int ep_is_linked(struct list_head *p)
298 {
299 return !list_empty(p);
300 }
302 /* Get the "struct epitem" from a wait queue pointer */
303 static inline struct epitem *ep_item_from_wait(wait_queue_t *p)
304 {
305 return container_of(p, struct eppoll_entry, wait)->base;
306 }
308 /* Get the "struct epitem" from an epoll queue wrapper */
309 static inline struct epitem *ep_item_from_epqueue(poll_table *p)
310 {
311 return container_of(p, struct ep_pqueue, pt)->epi;
312 }
314 /* Tells if the epoll_ctl(2) operation needs an event copy from userspace */
315 static inline int ep_op_has_event(int op)
316 {
317 return op != EPOLL_CTL_DEL;
318 }
320 /* Initialize the poll safe wake up structure */
321 static void ep_nested_calls_init(struct nested_calls *ncalls)
322 {
323 INIT_LIST_HEAD(&ncalls->tasks_call_list);
324 spin_lock_init(&ncalls->lock);
325 }
327 /**
328 * ep_events_available - Checks if ready events might be available.
329 *
330 * @ep: Pointer to the eventpoll context.
331 *
332 * Returns: Returns a value different than zero if ready events are available,
333 * or zero otherwise.
334 */
335 static inline int ep_events_available(struct eventpoll *ep)
336 {
337 return !list_empty(&ep->rdllist) || ep->ovflist != EP_UNACTIVE_PTR;
338 }
340 /**
341 * ep_call_nested - Perform a bound (possibly) nested call, by checking
342 * that the recursion limit is not exceeded, and that
343 * the same nested call (by the meaning of same cookie) is
344 * no re-entered.
345 *
346 * @ncalls: Pointer to the nested_calls structure to be used for this call.
347 * @max_nests: Maximum number of allowed nesting calls.
348 * @nproc: Nested call core function pointer.
349 * @priv: Opaque data to be passed to the @nproc callback.
350 * @cookie: Cookie to be used to identify this nested call.
351 * @ctx: This instance context.
352 *
353 * Returns: Returns the code returned by the @nproc callback, or -1 if
354 * the maximum recursion limit has been exceeded.
355 */
356 static int ep_call_nested(struct nested_calls *ncalls, int max_nests,
357 int (*nproc)(void *, void *, int), void *priv,
358 void *cookie, void *ctx)
359 {
360 int error, call_nests = 0;
361 unsigned long flags;
362 struct list_head *lsthead = &ncalls->tasks_call_list;
363 struct nested_call_node *tncur;
364 struct nested_call_node tnode;
366 spin_lock_irqsave(&ncalls->lock, flags);
368 /*
369 * Try to see if the current task is already inside this wakeup call.
370 * We use a list here, since the population inside this set is always
371 * very much limited.
372 */
373 list_for_each_entry(tncur, lsthead, llink) {
374 if (tncur->ctx == ctx &&
375 (tncur->cookie == cookie || ++call_nests > max_nests)) {
376 /*
377 * Ops ... loop detected or maximum nest level reached.
378 * We abort this wake by breaking the cycle itself.
379 */
380 error = -1;
381 goto out_unlock;
382 }
383 }
385 /* Add the current task and cookie to the list */
386 tnode.ctx = ctx;
387 tnode.cookie = cookie;
388 list_add(&tnode.llink, lsthead);
390 spin_unlock_irqrestore(&ncalls->lock, flags);
392 /* Call the nested function */
393 error = (*nproc)(priv, cookie, call_nests);
395 /* Remove the current task from the list */
396 spin_lock_irqsave(&ncalls->lock, flags);
397 list_del(&tnode.llink);
398 out_unlock:
399 spin_unlock_irqrestore(&ncalls->lock, flags);
401 return error;
402 }
404 #ifdef CONFIG_DEBUG_LOCK_ALLOC
405 static inline void ep_wake_up_nested(wait_queue_head_t *wqueue,
406 unsigned long events, int subclass)
407 {
408 unsigned long flags;
410 spin_lock_irqsave_nested(&wqueue->lock, flags, subclass);
411 wake_up_locked_poll(wqueue, events);
412 spin_unlock_irqrestore(&wqueue->lock, flags);
413 }
414 #else
415 static inline void ep_wake_up_nested(wait_queue_head_t *wqueue,
416 unsigned long events, int subclass)
417 {
418 wake_up_poll(wqueue, events);
419 }
420 #endif
422 static int ep_poll_wakeup_proc(void *priv, void *cookie, int call_nests)
423 {
424 ep_wake_up_nested((wait_queue_head_t *) cookie, POLLIN,
425 1 + call_nests);
426 return 0;
427 }
429 /*
430 * Perform a safe wake up of the poll wait list. The problem is that
431 * with the new callback'd wake up system, it is possible that the
432 * poll callback is reentered from inside the call to wake_up() done
433 * on the poll wait queue head. The rule is that we cannot reenter the
434 * wake up code from the same task more than EP_MAX_NESTS times,
435 * and we cannot reenter the same wait queue head at all. This will
436 * enable to have a hierarchy of epoll file descriptor of no more than
437 * EP_MAX_NESTS deep.
438 */
439 static void ep_poll_safewake(wait_queue_head_t *wq)
440 {
441 int this_cpu = get_cpu();
443 ep_call_nested(&poll_safewake_ncalls, EP_MAX_NESTS,
444 ep_poll_wakeup_proc, NULL, wq, (void *) (long) this_cpu);
446 put_cpu();
447 }
449 /*
450 * This function unregisters poll callbacks from the associated file
451 * descriptor. Must be called with "mtx" held (or "epmutex" if called from
452 * ep_free).
453 */
454 static void ep_unregister_pollwait(struct eventpoll *ep, struct epitem *epi)
455 {
456 struct list_head *lsthead = &epi->pwqlist;
457 struct eppoll_entry *pwq;
459 while (!list_empty(lsthead)) {
460 pwq = list_first_entry(lsthead, struct eppoll_entry, llink);
462 list_del(&pwq->llink);
463 remove_wait_queue(pwq->whead, &pwq->wait);
464 kmem_cache_free(pwq_cache, pwq);
465 }
466 }
468 /**
469 * ep_scan_ready_list - Scans the ready list in a way that makes possible for
470 * the scan code, to call f_op->poll(). Also allows for
471 * O(NumReady) performance.
472 *
473 * @ep: Pointer to the epoll private data structure.
474 * @sproc: Pointer to the scan callback.
475 * @priv: Private opaque data passed to the @sproc callback.
476 * @depth: The current depth of recursive f_op->poll calls.
477 *
478 * Returns: The same integer error code returned by the @sproc callback.
479 */
480 static int ep_scan_ready_list(struct eventpoll *ep,
481 int (*sproc)(struct eventpoll *,
482 struct list_head *, void *),
483 void *priv,
484 int depth)
485 {
486 int error, pwake = 0;
487 unsigned long flags;
488 struct epitem *epi, *nepi;
489 LIST_HEAD(txlist);
491 /*
492 * We need to lock this because we could be hit by
493 * eventpoll_release_file() and epoll_ctl().
494 */
495 mutex_lock_nested(&ep->mtx, depth);
497 /*
498 * Steal the ready list, and re-init the original one to the
499 * empty list. Also, set ep->ovflist to NULL so that events
500 * happening while looping w/out locks, are not lost. We cannot
501 * have the poll callback to queue directly on ep->rdllist,
502 * because we want the "sproc" callback to be able to do it
503 * in a lockless way.
504 */
505 spin_lock_irqsave(&ep->lock, flags);
506 list_splice_init(&ep->rdllist, &txlist);
507 ep->ovflist = NULL;
508 spin_unlock_irqrestore(&ep->lock, flags);
510 /*
511 * Now call the callback function.
512 */
513 error = (*sproc)(ep, &txlist, priv);
515 spin_lock_irqsave(&ep->lock, flags);
516 /*
517 * During the time we spent inside the "sproc" callback, some
518 * other events might have been queued by the poll callback.
519 * We re-insert them inside the main ready-list here.
520 */
521 for (nepi = ep->ovflist; (epi = nepi) != NULL;
522 nepi = epi->next, epi->next = EP_UNACTIVE_PTR) {
523 /*
524 * We need to check if the item is already in the list.
525 * During the "sproc" callback execution time, items are
526 * queued into ->ovflist but the "txlist" might already
527 * contain them, and the list_splice() below takes care of them.
528 */
529 if (!ep_is_linked(&epi->rdllink))
530 list_add_tail(&epi->rdllink, &ep->rdllist);
531 }
532 /*
533 * We need to set back ep->ovflist to EP_UNACTIVE_PTR, so that after
534 * releasing the lock, events will be queued in the normal way inside
535 * ep->rdllist.
536 */
537 ep->ovflist = EP_UNACTIVE_PTR;
539 /*
540 * Quickly re-inject items left on "txlist".
541 */
542 list_splice(&txlist, &ep->rdllist);
544 if (!list_empty(&ep->rdllist)) {
545 /*
546 * Wake up (if active) both the eventpoll wait list and
547 * the ->poll() wait list (delayed after we release the lock).
548 */
549 if (waitqueue_active(&ep->wq))
550 wake_up_locked(&ep->wq);
551 if (waitqueue_active(&ep->poll_wait))
552 pwake++;
553 }
554 spin_unlock_irqrestore(&ep->lock, flags);
556 mutex_unlock(&ep->mtx);
558 /* We have to call this outside the lock */
559 if (pwake)
560 ep_poll_safewake(&ep->poll_wait);
562 return error;
563 }
565 /*
566 * Removes a "struct epitem" from the eventpoll RB tree and deallocates
567 * all the associated resources. Must be called with "mtx" held.
568 */
569 static int ep_remove(struct eventpoll *ep, struct epitem *epi)
570 {
571 unsigned long flags;
572 struct file *file = epi->ffd.file;
574 /*
575 * Removes poll wait queue hooks. We _have_ to do this without holding
576 * the "ep->lock" otherwise a deadlock might occur. This because of the
577 * sequence of the lock acquisition. Here we do "ep->lock" then the wait
578 * queue head lock when unregistering the wait queue. The wakeup callback
579 * will run by holding the wait queue head lock and will call our callback
580 * that will try to get "ep->lock".
581 */
582 ep_unregister_pollwait(ep, epi);
584 /* Remove the current item from the list of epoll hooks */
585 spin_lock(&file->f_lock);
586 if (ep_is_linked(&epi->fllink))
587 list_del_init(&epi->fllink);
588 spin_unlock(&file->f_lock);
590 rb_erase(&epi->rbn, &ep->rbr);
592 spin_lock_irqsave(&ep->lock, flags);
593 if (ep_is_linked(&epi->rdllink))
594 list_del_init(&epi->rdllink);
595 spin_unlock_irqrestore(&ep->lock, flags);
597 /* At this point it is safe to free the eventpoll item */
598 kmem_cache_free(epi_cache, epi);
600 atomic_long_dec(&ep->user->epoll_watches);
602 return 0;
603 }
605 static void ep_free(struct eventpoll *ep)
606 {
607 struct rb_node *rbp;
608 struct epitem *epi;
610 /* We need to release all tasks waiting for these file */
611 if (waitqueue_active(&ep->poll_wait))
612 ep_poll_safewake(&ep->poll_wait);
614 /*
615 * We need to lock this because we could be hit by
616 * eventpoll_release_file() while we're freeing the "struct eventpoll".
617 * We do not need to hold "ep->mtx" here because the epoll file
618 * is on the way to be removed and no one has references to it
619 * anymore. The only hit might come from eventpoll_release_file() but
620 * holding "epmutex" is sufficient here.
621 */
622 mutex_lock(&epmutex);
624 /*
625 * Walks through the whole tree by unregistering poll callbacks.
626 */
627 for (rbp = rb_first(&ep->rbr); rbp; rbp = rb_next(rbp)) {
628 epi = rb_entry(rbp, struct epitem, rbn);
630 ep_unregister_pollwait(ep, epi);
631 }
633 /*
634 * Walks through the whole tree by freeing each "struct epitem". At this
635 * point we are sure no poll callbacks will be lingering around, and also by
636 * holding "epmutex" we can be sure that no file cleanup code will hit
637 * us during this operation. So we can avoid the lock on "ep->lock".
638 */
639 while ((rbp = rb_first(&ep->rbr)) != NULL) {
640 epi = rb_entry(rbp, struct epitem, rbn);
641 ep_remove(ep, epi);
642 }
644 mutex_unlock(&epmutex);
645 mutex_destroy(&ep->mtx);
646 free_uid(ep->user);
647 kfree(ep);
648 }
650 static int ep_eventpoll_release(struct inode *inode, struct file *file)
651 {
652 struct eventpoll *ep = file->private_data;
654 if (ep)
655 ep_free(ep);
657 return 0;
658 }
660 static int ep_read_events_proc(struct eventpoll *ep, struct list_head *head,
661 void *priv)
662 {
663 struct epitem *epi, *tmp;
665 list_for_each_entry_safe(epi, tmp, head, rdllink) {
666 if (epi->ffd.file->f_op->poll(epi->ffd.file, NULL) &
667 epi->event.events)
668 return POLLIN | POLLRDNORM;
669 else {
670 /*
671 * Item has been dropped into the ready list by the poll
672 * callback, but it's not actually ready, as far as
673 * caller requested events goes. We can remove it here.
674 */
675 list_del_init(&epi->rdllink);
676 }
677 }
679 return 0;
680 }
682 static int ep_poll_readyevents_proc(void *priv, void *cookie, int call_nests)
683 {
684 return ep_scan_ready_list(priv, ep_read_events_proc, NULL, call_nests + 1);
685 }
687 static unsigned int ep_eventpoll_poll(struct file *file, poll_table *wait)
688 {
689 int pollflags;
690 struct eventpoll *ep = file->private_data;
692 /* Insert inside our poll wait queue */
693 poll_wait(file, &ep->poll_wait, wait);
695 /*
696 * Proceed to find out if wanted events are really available inside
697 * the ready list. This need to be done under ep_call_nested()
698 * supervision, since the call to f_op->poll() done on listed files
699 * could re-enter here.
700 */
701 pollflags = ep_call_nested(&poll_readywalk_ncalls, EP_MAX_NESTS,
702 ep_poll_readyevents_proc, ep, ep, current);
704 return pollflags != -1 ? pollflags : 0;
705 }
707 /* File callbacks that implement the eventpoll file behaviour */
708 static const struct file_operations eventpoll_fops = {
709 .release = ep_eventpoll_release,
710 .poll = ep_eventpoll_poll,
711 .llseek = noop_llseek,
712 };
714 /* Fast test to see if the file is an eventpoll file */
715 static inline int is_file_epoll(struct file *f)
716 {
717 return f->f_op == &eventpoll_fops;
718 }
720 /*
721 * This is called from eventpoll_release() to unlink files from the eventpoll
722 * interface. We need to have this facility to cleanup correctly files that are
723 * closed without being removed from the eventpoll interface.
724 */
725 void eventpoll_release_file(struct file *file)
726 {
727 struct list_head *lsthead = &file->f_ep_links;
728 struct eventpoll *ep;
729 struct epitem *epi;
731 /*
732 * We don't want to get "file->f_lock" because it is not
733 * necessary. It is not necessary because we're in the "struct file"
734 * cleanup path, and this means that no one is using this file anymore.
735 * So, for example, epoll_ctl() cannot hit here since if we reach this
736 * point, the file counter already went to zero and fget() would fail.
737 * The only hit might come from ep_free() but by holding the mutex
738 * will correctly serialize the operation. We do need to acquire
739 * "ep->mtx" after "epmutex" because ep_remove() requires it when called
740 * from anywhere but ep_free().
741 *
742 * Besides, ep_remove() acquires the lock, so we can't hold it here.
743 */
744 mutex_lock(&epmutex);
746 while (!list_empty(lsthead)) {
747 epi = list_first_entry(lsthead, struct epitem, fllink);
749 ep = epi->ep;
750 list_del_init(&epi->fllink);
751 mutex_lock_nested(&ep->mtx, 0);
752 ep_remove(ep, epi);
753 mutex_unlock(&ep->mtx);
754 }
756 mutex_unlock(&epmutex);
757 }
759 static int ep_alloc(struct eventpoll **pep)
760 {
761 int error;
762 struct user_struct *user;
763 struct eventpoll *ep;
765 user = get_current_user();
766 error = -ENOMEM;
767 ep = kzalloc(sizeof(*ep), GFP_KERNEL);
768 if (unlikely(!ep))
769 goto free_uid;
771 spin_lock_init(&ep->lock);
772 mutex_init(&ep->mtx);
773 init_waitqueue_head(&ep->wq);
774 init_waitqueue_head(&ep->poll_wait);
775 INIT_LIST_HEAD(&ep->rdllist);
776 ep->rbr = RB_ROOT;
777 ep->ovflist = EP_UNACTIVE_PTR;
778 ep->user = user;
780 *pep = ep;
782 return 0;
784 free_uid:
785 free_uid(user);
786 return error;
787 }
789 /*
790 * Search the file inside the eventpoll tree. The RB tree operations
791 * are protected by the "mtx" mutex, and ep_find() must be called with
792 * "mtx" held.
793 */
794 static struct epitem *ep_find(struct eventpoll *ep, struct file *file, int fd)
795 {
796 int kcmp;
797 struct rb_node *rbp;
798 struct epitem *epi, *epir = NULL;
799 struct epoll_filefd ffd;
801 ep_set_ffd(&ffd, file, fd);
802 for (rbp = ep->rbr.rb_node; rbp; ) {
803 epi = rb_entry(rbp, struct epitem, rbn);
804 kcmp = ep_cmp_ffd(&ffd, &epi->ffd);
805 if (kcmp > 0)
806 rbp = rbp->rb_right;
807 else if (kcmp < 0)
808 rbp = rbp->rb_left;
809 else {
810 epir = epi;
811 break;
812 }
813 }
815 return epir;
816 }
818 /*
819 * This is the callback that is passed to the wait queue wakeup
820 * mechanism. It is called by the stored file descriptors when they
821 * have events to report.
822 */
823 static int ep_poll_callback(wait_queue_t *wait, unsigned mode, int sync, void *key)
824 {
825 int pwake = 0;
826 unsigned long flags;
827 struct epitem *epi = ep_item_from_wait(wait);
828 struct eventpoll *ep = epi->ep;
830 spin_lock_irqsave(&ep->lock, flags);
832 /*
833 * If the event mask does not contain any poll(2) event, we consider the
834 * descriptor to be disabled. This condition is likely the effect of the
835 * EPOLLONESHOT bit that disables the descriptor when an event is received,
836 * until the next EPOLL_CTL_MOD will be issued.
837 */
838 if (!(epi->event.events & ~EP_PRIVATE_BITS))
839 goto out_unlock;
841 /*
842 * Check the events coming with the callback. At this stage, not
843 * every device reports the events in the "key" parameter of the
844 * callback. We need to be able to handle both cases here, hence the
845 * test for "key" != NULL before the event match test.
846 */
847 if (key && !((unsigned long) key & epi->event.events))
848 goto out_unlock;
850 /*
851 * If we are transferring events to userspace, we can hold no locks
852 * (because we're accessing user memory, and because of linux f_op->poll()
853 * semantics). All the events that happen during that period of time are
854 * chained in ep->ovflist and requeued later on.
855 */
856 if (unlikely(ep->ovflist != EP_UNACTIVE_PTR)) {
857 if (epi->next == EP_UNACTIVE_PTR) {
858 epi->next = ep->ovflist;
859 ep->ovflist = epi;
860 }
861 goto out_unlock;
862 }
864 /* If this file is already in the ready list we exit soon */
865 if (!ep_is_linked(&epi->rdllink))
866 list_add_tail(&epi->rdllink, &ep->rdllist);
868 /*
869 * Wake up ( if active ) both the eventpoll wait list and the ->poll()
870 * wait list.
871 */
872 if (waitqueue_active(&ep->wq))
873 wake_up_locked(&ep->wq);
874 if (waitqueue_active(&ep->poll_wait))
875 pwake++;
877 out_unlock:
878 spin_unlock_irqrestore(&ep->lock, flags);
880 /* We have to call this outside the lock */
881 if (pwake)
882 ep_poll_safewake(&ep->poll_wait);
884 return 1;
885 }
887 /*
888 * This is the callback that is used to add our wait queue to the
889 * target file wakeup lists.
890 */
891 static void ep_ptable_queue_proc(struct file *file, wait_queue_head_t *whead,
892 poll_table *pt)
893 {
894 struct epitem *epi = ep_item_from_epqueue(pt);
895 struct eppoll_entry *pwq;
897 if (epi->nwait >= 0 && (pwq = kmem_cache_alloc(pwq_cache, GFP_KERNEL))) {
898 init_waitqueue_func_entry(&pwq->wait, ep_poll_callback);
899 pwq->whead = whead;
900 pwq->base = epi;
901 add_wait_queue(whead, &pwq->wait);
902 list_add_tail(&pwq->llink, &epi->pwqlist);
903 epi->nwait++;
904 } else {
905 /* We have to signal that an error occurred */
906 epi->nwait = -1;
907 }
908 }
910 static void ep_rbtree_insert(struct eventpoll *ep, struct epitem *epi)
911 {
912 int kcmp;
913 struct rb_node **p = &ep->rbr.rb_node, *parent = NULL;
914 struct epitem *epic;
916 while (*p) {
917 parent = *p;
918 epic = rb_entry(parent, struct epitem, rbn);
919 kcmp = ep_cmp_ffd(&epi->ffd, &epic->ffd);
920 if (kcmp > 0)
921 p = &parent->rb_right;
922 else
923 p = &parent->rb_left;
924 }
925 rb_link_node(&epi->rbn, parent, p);
926 rb_insert_color(&epi->rbn, &ep->rbr);
927 }
929 /*
930 * Must be called with "mtx" held.
931 */
932 static int ep_insert(struct eventpoll *ep, struct epoll_event *event,
933 struct file *tfile, int fd)
934 {
935 int error, revents, pwake = 0;
936 unsigned long flags;
937 long user_watches;
938 struct epitem *epi;
939 struct ep_pqueue epq;
941 user_watches = atomic_long_read(&ep->user->epoll_watches);
942 if (unlikely(user_watches >= max_user_watches))
943 return -ENOSPC;
944 if (!(epi = kmem_cache_alloc(epi_cache, GFP_KERNEL)))
945 return -ENOMEM;
947 /* Item initialization follow here ... */
948 INIT_LIST_HEAD(&epi->rdllink);
949 INIT_LIST_HEAD(&epi->fllink);
950 INIT_LIST_HEAD(&epi->pwqlist);
951 epi->ep = ep;
952 ep_set_ffd(&epi->ffd, tfile, fd);
953 epi->event = *event;
954 epi->nwait = 0;
955 epi->next = EP_UNACTIVE_PTR;
957 /* Initialize the poll table using the queue callback */
958 epq.epi = epi;
959 init_poll_funcptr(&epq.pt, ep_ptable_queue_proc);
961 /*
962 * Attach the item to the poll hooks and get current event bits.
963 * We can safely use the file* here because its usage count has
964 * been increased by the caller of this function. Note that after
965 * this operation completes, the poll callback can start hitting
966 * the new item.
967 */
968 revents = tfile->f_op->poll(tfile, &epq.pt);
970 /*
971 * We have to check if something went wrong during the poll wait queue
972 * install process. Namely an allocation for a wait queue failed due
973 * high memory pressure.
974 */
975 error = -ENOMEM;
976 if (epi->nwait < 0)
977 goto error_unregister;
979 /* Add the current item to the list of active epoll hook for this file */
980 spin_lock(&tfile->f_lock);
981 list_add_tail(&epi->fllink, &tfile->f_ep_links);
982 spin_unlock(&tfile->f_lock);
984 /*
985 * Add the current item to the RB tree. All RB tree operations are
986 * protected by "mtx", and ep_insert() is called with "mtx" held.
987 */
988 ep_rbtree_insert(ep, epi);
990 /* We have to drop the new item inside our item list to keep track of it */
991 spin_lock_irqsave(&ep->lock, flags);
993 /* If the file is already "ready" we drop it inside the ready list */
994 if ((revents & event->events) && !ep_is_linked(&epi->rdllink)) {
995 list_add_tail(&epi->rdllink, &ep->rdllist);
997 /* Notify waiting tasks that events are available */
998 if (waitqueue_active(&ep->wq))
999 wake_up_locked(&ep->wq);
1000 if (waitqueue_active(&ep->poll_wait))
1001 pwake++;
1002 }
1004 spin_unlock_irqrestore(&ep->lock, flags);
1006 atomic_long_inc(&ep->user->epoll_watches);
1008 /* We have to call this outside the lock */
1009 if (pwake)
1010 ep_poll_safewake(&ep->poll_wait);
1012 return 0;
1014 error_unregister:
1015 ep_unregister_pollwait(ep, epi);
1017 /*
1018 * We need to do this because an event could have been arrived on some
1019 * allocated wait queue. Note that we don't care about the ep->ovflist
1020 * list, since that is used/cleaned only inside a section bound by "mtx".
1021 * And ep_insert() is called with "mtx" held.
1022 */
1023 spin_lock_irqsave(&ep->lock, flags);
1024 if (ep_is_linked(&epi->rdllink))
1025 list_del_init(&epi->rdllink);
1026 spin_unlock_irqrestore(&ep->lock, flags);
1028 kmem_cache_free(epi_cache, epi);
1030 return error;
1031 }
1033 /*
1034 * Modify the interest event mask by dropping an event if the new mask
1035 * has a match in the current file status. Must be called with "mtx" held.
1036 */
1037 static int ep_modify(struct eventpoll *ep, struct epitem *epi, struct epoll_event *event)
1038 {
1039 int pwake = 0;
1040 unsigned int revents;
1042 /*
1043 * Set the new event interest mask before calling f_op->poll();
1044 * otherwise we might miss an event that happens between the
1045 * f_op->poll() call and the new event set registering.
1046 */
1047 epi->event.events = event->events;
1048 epi->event.data = event->data; /* protected by mtx */
1050 /*
1051 * Get current event bits. We can safely use the file* here because
1052 * its usage count has been increased by the caller of this function.
1053 */
1054 revents = epi->ffd.file->f_op->poll(epi->ffd.file, NULL);
1056 /*
1057 * If the item is "hot" and it is not registered inside the ready
1058 * list, push it inside.
1059 */
1060 if (revents & event->events) {
1061 spin_lock_irq(&ep->lock);
1062 if (!ep_is_linked(&epi->rdllink)) {
1063 list_add_tail(&epi->rdllink, &ep->rdllist);
1065 /* Notify waiting tasks that events are available */
1066 if (waitqueue_active(&ep->wq))
1067 wake_up_locked(&ep->wq);
1068 if (waitqueue_active(&ep->poll_wait))
1069 pwake++;
1070 }
1071 spin_unlock_irq(&ep->lock);
1072 }
1074 /* We have to call this outside the lock */
1075 if (pwake)
1076 ep_poll_safewake(&ep->poll_wait);
1078 return 0;
1079 }
1081 static int ep_send_events_proc(struct eventpoll *ep, struct list_head *head,
1082 void *priv)
1083 {
1084 struct ep_send_events_data *esed = priv;
1085 int eventcnt;
1086 unsigned int revents;
1087 struct epitem *epi;
1088 struct epoll_event __user *uevent;
1090 /*
1091 * We can loop without lock because we are passed a task private list.
1092 * Items cannot vanish during the loop because ep_scan_ready_list() is
1093 * holding "mtx" during this call.
1094 */
1095 for (eventcnt = 0, uevent = esed->events;
1096 !list_empty(head) && eventcnt < esed->maxevents;) {
1097 epi = list_first_entry(head, struct epitem, rdllink);
1099 list_del_init(&epi->rdllink);
1101 revents = epi->ffd.file->f_op->poll(epi->ffd.file, NULL) &
1102 epi->event.events;
1104 /*
1105 * If the event mask intersect the caller-requested one,
1106 * deliver the event to userspace. Again, ep_scan_ready_list()
1107 * is holding "mtx", so no operations coming from userspace
1108 * can change the item.
1109 */
1110 if (revents) {
1111 if (__put_user(revents, &uevent->events) ||
1112 __put_user(epi->event.data, &uevent->data)) {
1113 list_add(&epi->rdllink, head);
1114 return eventcnt ? eventcnt : -EFAULT;
1115 }
1116 eventcnt++;
1117 uevent++;
1118 if (epi->event.events & EPOLLONESHOT)
1119 epi->event.events &= EP_PRIVATE_BITS;
1120 else if (!(epi->event.events & EPOLLET)) {
1121 /*
1122 * If this file has been added with Level
1123 * Trigger mode, we need to insert back inside
1124 * the ready list, so that the next call to
1125 * epoll_wait() will check again the events
1126 * availability. At this point, no one can insert
1127 * into ep->rdllist besides us. The epoll_ctl()
1128 * callers are locked out by
1129 * ep_scan_ready_list() holding "mtx" and the
1130 * poll callback will queue them in ep->ovflist.
1131 */
1132 list_add_tail(&epi->rdllink, &ep->rdllist);
1133 }
1134 }
1135 }
1137 return eventcnt;
1138 }
1140 static int ep_send_events(struct eventpoll *ep,
1141 struct epoll_event __user *events, int maxevents)
1142 {
1143 struct ep_send_events_data esed;
1145 esed.maxevents = maxevents;
1146 esed.events = events;
1148 return ep_scan_ready_list(ep, ep_send_events_proc, &esed, 0);
1149 }
1151 static inline struct timespec ep_set_mstimeout(long ms)
1152 {
1153 struct timespec now, ts = {
1154 .tv_sec = ms / MSEC_PER_SEC,
1155 .tv_nsec = NSEC_PER_MSEC * (ms % MSEC_PER_SEC),
1156 };
1158 ktime_get_ts(&now);
1159 return timespec_add_safe(now, ts);
1160 }
1162 /**
1163 * ep_poll - Retrieves ready events, and delivers them to the caller supplied
1164 * event buffer.
1165 *
1166 * @ep: Pointer to the eventpoll context.
1167 * @events: Pointer to the userspace buffer where the ready events should be
1168 * stored.
1169 * @maxevents: Size (in terms of number of events) of the caller event buffer.
1170 * @timeout: Maximum timeout for the ready events fetch operation, in
1171 * milliseconds. If the @timeout is zero, the function will not block,
1172 * while if the @timeout is less than zero, the function will block
1173 * until at least one event has been retrieved (or an error
1174 * occurred).
1175 *
1176 * Returns: Returns the number of ready events which have been fetched, or an
1177 * error code, in case of error.
1178 */
1179 static int ep_poll(struct eventpoll *ep, struct epoll_event __user *events,
1180 int maxevents, long timeout)
1181 {
1182 int res = 0, eavail, timed_out = 0;
1183 unsigned long flags;
1184 long slack = 0;
1185 wait_queue_t wait;
1186 ktime_t expires, *to = NULL;
1188 if (timeout > 0) {
1189 struct timespec end_time = ep_set_mstimeout(timeout);
1191 slack = select_estimate_accuracy(&end_time);
1192 to = &expires;
1193 *to = timespec_to_ktime(end_time);
1194 } else if (timeout == 0) {
1195 /*
1196 * Avoid the unnecessary trip to the wait queue loop, if the
1197 * caller specified a non blocking operation.
1198 */
1199 timed_out = 1;
1200 spin_lock_irqsave(&ep->lock, flags);
1201 goto check_events;
1202 }
1204 fetch_events:
1205 spin_lock_irqsave(&ep->lock, flags);
1207 if (!ep_events_available(ep)) {
1208 /*
1209 * We don't have any available event to return to the caller.
1210 * We need to sleep here, and we will be wake up by
1211 * ep_poll_callback() when events will become available.
1212 */
1213 init_waitqueue_entry(&wait, current);
1214 __add_wait_queue_exclusive(&ep->wq, &wait);
1216 for (;;) {
1217 /*
1218 * We don't want to sleep if the ep_poll_callback() sends us
1219 * a wakeup in between. That's why we set the task state
1220 * to TASK_INTERRUPTIBLE before doing the checks.
1221 */
1222 set_current_state(TASK_INTERRUPTIBLE);
1223 if (ep_events_available(ep) || timed_out)
1224 break;
1225 if (signal_pending(current)) {
1226 res = -EINTR;
1227 break;
1228 }
1230 spin_unlock_irqrestore(&ep->lock, flags);
1231 if (!schedule_hrtimeout_range(to, slack, HRTIMER_MODE_ABS))
1232 timed_out = 1;
1234 spin_lock_irqsave(&ep->lock, flags);
1235 }
1236 __remove_wait_queue(&ep->wq, &wait);
1238 set_current_state(TASK_RUNNING);
1239 }
1240 check_events:
1241 /* Is it worth to try to dig for events ? */
1242 eavail = ep_events_available(ep);
1244 spin_unlock_irqrestore(&ep->lock, flags);
1246 /*
1247 * Try to transfer events to user space. In case we get 0 events and
1248 * there's still timeout left over, we go trying again in search of
1249 * more luck.
1250 */
1251 if (!res && eavail &&
1252 !(res = ep_send_events(ep, events, maxevents)) && !timed_out)
1253 goto fetch_events;
1255 return res;
1256 }
1258 /**
1259 * ep_loop_check_proc - Callback function to be passed to the @ep_call_nested()
1260 * API, to verify that adding an epoll file inside another
1261 * epoll structure, does not violate the constraints, in
1262 * terms of closed loops, or too deep chains (which can
1263 * result in excessive stack usage).
1264 *
1265 * @priv: Pointer to the epoll file to be currently checked.
1266 * @cookie: Original cookie for this call. This is the top-of-the-chain epoll
1267 * data structure pointer.
1268 * @call_nests: Current dept of the @ep_call_nested() call stack.
1269 *
1270 * Returns: Returns zero if adding the epoll @file inside current epoll
1271 * structure @ep does not violate the constraints, or -1 otherwise.
1272 */
1273 static int ep_loop_check_proc(void *priv, void *cookie, int call_nests)
1274 {
1275 int error = 0;
1276 struct file *file = priv;
1277 struct eventpoll *ep = file->private_data;
1278 struct rb_node *rbp;
1279 struct epitem *epi;
1281 mutex_lock_nested(&ep->mtx, call_nests + 1);
1282 for (rbp = rb_first(&ep->rbr); rbp; rbp = rb_next(rbp)) {
1283 epi = rb_entry(rbp, struct epitem, rbn);
1284 if (unlikely(is_file_epoll(epi->ffd.file))) {
1285 error = ep_call_nested(&poll_loop_ncalls, EP_MAX_NESTS,
1286 ep_loop_check_proc, epi->ffd.file,
1287 epi->ffd.file->private_data, current);
1288 if (error != 0)
1289 break;
1290 }
1291 }
1292 mutex_unlock(&ep->mtx);
1294 return error;
1295 }
1297 /**
1298 * ep_loop_check - Performs a check to verify that adding an epoll file (@file)
1299 * another epoll file (represented by @ep) does not create
1300 * closed loops or too deep chains.
1301 *
1302 * @ep: Pointer to the epoll private data structure.
1303 * @file: Pointer to the epoll file to be checked.
1304 *
1305 * Returns: Returns zero if adding the epoll @file inside current epoll
1306 * structure @ep does not violate the constraints, or -1 otherwise.
1307 */
1308 static int ep_loop_check(struct eventpoll *ep, struct file *file)
1309 {
1310 return ep_call_nested(&poll_loop_ncalls, EP_MAX_NESTS,
1311 ep_loop_check_proc, file, ep, current);
1312 }
1314 /*
1315 * Open an eventpoll file descriptor.
1316 */
1317 SYSCALL_DEFINE1(epoll_create1, int, flags)
1318 {
1319 int error;
1320 struct eventpoll *ep = NULL;
1322 /* Check the EPOLL_* constant for consistency. */
1323 BUILD_BUG_ON(EPOLL_CLOEXEC != O_CLOEXEC);
1325 if (flags & ~EPOLL_CLOEXEC)
1326 return -EINVAL;
1327 /*
1328 * Create the internal data structure ("struct eventpoll").
1329 */
1330 error = ep_alloc(&ep);
1331 if (error < 0)
1332 return error;
1333 /*
1334 * Creates all the items needed to setup an eventpoll file. That is,
1335 * a file structure and a free file descriptor.
1336 */
1337 error = anon_inode_getfd("[eventpoll]", &eventpoll_fops, ep,
1338 O_RDWR | (flags & O_CLOEXEC));
1339 if (error < 0)
1340 ep_free(ep);
1342 return error;
1343 }
1345 SYSCALL_DEFINE1(epoll_create, int, size)
1346 {
1347 if (size <= 0)
1348 return -EINVAL;
1350 return sys_epoll_create1(0);
1351 }
1353 /*
1354 * The following function implements the controller interface for
1355 * the eventpoll file that enables the insertion/removal/change of
1356 * file descriptors inside the interest set.
1357 */
1358 SYSCALL_DEFINE4(epoll_ctl, int, epfd, int, op, int, fd,
1359 struct epoll_event __user *, event)
1360 {
1361 int error;
1362 int did_lock_epmutex = 0;
1363 struct file *file, *tfile;
1364 struct eventpoll *ep;
1365 struct epitem *epi;
1366 struct epoll_event epds;
1368 error = -EFAULT;
1369 if (ep_op_has_event(op) &&
1370 copy_from_user(&epds, event, sizeof(struct epoll_event)))
1371 goto error_return;
1373 /* Get the "struct file *" for the eventpoll file */
1374 error = -EBADF;
1375 file = fget(epfd);
1376 if (!file)
1377 goto error_return;
1379 /* Get the "struct file *" for the target file */
1380 tfile = fget(fd);
1381 if (!tfile)
1382 goto error_fput;
1384 /* The target file descriptor must support poll */
1385 error = -EPERM;
1386 if (!tfile->f_op || !tfile->f_op->poll)
1387 goto error_tgt_fput;
1389 /*
1390 * We have to check that the file structure underneath the file descriptor
1391 * the user passed to us _is_ an eventpoll file. And also we do not permit
1392 * adding an epoll file descriptor inside itself.
1393 */
1394 error = -EINVAL;
1395 if (file == tfile || !is_file_epoll(file))
1396 goto error_tgt_fput;
1398 /*
1399 * At this point it is safe to assume that the "private_data" contains
1400 * our own data structure.
1401 */
1402 ep = file->private_data;
1404 /*
1405 * When we insert an epoll file descriptor, inside another epoll file
1406 * descriptor, there is the change of creating closed loops, which are
1407 * better be handled here, than in more critical paths.
1408 *
1409 * We hold epmutex across the loop check and the insert in this case, in
1410 * order to prevent two separate inserts from racing and each doing the
1411 * insert "at the same time" such that ep_loop_check passes on both
1412 * before either one does the insert, thereby creating a cycle.
1413 */
1414 if (unlikely(is_file_epoll(tfile) && op == EPOLL_CTL_ADD)) {
1415 mutex_lock(&epmutex);
1416 did_lock_epmutex = 1;
1417 error = -ELOOP;
1418 if (ep_loop_check(ep, tfile) != 0)
1419 goto error_tgt_fput;
1420 }
1423 mutex_lock_nested(&ep->mtx, 0);
1425 /*
1426 * Try to lookup the file inside our RB tree, Since we grabbed "mtx"
1427 * above, we can be sure to be able to use the item looked up by
1428 * ep_find() till we release the mutex.
1429 */
1430 epi = ep_find(ep, tfile, fd);
1432 error = -EINVAL;
1433 switch (op) {
1434 case EPOLL_CTL_ADD:
1435 if (!epi) {
1436 epds.events |= POLLERR | POLLHUP;
1437 error = ep_insert(ep, &epds, tfile, fd);
1438 } else
1439 error = -EEXIST;
1440 break;
1441 case EPOLL_CTL_DEL:
1442 if (epi)
1443 error = ep_remove(ep, epi);
1444 else
1445 error = -ENOENT;
1446 break;
1447 case EPOLL_CTL_MOD:
1448 if (epi) {
1449 epds.events |= POLLERR | POLLHUP;
1450 error = ep_modify(ep, epi, &epds);
1451 } else
1452 error = -ENOENT;
1453 break;
1454 }
1455 mutex_unlock(&ep->mtx);
1457 error_tgt_fput:
1458 if (unlikely(did_lock_epmutex))
1459 mutex_unlock(&epmutex);
1461 fput(tfile);
1462 error_fput:
1463 fput(file);
1464 error_return:
1466 return error;
1467 }
1469 /*
1470 * Implement the event wait interface for the eventpoll file. It is the kernel
1471 * part of the user space epoll_wait(2).
1472 */
1473 SYSCALL_DEFINE4(epoll_wait, int, epfd, struct epoll_event __user *, events,
1474 int, maxevents, int, timeout)
1475 {
1476 int error;
1477 struct file *file;
1478 struct eventpoll *ep;
1480 /* The maximum number of event must be greater than zero */
1481 if (maxevents <= 0 || maxevents > EP_MAX_EVENTS)
1482 return -EINVAL;
1484 /* Verify that the area passed by the user is writeable */
1485 if (!access_ok(VERIFY_WRITE, events, maxevents * sizeof(struct epoll_event))) {
1486 error = -EFAULT;
1487 goto error_return;
1488 }
1490 /* Get the "struct file *" for the eventpoll file */
1491 error = -EBADF;
1492 file = fget(epfd);
1493 if (!file)
1494 goto error_return;
1496 /*
1497 * We have to check that the file structure underneath the fd
1498 * the user passed to us _is_ an eventpoll file.
1499 */
1500 error = -EINVAL;
1501 if (!is_file_epoll(file))
1502 goto error_fput;
1504 /*
1505 * At this point it is safe to assume that the "private_data" contains
1506 * our own data structure.
1507 */
1508 ep = file->private_data;
1510 /* Time to fish for events ... */
1511 error = ep_poll(ep, events, maxevents, timeout);
1513 error_fput:
1514 fput(file);
1515 error_return:
1517 return error;
1518 }
1520 #ifdef HAVE_SET_RESTORE_SIGMASK
1522 /*
1523 * Implement the event wait interface for the eventpoll file. It is the kernel
1524 * part of the user space epoll_pwait(2).
1525 */
1526 SYSCALL_DEFINE6(epoll_pwait, int, epfd, struct epoll_event __user *, events,
1527 int, maxevents, int, timeout, const sigset_t __user *, sigmask,
1528 size_t, sigsetsize)
1529 {
1530 int error;
1531 sigset_t ksigmask, sigsaved;
1533 /*
1534 * If the caller wants a certain signal mask to be set during the wait,
1535 * we apply it here.
1536 */
1537 if (sigmask) {
1538 if (sigsetsize != sizeof(sigset_t))
1539 return -EINVAL;
1540 if (copy_from_user(&ksigmask, sigmask, sizeof(ksigmask)))
1541 return -EFAULT;
1542 sigdelsetmask(&ksigmask, sigmask(SIGKILL) | sigmask(SIGSTOP));
1543 sigprocmask(SIG_SETMASK, &ksigmask, &sigsaved);
1544 }
1546 error = sys_epoll_wait(epfd, events, maxevents, timeout);
1548 /*
1549 * If we changed the signal mask, we need to restore the original one.
1550 * In case we've got a signal while waiting, we do not restore the
1551 * signal mask yet, and we allow do_signal() to deliver the signal on
1552 * the way back to userspace, before the signal mask is restored.
1553 */
1554 if (sigmask) {
1555 if (error == -EINTR) {
1556 memcpy(¤t->saved_sigmask, &sigsaved,
1557 sizeof(sigsaved));
1558 set_restore_sigmask();
1559 } else
1560 sigprocmask(SIG_SETMASK, &sigsaved, NULL);
1561 }
1563 return error;
1564 }
1566 #endif /* HAVE_SET_RESTORE_SIGMASK */
1568 static int __init eventpoll_init(void)
1569 {
1570 struct sysinfo si;
1572 si_meminfo(&si);
1573 /*
1574 * Allows top 4% of lomem to be allocated for epoll watches (per user).
1575 */
1576 max_user_watches = (((si.totalram - si.totalhigh) / 25) << PAGE_SHIFT) /
1577 EP_ITEM_COST;
1578 BUG_ON(max_user_watches < 0);
1580 /*
1581 * Initialize the structure used to perform epoll file descriptor
1582 * inclusion loops checks.
1583 */
1584 ep_nested_calls_init(&poll_loop_ncalls);
1586 /* Initialize the structure used to perform safe poll wait head wake ups */
1587 ep_nested_calls_init(&poll_safewake_ncalls);
1589 /* Initialize the structure used to perform file's f_op->poll() calls */
1590 ep_nested_calls_init(&poll_readywalk_ncalls);
1592 /* Allocates slab cache used to allocate "struct epitem" items */
1593 epi_cache = kmem_cache_create("eventpoll_epi", sizeof(struct epitem),
1594 0, SLAB_HWCACHE_ALIGN | SLAB_PANIC, NULL);
1596 /* Allocates slab cache used to allocate "struct eppoll_entry" */
1597 pwq_cache = kmem_cache_create("eventpoll_pwq",
1598 sizeof(struct eppoll_entry), 0, SLAB_PANIC, NULL);
1600 return 0;
1601 }
1602 fs_initcall(eventpoll_init);