]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - init/do_mounts_initrd.c
musb: adding support for am335x
[sitara-epos/sitara-epos-kernel.git] / init / do_mounts_initrd.c
1 #include <linux/unistd.h>
2 #include <linux/kernel.h>
3 #include <linux/fs.h>
4 #include <linux/minix_fs.h>
5 #include <linux/ext2_fs.h>
6 #include <linux/romfs_fs.h>
7 #include <linux/initrd.h>
8 #include <linux/sched.h>
9 #include <linux/freezer.h>
11 #include "do_mounts.h"
13 unsigned long initrd_start, initrd_end;
14 int initrd_below_start_ok;
15 unsigned int real_root_dev;     /* do_proc_dointvec cannot handle kdev_t */
16 static int __initdata old_fd, root_fd;
17 static int __initdata mount_initrd = 1;
19 static int __init no_initrd(char *str)
20 {
21         mount_initrd = 0;
22         return 1;
23 }
25 __setup("noinitrd", no_initrd);
27 static int __init do_linuxrc(void *_shell)
28 {
29         static const char *argv[] = { "linuxrc", NULL, };
30         extern const char *envp_init[];
31         const char *shell = _shell;
33         sys_close(old_fd);sys_close(root_fd);
34         sys_setsid();
35         return kernel_execve(shell, argv, envp_init);
36 }
38 static void __init handle_initrd(void)
39 {
40         int error;
41         int pid;
43         real_root_dev = new_encode_dev(ROOT_DEV);
44         create_dev("/dev/root.old", Root_RAM0);
45         /* mount initrd on rootfs' /root */
46         mount_block_root("/dev/root.old", root_mountflags & ~MS_RDONLY);
47         sys_mkdir("/old", 0700);
48         root_fd = sys_open("/", 0, 0);
49         old_fd = sys_open("/old", 0, 0);
50         /* move initrd over / and chdir/chroot in initrd root */
51         sys_chdir("/root");
52         sys_mount(".", "/", NULL, MS_MOVE, NULL);
53         sys_chroot(".");
55         /*
56          * In case that a resume from disk is carried out by linuxrc or one of
57          * its children, we need to tell the freezer not to wait for us.
58          */
59         current->flags |= PF_FREEZER_SKIP;
61         pid = kernel_thread(do_linuxrc, "/linuxrc", SIGCHLD);
62         if (pid > 0)
63                 while (pid != sys_wait4(-1, NULL, 0, NULL))
64                         yield();
66         current->flags &= ~PF_FREEZER_SKIP;
68         /* move initrd to rootfs' /old */
69         sys_fchdir(old_fd);
70         sys_mount("/", ".", NULL, MS_MOVE, NULL);
71         /* switch root and cwd back to / of rootfs */
72         sys_fchdir(root_fd);
73         sys_chroot(".");
74         sys_close(old_fd);
75         sys_close(root_fd);
77         if (new_decode_dev(real_root_dev) == Root_RAM0) {
78                 sys_chdir("/old");
79                 return;
80         }
82         ROOT_DEV = new_decode_dev(real_root_dev);
83         mount_root();
85         printk(KERN_NOTICE "Trying to move old root to /initrd ... ");
86         error = sys_mount("/old", "/root/initrd", NULL, MS_MOVE, NULL);
87         if (!error)
88                 printk("okay\n");
89         else {
90                 int fd = sys_open("/dev/root.old", O_RDWR, 0);
91                 if (error == -ENOENT)
92                         printk("/initrd does not exist. Ignored.\n");
93                 else
94                         printk("failed\n");
95                 printk(KERN_NOTICE "Unmounting old root\n");
96                 sys_umount("/old", MNT_DETACH);
97                 printk(KERN_NOTICE "Trying to free ramdisk memory ... ");
98                 if (fd < 0) {
99                         error = fd;
100                 } else {
101                         error = sys_ioctl(fd, BLKFLSBUF, 0);
102                         sys_close(fd);
103                 }
104                 printk(!error ? "okay\n" : "failed\n");
105         }
108 int __init initrd_load(void)
110         if (mount_initrd) {
111                 create_dev("/dev/ram", Root_RAM0);
112                 /*
113                  * Load the initrd data into /dev/ram0. Execute it as initrd
114                  * unless /dev/ram0 is supposed to be our actual root device,
115                  * in that case the ram disk is just set up here, and gets
116                  * mounted in the normal path.
117                  */
118                 if (rd_load_image("/initrd.image") && ROOT_DEV != Root_RAM0) {
119                         sys_unlink("/initrd.image");
120                         handle_initrd();
121                         return 1;
122                 }
123         }
124         sys_unlink("/initrd.image");
125         return 0;