]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - init/noinitramfs.c
video: da8xx-fb: correct suspend/resume sequence
[sitara-epos/sitara-epos-kernel.git] / init / noinitramfs.c
1 /*
2  * init/noinitramfs.c
3  *
4  * Copyright (C) 2006, NXP Semiconductors, All Rights Reserved
5  * Author: Jean-Paul Saman <jean-paul.saman@nxp.com>
6  *
7  * This program is free software; you can redistribute it and/or modify
8  * it under the terms of the GNU General Public License as published by
9  * the Free Software Foundation; version 2 of the License.
10  *
11  * This program is distributed in the hope that it will be useful,
12  * but WITHOUT ANY WARRANTY; without even the implied warranty of
13  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
14  * GNU General Public License for more details.
15  *
16  * You should have received a copy of the GNU General Public License
17  * along with this program; if not, write to the Free Software
18  * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA
19  */
20 #include <linux/init.h>
21 #include <linux/stat.h>
22 #include <linux/kdev_t.h>
23 #include <linux/syscalls.h>
25 /*
26  * Create a simple rootfs that is similar to the default initramfs
27  */
28 static int __init default_rootfs(void)
29 {
30         int err;
32         err = sys_mkdir((const char __user __force *) "/dev", 0755);
33         if (err < 0)
34                 goto out;
36         err = sys_mknod((const char __user __force *) "/dev/console",
37                         S_IFCHR | S_IRUSR | S_IWUSR,
38                         new_encode_dev(MKDEV(5, 1)));
39         if (err < 0)
40                 goto out;
42         err = sys_mkdir((const char __user __force *) "/root", 0700);
43         if (err < 0)
44                 goto out;
46         return 0;
48 out:
49         printk(KERN_WARNING "Failed to create a rootfs\n");
50         return err;
51 }
52 rootfs_initcall(default_rootfs);