]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - kernel/capability.c
am335x: lis33ldlh: Add accelerometer support to AM335X
[sitara-epos/sitara-epos-kernel.git] / kernel / capability.c
1 /*
2  * linux/kernel/capability.c
3  *
4  * Copyright (C) 1997  Andrew Main <zefram@fysh.org>
5  *
6  * Integrated into 2.1.97+,  Andrew G. Morgan <morgan@kernel.org>
7  * 30 May 2002: Cleanup, Robert M. Love <rml@tech9.net>
8  */
10 #include <linux/audit.h>
11 #include <linux/capability.h>
12 #include <linux/mm.h>
13 #include <linux/export.h>
14 #include <linux/security.h>
15 #include <linux/syscalls.h>
16 #include <linux/pid_namespace.h>
17 #include <linux/user_namespace.h>
18 #include <asm/uaccess.h>
20 /*
21  * Leveraged for setting/resetting capabilities
22  */
24 const kernel_cap_t __cap_empty_set = CAP_EMPTY_SET;
26 EXPORT_SYMBOL(__cap_empty_set);
28 int file_caps_enabled = 1;
30 static int __init file_caps_disable(char *str)
31 {
32         file_caps_enabled = 0;
33         return 1;
34 }
35 __setup("no_file_caps", file_caps_disable);
37 /*
38  * More recent versions of libcap are available from:
39  *
40  *   http://www.kernel.org/pub/linux/libs/security/linux-privs/
41  */
43 static void warn_legacy_capability_use(void)
44 {
45         static int warned;
46         if (!warned) {
47                 char name[sizeof(current->comm)];
49                 printk(KERN_INFO "warning: `%s' uses 32-bit capabilities"
50                        " (legacy support in use)\n",
51                        get_task_comm(name, current));
52                 warned = 1;
53         }
54 }
56 /*
57  * Version 2 capabilities worked fine, but the linux/capability.h file
58  * that accompanied their introduction encouraged their use without
59  * the necessary user-space source code changes. As such, we have
60  * created a version 3 with equivalent functionality to version 2, but
61  * with a header change to protect legacy source code from using
62  * version 2 when it wanted to use version 1. If your system has code
63  * that trips the following warning, it is using version 2 specific
64  * capabilities and may be doing so insecurely.
65  *
66  * The remedy is to either upgrade your version of libcap (to 2.10+,
67  * if the application is linked against it), or recompile your
68  * application with modern kernel headers and this warning will go
69  * away.
70  */
72 static void warn_deprecated_v2(void)
73 {
74         static int warned;
76         if (!warned) {
77                 char name[sizeof(current->comm)];
79                 printk(KERN_INFO "warning: `%s' uses deprecated v2"
80                        " capabilities in a way that may be insecure.\n",
81                        get_task_comm(name, current));
82                 warned = 1;
83         }
84 }
86 /*
87  * Version check. Return the number of u32s in each capability flag
88  * array, or a negative value on error.
89  */
90 static int cap_validate_magic(cap_user_header_t header, unsigned *tocopy)
91 {
92         __u32 version;
94         if (get_user(version, &header->version))
95                 return -EFAULT;
97         switch (version) {
98         case _LINUX_CAPABILITY_VERSION_1:
99                 warn_legacy_capability_use();
100                 *tocopy = _LINUX_CAPABILITY_U32S_1;
101                 break;
102         case _LINUX_CAPABILITY_VERSION_2:
103                 warn_deprecated_v2();
104                 /*
105                  * fall through - v3 is otherwise equivalent to v2.
106                  */
107         case _LINUX_CAPABILITY_VERSION_3:
108                 *tocopy = _LINUX_CAPABILITY_U32S_3;
109                 break;
110         default:
111                 if (put_user((u32)_KERNEL_CAPABILITY_VERSION, &header->version))
112                         return -EFAULT;
113                 return -EINVAL;
114         }
116         return 0;
119 /*
120  * The only thing that can change the capabilities of the current
121  * process is the current process. As such, we can't be in this code
122  * at the same time as we are in the process of setting capabilities
123  * in this process. The net result is that we can limit our use of
124  * locks to when we are reading the caps of another process.
125  */
126 static inline int cap_get_target_pid(pid_t pid, kernel_cap_t *pEp,
127                                      kernel_cap_t *pIp, kernel_cap_t *pPp)
129         int ret;
131         if (pid && (pid != task_pid_vnr(current))) {
132                 struct task_struct *target;
134                 rcu_read_lock();
136                 target = find_task_by_vpid(pid);
137                 if (!target)
138                         ret = -ESRCH;
139                 else
140                         ret = security_capget(target, pEp, pIp, pPp);
142                 rcu_read_unlock();
143         } else
144                 ret = security_capget(current, pEp, pIp, pPp);
146         return ret;
149 /**
150  * sys_capget - get the capabilities of a given process.
151  * @header: pointer to struct that contains capability version and
152  *      target pid data
153  * @dataptr: pointer to struct that contains the effective, permitted,
154  *      and inheritable capabilities that are returned
155  *
156  * Returns 0 on success and < 0 on error.
157  */
158 SYSCALL_DEFINE2(capget, cap_user_header_t, header, cap_user_data_t, dataptr)
160         int ret = 0;
161         pid_t pid;
162         unsigned tocopy;
163         kernel_cap_t pE, pI, pP;
165         ret = cap_validate_magic(header, &tocopy);
166         if ((dataptr == NULL) || (ret != 0))
167                 return ((dataptr == NULL) && (ret == -EINVAL)) ? 0 : ret;
169         if (get_user(pid, &header->pid))
170                 return -EFAULT;
172         if (pid < 0)
173                 return -EINVAL;
175         ret = cap_get_target_pid(pid, &pE, &pI, &pP);
176         if (!ret) {
177                 struct __user_cap_data_struct kdata[_KERNEL_CAPABILITY_U32S];
178                 unsigned i;
180                 for (i = 0; i < tocopy; i++) {
181                         kdata[i].effective = pE.cap[i];
182                         kdata[i].permitted = pP.cap[i];
183                         kdata[i].inheritable = pI.cap[i];
184                 }
186                 /*
187                  * Note, in the case, tocopy < _KERNEL_CAPABILITY_U32S,
188                  * we silently drop the upper capabilities here. This
189                  * has the effect of making older libcap
190                  * implementations implicitly drop upper capability
191                  * bits when they perform a: capget/modify/capset
192                  * sequence.
193                  *
194                  * This behavior is considered fail-safe
195                  * behavior. Upgrading the application to a newer
196                  * version of libcap will enable access to the newer
197                  * capabilities.
198                  *
199                  * An alternative would be to return an error here
200                  * (-ERANGE), but that causes legacy applications to
201                  * unexpectidly fail; the capget/modify/capset aborts
202                  * before modification is attempted and the application
203                  * fails.
204                  */
205                 if (copy_to_user(dataptr, kdata, tocopy
206                                  * sizeof(struct __user_cap_data_struct))) {
207                         return -EFAULT;
208                 }
209         }
211         return ret;
214 /**
215  * sys_capset - set capabilities for a process or (*) a group of processes
216  * @header: pointer to struct that contains capability version and
217  *      target pid data
218  * @data: pointer to struct that contains the effective, permitted,
219  *      and inheritable capabilities
220  *
221  * Set capabilities for the current process only.  The ability to any other
222  * process(es) has been deprecated and removed.
223  *
224  * The restrictions on setting capabilities are specified as:
225  *
226  * I: any raised capabilities must be a subset of the old permitted
227  * P: any raised capabilities must be a subset of the old permitted
228  * E: must be set to a subset of new permitted
229  *
230  * Returns 0 on success and < 0 on error.
231  */
232 SYSCALL_DEFINE2(capset, cap_user_header_t, header, const cap_user_data_t, data)
234         struct __user_cap_data_struct kdata[_KERNEL_CAPABILITY_U32S];
235         unsigned i, tocopy, copybytes;
236         kernel_cap_t inheritable, permitted, effective;
237         struct cred *new;
238         int ret;
239         pid_t pid;
241         ret = cap_validate_magic(header, &tocopy);
242         if (ret != 0)
243                 return ret;
245         if (get_user(pid, &header->pid))
246                 return -EFAULT;
248         /* may only affect current now */
249         if (pid != 0 && pid != task_pid_vnr(current))
250                 return -EPERM;
252         copybytes = tocopy * sizeof(struct __user_cap_data_struct);
253         if (copybytes > sizeof(kdata))
254                 return -EFAULT;
256         if (copy_from_user(&kdata, data, copybytes))
257                 return -EFAULT;
259         for (i = 0; i < tocopy; i++) {
260                 effective.cap[i] = kdata[i].effective;
261                 permitted.cap[i] = kdata[i].permitted;
262                 inheritable.cap[i] = kdata[i].inheritable;
263         }
264         while (i < _KERNEL_CAPABILITY_U32S) {
265                 effective.cap[i] = 0;
266                 permitted.cap[i] = 0;
267                 inheritable.cap[i] = 0;
268                 i++;
269         }
271         new = prepare_creds();
272         if (!new)
273                 return -ENOMEM;
275         ret = security_capset(new, current_cred(),
276                               &effective, &inheritable, &permitted);
277         if (ret < 0)
278                 goto error;
280         audit_log_capset(pid, new, current_cred());
282         return commit_creds(new);
284 error:
285         abort_creds(new);
286         return ret;
289 /**
290  * has_capability - Does a task have a capability in init_user_ns
291  * @t: The task in question
292  * @cap: The capability to be tested for
293  *
294  * Return true if the specified task has the given superior capability
295  * currently in effect to the initial user namespace, false if not.
296  *
297  * Note that this does not set PF_SUPERPRIV on the task.
298  */
299 bool has_capability(struct task_struct *t, int cap)
301         int ret = security_real_capable(t, &init_user_ns, cap);
303         return (ret == 0);
306 /**
307  * has_capability - Does a task have a capability in a specific user ns
308  * @t: The task in question
309  * @ns: target user namespace
310  * @cap: The capability to be tested for
311  *
312  * Return true if the specified task has the given superior capability
313  * currently in effect to the specified user namespace, false if not.
314  *
315  * Note that this does not set PF_SUPERPRIV on the task.
316  */
317 bool has_ns_capability(struct task_struct *t,
318                        struct user_namespace *ns, int cap)
320         int ret = security_real_capable(t, ns, cap);
322         return (ret == 0);
325 /**
326  * has_capability_noaudit - Does a task have a capability (unaudited)
327  * @t: The task in question
328  * @cap: The capability to be tested for
329  *
330  * Return true if the specified task has the given superior capability
331  * currently in effect to init_user_ns, false if not.  Don't write an
332  * audit message for the check.
333  *
334  * Note that this does not set PF_SUPERPRIV on the task.
335  */
336 bool has_capability_noaudit(struct task_struct *t, int cap)
338         int ret = security_real_capable_noaudit(t, &init_user_ns, cap);
340         return (ret == 0);
343 /**
344  * capable - Determine if the current task has a superior capability in effect
345  * @cap: The capability to be tested for
346  *
347  * Return true if the current task has the given superior capability currently
348  * available for use, false if not.
349  *
350  * This sets PF_SUPERPRIV on the task if the capability is available on the
351  * assumption that it's about to be used.
352  */
353 bool capable(int cap)
355         return ns_capable(&init_user_ns, cap);
357 EXPORT_SYMBOL(capable);
359 /**
360  * ns_capable - Determine if the current task has a superior capability in effect
361  * @ns:  The usernamespace we want the capability in
362  * @cap: The capability to be tested for
363  *
364  * Return true if the current task has the given superior capability currently
365  * available for use, false if not.
366  *
367  * This sets PF_SUPERPRIV on the task if the capability is available on the
368  * assumption that it's about to be used.
369  */
370 bool ns_capable(struct user_namespace *ns, int cap)
372         if (unlikely(!cap_valid(cap))) {
373                 printk(KERN_CRIT "capable() called with invalid cap=%u\n", cap);
374                 BUG();
375         }
377         if (security_capable(ns, current_cred(), cap) == 0) {
378                 current->flags |= PF_SUPERPRIV;
379                 return true;
380         }
381         return false;
383 EXPORT_SYMBOL(ns_capable);
385 /**
386  * task_ns_capable - Determine whether current task has a superior
387  * capability targeted at a specific task's user namespace.
388  * @t: The task whose user namespace is targeted.
389  * @cap: The capability in question.
390  *
391  *  Return true if it does, false otherwise.
392  */
393 bool task_ns_capable(struct task_struct *t, int cap)
395         return ns_capable(task_cred_xxx(t, user)->user_ns, cap);
397 EXPORT_SYMBOL(task_ns_capable);
399 /**
400  * nsown_capable - Check superior capability to one's own user_ns
401  * @cap: The capability in question
402  *
403  * Return true if the current task has the given superior capability
404  * targeted at its own user namespace.
405  */
406 bool nsown_capable(int cap)
408         return ns_capable(current_user_ns(), cap);