]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - kernel/panic.c
am335x: lis33ldlh: Add accelerometer support to AM335X
[sitara-epos/sitara-epos-kernel.git] / kernel / panic.c
1 /*
2  *  linux/kernel/panic.c
3  *
4  *  Copyright (C) 1991, 1992  Linus Torvalds
5  */
7 /*
8  * This function is used through-out the kernel (including mm and fs)
9  * to indicate a major problem.
10  */
11 #include <linux/debug_locks.h>
12 #include <linux/interrupt.h>
13 #include <linux/kmsg_dump.h>
14 #include <linux/kallsyms.h>
15 #include <linux/notifier.h>
16 #include <linux/module.h>
17 #include <linux/random.h>
18 #include <linux/reboot.h>
19 #include <linux/delay.h>
20 #include <linux/kexec.h>
21 #include <linux/sched.h>
22 #include <linux/sysrq.h>
23 #include <linux/init.h>
24 #include <linux/nmi.h>
25 #include <linux/dmi.h>
27 #define PANIC_TIMER_STEP 100
28 #define PANIC_BLINK_SPD 18
30 int panic_on_oops;
31 static unsigned long tainted_mask;
32 static int pause_on_oops;
33 static int pause_on_oops_flag;
34 static DEFINE_SPINLOCK(pause_on_oops_lock);
36 int panic_timeout;
37 EXPORT_SYMBOL_GPL(panic_timeout);
39 ATOMIC_NOTIFIER_HEAD(panic_notifier_list);
41 EXPORT_SYMBOL(panic_notifier_list);
43 static long no_blink(int state)
44 {
45         return 0;
46 }
48 /* Returns how long it waited in ms */
49 long (*panic_blink)(int state);
50 EXPORT_SYMBOL(panic_blink);
52 /**
53  *      panic - halt the system
54  *      @fmt: The text string to print
55  *
56  *      Display a message, then perform cleanups.
57  *
58  *      This function never returns.
59  */
60 NORET_TYPE void panic(const char * fmt, ...)
61 {
62         static char buf[1024];
63         va_list args;
64         long i, i_next = 0;
65         int state = 0;
67         /*
68          * It's possible to come here directly from a panic-assertion and
69          * not have preempt disabled. Some functions called from here want
70          * preempt to be disabled. No point enabling it later though...
71          */
72         preempt_disable();
74         console_verbose();
75         bust_spinlocks(1);
76         va_start(args, fmt);
77         vsnprintf(buf, sizeof(buf), fmt, args);
78         va_end(args);
79         printk(KERN_EMERG "Kernel panic - not syncing: %s\n",buf);
80 #ifdef CONFIG_DEBUG_BUGVERBOSE
81         dump_stack();
82 #endif
84         /*
85          * If we have crashed and we have a crash kernel loaded let it handle
86          * everything else.
87          * Do we want to call this before we try to display a message?
88          */
89         crash_kexec(NULL);
91         kmsg_dump(KMSG_DUMP_PANIC);
93         /*
94          * Note smp_send_stop is the usual smp shutdown function, which
95          * unfortunately means it may not be hardened to work in a panic
96          * situation.
97          */
98         smp_send_stop();
100         atomic_notifier_call_chain(&panic_notifier_list, 0, buf);
102         bust_spinlocks(0);
104         if (!panic_blink)
105                 panic_blink = no_blink;
107         if (panic_timeout > 0) {
108                 /*
109                  * Delay timeout seconds before rebooting the machine.
110                  * We can't use the "normal" timers since we just panicked.
111                  */
112                 printk(KERN_EMERG "Rebooting in %d seconds..", panic_timeout);
114                 for (i = 0; i < panic_timeout * 1000; i += PANIC_TIMER_STEP) {
115                         touch_nmi_watchdog();
116                         if (i >= i_next) {
117                                 i += panic_blink(state ^= 1);
118                                 i_next = i + 3600 / PANIC_BLINK_SPD;
119                         }
120                         mdelay(PANIC_TIMER_STEP);
121                 }
122         }
123         if (panic_timeout != 0) {
124                 /*
125                  * This will not be a clean reboot, with everything
126                  * shutting down.  But if there is a chance of
127                  * rebooting the system it will be rebooted.
128                  */
129                 emergency_restart();
130         }
131 #ifdef __sparc__
132         {
133                 extern int stop_a_enabled;
134                 /* Make sure the user can actually press Stop-A (L1-A) */
135                 stop_a_enabled = 1;
136                 printk(KERN_EMERG "Press Stop-A (L1-A) to return to the boot prom\n");
137         }
138 #endif
139 #if defined(CONFIG_S390)
140         {
141                 unsigned long caller;
143                 caller = (unsigned long)__builtin_return_address(0);
144                 disabled_wait(caller);
145         }
146 #endif
147         local_irq_enable();
148         for (i = 0; ; i += PANIC_TIMER_STEP) {
149                 touch_softlockup_watchdog();
150                 if (i >= i_next) {
151                         i += panic_blink(state ^= 1);
152                         i_next = i + 3600 / PANIC_BLINK_SPD;
153                 }
154                 mdelay(PANIC_TIMER_STEP);
155         }
158 EXPORT_SYMBOL(panic);
161 struct tnt {
162         u8      bit;
163         char    true;
164         char    false;
165 };
167 static const struct tnt tnts[] = {
168         { TAINT_PROPRIETARY_MODULE,     'P', 'G' },
169         { TAINT_FORCED_MODULE,          'F', ' ' },
170         { TAINT_UNSAFE_SMP,             'S', ' ' },
171         { TAINT_FORCED_RMMOD,           'R', ' ' },
172         { TAINT_MACHINE_CHECK,          'M', ' ' },
173         { TAINT_BAD_PAGE,               'B', ' ' },
174         { TAINT_USER,                   'U', ' ' },
175         { TAINT_DIE,                    'D', ' ' },
176         { TAINT_OVERRIDDEN_ACPI_TABLE,  'A', ' ' },
177         { TAINT_WARN,                   'W', ' ' },
178         { TAINT_CRAP,                   'C', ' ' },
179         { TAINT_FIRMWARE_WORKAROUND,    'I', ' ' },
180         { TAINT_OOT_MODULE,             'O', ' ' },
181 };
183 /**
184  *      print_tainted - return a string to represent the kernel taint state.
185  *
186  *  'P' - Proprietary module has been loaded.
187  *  'F' - Module has been forcibly loaded.
188  *  'S' - SMP with CPUs not designed for SMP.
189  *  'R' - User forced a module unload.
190  *  'M' - System experienced a machine check exception.
191  *  'B' - System has hit bad_page.
192  *  'U' - Userspace-defined naughtiness.
193  *  'D' - Kernel has oopsed before
194  *  'A' - ACPI table overridden.
195  *  'W' - Taint on warning.
196  *  'C' - modules from drivers/staging are loaded.
197  *  'I' - Working around severe firmware bug.
198  *  'O' - Out-of-tree module has been loaded.
199  *
200  *      The string is overwritten by the next call to print_tainted().
201  */
202 const char *print_tainted(void)
204         static char buf[ARRAY_SIZE(tnts) + sizeof("Tainted: ") + 1];
206         if (tainted_mask) {
207                 char *s;
208                 int i;
210                 s = buf + sprintf(buf, "Tainted: ");
211                 for (i = 0; i < ARRAY_SIZE(tnts); i++) {
212                         const struct tnt *t = &tnts[i];
213                         *s++ = test_bit(t->bit, &tainted_mask) ?
214                                         t->true : t->false;
215                 }
216                 *s = 0;
217         } else
218                 snprintf(buf, sizeof(buf), "Not tainted");
220         return buf;
223 int test_taint(unsigned flag)
225         return test_bit(flag, &tainted_mask);
227 EXPORT_SYMBOL(test_taint);
229 unsigned long get_taint(void)
231         return tainted_mask;
234 void add_taint(unsigned flag)
236         /*
237          * Can't trust the integrity of the kernel anymore.
238          * We don't call directly debug_locks_off() because the issue
239          * is not necessarily serious enough to set oops_in_progress to 1
240          * Also we want to keep up lockdep for staging development and
241          * post-warning case.
242          */
243         if (flag != TAINT_CRAP && flag != TAINT_WARN && __debug_locks_off())
244                 printk(KERN_WARNING "Disabling lock debugging due to kernel taint\n");
246         set_bit(flag, &tainted_mask);
248 EXPORT_SYMBOL(add_taint);
250 static void spin_msec(int msecs)
252         int i;
254         for (i = 0; i < msecs; i++) {
255                 touch_nmi_watchdog();
256                 mdelay(1);
257         }
260 /*
261  * It just happens that oops_enter() and oops_exit() are identically
262  * implemented...
263  */
264 static void do_oops_enter_exit(void)
266         unsigned long flags;
267         static int spin_counter;
269         if (!pause_on_oops)
270                 return;
272         spin_lock_irqsave(&pause_on_oops_lock, flags);
273         if (pause_on_oops_flag == 0) {
274                 /* This CPU may now print the oops message */
275                 pause_on_oops_flag = 1;
276         } else {
277                 /* We need to stall this CPU */
278                 if (!spin_counter) {
279                         /* This CPU gets to do the counting */
280                         spin_counter = pause_on_oops;
281                         do {
282                                 spin_unlock(&pause_on_oops_lock);
283                                 spin_msec(MSEC_PER_SEC);
284                                 spin_lock(&pause_on_oops_lock);
285                         } while (--spin_counter);
286                         pause_on_oops_flag = 0;
287                 } else {
288                         /* This CPU waits for a different one */
289                         while (spin_counter) {
290                                 spin_unlock(&pause_on_oops_lock);
291                                 spin_msec(1);
292                                 spin_lock(&pause_on_oops_lock);
293                         }
294                 }
295         }
296         spin_unlock_irqrestore(&pause_on_oops_lock, flags);
299 /*
300  * Return true if the calling CPU is allowed to print oops-related info.
301  * This is a bit racy..
302  */
303 int oops_may_print(void)
305         return pause_on_oops_flag == 0;
308 /*
309  * Called when the architecture enters its oops handler, before it prints
310  * anything.  If this is the first CPU to oops, and it's oopsing the first
311  * time then let it proceed.
312  *
313  * This is all enabled by the pause_on_oops kernel boot option.  We do all
314  * this to ensure that oopses don't scroll off the screen.  It has the
315  * side-effect of preventing later-oopsing CPUs from mucking up the display,
316  * too.
317  *
318  * It turns out that the CPU which is allowed to print ends up pausing for
319  * the right duration, whereas all the other CPUs pause for twice as long:
320  * once in oops_enter(), once in oops_exit().
321  */
322 void oops_enter(void)
324         tracing_off();
325         /* can't trust the integrity of the kernel anymore: */
326         debug_locks_off();
327         do_oops_enter_exit();
330 /*
331  * 64-bit random ID for oopses:
332  */
333 static u64 oops_id;
335 static int init_oops_id(void)
337         if (!oops_id)
338                 get_random_bytes(&oops_id, sizeof(oops_id));
339         else
340                 oops_id++;
342         return 0;
344 late_initcall(init_oops_id);
346 void print_oops_end_marker(void)
348         init_oops_id();
349         printk(KERN_WARNING "---[ end trace %016llx ]---\n",
350                 (unsigned long long)oops_id);
353 /*
354  * Called when the architecture exits its oops handler, after printing
355  * everything.
356  */
357 void oops_exit(void)
359         do_oops_enter_exit();
360         print_oops_end_marker();
361         kmsg_dump(KMSG_DUMP_OOPS);
364 #ifdef WANT_WARN_ON_SLOWPATH
365 struct slowpath_args {
366         const char *fmt;
367         va_list args;
368 };
370 static void warn_slowpath_common(const char *file, int line, void *caller,
371                                  unsigned taint, struct slowpath_args *args)
373         const char *board;
375         printk(KERN_WARNING "------------[ cut here ]------------\n");
376         printk(KERN_WARNING "WARNING: at %s:%d %pS()\n", file, line, caller);
377         board = dmi_get_system_info(DMI_PRODUCT_NAME);
378         if (board)
379                 printk(KERN_WARNING "Hardware name: %s\n", board);
381         if (args)
382                 vprintk(args->fmt, args->args);
384         print_modules();
385         dump_stack();
386         print_oops_end_marker();
387         add_taint(taint);
390 void warn_slowpath_fmt(const char *file, int line, const char *fmt, ...)
392         struct slowpath_args args;
394         args.fmt = fmt;
395         va_start(args.args, fmt);
396         warn_slowpath_common(file, line, __builtin_return_address(0),
397                              TAINT_WARN, &args);
398         va_end(args.args);
400 EXPORT_SYMBOL(warn_slowpath_fmt);
402 void warn_slowpath_fmt_taint(const char *file, int line,
403                              unsigned taint, const char *fmt, ...)
405         struct slowpath_args args;
407         args.fmt = fmt;
408         va_start(args.args, fmt);
409         warn_slowpath_common(file, line, __builtin_return_address(0),
410                              taint, &args);
411         va_end(args.args);
413 EXPORT_SYMBOL(warn_slowpath_fmt_taint);
415 void warn_slowpath_null(const char *file, int line)
417         warn_slowpath_common(file, line, __builtin_return_address(0),
418                              TAINT_WARN, NULL);
420 EXPORT_SYMBOL(warn_slowpath_null);
421 #endif
423 #ifdef CONFIG_CC_STACKPROTECTOR
425 /*
426  * Called when gcc's -fstack-protector feature is used, and
427  * gcc detects corruption of the on-stack canary value
428  */
429 void __stack_chk_fail(void)
431         panic("stack-protector: Kernel stack is corrupted in: %p\n",
432                 __builtin_return_address(0));
434 EXPORT_SYMBOL(__stack_chk_fail);
436 #endif
438 core_param(panic, panic_timeout, int, 0644);
439 core_param(pause_on_oops, pause_on_oops, int, 0644);
441 static int __init oops_setup(char *s)
443         if (!s)
444                 return -EINVAL;
445         if (!strcmp(s, "panic"))
446                 panic_on_oops = 1;
447         return 0;
449 early_param("oops", oops_setup);