1 /*
2 * linux/kernel/posix-timers.c
3 *
4 *
5 * 2002-10-15 Posix Clocks & timers
6 * by George Anzinger george@mvista.com
7 *
8 * Copyright (C) 2002 2003 by MontaVista Software.
9 *
10 * 2004-06-01 Fix CLOCK_REALTIME clock/timer TIMER_ABSTIME bug.
11 * Copyright (C) 2004 Boris Hu
12 *
13 * This program is free software; you can redistribute it and/or modify
14 * it under the terms of the GNU General Public License as published by
15 * the Free Software Foundation; either version 2 of the License, or (at
16 * your option) any later version.
17 *
18 * This program is distributed in the hope that it will be useful, but
19 * WITHOUT ANY WARRANTY; without even the implied warranty of
20 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
21 * General Public License for more details.
23 * You should have received a copy of the GNU General Public License
24 * along with this program; if not, write to the Free Software
25 * Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139, USA.
26 *
27 * MontaVista Software | 1237 East Arques Avenue | Sunnyvale | CA 94085 | USA
28 */
30 /* These are all the functions necessary to implement
31 * POSIX clocks & timers
32 */
33 #include <linux/mm.h>
34 #include <linux/interrupt.h>
35 #include <linux/slab.h>
36 #include <linux/time.h>
37 #include <linux/mutex.h>
39 #include <asm/uaccess.h>
40 #include <linux/list.h>
41 #include <linux/init.h>
42 #include <linux/compiler.h>
43 #include <linux/idr.h>
44 #include <linux/posix-clock.h>
45 #include <linux/posix-timers.h>
46 #include <linux/syscalls.h>
47 #include <linux/wait.h>
48 #include <linux/workqueue.h>
49 #include <linux/export.h>
51 /*
52 * Management arrays for POSIX timers. Timers are kept in slab memory
53 * Timer ids are allocated by an external routine that keeps track of the
54 * id and the timer. The external interface is:
55 *
56 * void *idr_find(struct idr *idp, int id); to find timer_id <id>
57 * int idr_get_new(struct idr *idp, void *ptr); to get a new id and
58 * related it to <ptr>
59 * void idr_remove(struct idr *idp, int id); to release <id>
60 * void idr_init(struct idr *idp); to initialize <idp>
61 * which we supply.
62 * The idr_get_new *may* call slab for more memory so it must not be
63 * called under a spin lock. Likewise idr_remore may release memory
64 * (but it may be ok to do this under a lock...).
65 * idr_find is just a memory look up and is quite fast. A -1 return
66 * indicates that the requested id does not exist.
67 */
69 /*
70 * Lets keep our timers in a slab cache :-)
71 */
72 static struct kmem_cache *posix_timers_cache;
73 static struct idr posix_timers_id;
74 static DEFINE_SPINLOCK(idr_lock);
76 /*
77 * we assume that the new SIGEV_THREAD_ID shares no bits with the other
78 * SIGEV values. Here we put out an error if this assumption fails.
79 */
80 #if SIGEV_THREAD_ID != (SIGEV_THREAD_ID & \
81 ~(SIGEV_SIGNAL | SIGEV_NONE | SIGEV_THREAD))
82 #error "SIGEV_THREAD_ID must not share bit with other SIGEV values!"
83 #endif
85 /*
86 * parisc wants ENOTSUP instead of EOPNOTSUPP
87 */
88 #ifndef ENOTSUP
89 # define ENANOSLEEP_NOTSUP EOPNOTSUPP
90 #else
91 # define ENANOSLEEP_NOTSUP ENOTSUP
92 #endif
94 /*
95 * The timer ID is turned into a timer address by idr_find().
96 * Verifying a valid ID consists of:
97 *
98 * a) checking that idr_find() returns other than -1.
99 * b) checking that the timer id matches the one in the timer itself.
100 * c) that the timer owner is in the callers thread group.
101 */
103 /*
104 * CLOCKs: The POSIX standard calls for a couple of clocks and allows us
105 * to implement others. This structure defines the various
106 * clocks.
107 *
108 * RESOLUTION: Clock resolution is used to round up timer and interval
109 * times, NOT to report clock times, which are reported with as
110 * much resolution as the system can muster. In some cases this
111 * resolution may depend on the underlying clock hardware and
112 * may not be quantifiable until run time, and only then is the
113 * necessary code is written. The standard says we should say
114 * something about this issue in the documentation...
115 *
116 * FUNCTIONS: The CLOCKs structure defines possible functions to
117 * handle various clock functions.
118 *
119 * The standard POSIX timer management code assumes the
120 * following: 1.) The k_itimer struct (sched.h) is used for
121 * the timer. 2.) The list, it_lock, it_clock, it_id and
122 * it_pid fields are not modified by timer code.
123 *
124 * Permissions: It is assumed that the clock_settime() function defined
125 * for each clock will take care of permission checks. Some
126 * clocks may be set able by any user (i.e. local process
127 * clocks) others not. Currently the only set able clock we
128 * have is CLOCK_REALTIME and its high res counter part, both of
129 * which we beg off on and pass to do_sys_settimeofday().
130 */
132 static struct k_clock posix_clocks[MAX_CLOCKS];
134 /*
135 * These ones are defined below.
136 */
137 static int common_nsleep(const clockid_t, int flags, struct timespec *t,
138 struct timespec __user *rmtp);
139 static int common_timer_create(struct k_itimer *new_timer);
140 static void common_timer_get(struct k_itimer *, struct itimerspec *);
141 static int common_timer_set(struct k_itimer *, int,
142 struct itimerspec *, struct itimerspec *);
143 static int common_timer_del(struct k_itimer *timer);
145 static enum hrtimer_restart posix_timer_fn(struct hrtimer *data);
147 static struct k_itimer *__lock_timer(timer_t timer_id, unsigned long *flags);
149 #define lock_timer(tid, flags) \
150 ({ struct k_itimer *__timr; \
151 __cond_lock(&__timr->it_lock, __timr = __lock_timer(tid, flags)); \
152 __timr; \
153 })
155 static inline void unlock_timer(struct k_itimer *timr, unsigned long flags)
156 {
157 spin_unlock_irqrestore(&timr->it_lock, flags);
158 }
160 /* Get clock_realtime */
161 static int posix_clock_realtime_get(clockid_t which_clock, struct timespec *tp)
162 {
163 ktime_get_real_ts(tp);
164 return 0;
165 }
167 /* Set clock_realtime */
168 static int posix_clock_realtime_set(const clockid_t which_clock,
169 const struct timespec *tp)
170 {
171 return do_sys_settimeofday(tp, NULL);
172 }
174 static int posix_clock_realtime_adj(const clockid_t which_clock,
175 struct timex *t)
176 {
177 return do_adjtimex(t);
178 }
180 /*
181 * Get monotonic time for posix timers
182 */
183 static int posix_ktime_get_ts(clockid_t which_clock, struct timespec *tp)
184 {
185 ktime_get_ts(tp);
186 return 0;
187 }
189 /*
190 * Get monotonic-raw time for posix timers
191 */
192 static int posix_get_monotonic_raw(clockid_t which_clock, struct timespec *tp)
193 {
194 getrawmonotonic(tp);
195 return 0;
196 }
199 static int posix_get_realtime_coarse(clockid_t which_clock, struct timespec *tp)
200 {
201 *tp = current_kernel_time();
202 return 0;
203 }
205 static int posix_get_monotonic_coarse(clockid_t which_clock,
206 struct timespec *tp)
207 {
208 *tp = get_monotonic_coarse();
209 return 0;
210 }
212 static int posix_get_coarse_res(const clockid_t which_clock, struct timespec *tp)
213 {
214 *tp = ktime_to_timespec(KTIME_LOW_RES);
215 return 0;
216 }
218 static int posix_get_boottime(const clockid_t which_clock, struct timespec *tp)
219 {
220 get_monotonic_boottime(tp);
221 return 0;
222 }
225 /*
226 * Initialize everything, well, just everything in Posix clocks/timers ;)
227 */
228 static __init int init_posix_timers(void)
229 {
230 struct k_clock clock_realtime = {
231 .clock_getres = hrtimer_get_res,
232 .clock_get = posix_clock_realtime_get,
233 .clock_set = posix_clock_realtime_set,
234 .clock_adj = posix_clock_realtime_adj,
235 .nsleep = common_nsleep,
236 .nsleep_restart = hrtimer_nanosleep_restart,
237 .timer_create = common_timer_create,
238 .timer_set = common_timer_set,
239 .timer_get = common_timer_get,
240 .timer_del = common_timer_del,
241 };
242 struct k_clock clock_monotonic = {
243 .clock_getres = hrtimer_get_res,
244 .clock_get = posix_ktime_get_ts,
245 .nsleep = common_nsleep,
246 .nsleep_restart = hrtimer_nanosleep_restart,
247 .timer_create = common_timer_create,
248 .timer_set = common_timer_set,
249 .timer_get = common_timer_get,
250 .timer_del = common_timer_del,
251 };
252 struct k_clock clock_monotonic_raw = {
253 .clock_getres = hrtimer_get_res,
254 .clock_get = posix_get_monotonic_raw,
255 };
256 struct k_clock clock_realtime_coarse = {
257 .clock_getres = posix_get_coarse_res,
258 .clock_get = posix_get_realtime_coarse,
259 };
260 struct k_clock clock_monotonic_coarse = {
261 .clock_getres = posix_get_coarse_res,
262 .clock_get = posix_get_monotonic_coarse,
263 };
264 struct k_clock clock_boottime = {
265 .clock_getres = hrtimer_get_res,
266 .clock_get = posix_get_boottime,
267 .nsleep = common_nsleep,
268 .nsleep_restart = hrtimer_nanosleep_restart,
269 .timer_create = common_timer_create,
270 .timer_set = common_timer_set,
271 .timer_get = common_timer_get,
272 .timer_del = common_timer_del,
273 };
275 posix_timers_register_clock(CLOCK_REALTIME, &clock_realtime);
276 posix_timers_register_clock(CLOCK_MONOTONIC, &clock_monotonic);
277 posix_timers_register_clock(CLOCK_MONOTONIC_RAW, &clock_monotonic_raw);
278 posix_timers_register_clock(CLOCK_REALTIME_COARSE, &clock_realtime_coarse);
279 posix_timers_register_clock(CLOCK_MONOTONIC_COARSE, &clock_monotonic_coarse);
280 posix_timers_register_clock(CLOCK_BOOTTIME, &clock_boottime);
282 posix_timers_cache = kmem_cache_create("posix_timers_cache",
283 sizeof (struct k_itimer), 0, SLAB_PANIC,
284 NULL);
285 idr_init(&posix_timers_id);
286 return 0;
287 }
289 __initcall(init_posix_timers);
291 static void schedule_next_timer(struct k_itimer *timr)
292 {
293 struct hrtimer *timer = &timr->it.real.timer;
295 if (timr->it.real.interval.tv64 == 0)
296 return;
298 timr->it_overrun += (unsigned int) hrtimer_forward(timer,
299 timer->base->get_time(),
300 timr->it.real.interval);
302 timr->it_overrun_last = timr->it_overrun;
303 timr->it_overrun = -1;
304 ++timr->it_requeue_pending;
305 hrtimer_restart(timer);
306 }
308 /*
309 * This function is exported for use by the signal deliver code. It is
310 * called just prior to the info block being released and passes that
311 * block to us. It's function is to update the overrun entry AND to
312 * restart the timer. It should only be called if the timer is to be
313 * restarted (i.e. we have flagged this in the sys_private entry of the
314 * info block).
315 *
316 * To protect against the timer going away while the interrupt is queued,
317 * we require that the it_requeue_pending flag be set.
318 */
319 void do_schedule_next_timer(struct siginfo *info)
320 {
321 struct k_itimer *timr;
322 unsigned long flags;
324 timr = lock_timer(info->si_tid, &flags);
326 if (timr && timr->it_requeue_pending == info->si_sys_private) {
327 if (timr->it_clock < 0)
328 posix_cpu_timer_schedule(timr);
329 else
330 schedule_next_timer(timr);
332 info->si_overrun += timr->it_overrun_last;
333 }
335 if (timr)
336 unlock_timer(timr, flags);
337 }
339 int posix_timer_event(struct k_itimer *timr, int si_private)
340 {
341 struct task_struct *task;
342 int shared, ret = -1;
343 /*
344 * FIXME: if ->sigq is queued we can race with
345 * dequeue_signal()->do_schedule_next_timer().
346 *
347 * If dequeue_signal() sees the "right" value of
348 * si_sys_private it calls do_schedule_next_timer().
349 * We re-queue ->sigq and drop ->it_lock().
350 * do_schedule_next_timer() locks the timer
351 * and re-schedules it while ->sigq is pending.
352 * Not really bad, but not that we want.
353 */
354 timr->sigq->info.si_sys_private = si_private;
356 rcu_read_lock();
357 task = pid_task(timr->it_pid, PIDTYPE_PID);
358 if (task) {
359 shared = !(timr->it_sigev_notify & SIGEV_THREAD_ID);
360 ret = send_sigqueue(timr->sigq, task, shared);
361 }
362 rcu_read_unlock();
363 /* If we failed to send the signal the timer stops. */
364 return ret > 0;
365 }
366 EXPORT_SYMBOL_GPL(posix_timer_event);
368 /*
369 * This function gets called when a POSIX.1b interval timer expires. It
370 * is used as a callback from the kernel internal timer. The
371 * run_timer_list code ALWAYS calls with interrupts on.
373 * This code is for CLOCK_REALTIME* and CLOCK_MONOTONIC* timers.
374 */
375 static enum hrtimer_restart posix_timer_fn(struct hrtimer *timer)
376 {
377 struct k_itimer *timr;
378 unsigned long flags;
379 int si_private = 0;
380 enum hrtimer_restart ret = HRTIMER_NORESTART;
382 timr = container_of(timer, struct k_itimer, it.real.timer);
383 spin_lock_irqsave(&timr->it_lock, flags);
385 if (timr->it.real.interval.tv64 != 0)
386 si_private = ++timr->it_requeue_pending;
388 if (posix_timer_event(timr, si_private)) {
389 /*
390 * signal was not sent because of sig_ignor
391 * we will not get a call back to restart it AND
392 * it should be restarted.
393 */
394 if (timr->it.real.interval.tv64 != 0) {
395 ktime_t now = hrtimer_cb_get_time(timer);
397 /*
398 * FIXME: What we really want, is to stop this
399 * timer completely and restart it in case the
400 * SIG_IGN is removed. This is a non trivial
401 * change which involves sighand locking
402 * (sigh !), which we don't want to do late in
403 * the release cycle.
404 *
405 * For now we just let timers with an interval
406 * less than a jiffie expire every jiffie to
407 * avoid softirq starvation in case of SIG_IGN
408 * and a very small interval, which would put
409 * the timer right back on the softirq pending
410 * list. By moving now ahead of time we trick
411 * hrtimer_forward() to expire the timer
412 * later, while we still maintain the overrun
413 * accuracy, but have some inconsistency in
414 * the timer_gettime() case. This is at least
415 * better than a starved softirq. A more
416 * complex fix which solves also another related
417 * inconsistency is already in the pipeline.
418 */
419 #ifdef CONFIG_HIGH_RES_TIMERS
420 {
421 ktime_t kj = ktime_set(0, NSEC_PER_SEC / HZ);
423 if (timr->it.real.interval.tv64 < kj.tv64)
424 now = ktime_add(now, kj);
425 }
426 #endif
427 timr->it_overrun += (unsigned int)
428 hrtimer_forward(timer, now,
429 timr->it.real.interval);
430 ret = HRTIMER_RESTART;
431 ++timr->it_requeue_pending;
432 }
433 }
435 unlock_timer(timr, flags);
436 return ret;
437 }
439 static struct pid *good_sigevent(sigevent_t * event)
440 {
441 struct task_struct *rtn = current->group_leader;
443 if ((event->sigev_notify & SIGEV_THREAD_ID ) &&
444 (!(rtn = find_task_by_vpid(event->sigev_notify_thread_id)) ||
445 !same_thread_group(rtn, current) ||
446 (event->sigev_notify & ~SIGEV_THREAD_ID) != SIGEV_SIGNAL))
447 return NULL;
449 if (((event->sigev_notify & ~SIGEV_THREAD_ID) != SIGEV_NONE) &&
450 ((event->sigev_signo <= 0) || (event->sigev_signo > SIGRTMAX)))
451 return NULL;
453 return task_pid(rtn);
454 }
456 void posix_timers_register_clock(const clockid_t clock_id,
457 struct k_clock *new_clock)
458 {
459 if ((unsigned) clock_id >= MAX_CLOCKS) {
460 printk(KERN_WARNING "POSIX clock register failed for clock_id %d\n",
461 clock_id);
462 return;
463 }
465 if (!new_clock->clock_get) {
466 printk(KERN_WARNING "POSIX clock id %d lacks clock_get()\n",
467 clock_id);
468 return;
469 }
470 if (!new_clock->clock_getres) {
471 printk(KERN_WARNING "POSIX clock id %d lacks clock_getres()\n",
472 clock_id);
473 return;
474 }
476 posix_clocks[clock_id] = *new_clock;
477 }
478 EXPORT_SYMBOL_GPL(posix_timers_register_clock);
480 static struct k_itimer * alloc_posix_timer(void)
481 {
482 struct k_itimer *tmr;
483 tmr = kmem_cache_zalloc(posix_timers_cache, GFP_KERNEL);
484 if (!tmr)
485 return tmr;
486 if (unlikely(!(tmr->sigq = sigqueue_alloc()))) {
487 kmem_cache_free(posix_timers_cache, tmr);
488 return NULL;
489 }
490 memset(&tmr->sigq->info, 0, sizeof(siginfo_t));
491 return tmr;
492 }
494 static void k_itimer_rcu_free(struct rcu_head *head)
495 {
496 struct k_itimer *tmr = container_of(head, struct k_itimer, it.rcu);
498 kmem_cache_free(posix_timers_cache, tmr);
499 }
501 #define IT_ID_SET 1
502 #define IT_ID_NOT_SET 0
503 static void release_posix_timer(struct k_itimer *tmr, int it_id_set)
504 {
505 if (it_id_set) {
506 unsigned long flags;
507 spin_lock_irqsave(&idr_lock, flags);
508 idr_remove(&posix_timers_id, tmr->it_id);
509 spin_unlock_irqrestore(&idr_lock, flags);
510 }
511 put_pid(tmr->it_pid);
512 sigqueue_free(tmr->sigq);
513 call_rcu(&tmr->it.rcu, k_itimer_rcu_free);
514 }
516 static struct k_clock *clockid_to_kclock(const clockid_t id)
517 {
518 if (id < 0)
519 return (id & CLOCKFD_MASK) == CLOCKFD ?
520 &clock_posix_dynamic : &clock_posix_cpu;
522 if (id >= MAX_CLOCKS || !posix_clocks[id].clock_getres)
523 return NULL;
524 return &posix_clocks[id];
525 }
527 static int common_timer_create(struct k_itimer *new_timer)
528 {
529 hrtimer_init(&new_timer->it.real.timer, new_timer->it_clock, 0);
530 return 0;
531 }
533 /* Create a POSIX.1b interval timer. */
535 SYSCALL_DEFINE3(timer_create, const clockid_t, which_clock,
536 struct sigevent __user *, timer_event_spec,
537 timer_t __user *, created_timer_id)
538 {
539 struct k_clock *kc = clockid_to_kclock(which_clock);
540 struct k_itimer *new_timer;
541 int error, new_timer_id;
542 sigevent_t event;
543 int it_id_set = IT_ID_NOT_SET;
545 if (!kc)
546 return -EINVAL;
547 if (!kc->timer_create)
548 return -EOPNOTSUPP;
550 new_timer = alloc_posix_timer();
551 if (unlikely(!new_timer))
552 return -EAGAIN;
554 spin_lock_init(&new_timer->it_lock);
555 retry:
556 if (unlikely(!idr_pre_get(&posix_timers_id, GFP_KERNEL))) {
557 error = -EAGAIN;
558 goto out;
559 }
560 spin_lock_irq(&idr_lock);
561 error = idr_get_new(&posix_timers_id, new_timer, &new_timer_id);
562 spin_unlock_irq(&idr_lock);
563 if (error) {
564 if (error == -EAGAIN)
565 goto retry;
566 /*
567 * Weird looking, but we return EAGAIN if the IDR is
568 * full (proper POSIX return value for this)
569 */
570 error = -EAGAIN;
571 goto out;
572 }
574 it_id_set = IT_ID_SET;
575 new_timer->it_id = (timer_t) new_timer_id;
576 new_timer->it_clock = which_clock;
577 new_timer->it_overrun = -1;
579 if (timer_event_spec) {
580 if (copy_from_user(&event, timer_event_spec, sizeof (event))) {
581 error = -EFAULT;
582 goto out;
583 }
584 rcu_read_lock();
585 new_timer->it_pid = get_pid(good_sigevent(&event));
586 rcu_read_unlock();
587 if (!new_timer->it_pid) {
588 error = -EINVAL;
589 goto out;
590 }
591 } else {
592 event.sigev_notify = SIGEV_SIGNAL;
593 event.sigev_signo = SIGALRM;
594 event.sigev_value.sival_int = new_timer->it_id;
595 new_timer->it_pid = get_pid(task_tgid(current));
596 }
598 new_timer->it_sigev_notify = event.sigev_notify;
599 new_timer->sigq->info.si_signo = event.sigev_signo;
600 new_timer->sigq->info.si_value = event.sigev_value;
601 new_timer->sigq->info.si_tid = new_timer->it_id;
602 new_timer->sigq->info.si_code = SI_TIMER;
604 if (copy_to_user(created_timer_id,
605 &new_timer_id, sizeof (new_timer_id))) {
606 error = -EFAULT;
607 goto out;
608 }
610 error = kc->timer_create(new_timer);
611 if (error)
612 goto out;
614 spin_lock_irq(¤t->sighand->siglock);
615 new_timer->it_signal = current->signal;
616 list_add(&new_timer->list, ¤t->signal->posix_timers);
617 spin_unlock_irq(¤t->sighand->siglock);
619 return 0;
620 /*
621 * In the case of the timer belonging to another task, after
622 * the task is unlocked, the timer is owned by the other task
623 * and may cease to exist at any time. Don't use or modify
624 * new_timer after the unlock call.
625 */
626 out:
627 release_posix_timer(new_timer, it_id_set);
628 return error;
629 }
631 /*
632 * Locking issues: We need to protect the result of the id look up until
633 * we get the timer locked down so it is not deleted under us. The
634 * removal is done under the idr spinlock so we use that here to bridge
635 * the find to the timer lock. To avoid a dead lock, the timer id MUST
636 * be release with out holding the timer lock.
637 */
638 static struct k_itimer *__lock_timer(timer_t timer_id, unsigned long *flags)
639 {
640 struct k_itimer *timr;
642 rcu_read_lock();
643 timr = idr_find(&posix_timers_id, (int)timer_id);
644 if (timr) {
645 spin_lock_irqsave(&timr->it_lock, *flags);
646 if (timr->it_signal == current->signal) {
647 rcu_read_unlock();
648 return timr;
649 }
650 spin_unlock_irqrestore(&timr->it_lock, *flags);
651 }
652 rcu_read_unlock();
654 return NULL;
655 }
657 /*
658 * Get the time remaining on a POSIX.1b interval timer. This function
659 * is ALWAYS called with spin_lock_irq on the timer, thus it must not
660 * mess with irq.
661 *
662 * We have a couple of messes to clean up here. First there is the case
663 * of a timer that has a requeue pending. These timers should appear to
664 * be in the timer list with an expiry as if we were to requeue them
665 * now.
666 *
667 * The second issue is the SIGEV_NONE timer which may be active but is
668 * not really ever put in the timer list (to save system resources).
669 * This timer may be expired, and if so, we will do it here. Otherwise
670 * it is the same as a requeue pending timer WRT to what we should
671 * report.
672 */
673 static void
674 common_timer_get(struct k_itimer *timr, struct itimerspec *cur_setting)
675 {
676 ktime_t now, remaining, iv;
677 struct hrtimer *timer = &timr->it.real.timer;
679 memset(cur_setting, 0, sizeof(struct itimerspec));
681 iv = timr->it.real.interval;
683 /* interval timer ? */
684 if (iv.tv64)
685 cur_setting->it_interval = ktime_to_timespec(iv);
686 else if (!hrtimer_active(timer) &&
687 (timr->it_sigev_notify & ~SIGEV_THREAD_ID) != SIGEV_NONE)
688 return;
690 now = timer->base->get_time();
692 /*
693 * When a requeue is pending or this is a SIGEV_NONE
694 * timer move the expiry time forward by intervals, so
695 * expiry is > now.
696 */
697 if (iv.tv64 && (timr->it_requeue_pending & REQUEUE_PENDING ||
698 (timr->it_sigev_notify & ~SIGEV_THREAD_ID) == SIGEV_NONE))
699 timr->it_overrun += (unsigned int) hrtimer_forward(timer, now, iv);
701 remaining = ktime_sub(hrtimer_get_expires(timer), now);
702 /* Return 0 only, when the timer is expired and not pending */
703 if (remaining.tv64 <= 0) {
704 /*
705 * A single shot SIGEV_NONE timer must return 0, when
706 * it is expired !
707 */
708 if ((timr->it_sigev_notify & ~SIGEV_THREAD_ID) != SIGEV_NONE)
709 cur_setting->it_value.tv_nsec = 1;
710 } else
711 cur_setting->it_value = ktime_to_timespec(remaining);
712 }
714 /* Get the time remaining on a POSIX.1b interval timer. */
715 SYSCALL_DEFINE2(timer_gettime, timer_t, timer_id,
716 struct itimerspec __user *, setting)
717 {
718 struct itimerspec cur_setting;
719 struct k_itimer *timr;
720 struct k_clock *kc;
721 unsigned long flags;
722 int ret = 0;
724 timr = lock_timer(timer_id, &flags);
725 if (!timr)
726 return -EINVAL;
728 kc = clockid_to_kclock(timr->it_clock);
729 if (WARN_ON_ONCE(!kc || !kc->timer_get))
730 ret = -EINVAL;
731 else
732 kc->timer_get(timr, &cur_setting);
734 unlock_timer(timr, flags);
736 if (!ret && copy_to_user(setting, &cur_setting, sizeof (cur_setting)))
737 return -EFAULT;
739 return ret;
740 }
742 /*
743 * Get the number of overruns of a POSIX.1b interval timer. This is to
744 * be the overrun of the timer last delivered. At the same time we are
745 * accumulating overruns on the next timer. The overrun is frozen when
746 * the signal is delivered, either at the notify time (if the info block
747 * is not queued) or at the actual delivery time (as we are informed by
748 * the call back to do_schedule_next_timer(). So all we need to do is
749 * to pick up the frozen overrun.
750 */
751 SYSCALL_DEFINE1(timer_getoverrun, timer_t, timer_id)
752 {
753 struct k_itimer *timr;
754 int overrun;
755 unsigned long flags;
757 timr = lock_timer(timer_id, &flags);
758 if (!timr)
759 return -EINVAL;
761 overrun = timr->it_overrun_last;
762 unlock_timer(timr, flags);
764 return overrun;
765 }
767 /* Set a POSIX.1b interval timer. */
768 /* timr->it_lock is taken. */
769 static int
770 common_timer_set(struct k_itimer *timr, int flags,
771 struct itimerspec *new_setting, struct itimerspec *old_setting)
772 {
773 struct hrtimer *timer = &timr->it.real.timer;
774 enum hrtimer_mode mode;
776 if (old_setting)
777 common_timer_get(timr, old_setting);
779 /* disable the timer */
780 timr->it.real.interval.tv64 = 0;
781 /*
782 * careful here. If smp we could be in the "fire" routine which will
783 * be spinning as we hold the lock. But this is ONLY an SMP issue.
784 */
785 if (hrtimer_try_to_cancel(timer) < 0)
786 return TIMER_RETRY;
788 timr->it_requeue_pending = (timr->it_requeue_pending + 2) &
789 ~REQUEUE_PENDING;
790 timr->it_overrun_last = 0;
792 /* switch off the timer when it_value is zero */
793 if (!new_setting->it_value.tv_sec && !new_setting->it_value.tv_nsec)
794 return 0;
796 mode = flags & TIMER_ABSTIME ? HRTIMER_MODE_ABS : HRTIMER_MODE_REL;
797 hrtimer_init(&timr->it.real.timer, timr->it_clock, mode);
798 timr->it.real.timer.function = posix_timer_fn;
800 hrtimer_set_expires(timer, timespec_to_ktime(new_setting->it_value));
802 /* Convert interval */
803 timr->it.real.interval = timespec_to_ktime(new_setting->it_interval);
805 /* SIGEV_NONE timers are not queued ! See common_timer_get */
806 if (((timr->it_sigev_notify & ~SIGEV_THREAD_ID) == SIGEV_NONE)) {
807 /* Setup correct expiry time for relative timers */
808 if (mode == HRTIMER_MODE_REL) {
809 hrtimer_add_expires(timer, timer->base->get_time());
810 }
811 return 0;
812 }
814 hrtimer_start_expires(timer, mode);
815 return 0;
816 }
818 /* Set a POSIX.1b interval timer */
819 SYSCALL_DEFINE4(timer_settime, timer_t, timer_id, int, flags,
820 const struct itimerspec __user *, new_setting,
821 struct itimerspec __user *, old_setting)
822 {
823 struct k_itimer *timr;
824 struct itimerspec new_spec, old_spec;
825 int error = 0;
826 unsigned long flag;
827 struct itimerspec *rtn = old_setting ? &old_spec : NULL;
828 struct k_clock *kc;
830 if (!new_setting)
831 return -EINVAL;
833 if (copy_from_user(&new_spec, new_setting, sizeof (new_spec)))
834 return -EFAULT;
836 if (!timespec_valid(&new_spec.it_interval) ||
837 !timespec_valid(&new_spec.it_value))
838 return -EINVAL;
839 retry:
840 timr = lock_timer(timer_id, &flag);
841 if (!timr)
842 return -EINVAL;
844 kc = clockid_to_kclock(timr->it_clock);
845 if (WARN_ON_ONCE(!kc || !kc->timer_set))
846 error = -EINVAL;
847 else
848 error = kc->timer_set(timr, flags, &new_spec, rtn);
850 unlock_timer(timr, flag);
851 if (error == TIMER_RETRY) {
852 rtn = NULL; // We already got the old time...
853 goto retry;
854 }
856 if (old_setting && !error &&
857 copy_to_user(old_setting, &old_spec, sizeof (old_spec)))
858 error = -EFAULT;
860 return error;
861 }
863 static int common_timer_del(struct k_itimer *timer)
864 {
865 timer->it.real.interval.tv64 = 0;
867 if (hrtimer_try_to_cancel(&timer->it.real.timer) < 0)
868 return TIMER_RETRY;
869 return 0;
870 }
872 static inline int timer_delete_hook(struct k_itimer *timer)
873 {
874 struct k_clock *kc = clockid_to_kclock(timer->it_clock);
876 if (WARN_ON_ONCE(!kc || !kc->timer_del))
877 return -EINVAL;
878 return kc->timer_del(timer);
879 }
881 /* Delete a POSIX.1b interval timer. */
882 SYSCALL_DEFINE1(timer_delete, timer_t, timer_id)
883 {
884 struct k_itimer *timer;
885 unsigned long flags;
887 retry_delete:
888 timer = lock_timer(timer_id, &flags);
889 if (!timer)
890 return -EINVAL;
892 if (timer_delete_hook(timer) == TIMER_RETRY) {
893 unlock_timer(timer, flags);
894 goto retry_delete;
895 }
897 spin_lock(¤t->sighand->siglock);
898 list_del(&timer->list);
899 spin_unlock(¤t->sighand->siglock);
900 /*
901 * This keeps any tasks waiting on the spin lock from thinking
902 * they got something (see the lock code above).
903 */
904 timer->it_signal = NULL;
906 unlock_timer(timer, flags);
907 release_posix_timer(timer, IT_ID_SET);
908 return 0;
909 }
911 /*
912 * return timer owned by the process, used by exit_itimers
913 */
914 static void itimer_delete(struct k_itimer *timer)
915 {
916 unsigned long flags;
918 retry_delete:
919 spin_lock_irqsave(&timer->it_lock, flags);
921 if (timer_delete_hook(timer) == TIMER_RETRY) {
922 unlock_timer(timer, flags);
923 goto retry_delete;
924 }
925 list_del(&timer->list);
926 /*
927 * This keeps any tasks waiting on the spin lock from thinking
928 * they got something (see the lock code above).
929 */
930 timer->it_signal = NULL;
932 unlock_timer(timer, flags);
933 release_posix_timer(timer, IT_ID_SET);
934 }
936 /*
937 * This is called by do_exit or de_thread, only when there are no more
938 * references to the shared signal_struct.
939 */
940 void exit_itimers(struct signal_struct *sig)
941 {
942 struct k_itimer *tmr;
944 while (!list_empty(&sig->posix_timers)) {
945 tmr = list_entry(sig->posix_timers.next, struct k_itimer, list);
946 itimer_delete(tmr);
947 }
948 }
950 SYSCALL_DEFINE2(clock_settime, const clockid_t, which_clock,
951 const struct timespec __user *, tp)
952 {
953 struct k_clock *kc = clockid_to_kclock(which_clock);
954 struct timespec new_tp;
956 if (!kc || !kc->clock_set)
957 return -EINVAL;
959 if (copy_from_user(&new_tp, tp, sizeof (*tp)))
960 return -EFAULT;
962 return kc->clock_set(which_clock, &new_tp);
963 }
965 SYSCALL_DEFINE2(clock_gettime, const clockid_t, which_clock,
966 struct timespec __user *,tp)
967 {
968 struct k_clock *kc = clockid_to_kclock(which_clock);
969 struct timespec kernel_tp;
970 int error;
972 if (!kc)
973 return -EINVAL;
975 error = kc->clock_get(which_clock, &kernel_tp);
977 if (!error && copy_to_user(tp, &kernel_tp, sizeof (kernel_tp)))
978 error = -EFAULT;
980 return error;
981 }
983 SYSCALL_DEFINE2(clock_adjtime, const clockid_t, which_clock,
984 struct timex __user *, utx)
985 {
986 struct k_clock *kc = clockid_to_kclock(which_clock);
987 struct timex ktx;
988 int err;
990 if (!kc)
991 return -EINVAL;
992 if (!kc->clock_adj)
993 return -EOPNOTSUPP;
995 if (copy_from_user(&ktx, utx, sizeof(ktx)))
996 return -EFAULT;
998 err = kc->clock_adj(which_clock, &ktx);
1000 if (!err && copy_to_user(utx, &ktx, sizeof(ktx)))
1001 return -EFAULT;
1003 return err;
1004 }
1006 SYSCALL_DEFINE2(clock_getres, const clockid_t, which_clock,
1007 struct timespec __user *, tp)
1008 {
1009 struct k_clock *kc = clockid_to_kclock(which_clock);
1010 struct timespec rtn_tp;
1011 int error;
1013 if (!kc)
1014 return -EINVAL;
1016 error = kc->clock_getres(which_clock, &rtn_tp);
1018 if (!error && tp && copy_to_user(tp, &rtn_tp, sizeof (rtn_tp)))
1019 error = -EFAULT;
1021 return error;
1022 }
1024 /*
1025 * nanosleep for monotonic and realtime clocks
1026 */
1027 static int common_nsleep(const clockid_t which_clock, int flags,
1028 struct timespec *tsave, struct timespec __user *rmtp)
1029 {
1030 return hrtimer_nanosleep(tsave, rmtp, flags & TIMER_ABSTIME ?
1031 HRTIMER_MODE_ABS : HRTIMER_MODE_REL,
1032 which_clock);
1033 }
1035 SYSCALL_DEFINE4(clock_nanosleep, const clockid_t, which_clock, int, flags,
1036 const struct timespec __user *, rqtp,
1037 struct timespec __user *, rmtp)
1038 {
1039 struct k_clock *kc = clockid_to_kclock(which_clock);
1040 struct timespec t;
1042 if (!kc)
1043 return -EINVAL;
1044 if (!kc->nsleep)
1045 return -ENANOSLEEP_NOTSUP;
1047 if (copy_from_user(&t, rqtp, sizeof (struct timespec)))
1048 return -EFAULT;
1050 if (!timespec_valid(&t))
1051 return -EINVAL;
1053 return kc->nsleep(which_clock, flags, &t, rmtp);
1054 }
1056 /*
1057 * This will restart clock_nanosleep. This is required only by
1058 * compat_clock_nanosleep_restart for now.
1059 */
1060 long clock_nanosleep_restart(struct restart_block *restart_block)
1061 {
1062 clockid_t which_clock = restart_block->nanosleep.clockid;
1063 struct k_clock *kc = clockid_to_kclock(which_clock);
1065 if (WARN_ON_ONCE(!kc || !kc->nsleep_restart))
1066 return -EINVAL;
1068 return kc->nsleep_restart(restart_block);
1069 }