1 /*
2 * Read-Copy Update mechanism for mutual exclusion, the Bloatwatch edition.
3 *
4 * This program is free software; you can redistribute it and/or modify
5 * it under the terms of the GNU General Public License as published by
6 * the Free Software Foundation; either version 2 of the License, or
7 * (at your option) any later version.
8 *
9 * This program is distributed in the hope that it will be useful,
10 * but WITHOUT ANY WARRANTY; without even the implied warranty of
11 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
12 * GNU General Public License for more details.
13 *
14 * You should have received a copy of the GNU General Public License
15 * along with this program; if not, write to the Free Software
16 * Foundation, Inc., 59 Temple Place - Suite 330, Boston, MA 02111-1307, USA.
17 *
18 * Copyright IBM Corporation, 2008
19 *
20 * Author: Paul E. McKenney <paulmck@linux.vnet.ibm.com>
21 *
22 * For detailed explanation of Read-Copy Update mechanism see -
23 * Documentation/RCU
24 */
25 #include <linux/completion.h>
26 #include <linux/interrupt.h>
27 #include <linux/notifier.h>
28 #include <linux/rcupdate.h>
29 #include <linux/kernel.h>
30 #include <linux/export.h>
31 #include <linux/mutex.h>
32 #include <linux/sched.h>
33 #include <linux/types.h>
34 #include <linux/init.h>
35 #include <linux/time.h>
36 #include <linux/cpu.h>
37 #include <linux/prefetch.h>
39 #ifdef CONFIG_RCU_TRACE
40 #include <trace/events/rcu.h>
41 #endif /* #else #ifdef CONFIG_RCU_TRACE */
43 #include "rcu.h"
45 /* Forward declarations for rcutiny_plugin.h. */
46 struct rcu_ctrlblk;
47 static void invoke_rcu_callbacks(void);
48 static void __rcu_process_callbacks(struct rcu_ctrlblk *rcp);
49 static void rcu_process_callbacks(struct softirq_action *unused);
50 static void __call_rcu(struct rcu_head *head,
51 void (*func)(struct rcu_head *rcu),
52 struct rcu_ctrlblk *rcp);
54 #include "rcutiny_plugin.h"
56 #ifdef CONFIG_NO_HZ
58 static long rcu_dynticks_nesting = 1;
60 /*
61 * Enter dynticks-idle mode, which is an extended quiescent state
62 * if we have fully entered that mode (i.e., if the new value of
63 * dynticks_nesting is zero).
64 */
65 void rcu_enter_nohz(void)
66 {
67 if (--rcu_dynticks_nesting == 0)
68 rcu_sched_qs(0); /* implies rcu_bh_qsctr_inc(0) */
69 }
71 /*
72 * Exit dynticks-idle mode, so that we are no longer in an extended
73 * quiescent state.
74 */
75 void rcu_exit_nohz(void)
76 {
77 rcu_dynticks_nesting++;
78 }
80 #endif /* #ifdef CONFIG_NO_HZ */
82 /*
83 * Helper function for rcu_sched_qs() and rcu_bh_qs().
84 * Also irqs are disabled to avoid confusion due to interrupt handlers
85 * invoking call_rcu().
86 */
87 static int rcu_qsctr_help(struct rcu_ctrlblk *rcp)
88 {
89 if (rcp->rcucblist != NULL &&
90 rcp->donetail != rcp->curtail) {
91 rcp->donetail = rcp->curtail;
92 return 1;
93 }
95 return 0;
96 }
98 /*
99 * Record an rcu quiescent state. And an rcu_bh quiescent state while we
100 * are at it, given that any rcu quiescent state is also an rcu_bh
101 * quiescent state. Use "+" instead of "||" to defeat short circuiting.
102 */
103 void rcu_sched_qs(int cpu)
104 {
105 unsigned long flags;
107 local_irq_save(flags);
108 if (rcu_qsctr_help(&rcu_sched_ctrlblk) +
109 rcu_qsctr_help(&rcu_bh_ctrlblk))
110 invoke_rcu_callbacks();
111 local_irq_restore(flags);
112 }
114 /*
115 * Record an rcu_bh quiescent state.
116 */
117 void rcu_bh_qs(int cpu)
118 {
119 unsigned long flags;
121 local_irq_save(flags);
122 if (rcu_qsctr_help(&rcu_bh_ctrlblk))
123 invoke_rcu_callbacks();
124 local_irq_restore(flags);
125 }
127 /*
128 * Check to see if the scheduling-clock interrupt came from an extended
129 * quiescent state, and, if so, tell RCU about it.
130 */
131 void rcu_check_callbacks(int cpu, int user)
132 {
133 if (user ||
134 (idle_cpu(cpu) &&
135 !in_softirq() &&
136 hardirq_count() <= (1 << HARDIRQ_SHIFT)))
137 rcu_sched_qs(cpu);
138 else if (!in_softirq())
139 rcu_bh_qs(cpu);
140 rcu_preempt_check_callbacks();
141 }
143 /*
144 * Invoke the RCU callbacks on the specified rcu_ctrlkblk structure
145 * whose grace period has elapsed.
146 */
147 static void __rcu_process_callbacks(struct rcu_ctrlblk *rcp)
148 {
149 char *rn = NULL;
150 struct rcu_head *next, *list;
151 unsigned long flags;
152 RCU_TRACE(int cb_count = 0);
154 /* If no RCU callbacks ready to invoke, just return. */
155 if (&rcp->rcucblist == rcp->donetail) {
156 RCU_TRACE(trace_rcu_batch_start(rcp->name, 0, -1));
157 RCU_TRACE(trace_rcu_batch_end(rcp->name, 0));
158 return;
159 }
161 /* Move the ready-to-invoke callbacks to a local list. */
162 local_irq_save(flags);
163 RCU_TRACE(trace_rcu_batch_start(rcp->name, 0, -1));
164 list = rcp->rcucblist;
165 rcp->rcucblist = *rcp->donetail;
166 *rcp->donetail = NULL;
167 if (rcp->curtail == rcp->donetail)
168 rcp->curtail = &rcp->rcucblist;
169 rcu_preempt_remove_callbacks(rcp);
170 rcp->donetail = &rcp->rcucblist;
171 local_irq_restore(flags);
173 /* Invoke the callbacks on the local list. */
174 RCU_TRACE(rn = rcp->name);
175 while (list) {
176 next = list->next;
177 prefetch(next);
178 debug_rcu_head_unqueue(list);
179 local_bh_disable();
180 __rcu_reclaim(rn, list);
181 local_bh_enable();
182 list = next;
183 RCU_TRACE(cb_count++);
184 }
185 RCU_TRACE(rcu_trace_sub_qlen(rcp, cb_count));
186 RCU_TRACE(trace_rcu_batch_end(rcp->name, cb_count));
187 }
189 static void rcu_process_callbacks(struct softirq_action *unused)
190 {
191 __rcu_process_callbacks(&rcu_sched_ctrlblk);
192 __rcu_process_callbacks(&rcu_bh_ctrlblk);
193 rcu_preempt_process_callbacks();
194 }
196 /*
197 * Wait for a grace period to elapse. But it is illegal to invoke
198 * synchronize_sched() from within an RCU read-side critical section.
199 * Therefore, any legal call to synchronize_sched() is a quiescent
200 * state, and so on a UP system, synchronize_sched() need do nothing.
201 * Ditto for synchronize_rcu_bh(). (But Lai Jiangshan points out the
202 * benefits of doing might_sleep() to reduce latency.)
203 *
204 * Cool, huh? (Due to Josh Triplett.)
205 *
206 * But we want to make this a static inline later. The cond_resched()
207 * currently makes this problematic.
208 */
209 void synchronize_sched(void)
210 {
211 cond_resched();
212 }
213 EXPORT_SYMBOL_GPL(synchronize_sched);
215 /*
216 * Helper function for call_rcu() and call_rcu_bh().
217 */
218 static void __call_rcu(struct rcu_head *head,
219 void (*func)(struct rcu_head *rcu),
220 struct rcu_ctrlblk *rcp)
221 {
222 unsigned long flags;
224 debug_rcu_head_queue(head);
225 head->func = func;
226 head->next = NULL;
228 local_irq_save(flags);
229 *rcp->curtail = head;
230 rcp->curtail = &head->next;
231 RCU_TRACE(rcp->qlen++);
232 local_irq_restore(flags);
233 }
235 /*
236 * Post an RCU callback to be invoked after the end of an RCU-sched grace
237 * period. But since we have but one CPU, that would be after any
238 * quiescent state.
239 */
240 void call_rcu_sched(struct rcu_head *head, void (*func)(struct rcu_head *rcu))
241 {
242 __call_rcu(head, func, &rcu_sched_ctrlblk);
243 }
244 EXPORT_SYMBOL_GPL(call_rcu_sched);
246 /*
247 * Post an RCU bottom-half callback to be invoked after any subsequent
248 * quiescent state.
249 */
250 void call_rcu_bh(struct rcu_head *head, void (*func)(struct rcu_head *rcu))
251 {
252 __call_rcu(head, func, &rcu_bh_ctrlblk);
253 }
254 EXPORT_SYMBOL_GPL(call_rcu_bh);