]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - kernel/sched_autogroup.c
video: da8xx-fb: correct suspend/resume sequence
[sitara-epos/sitara-epos-kernel.git] / kernel / sched_autogroup.c
1 #ifdef CONFIG_SCHED_AUTOGROUP
3 #include <linux/proc_fs.h>
4 #include <linux/seq_file.h>
5 #include <linux/kallsyms.h>
6 #include <linux/utsname.h>
8 unsigned int __read_mostly sysctl_sched_autogroup_enabled = 1;
9 static struct autogroup autogroup_default;
10 static atomic_t autogroup_seq_nr;
12 static void __init autogroup_init(struct task_struct *init_task)
13 {
14         autogroup_default.tg = &root_task_group;
15         kref_init(&autogroup_default.kref);
16         init_rwsem(&autogroup_default.lock);
17         init_task->signal->autogroup = &autogroup_default;
18 }
20 static inline void autogroup_free(struct task_group *tg)
21 {
22         kfree(tg->autogroup);
23 }
25 static inline void autogroup_destroy(struct kref *kref)
26 {
27         struct autogroup *ag = container_of(kref, struct autogroup, kref);
29 #ifdef CONFIG_RT_GROUP_SCHED
30         /* We've redirected RT tasks to the root task group... */
31         ag->tg->rt_se = NULL;
32         ag->tg->rt_rq = NULL;
33 #endif
34         sched_destroy_group(ag->tg);
35 }
37 static inline void autogroup_kref_put(struct autogroup *ag)
38 {
39         kref_put(&ag->kref, autogroup_destroy);
40 }
42 static inline struct autogroup *autogroup_kref_get(struct autogroup *ag)
43 {
44         kref_get(&ag->kref);
45         return ag;
46 }
48 static inline struct autogroup *autogroup_task_get(struct task_struct *p)
49 {
50         struct autogroup *ag;
51         unsigned long flags;
53         if (!lock_task_sighand(p, &flags))
54                 return autogroup_kref_get(&autogroup_default);
56         ag = autogroup_kref_get(p->signal->autogroup);
57         unlock_task_sighand(p, &flags);
59         return ag;
60 }
62 #ifdef CONFIG_RT_GROUP_SCHED
63 static void free_rt_sched_group(struct task_group *tg);
64 #endif
66 static inline struct autogroup *autogroup_create(void)
67 {
68         struct autogroup *ag = kzalloc(sizeof(*ag), GFP_KERNEL);
69         struct task_group *tg;
71         if (!ag)
72                 goto out_fail;
74         tg = sched_create_group(&root_task_group);
76         if (IS_ERR(tg))
77                 goto out_free;
79         kref_init(&ag->kref);
80         init_rwsem(&ag->lock);
81         ag->id = atomic_inc_return(&autogroup_seq_nr);
82         ag->tg = tg;
83 #ifdef CONFIG_RT_GROUP_SCHED
84         /*
85          * Autogroup RT tasks are redirected to the root task group
86          * so we don't have to move tasks around upon policy change,
87          * or flail around trying to allocate bandwidth on the fly.
88          * A bandwidth exception in __sched_setscheduler() allows
89          * the policy change to proceed.  Thereafter, task_group()
90          * returns &root_task_group, so zero bandwidth is required.
91          */
92         free_rt_sched_group(tg);
93         tg->rt_se = root_task_group.rt_se;
94         tg->rt_rq = root_task_group.rt_rq;
95 #endif
96         tg->autogroup = ag;
98         return ag;
100 out_free:
101         kfree(ag);
102 out_fail:
103         if (printk_ratelimit()) {
104                 printk(KERN_WARNING "autogroup_create: %s failure.\n",
105                         ag ? "sched_create_group()" : "kmalloc()");
106         }
108         return autogroup_kref_get(&autogroup_default);
111 static inline bool
112 task_wants_autogroup(struct task_struct *p, struct task_group *tg)
114         if (tg != &root_task_group)
115                 return false;
117         if (p->sched_class != &fair_sched_class)
118                 return false;
120         /*
121          * We can only assume the task group can't go away on us if
122          * autogroup_move_group() can see us on ->thread_group list.
123          */
124         if (p->flags & PF_EXITING)
125                 return false;
127         return true;
130 static inline bool task_group_is_autogroup(struct task_group *tg)
132         return !!tg->autogroup;
135 static inline struct task_group *
136 autogroup_task_group(struct task_struct *p, struct task_group *tg)
138         int enabled = ACCESS_ONCE(sysctl_sched_autogroup_enabled);
140         if (enabled && task_wants_autogroup(p, tg))
141                 return p->signal->autogroup->tg;
143         return tg;
146 static void
147 autogroup_move_group(struct task_struct *p, struct autogroup *ag)
149         struct autogroup *prev;
150         struct task_struct *t;
151         unsigned long flags;
153         BUG_ON(!lock_task_sighand(p, &flags));
155         prev = p->signal->autogroup;
156         if (prev == ag) {
157                 unlock_task_sighand(p, &flags);
158                 return;
159         }
161         p->signal->autogroup = autogroup_kref_get(ag);
163         if (!ACCESS_ONCE(sysctl_sched_autogroup_enabled))
164                 goto out;
166         t = p;
167         do {
168                 sched_move_task(t);
169         } while_each_thread(p, t);
171 out:
172         unlock_task_sighand(p, &flags);
173         autogroup_kref_put(prev);
176 /* Allocates GFP_KERNEL, cannot be called under any spinlock */
177 void sched_autogroup_create_attach(struct task_struct *p)
179         struct autogroup *ag = autogroup_create();
181         autogroup_move_group(p, ag);
182         /* drop extra reference added by autogroup_create() */
183         autogroup_kref_put(ag);
185 EXPORT_SYMBOL(sched_autogroup_create_attach);
187 /* Cannot be called under siglock.  Currently has no users */
188 void sched_autogroup_detach(struct task_struct *p)
190         autogroup_move_group(p, &autogroup_default);
192 EXPORT_SYMBOL(sched_autogroup_detach);
194 void sched_autogroup_fork(struct signal_struct *sig)
196         sig->autogroup = autogroup_task_get(current);
199 void sched_autogroup_exit(struct signal_struct *sig)
201         autogroup_kref_put(sig->autogroup);
204 static int __init setup_autogroup(char *str)
206         sysctl_sched_autogroup_enabled = 0;
208         return 1;
211 __setup("noautogroup", setup_autogroup);
213 #ifdef CONFIG_PROC_FS
215 int proc_sched_autogroup_set_nice(struct task_struct *p, int *nice)
217         static unsigned long next = INITIAL_JIFFIES;
218         struct autogroup *ag;
219         int err;
221         if (*nice < -20 || *nice > 19)
222                 return -EINVAL;
224         err = security_task_setnice(current, *nice);
225         if (err)
226                 return err;
228         if (*nice < 0 && !can_nice(current, *nice))
229                 return -EPERM;
231         /* this is a heavy operation taking global locks.. */
232         if (!capable(CAP_SYS_ADMIN) && time_before(jiffies, next))
233                 return -EAGAIN;
235         next = HZ / 10 + jiffies;
236         ag = autogroup_task_get(p);
238         down_write(&ag->lock);
239         err = sched_group_set_shares(ag->tg, prio_to_weight[*nice + 20]);
240         if (!err)
241                 ag->nice = *nice;
242         up_write(&ag->lock);
244         autogroup_kref_put(ag);
246         return err;
249 void proc_sched_autogroup_show_task(struct task_struct *p, struct seq_file *m)
251         struct autogroup *ag = autogroup_task_get(p);
253         if (!task_group_is_autogroup(ag->tg))
254                 goto out;
256         down_read(&ag->lock);
257         seq_printf(m, "/autogroup-%ld nice %d\n", ag->id, ag->nice);
258         up_read(&ag->lock);
260 out:
261         autogroup_kref_put(ag);
263 #endif /* CONFIG_PROC_FS */
265 #ifdef CONFIG_SCHED_DEBUG
266 static inline int autogroup_path(struct task_group *tg, char *buf, int buflen)
268         if (!task_group_is_autogroup(tg))
269                 return 0;
271         return snprintf(buf, buflen, "%s-%ld", "/autogroup", tg->autogroup->id);
273 #endif /* CONFIG_SCHED_DEBUG */
275 #endif /* CONFIG_SCHED_AUTOGROUP */