1 /*
2 * lib/btree.c - Simple In-memory B+Tree
3 *
4 * As should be obvious for Linux kernel code, license is GPLv2
5 *
6 * Copyright (c) 2007-2008 Joern Engel <joern@logfs.org>
7 * Bits and pieces stolen from Peter Zijlstra's code, which is
8 * Copyright 2007, Red Hat Inc. Peter Zijlstra <pzijlstr@redhat.com>
9 * GPLv2
10 *
11 * see http://programming.kicks-ass.net/kernel-patches/vma_lookup/btree.patch
12 *
13 * A relatively simple B+Tree implementation. I have written it as a learning
14 * exercise to understand how B+Trees work. Turned out to be useful as well.
15 *
16 * B+Trees can be used similar to Linux radix trees (which don't have anything
17 * in common with textbook radix trees, beware). Prerequisite for them working
18 * well is that access to a random tree node is much faster than a large number
19 * of operations within each node.
20 *
21 * Disks have fulfilled the prerequisite for a long time. More recently DRAM
22 * has gained similar properties, as memory access times, when measured in cpu
23 * cycles, have increased. Cacheline sizes have increased as well, which also
24 * helps B+Trees.
25 *
26 * Compared to radix trees, B+Trees are more efficient when dealing with a
27 * sparsely populated address space. Between 25% and 50% of the memory is
28 * occupied with valid pointers. When densely populated, radix trees contain
29 * ~98% pointers - hard to beat. Very sparse radix trees contain only ~2%
30 * pointers.
31 *
32 * This particular implementation stores pointers identified by a long value.
33 * Storing NULL pointers is illegal, lookup will return NULL when no entry
34 * was found.
35 *
36 * A tricks was used that is not commonly found in textbooks. The lowest
37 * values are to the right, not to the left. All used slots within a node
38 * are on the left, all unused slots contain NUL values. Most operations
39 * simply loop once over all slots and terminate on the first NUL.
40 */
42 #include <linux/btree.h>
43 #include <linux/cache.h>
44 #include <linux/kernel.h>
45 #include <linux/slab.h>
46 #include <linux/module.h>
48 #define MAX(a, b) ((a) > (b) ? (a) : (b))
49 #define NODESIZE MAX(L1_CACHE_BYTES, 128)
51 struct btree_geo {
52 int keylen;
53 int no_pairs;
54 int no_longs;
55 };
57 struct btree_geo btree_geo32 = {
58 .keylen = 1,
59 .no_pairs = NODESIZE / sizeof(long) / 2,
60 .no_longs = NODESIZE / sizeof(long) / 2,
61 };
62 EXPORT_SYMBOL_GPL(btree_geo32);
64 #define LONG_PER_U64 (64 / BITS_PER_LONG)
65 struct btree_geo btree_geo64 = {
66 .keylen = LONG_PER_U64,
67 .no_pairs = NODESIZE / sizeof(long) / (1 + LONG_PER_U64),
68 .no_longs = LONG_PER_U64 * (NODESIZE / sizeof(long) / (1 + LONG_PER_U64)),
69 };
70 EXPORT_SYMBOL_GPL(btree_geo64);
72 struct btree_geo btree_geo128 = {
73 .keylen = 2 * LONG_PER_U64,
74 .no_pairs = NODESIZE / sizeof(long) / (1 + 2 * LONG_PER_U64),
75 .no_longs = 2 * LONG_PER_U64 * (NODESIZE / sizeof(long) / (1 + 2 * LONG_PER_U64)),
76 };
77 EXPORT_SYMBOL_GPL(btree_geo128);
79 static struct kmem_cache *btree_cachep;
81 void *btree_alloc(gfp_t gfp_mask, void *pool_data)
82 {
83 return kmem_cache_alloc(btree_cachep, gfp_mask);
84 }
85 EXPORT_SYMBOL_GPL(btree_alloc);
87 void btree_free(void *element, void *pool_data)
88 {
89 kmem_cache_free(btree_cachep, element);
90 }
91 EXPORT_SYMBOL_GPL(btree_free);
93 static unsigned long *btree_node_alloc(struct btree_head *head, gfp_t gfp)
94 {
95 unsigned long *node;
97 node = mempool_alloc(head->mempool, gfp);
98 if (likely(node))
99 memset(node, 0, NODESIZE);
100 return node;
101 }
103 static int longcmp(const unsigned long *l1, const unsigned long *l2, size_t n)
104 {
105 size_t i;
107 for (i = 0; i < n; i++) {
108 if (l1[i] < l2[i])
109 return -1;
110 if (l1[i] > l2[i])
111 return 1;
112 }
113 return 0;
114 }
116 static unsigned long *longcpy(unsigned long *dest, const unsigned long *src,
117 size_t n)
118 {
119 size_t i;
121 for (i = 0; i < n; i++)
122 dest[i] = src[i];
123 return dest;
124 }
126 static unsigned long *longset(unsigned long *s, unsigned long c, size_t n)
127 {
128 size_t i;
130 for (i = 0; i < n; i++)
131 s[i] = c;
132 return s;
133 }
135 static void dec_key(struct btree_geo *geo, unsigned long *key)
136 {
137 unsigned long val;
138 int i;
140 for (i = geo->keylen - 1; i >= 0; i--) {
141 val = key[i];
142 key[i] = val - 1;
143 if (val)
144 break;
145 }
146 }
148 static unsigned long *bkey(struct btree_geo *geo, unsigned long *node, int n)
149 {
150 return &node[n * geo->keylen];
151 }
153 static void *bval(struct btree_geo *geo, unsigned long *node, int n)
154 {
155 return (void *)node[geo->no_longs + n];
156 }
158 static void setkey(struct btree_geo *geo, unsigned long *node, int n,
159 unsigned long *key)
160 {
161 longcpy(bkey(geo, node, n), key, geo->keylen);
162 }
164 static void setval(struct btree_geo *geo, unsigned long *node, int n,
165 void *val)
166 {
167 node[geo->no_longs + n] = (unsigned long) val;
168 }
170 static void clearpair(struct btree_geo *geo, unsigned long *node, int n)
171 {
172 longset(bkey(geo, node, n), 0, geo->keylen);
173 node[geo->no_longs + n] = 0;
174 }
176 static inline void __btree_init(struct btree_head *head)
177 {
178 head->node = NULL;
179 head->height = 0;
180 }
182 void btree_init_mempool(struct btree_head *head, mempool_t *mempool)
183 {
184 __btree_init(head);
185 head->mempool = mempool;
186 }
187 EXPORT_SYMBOL_GPL(btree_init_mempool);
189 int btree_init(struct btree_head *head)
190 {
191 __btree_init(head);
192 head->mempool = mempool_create(0, btree_alloc, btree_free, NULL);
193 if (!head->mempool)
194 return -ENOMEM;
195 return 0;
196 }
197 EXPORT_SYMBOL_GPL(btree_init);
199 void btree_destroy(struct btree_head *head)
200 {
201 mempool_destroy(head->mempool);
202 head->mempool = NULL;
203 }
204 EXPORT_SYMBOL_GPL(btree_destroy);
206 void *btree_last(struct btree_head *head, struct btree_geo *geo,
207 unsigned long *key)
208 {
209 int height = head->height;
210 unsigned long *node = head->node;
212 if (height == 0)
213 return NULL;
215 for ( ; height > 1; height--)
216 node = bval(geo, node, 0);
218 longcpy(key, bkey(geo, node, 0), geo->keylen);
219 return bval(geo, node, 0);
220 }
221 EXPORT_SYMBOL_GPL(btree_last);
223 static int keycmp(struct btree_geo *geo, unsigned long *node, int pos,
224 unsigned long *key)
225 {
226 return longcmp(bkey(geo, node, pos), key, geo->keylen);
227 }
229 static int keyzero(struct btree_geo *geo, unsigned long *key)
230 {
231 int i;
233 for (i = 0; i < geo->keylen; i++)
234 if (key[i])
235 return 0;
237 return 1;
238 }
240 void *btree_lookup(struct btree_head *head, struct btree_geo *geo,
241 unsigned long *key)
242 {
243 int i, height = head->height;
244 unsigned long *node = head->node;
246 if (height == 0)
247 return NULL;
249 for ( ; height > 1; height--) {
250 for (i = 0; i < geo->no_pairs; i++)
251 if (keycmp(geo, node, i, key) <= 0)
252 break;
253 if (i == geo->no_pairs)
254 return NULL;
255 node = bval(geo, node, i);
256 if (!node)
257 return NULL;
258 }
260 if (!node)
261 return NULL;
263 for (i = 0; i < geo->no_pairs; i++)
264 if (keycmp(geo, node, i, key) == 0)
265 return bval(geo, node, i);
266 return NULL;
267 }
268 EXPORT_SYMBOL_GPL(btree_lookup);
270 int btree_update(struct btree_head *head, struct btree_geo *geo,
271 unsigned long *key, void *val)
272 {
273 int i, height = head->height;
274 unsigned long *node = head->node;
276 if (height == 0)
277 return -ENOENT;
279 for ( ; height > 1; height--) {
280 for (i = 0; i < geo->no_pairs; i++)
281 if (keycmp(geo, node, i, key) <= 0)
282 break;
283 if (i == geo->no_pairs)
284 return -ENOENT;
285 node = bval(geo, node, i);
286 if (!node)
287 return -ENOENT;
288 }
290 if (!node)
291 return -ENOENT;
293 for (i = 0; i < geo->no_pairs; i++)
294 if (keycmp(geo, node, i, key) == 0) {
295 setval(geo, node, i, val);
296 return 0;
297 }
298 return -ENOENT;
299 }
300 EXPORT_SYMBOL_GPL(btree_update);
302 /*
303 * Usually this function is quite similar to normal lookup. But the key of
304 * a parent node may be smaller than the smallest key of all its siblings.
305 * In such a case we cannot just return NULL, as we have only proven that no
306 * key smaller than __key, but larger than this parent key exists.
307 * So we set __key to the parent key and retry. We have to use the smallest
308 * such parent key, which is the last parent key we encountered.
309 */
310 void *btree_get_prev(struct btree_head *head, struct btree_geo *geo,
311 unsigned long *__key)
312 {
313 int i, height;
314 unsigned long *node, *oldnode;
315 unsigned long *retry_key = NULL, key[geo->keylen];
317 if (keyzero(geo, __key))
318 return NULL;
320 if (head->height == 0)
321 return NULL;
322 retry:
323 longcpy(key, __key, geo->keylen);
324 dec_key(geo, key);
326 node = head->node;
327 for (height = head->height ; height > 1; height--) {
328 for (i = 0; i < geo->no_pairs; i++)
329 if (keycmp(geo, node, i, key) <= 0)
330 break;
331 if (i == geo->no_pairs)
332 goto miss;
333 oldnode = node;
334 node = bval(geo, node, i);
335 if (!node)
336 goto miss;
337 retry_key = bkey(geo, oldnode, i);
338 }
340 if (!node)
341 goto miss;
343 for (i = 0; i < geo->no_pairs; i++) {
344 if (keycmp(geo, node, i, key) <= 0) {
345 if (bval(geo, node, i)) {
346 longcpy(__key, bkey(geo, node, i), geo->keylen);
347 return bval(geo, node, i);
348 } else
349 goto miss;
350 }
351 }
352 miss:
353 if (retry_key) {
354 __key = retry_key;
355 retry_key = NULL;
356 goto retry;
357 }
358 return NULL;
359 }
361 static int getpos(struct btree_geo *geo, unsigned long *node,
362 unsigned long *key)
363 {
364 int i;
366 for (i = 0; i < geo->no_pairs; i++) {
367 if (keycmp(geo, node, i, key) <= 0)
368 break;
369 }
370 return i;
371 }
373 static int getfill(struct btree_geo *geo, unsigned long *node, int start)
374 {
375 int i;
377 for (i = start; i < geo->no_pairs; i++)
378 if (!bval(geo, node, i))
379 break;
380 return i;
381 }
383 /*
384 * locate the correct leaf node in the btree
385 */
386 static unsigned long *find_level(struct btree_head *head, struct btree_geo *geo,
387 unsigned long *key, int level)
388 {
389 unsigned long *node = head->node;
390 int i, height;
392 for (height = head->height; height > level; height--) {
393 for (i = 0; i < geo->no_pairs; i++)
394 if (keycmp(geo, node, i, key) <= 0)
395 break;
397 if ((i == geo->no_pairs) || !bval(geo, node, i)) {
398 /* right-most key is too large, update it */
399 /* FIXME: If the right-most key on higher levels is
400 * always zero, this wouldn't be necessary. */
401 i--;
402 setkey(geo, node, i, key);
403 }
404 BUG_ON(i < 0);
405 node = bval(geo, node, i);
406 }
407 BUG_ON(!node);
408 return node;
409 }
411 static int btree_grow(struct btree_head *head, struct btree_geo *geo,
412 gfp_t gfp)
413 {
414 unsigned long *node;
415 int fill;
417 node = btree_node_alloc(head, gfp);
418 if (!node)
419 return -ENOMEM;
420 if (head->node) {
421 fill = getfill(geo, head->node, 0);
422 setkey(geo, node, 0, bkey(geo, head->node, fill - 1));
423 setval(geo, node, 0, head->node);
424 }
425 head->node = node;
426 head->height++;
427 return 0;
428 }
430 static void btree_shrink(struct btree_head *head, struct btree_geo *geo)
431 {
432 unsigned long *node;
433 int fill;
435 if (head->height <= 1)
436 return;
438 node = head->node;
439 fill = getfill(geo, node, 0);
440 BUG_ON(fill > 1);
441 head->node = bval(geo, node, 0);
442 head->height--;
443 mempool_free(node, head->mempool);
444 }
446 static int btree_insert_level(struct btree_head *head, struct btree_geo *geo,
447 unsigned long *key, void *val, int level,
448 gfp_t gfp)
449 {
450 unsigned long *node;
451 int i, pos, fill, err;
453 BUG_ON(!val);
454 if (head->height < level) {
455 err = btree_grow(head, geo, gfp);
456 if (err)
457 return err;
458 }
460 retry:
461 node = find_level(head, geo, key, level);
462 pos = getpos(geo, node, key);
463 fill = getfill(geo, node, pos);
464 /* two identical keys are not allowed */
465 BUG_ON(pos < fill && keycmp(geo, node, pos, key) == 0);
467 if (fill == geo->no_pairs) {
468 /* need to split node */
469 unsigned long *new;
471 new = btree_node_alloc(head, gfp);
472 if (!new)
473 return -ENOMEM;
474 err = btree_insert_level(head, geo,
475 bkey(geo, node, fill / 2 - 1),
476 new, level + 1, gfp);
477 if (err) {
478 mempool_free(new, head->mempool);
479 return err;
480 }
481 for (i = 0; i < fill / 2; i++) {
482 setkey(geo, new, i, bkey(geo, node, i));
483 setval(geo, new, i, bval(geo, node, i));
484 setkey(geo, node, i, bkey(geo, node, i + fill / 2));
485 setval(geo, node, i, bval(geo, node, i + fill / 2));
486 clearpair(geo, node, i + fill / 2);
487 }
488 if (fill & 1) {
489 setkey(geo, node, i, bkey(geo, node, fill - 1));
490 setval(geo, node, i, bval(geo, node, fill - 1));
491 clearpair(geo, node, fill - 1);
492 }
493 goto retry;
494 }
495 BUG_ON(fill >= geo->no_pairs);
497 /* shift and insert */
498 for (i = fill; i > pos; i--) {
499 setkey(geo, node, i, bkey(geo, node, i - 1));
500 setval(geo, node, i, bval(geo, node, i - 1));
501 }
502 setkey(geo, node, pos, key);
503 setval(geo, node, pos, val);
505 return 0;
506 }
508 int btree_insert(struct btree_head *head, struct btree_geo *geo,
509 unsigned long *key, void *val, gfp_t gfp)
510 {
511 return btree_insert_level(head, geo, key, val, 1, gfp);
512 }
513 EXPORT_SYMBOL_GPL(btree_insert);
515 static void *btree_remove_level(struct btree_head *head, struct btree_geo *geo,
516 unsigned long *key, int level);
517 static void merge(struct btree_head *head, struct btree_geo *geo, int level,
518 unsigned long *left, int lfill,
519 unsigned long *right, int rfill,
520 unsigned long *parent, int lpos)
521 {
522 int i;
524 for (i = 0; i < rfill; i++) {
525 /* Move all keys to the left */
526 setkey(geo, left, lfill + i, bkey(geo, right, i));
527 setval(geo, left, lfill + i, bval(geo, right, i));
528 }
529 /* Exchange left and right child in parent */
530 setval(geo, parent, lpos, right);
531 setval(geo, parent, lpos + 1, left);
532 /* Remove left (formerly right) child from parent */
533 btree_remove_level(head, geo, bkey(geo, parent, lpos), level + 1);
534 mempool_free(right, head->mempool);
535 }
537 static void rebalance(struct btree_head *head, struct btree_geo *geo,
538 unsigned long *key, int level, unsigned long *child, int fill)
539 {
540 unsigned long *parent, *left = NULL, *right = NULL;
541 int i, no_left, no_right;
543 if (fill == 0) {
544 /* Because we don't steal entries from a neighbour, this case
545 * can happen. Parent node contains a single child, this
546 * node, so merging with a sibling never happens.
547 */
548 btree_remove_level(head, geo, key, level + 1);
549 mempool_free(child, head->mempool);
550 return;
551 }
553 parent = find_level(head, geo, key, level + 1);
554 i = getpos(geo, parent, key);
555 BUG_ON(bval(geo, parent, i) != child);
557 if (i > 0) {
558 left = bval(geo, parent, i - 1);
559 no_left = getfill(geo, left, 0);
560 if (fill + no_left <= geo->no_pairs) {
561 merge(head, geo, level,
562 left, no_left,
563 child, fill,
564 parent, i - 1);
565 return;
566 }
567 }
568 if (i + 1 < getfill(geo, parent, i)) {
569 right = bval(geo, parent, i + 1);
570 no_right = getfill(geo, right, 0);
571 if (fill + no_right <= geo->no_pairs) {
572 merge(head, geo, level,
573 child, fill,
574 right, no_right,
575 parent, i);
576 return;
577 }
578 }
579 /*
580 * We could also try to steal one entry from the left or right
581 * neighbor. By not doing so we changed the invariant from
582 * "all nodes are at least half full" to "no two neighboring
583 * nodes can be merged". Which means that the average fill of
584 * all nodes is still half or better.
585 */
586 }
588 static void *btree_remove_level(struct btree_head *head, struct btree_geo *geo,
589 unsigned long *key, int level)
590 {
591 unsigned long *node;
592 int i, pos, fill;
593 void *ret;
595 if (level > head->height) {
596 /* we recursed all the way up */
597 head->height = 0;
598 head->node = NULL;
599 return NULL;
600 }
602 node = find_level(head, geo, key, level);
603 pos = getpos(geo, node, key);
604 fill = getfill(geo, node, pos);
605 if ((level == 1) && (keycmp(geo, node, pos, key) != 0))
606 return NULL;
607 ret = bval(geo, node, pos);
609 /* remove and shift */
610 for (i = pos; i < fill - 1; i++) {
611 setkey(geo, node, i, bkey(geo, node, i + 1));
612 setval(geo, node, i, bval(geo, node, i + 1));
613 }
614 clearpair(geo, node, fill - 1);
616 if (fill - 1 < geo->no_pairs / 2) {
617 if (level < head->height)
618 rebalance(head, geo, key, level, node, fill - 1);
619 else if (fill - 1 == 1)
620 btree_shrink(head, geo);
621 }
623 return ret;
624 }
626 void *btree_remove(struct btree_head *head, struct btree_geo *geo,
627 unsigned long *key)
628 {
629 if (head->height == 0)
630 return NULL;
632 return btree_remove_level(head, geo, key, 1);
633 }
634 EXPORT_SYMBOL_GPL(btree_remove);
636 int btree_merge(struct btree_head *target, struct btree_head *victim,
637 struct btree_geo *geo, gfp_t gfp)
638 {
639 unsigned long key[geo->keylen];
640 unsigned long dup[geo->keylen];
641 void *val;
642 int err;
644 BUG_ON(target == victim);
646 if (!(target->node)) {
647 /* target is empty, just copy fields over */
648 target->node = victim->node;
649 target->height = victim->height;
650 __btree_init(victim);
651 return 0;
652 }
654 /* TODO: This needs some optimizations. Currently we do three tree
655 * walks to remove a single object from the victim.
656 */
657 for (;;) {
658 if (!btree_last(victim, geo, key))
659 break;
660 val = btree_lookup(victim, geo, key);
661 err = btree_insert(target, geo, key, val, gfp);
662 if (err)
663 return err;
664 /* We must make a copy of the key, as the original will get
665 * mangled inside btree_remove. */
666 longcpy(dup, key, geo->keylen);
667 btree_remove(victim, geo, dup);
668 }
669 return 0;
670 }
671 EXPORT_SYMBOL_GPL(btree_merge);
673 static size_t __btree_for_each(struct btree_head *head, struct btree_geo *geo,
674 unsigned long *node, unsigned long opaque,
675 void (*func)(void *elem, unsigned long opaque,
676 unsigned long *key, size_t index,
677 void *func2),
678 void *func2, int reap, int height, size_t count)
679 {
680 int i;
681 unsigned long *child;
683 for (i = 0; i < geo->no_pairs; i++) {
684 child = bval(geo, node, i);
685 if (!child)
686 break;
687 if (height > 1)
688 count = __btree_for_each(head, geo, child, opaque,
689 func, func2, reap, height - 1, count);
690 else
691 func(child, opaque, bkey(geo, node, i), count++,
692 func2);
693 }
694 if (reap)
695 mempool_free(node, head->mempool);
696 return count;
697 }
699 static void empty(void *elem, unsigned long opaque, unsigned long *key,
700 size_t index, void *func2)
701 {
702 }
704 void visitorl(void *elem, unsigned long opaque, unsigned long *key,
705 size_t index, void *__func)
706 {
707 visitorl_t func = __func;
709 func(elem, opaque, *key, index);
710 }
711 EXPORT_SYMBOL_GPL(visitorl);
713 void visitor32(void *elem, unsigned long opaque, unsigned long *__key,
714 size_t index, void *__func)
715 {
716 visitor32_t func = __func;
717 u32 *key = (void *)__key;
719 func(elem, opaque, *key, index);
720 }
721 EXPORT_SYMBOL_GPL(visitor32);
723 void visitor64(void *elem, unsigned long opaque, unsigned long *__key,
724 size_t index, void *__func)
725 {
726 visitor64_t func = __func;
727 u64 *key = (void *)__key;
729 func(elem, opaque, *key, index);
730 }
731 EXPORT_SYMBOL_GPL(visitor64);
733 void visitor128(void *elem, unsigned long opaque, unsigned long *__key,
734 size_t index, void *__func)
735 {
736 visitor128_t func = __func;
737 u64 *key = (void *)__key;
739 func(elem, opaque, key[0], key[1], index);
740 }
741 EXPORT_SYMBOL_GPL(visitor128);
743 size_t btree_visitor(struct btree_head *head, struct btree_geo *geo,
744 unsigned long opaque,
745 void (*func)(void *elem, unsigned long opaque,
746 unsigned long *key,
747 size_t index, void *func2),
748 void *func2)
749 {
750 size_t count = 0;
752 if (!func2)
753 func = empty;
754 if (head->node)
755 count = __btree_for_each(head, geo, head->node, opaque, func,
756 func2, 0, head->height, 0);
757 return count;
758 }
759 EXPORT_SYMBOL_GPL(btree_visitor);
761 size_t btree_grim_visitor(struct btree_head *head, struct btree_geo *geo,
762 unsigned long opaque,
763 void (*func)(void *elem, unsigned long opaque,
764 unsigned long *key,
765 size_t index, void *func2),
766 void *func2)
767 {
768 size_t count = 0;
770 if (!func2)
771 func = empty;
772 if (head->node)
773 count = __btree_for_each(head, geo, head->node, opaque, func,
774 func2, 1, head->height, 0);
775 __btree_init(head);
776 return count;
777 }
778 EXPORT_SYMBOL_GPL(btree_grim_visitor);
780 static int __init btree_module_init(void)
781 {
782 btree_cachep = kmem_cache_create("btree_node", NODESIZE, 0,
783 SLAB_HWCACHE_ALIGN, NULL);
784 return 0;
785 }
787 static void __exit btree_module_exit(void)
788 {
789 kmem_cache_destroy(btree_cachep);
790 }
792 /* If core code starts using btree, initialization should happen even earlier */
793 module_init(btree_module_init);
794 module_exit(btree_module_exit);
796 MODULE_AUTHOR("Joern Engel <joern@logfs.org>");
797 MODULE_AUTHOR("Johannes Berg <johannes@sipsolutions.net>");
798 MODULE_LICENSE("GPL");