]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - lib/textsearch.c
video: da8xx-fb: correct suspend/resume sequence
[sitara-epos/sitara-epos-kernel.git] / lib / textsearch.c
1 /*
2  * lib/textsearch.c     Generic text search interface
3  *
4  *              This program is free software; you can redistribute it and/or
5  *              modify it under the terms of the GNU General Public License
6  *              as published by the Free Software Foundation; either version
7  *              2 of the License, or (at your option) any later version.
8  *
9  * Authors:     Thomas Graf <tgraf@suug.ch>
10  *              Pablo Neira Ayuso <pablo@netfilter.org>
11  *
12  * ==========================================================================
13  *
14  * INTRODUCTION
15  *
16  *   The textsearch infrastructure provides text searching facilities for
17  *   both linear and non-linear data. Individual search algorithms are
18  *   implemented in modules and chosen by the user.
19  *
20  * ARCHITECTURE
21  *
22  *      User
23  *     +----------------+
24  *     |        finish()|<--------------(6)-----------------+
25  *     |get_next_block()|<--------------(5)---------------+ |
26  *     |                |                     Algorithm   | |
27  *     |                |                    +------------------------------+
28  *     |                |                    |  init()   find()   destroy() |
29  *     |                |                    +------------------------------+
30  *     |                |       Core API           ^       ^          ^
31  *     |                |      +---------------+  (2)     (4)        (8)
32  *     |             (1)|----->| prepare()     |---+       |          |
33  *     |             (3)|----->| find()/next() |-----------+          |
34  *     |             (7)|----->| destroy()     |----------------------+
35  *     +----------------+      +---------------+
36  *  
37  *   (1) User configures a search by calling _prepare() specifying the
38  *       search parameters such as the pattern and algorithm name.
39  *   (2) Core requests the algorithm to allocate and initialize a search
40  *       configuration according to the specified parameters.
41  *   (3) User starts the search(es) by calling _find() or _next() to
42  *       fetch subsequent occurrences. A state variable is provided
43  *       to the algorithm to store persistent variables.
44  *   (4) Core eventually resets the search offset and forwards the find()
45  *       request to the algorithm.
46  *   (5) Algorithm calls get_next_block() provided by the user continuously
47  *       to fetch the data to be searched in block by block.
48  *   (6) Algorithm invokes finish() after the last call to get_next_block
49  *       to clean up any leftovers from get_next_block. (Optional)
50  *   (7) User destroys the configuration by calling _destroy().
51  *   (8) Core notifies the algorithm to destroy algorithm specific
52  *       allocations. (Optional)
53  *
54  * USAGE
55  *
56  *   Before a search can be performed, a configuration must be created
57  *   by calling textsearch_prepare() specifying the searching algorithm,
58  *   the pattern to look for and flags. As a flag, you can set TS_IGNORECASE
59  *   to perform case insensitive matching. But it might slow down
60  *   performance of algorithm, so you should use it at own your risk.
61  *   The returned configuration may then be used for an arbitrary
62  *   amount of times and even in parallel as long as a separate struct
63  *   ts_state variable is provided to every instance.
64  *
65  *   The actual search is performed by either calling textsearch_find_-
66  *   continuous() for linear data or by providing an own get_next_block()
67  *   implementation and calling textsearch_find(). Both functions return
68  *   the position of the first occurrence of the pattern or UINT_MAX if
69  *   no match was found. Subsequent occurrences can be found by calling
70  *   textsearch_next() regardless of the linearity of the data.
71  *
72  *   Once you're done using a configuration it must be given back via
73  *   textsearch_destroy.
74  *
75  * EXAMPLE
76  *
77  *   int pos;
78  *   struct ts_config *conf;
79  *   struct ts_state state;
80  *   const char *pattern = "chicken";
81  *   const char *example = "We dance the funky chicken";
82  *
83  *   conf = textsearch_prepare("kmp", pattern, strlen(pattern),
84  *                             GFP_KERNEL, TS_AUTOLOAD);
85  *   if (IS_ERR(conf)) {
86  *       err = PTR_ERR(conf);
87  *       goto errout;
88  *   }
89  *
90  *   pos = textsearch_find_continuous(conf, &state, example, strlen(example));
91  *   if (pos != UINT_MAX)
92  *       panic("Oh my god, dancing chickens at %d\n", pos);
93  *
94  *   textsearch_destroy(conf);
95  * ==========================================================================
96  */
98 #include <linux/module.h>
99 #include <linux/types.h>
100 #include <linux/string.h>
101 #include <linux/init.h>
102 #include <linux/rculist.h>
103 #include <linux/rcupdate.h>
104 #include <linux/err.h>
105 #include <linux/textsearch.h>
106 #include <linux/slab.h>
108 static LIST_HEAD(ts_ops);
109 static DEFINE_SPINLOCK(ts_mod_lock);
111 static inline struct ts_ops *lookup_ts_algo(const char *name)
113         struct ts_ops *o;
115         rcu_read_lock();
116         list_for_each_entry_rcu(o, &ts_ops, list) {
117                 if (!strcmp(name, o->name)) {
118                         if (!try_module_get(o->owner))
119                                 o = NULL;
120                         rcu_read_unlock();
121                         return o;
122                 }
123         }
124         rcu_read_unlock();
126         return NULL;
129 /**
130  * textsearch_register - register a textsearch module
131  * @ops: operations lookup table
132  *
133  * This function must be called by textsearch modules to announce
134  * their presence. The specified &@ops must have %name set to a
135  * unique identifier and the callbacks find(), init(), get_pattern(),
136  * and get_pattern_len() must be implemented.
137  *
138  * Returns 0 or -EEXISTS if another module has already registered
139  * with same name.
140  */
141 int textsearch_register(struct ts_ops *ops)
143         int err = -EEXIST;
144         struct ts_ops *o;
146         if (ops->name == NULL || ops->find == NULL || ops->init == NULL ||
147             ops->get_pattern == NULL || ops->get_pattern_len == NULL)
148                 return -EINVAL;
150         spin_lock(&ts_mod_lock);
151         list_for_each_entry(o, &ts_ops, list) {
152                 if (!strcmp(ops->name, o->name))
153                         goto errout;
154         }
156         list_add_tail_rcu(&ops->list, &ts_ops);
157         err = 0;
158 errout:
159         spin_unlock(&ts_mod_lock);
160         return err;
163 /**
164  * textsearch_unregister - unregister a textsearch module
165  * @ops: operations lookup table
166  *
167  * This function must be called by textsearch modules to announce
168  * their disappearance for examples when the module gets unloaded.
169  * The &ops parameter must be the same as the one during the
170  * registration.
171  *
172  * Returns 0 on success or -ENOENT if no matching textsearch
173  * registration was found.
174  */
175 int textsearch_unregister(struct ts_ops *ops)
177         int err = 0;
178         struct ts_ops *o;
180         spin_lock(&ts_mod_lock);
181         list_for_each_entry(o, &ts_ops, list) {
182                 if (o == ops) {
183                         list_del_rcu(&o->list);
184                         goto out;
185                 }
186         }
188         err = -ENOENT;
189 out:
190         spin_unlock(&ts_mod_lock);
191         return err;
194 struct ts_linear_state
196         unsigned int    len;
197         const void      *data;
198 };
200 static unsigned int get_linear_data(unsigned int consumed, const u8 **dst,
201                                     struct ts_config *conf,
202                                     struct ts_state *state)
204         struct ts_linear_state *st = (struct ts_linear_state *) state->cb;
206         if (likely(consumed < st->len)) {
207                 *dst = st->data + consumed;
208                 return st->len - consumed;
209         }
211         return 0;
214 /**
215  * textsearch_find_continuous - search a pattern in continuous/linear data
216  * @conf: search configuration
217  * @state: search state
218  * @data: data to search in
219  * @len: length of data
220  *
221  * A simplified version of textsearch_find() for continuous/linear data.
222  * Call textsearch_next() to retrieve subsequent matches.
223  *
224  * Returns the position of first occurrence of the pattern or
225  * %UINT_MAX if no occurrence was found.
226  */ 
227 unsigned int textsearch_find_continuous(struct ts_config *conf,
228                                         struct ts_state *state,
229                                         const void *data, unsigned int len)
231         struct ts_linear_state *st = (struct ts_linear_state *) state->cb;
233         conf->get_next_block = get_linear_data;
234         st->data = data;
235         st->len = len;
237         return textsearch_find(conf, state);
240 /**
241  * textsearch_prepare - Prepare a search
242  * @algo: name of search algorithm
243  * @pattern: pattern data
244  * @len: length of pattern
245  * @gfp_mask: allocation mask
246  * @flags: search flags
247  *
248  * Looks up the search algorithm module and creates a new textsearch
249  * configuration for the specified pattern. Upon completion all
250  * necessary refcnts are held and the configuration must be put back
251  * using textsearch_put() after usage.
252  *
253  * Note: The format of the pattern may not be compatible between
254  *       the various search algorithms.
255  *
256  * Returns a new textsearch configuration according to the specified
257  * parameters or a ERR_PTR(). If a zero length pattern is passed, this
258  * function returns EINVAL.
259  */
260 struct ts_config *textsearch_prepare(const char *algo, const void *pattern,
261                                      unsigned int len, gfp_t gfp_mask, int flags)
263         int err = -ENOENT;
264         struct ts_config *conf;
265         struct ts_ops *ops;
266         
267         if (len == 0)
268                 return ERR_PTR(-EINVAL);
270         ops = lookup_ts_algo(algo);
271 #ifdef CONFIG_MODULES
272         /*
273          * Why not always autoload you may ask. Some users are
274          * in a situation where requesting a module may deadlock,
275          * especially when the module is located on a NFS mount.
276          */
277         if (ops == NULL && flags & TS_AUTOLOAD) {
278                 request_module("ts_%s", algo);
279                 ops = lookup_ts_algo(algo);
280         }
281 #endif
283         if (ops == NULL)
284                 goto errout;
286         conf = ops->init(pattern, len, gfp_mask, flags);
287         if (IS_ERR(conf)) {
288                 err = PTR_ERR(conf);
289                 goto errout;
290         }
292         conf->ops = ops;
293         return conf;
295 errout:
296         if (ops)
297                 module_put(ops->owner);
298                 
299         return ERR_PTR(err);
302 /**
303  * textsearch_destroy - destroy a search configuration
304  * @conf: search configuration
305  *
306  * Releases all references of the configuration and frees
307  * up the memory.
308  */
309 void textsearch_destroy(struct ts_config *conf)
311         if (conf->ops) {
312                 if (conf->ops->destroy)
313                         conf->ops->destroy(conf);
314                 module_put(conf->ops->owner);
315         }
317         kfree(conf);
320 EXPORT_SYMBOL(textsearch_register);
321 EXPORT_SYMBOL(textsearch_unregister);
322 EXPORT_SYMBOL(textsearch_prepare);
323 EXPORT_SYMBOL(textsearch_find_continuous);
324 EXPORT_SYMBOL(textsearch_destroy);