]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - lib/uuid.c
am335x: lis33ldlh: Add accelerometer support to AM335X
[sitara-epos/sitara-epos-kernel.git] / lib / uuid.c
1 /*
2  * Unified UUID/GUID definition
3  *
4  * Copyright (C) 2009, Intel Corp.
5  *      Huang Ying <ying.huang@intel.com>
6  *
7  * This program is free software; you can redistribute it and/or
8  * modify it under the terms of the GNU General Public License version
9  * 2 as published by the Free Software Foundation;
10  *
11  * This program is distributed in the hope that it will be useful,
12  * but WITHOUT ANY WARRANTY; without even the implied warranty of
13  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
14  * GNU General Public License for more details.
15  *
16  * You should have received a copy of the GNU General Public License
17  * along with this program; if not, write to the Free Software
18  * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
19  */
21 #include <linux/kernel.h>
22 #include <linux/module.h>
23 #include <linux/uuid.h>
24 #include <linux/random.h>
26 static void __uuid_gen_common(__u8 b[16])
27 {
28         int i;
29         u32 r;
31         for (i = 0; i < 4; i++) {
32                 r = random32();
33                 memcpy(b + i * 4, &r, 4);
34         }
35         /* reversion 0b10 */
36         b[8] = (b[8] & 0x3F) | 0x80;
37 }
39 void uuid_le_gen(uuid_le *lu)
40 {
41         __uuid_gen_common(lu->b);
42         /* version 4 : random generation */
43         lu->b[7] = (lu->b[7] & 0x0F) | 0x40;
44 }
45 EXPORT_SYMBOL_GPL(uuid_le_gen);
47 void uuid_be_gen(uuid_be *bu)
48 {
49         __uuid_gen_common(bu->b);
50         /* version 4 : random generation */
51         bu->b[6] = (bu->b[6] & 0x0F) | 0x40;
52 }
53 EXPORT_SYMBOL_GPL(uuid_be_gen);