2 #include <linux/wait.h>
3 #include <linux/backing-dev.h>
4 #include <linux/kthread.h>
5 #include <linux/freezer.h>
6 #include <linux/fs.h>
7 #include <linux/pagemap.h>
8 #include <linux/mm.h>
9 #include <linux/sched.h>
10 #include <linux/module.h>
11 #include <linux/writeback.h>
12 #include <linux/device.h>
13 #include <trace/events/writeback.h>
15 static atomic_long_t bdi_seq = ATOMIC_LONG_INIT(0);
17 struct backing_dev_info default_backing_dev_info = {
18 .name = "default",
19 .ra_pages = VM_MAX_READAHEAD * 1024 / PAGE_CACHE_SIZE,
20 .state = 0,
21 .capabilities = BDI_CAP_MAP_COPY,
22 };
23 EXPORT_SYMBOL_GPL(default_backing_dev_info);
25 struct backing_dev_info noop_backing_dev_info = {
26 .name = "noop",
27 .capabilities = BDI_CAP_NO_ACCT_AND_WRITEBACK,
28 };
29 EXPORT_SYMBOL_GPL(noop_backing_dev_info);
31 static struct class *bdi_class;
33 /*
34 * bdi_lock protects updates to bdi_list and bdi_pending_list, as well as
35 * reader side protection for bdi_pending_list. bdi_list has RCU reader side
36 * locking.
37 */
38 DEFINE_SPINLOCK(bdi_lock);
39 LIST_HEAD(bdi_list);
40 LIST_HEAD(bdi_pending_list);
42 static struct task_struct *sync_supers_tsk;
43 static struct timer_list sync_supers_timer;
45 static int bdi_sync_supers(void *);
46 static void sync_supers_timer_fn(unsigned long);
48 void bdi_lock_two(struct bdi_writeback *wb1, struct bdi_writeback *wb2)
49 {
50 if (wb1 < wb2) {
51 spin_lock(&wb1->list_lock);
52 spin_lock_nested(&wb2->list_lock, 1);
53 } else {
54 spin_lock(&wb2->list_lock);
55 spin_lock_nested(&wb1->list_lock, 1);
56 }
57 }
59 #ifdef CONFIG_DEBUG_FS
60 #include <linux/debugfs.h>
61 #include <linux/seq_file.h>
63 static struct dentry *bdi_debug_root;
65 static void bdi_debug_init(void)
66 {
67 bdi_debug_root = debugfs_create_dir("bdi", NULL);
68 }
70 static int bdi_debug_stats_show(struct seq_file *m, void *v)
71 {
72 struct backing_dev_info *bdi = m->private;
73 struct bdi_writeback *wb = &bdi->wb;
74 unsigned long background_thresh;
75 unsigned long dirty_thresh;
76 unsigned long bdi_thresh;
77 unsigned long nr_dirty, nr_io, nr_more_io;
78 struct inode *inode;
80 nr_dirty = nr_io = nr_more_io = 0;
81 spin_lock(&wb->list_lock);
82 list_for_each_entry(inode, &wb->b_dirty, i_wb_list)
83 nr_dirty++;
84 list_for_each_entry(inode, &wb->b_io, i_wb_list)
85 nr_io++;
86 list_for_each_entry(inode, &wb->b_more_io, i_wb_list)
87 nr_more_io++;
88 spin_unlock(&wb->list_lock);
90 global_dirty_limits(&background_thresh, &dirty_thresh);
91 bdi_thresh = bdi_dirty_limit(bdi, dirty_thresh);
93 #define K(x) ((x) << (PAGE_SHIFT - 10))
94 seq_printf(m,
95 "BdiWriteback: %10lu kB\n"
96 "BdiReclaimable: %10lu kB\n"
97 "BdiDirtyThresh: %10lu kB\n"
98 "DirtyThresh: %10lu kB\n"
99 "BackgroundThresh: %10lu kB\n"
100 "BdiDirtied: %10lu kB\n"
101 "BdiWritten: %10lu kB\n"
102 "BdiWriteBandwidth: %10lu kBps\n"
103 "b_dirty: %10lu\n"
104 "b_io: %10lu\n"
105 "b_more_io: %10lu\n"
106 "bdi_list: %10u\n"
107 "state: %10lx\n",
108 (unsigned long) K(bdi_stat(bdi, BDI_WRITEBACK)),
109 (unsigned long) K(bdi_stat(bdi, BDI_RECLAIMABLE)),
110 K(bdi_thresh),
111 K(dirty_thresh),
112 K(background_thresh),
113 (unsigned long) K(bdi_stat(bdi, BDI_DIRTIED)),
114 (unsigned long) K(bdi_stat(bdi, BDI_WRITTEN)),
115 (unsigned long) K(bdi->write_bandwidth),
116 nr_dirty,
117 nr_io,
118 nr_more_io,
119 !list_empty(&bdi->bdi_list), bdi->state);
120 #undef K
122 return 0;
123 }
125 static int bdi_debug_stats_open(struct inode *inode, struct file *file)
126 {
127 return single_open(file, bdi_debug_stats_show, inode->i_private);
128 }
130 static const struct file_operations bdi_debug_stats_fops = {
131 .open = bdi_debug_stats_open,
132 .read = seq_read,
133 .llseek = seq_lseek,
134 .release = single_release,
135 };
137 static void bdi_debug_register(struct backing_dev_info *bdi, const char *name)
138 {
139 bdi->debug_dir = debugfs_create_dir(name, bdi_debug_root);
140 bdi->debug_stats = debugfs_create_file("stats", 0444, bdi->debug_dir,
141 bdi, &bdi_debug_stats_fops);
142 }
144 static void bdi_debug_unregister(struct backing_dev_info *bdi)
145 {
146 debugfs_remove(bdi->debug_stats);
147 debugfs_remove(bdi->debug_dir);
148 }
149 #else
150 static inline void bdi_debug_init(void)
151 {
152 }
153 static inline void bdi_debug_register(struct backing_dev_info *bdi,
154 const char *name)
155 {
156 }
157 static inline void bdi_debug_unregister(struct backing_dev_info *bdi)
158 {
159 }
160 #endif
162 static ssize_t read_ahead_kb_store(struct device *dev,
163 struct device_attribute *attr,
164 const char *buf, size_t count)
165 {
166 struct backing_dev_info *bdi = dev_get_drvdata(dev);
167 char *end;
168 unsigned long read_ahead_kb;
169 ssize_t ret = -EINVAL;
171 read_ahead_kb = simple_strtoul(buf, &end, 10);
172 if (*buf && (end[0] == '\0' || (end[0] == '\n' && end[1] == '\0'))) {
173 bdi->ra_pages = read_ahead_kb >> (PAGE_SHIFT - 10);
174 ret = count;
175 }
176 return ret;
177 }
179 #define K(pages) ((pages) << (PAGE_SHIFT - 10))
181 #define BDI_SHOW(name, expr) \
182 static ssize_t name##_show(struct device *dev, \
183 struct device_attribute *attr, char *page) \
184 { \
185 struct backing_dev_info *bdi = dev_get_drvdata(dev); \
186 \
187 return snprintf(page, PAGE_SIZE-1, "%lld\n", (long long)expr); \
188 }
190 BDI_SHOW(read_ahead_kb, K(bdi->ra_pages))
192 static ssize_t min_ratio_store(struct device *dev,
193 struct device_attribute *attr, const char *buf, size_t count)
194 {
195 struct backing_dev_info *bdi = dev_get_drvdata(dev);
196 char *end;
197 unsigned int ratio;
198 ssize_t ret = -EINVAL;
200 ratio = simple_strtoul(buf, &end, 10);
201 if (*buf && (end[0] == '\0' || (end[0] == '\n' && end[1] == '\0'))) {
202 ret = bdi_set_min_ratio(bdi, ratio);
203 if (!ret)
204 ret = count;
205 }
206 return ret;
207 }
208 BDI_SHOW(min_ratio, bdi->min_ratio)
210 static ssize_t max_ratio_store(struct device *dev,
211 struct device_attribute *attr, const char *buf, size_t count)
212 {
213 struct backing_dev_info *bdi = dev_get_drvdata(dev);
214 char *end;
215 unsigned int ratio;
216 ssize_t ret = -EINVAL;
218 ratio = simple_strtoul(buf, &end, 10);
219 if (*buf && (end[0] == '\0' || (end[0] == '\n' && end[1] == '\0'))) {
220 ret = bdi_set_max_ratio(bdi, ratio);
221 if (!ret)
222 ret = count;
223 }
224 return ret;
225 }
226 BDI_SHOW(max_ratio, bdi->max_ratio)
228 #define __ATTR_RW(attr) __ATTR(attr, 0644, attr##_show, attr##_store)
230 static struct device_attribute bdi_dev_attrs[] = {
231 __ATTR_RW(read_ahead_kb),
232 __ATTR_RW(min_ratio),
233 __ATTR_RW(max_ratio),
234 __ATTR_NULL,
235 };
237 static __init int bdi_class_init(void)
238 {
239 bdi_class = class_create(THIS_MODULE, "bdi");
240 if (IS_ERR(bdi_class))
241 return PTR_ERR(bdi_class);
243 bdi_class->dev_attrs = bdi_dev_attrs;
244 bdi_debug_init();
245 return 0;
246 }
247 postcore_initcall(bdi_class_init);
249 static int __init default_bdi_init(void)
250 {
251 int err;
253 sync_supers_tsk = kthread_run(bdi_sync_supers, NULL, "sync_supers");
254 BUG_ON(IS_ERR(sync_supers_tsk));
256 setup_timer(&sync_supers_timer, sync_supers_timer_fn, 0);
257 bdi_arm_supers_timer();
259 err = bdi_init(&default_backing_dev_info);
260 if (!err)
261 bdi_register(&default_backing_dev_info, NULL, "default");
262 err = bdi_init(&noop_backing_dev_info);
264 return err;
265 }
266 subsys_initcall(default_bdi_init);
268 int bdi_has_dirty_io(struct backing_dev_info *bdi)
269 {
270 return wb_has_dirty_io(&bdi->wb);
271 }
273 /*
274 * kupdated() used to do this. We cannot do it from the bdi_forker_thread()
275 * or we risk deadlocking on ->s_umount. The longer term solution would be
276 * to implement sync_supers_bdi() or similar and simply do it from the
277 * bdi writeback thread individually.
278 */
279 static int bdi_sync_supers(void *unused)
280 {
281 set_user_nice(current, 0);
283 while (!kthread_should_stop()) {
284 set_current_state(TASK_INTERRUPTIBLE);
285 schedule();
287 /*
288 * Do this periodically, like kupdated() did before.
289 */
290 sync_supers();
291 }
293 return 0;
294 }
296 void bdi_arm_supers_timer(void)
297 {
298 unsigned long next;
300 if (!dirty_writeback_interval)
301 return;
303 next = msecs_to_jiffies(dirty_writeback_interval * 10) + jiffies;
304 mod_timer(&sync_supers_timer, round_jiffies_up(next));
305 }
307 static void sync_supers_timer_fn(unsigned long unused)
308 {
309 wake_up_process(sync_supers_tsk);
310 bdi_arm_supers_timer();
311 }
313 static void wakeup_timer_fn(unsigned long data)
314 {
315 struct backing_dev_info *bdi = (struct backing_dev_info *)data;
317 spin_lock_bh(&bdi->wb_lock);
318 if (bdi->wb.task) {
319 trace_writeback_wake_thread(bdi);
320 wake_up_process(bdi->wb.task);
321 } else {
322 /*
323 * When bdi tasks are inactive for long time, they are killed.
324 * In this case we have to wake-up the forker thread which
325 * should create and run the bdi thread.
326 */
327 trace_writeback_wake_forker_thread(bdi);
328 wake_up_process(default_backing_dev_info.wb.task);
329 }
330 spin_unlock_bh(&bdi->wb_lock);
331 }
333 /*
334 * This function is used when the first inode for this bdi is marked dirty. It
335 * wakes-up the corresponding bdi thread which should then take care of the
336 * periodic background write-out of dirty inodes. Since the write-out would
337 * starts only 'dirty_writeback_interval' centisecs from now anyway, we just
338 * set up a timer which wakes the bdi thread up later.
339 *
340 * Note, we wouldn't bother setting up the timer, but this function is on the
341 * fast-path (used by '__mark_inode_dirty()'), so we save few context switches
342 * by delaying the wake-up.
343 */
344 void bdi_wakeup_thread_delayed(struct backing_dev_info *bdi)
345 {
346 unsigned long timeout;
348 timeout = msecs_to_jiffies(dirty_writeback_interval * 10);
349 mod_timer(&bdi->wb.wakeup_timer, jiffies + timeout);
350 }
352 /*
353 * Calculate the longest interval (jiffies) bdi threads are allowed to be
354 * inactive.
355 */
356 static unsigned long bdi_longest_inactive(void)
357 {
358 unsigned long interval;
360 interval = msecs_to_jiffies(dirty_writeback_interval * 10);
361 return max(5UL * 60 * HZ, interval);
362 }
364 /*
365 * Clear pending bit and wakeup anybody waiting for flusher thread creation or
366 * shutdown
367 */
368 static void bdi_clear_pending(struct backing_dev_info *bdi)
369 {
370 clear_bit(BDI_pending, &bdi->state);
371 smp_mb__after_clear_bit();
372 wake_up_bit(&bdi->state, BDI_pending);
373 }
375 static int bdi_forker_thread(void *ptr)
376 {
377 struct bdi_writeback *me = ptr;
379 current->flags |= PF_SWAPWRITE;
380 set_freezable();
382 /*
383 * Our parent may run at a different priority, just set us to normal
384 */
385 set_user_nice(current, 0);
387 for (;;) {
388 struct task_struct *task = NULL;
389 struct backing_dev_info *bdi;
390 enum {
391 NO_ACTION, /* Nothing to do */
392 FORK_THREAD, /* Fork bdi thread */
393 KILL_THREAD, /* Kill inactive bdi thread */
394 } action = NO_ACTION;
396 /*
397 * Temporary measure, we want to make sure we don't see
398 * dirty data on the default backing_dev_info
399 */
400 if (wb_has_dirty_io(me) || !list_empty(&me->bdi->work_list)) {
401 del_timer(&me->wakeup_timer);
402 wb_do_writeback(me, 0);
403 }
405 spin_lock_bh(&bdi_lock);
406 /*
407 * In the following loop we are going to check whether we have
408 * some work to do without any synchronization with tasks
409 * waking us up to do work for them. Set the task state here
410 * so that we don't miss wakeups after verifying conditions.
411 */
412 set_current_state(TASK_INTERRUPTIBLE);
414 list_for_each_entry(bdi, &bdi_list, bdi_list) {
415 bool have_dirty_io;
417 if (!bdi_cap_writeback_dirty(bdi) ||
418 bdi_cap_flush_forker(bdi))
419 continue;
421 WARN(!test_bit(BDI_registered, &bdi->state),
422 "bdi %p/%s is not registered!\n", bdi, bdi->name);
424 have_dirty_io = !list_empty(&bdi->work_list) ||
425 wb_has_dirty_io(&bdi->wb);
427 /*
428 * If the bdi has work to do, but the thread does not
429 * exist - create it.
430 */
431 if (!bdi->wb.task && have_dirty_io) {
432 /*
433 * Set the pending bit - if someone will try to
434 * unregister this bdi - it'll wait on this bit.
435 */
436 set_bit(BDI_pending, &bdi->state);
437 action = FORK_THREAD;
438 break;
439 }
441 spin_lock(&bdi->wb_lock);
443 /*
444 * If there is no work to do and the bdi thread was
445 * inactive long enough - kill it. The wb_lock is taken
446 * to make sure no-one adds more work to this bdi and
447 * wakes the bdi thread up.
448 */
449 if (bdi->wb.task && !have_dirty_io &&
450 time_after(jiffies, bdi->wb.last_active +
451 bdi_longest_inactive())) {
452 task = bdi->wb.task;
453 bdi->wb.task = NULL;
454 spin_unlock(&bdi->wb_lock);
455 set_bit(BDI_pending, &bdi->state);
456 action = KILL_THREAD;
457 break;
458 }
459 spin_unlock(&bdi->wb_lock);
460 }
461 spin_unlock_bh(&bdi_lock);
463 /* Keep working if default bdi still has things to do */
464 if (!list_empty(&me->bdi->work_list))
465 __set_current_state(TASK_RUNNING);
467 switch (action) {
468 case FORK_THREAD:
469 __set_current_state(TASK_RUNNING);
470 task = kthread_create(bdi_writeback_thread, &bdi->wb,
471 "flush-%s", dev_name(bdi->dev));
472 if (IS_ERR(task)) {
473 /*
474 * If thread creation fails, force writeout of
475 * the bdi from the thread. Hopefully 1024 is
476 * large enough for efficient IO.
477 */
478 writeback_inodes_wb(&bdi->wb, 1024,
479 WB_REASON_FORKER_THREAD);
480 } else {
481 /*
482 * The spinlock makes sure we do not lose
483 * wake-ups when racing with 'bdi_queue_work()'.
484 * And as soon as the bdi thread is visible, we
485 * can start it.
486 */
487 spin_lock_bh(&bdi->wb_lock);
488 bdi->wb.task = task;
489 spin_unlock_bh(&bdi->wb_lock);
490 wake_up_process(task);
491 }
492 bdi_clear_pending(bdi);
493 break;
495 case KILL_THREAD:
496 __set_current_state(TASK_RUNNING);
497 kthread_stop(task);
498 bdi_clear_pending(bdi);
499 break;
501 case NO_ACTION:
502 if (!wb_has_dirty_io(me) || !dirty_writeback_interval)
503 /*
504 * There are no dirty data. The only thing we
505 * should now care about is checking for
506 * inactive bdi threads and killing them. Thus,
507 * let's sleep for longer time, save energy and
508 * be friendly for battery-driven devices.
509 */
510 schedule_timeout(bdi_longest_inactive());
511 else
512 schedule_timeout(msecs_to_jiffies(dirty_writeback_interval * 10));
513 try_to_freeze();
514 break;
515 }
516 }
518 return 0;
519 }
521 /*
522 * Remove bdi from bdi_list, and ensure that it is no longer visible
523 */
524 static void bdi_remove_from_list(struct backing_dev_info *bdi)
525 {
526 spin_lock_bh(&bdi_lock);
527 list_del_rcu(&bdi->bdi_list);
528 spin_unlock_bh(&bdi_lock);
530 synchronize_rcu_expedited();
531 }
533 int bdi_register(struct backing_dev_info *bdi, struct device *parent,
534 const char *fmt, ...)
535 {
536 va_list args;
537 struct device *dev;
539 if (bdi->dev) /* The driver needs to use separate queues per device */
540 return 0;
542 va_start(args, fmt);
543 dev = device_create_vargs(bdi_class, parent, MKDEV(0, 0), bdi, fmt, args);
544 va_end(args);
545 if (IS_ERR(dev))
546 return PTR_ERR(dev);
548 bdi->dev = dev;
550 /*
551 * Just start the forker thread for our default backing_dev_info,
552 * and add other bdi's to the list. They will get a thread created
553 * on-demand when they need it.
554 */
555 if (bdi_cap_flush_forker(bdi)) {
556 struct bdi_writeback *wb = &bdi->wb;
558 wb->task = kthread_run(bdi_forker_thread, wb, "bdi-%s",
559 dev_name(dev));
560 if (IS_ERR(wb->task))
561 return PTR_ERR(wb->task);
562 }
564 bdi_debug_register(bdi, dev_name(dev));
565 set_bit(BDI_registered, &bdi->state);
567 spin_lock_bh(&bdi_lock);
568 list_add_tail_rcu(&bdi->bdi_list, &bdi_list);
569 spin_unlock_bh(&bdi_lock);
571 trace_writeback_bdi_register(bdi);
572 return 0;
573 }
574 EXPORT_SYMBOL(bdi_register);
576 int bdi_register_dev(struct backing_dev_info *bdi, dev_t dev)
577 {
578 return bdi_register(bdi, NULL, "%u:%u", MAJOR(dev), MINOR(dev));
579 }
580 EXPORT_SYMBOL(bdi_register_dev);
582 /*
583 * Remove bdi from the global list and shutdown any threads we have running
584 */
585 static void bdi_wb_shutdown(struct backing_dev_info *bdi)
586 {
587 if (!bdi_cap_writeback_dirty(bdi))
588 return;
590 /*
591 * Make sure nobody finds us on the bdi_list anymore
592 */
593 bdi_remove_from_list(bdi);
595 /*
596 * If setup is pending, wait for that to complete first
597 */
598 wait_on_bit(&bdi->state, BDI_pending, bdi_sched_wait,
599 TASK_UNINTERRUPTIBLE);
601 /*
602 * Finally, kill the kernel thread. We don't need to be RCU
603 * safe anymore, since the bdi is gone from visibility. Force
604 * unfreeze of the thread before calling kthread_stop(), otherwise
605 * it would never exet if it is currently stuck in the refrigerator.
606 */
607 if (bdi->wb.task) {
608 thaw_process(bdi->wb.task);
609 kthread_stop(bdi->wb.task);
610 }
611 }
613 /*
614 * This bdi is going away now, make sure that no super_blocks point to it
615 */
616 static void bdi_prune_sb(struct backing_dev_info *bdi)
617 {
618 struct super_block *sb;
620 spin_lock(&sb_lock);
621 list_for_each_entry(sb, &super_blocks, s_list) {
622 if (sb->s_bdi == bdi)
623 sb->s_bdi = &default_backing_dev_info;
624 }
625 spin_unlock(&sb_lock);
626 }
628 void bdi_unregister(struct backing_dev_info *bdi)
629 {
630 if (bdi->dev) {
631 bdi_set_min_ratio(bdi, 0);
632 trace_writeback_bdi_unregister(bdi);
633 bdi_prune_sb(bdi);
634 del_timer_sync(&bdi->wb.wakeup_timer);
636 if (!bdi_cap_flush_forker(bdi))
637 bdi_wb_shutdown(bdi);
638 bdi_debug_unregister(bdi);
639 device_unregister(bdi->dev);
640 bdi->dev = NULL;
641 }
642 }
643 EXPORT_SYMBOL(bdi_unregister);
645 static void bdi_wb_init(struct bdi_writeback *wb, struct backing_dev_info *bdi)
646 {
647 memset(wb, 0, sizeof(*wb));
649 wb->bdi = bdi;
650 wb->last_old_flush = jiffies;
651 INIT_LIST_HEAD(&wb->b_dirty);
652 INIT_LIST_HEAD(&wb->b_io);
653 INIT_LIST_HEAD(&wb->b_more_io);
654 spin_lock_init(&wb->list_lock);
655 setup_timer(&wb->wakeup_timer, wakeup_timer_fn, (unsigned long)bdi);
656 }
658 /*
659 * Initial write bandwidth: 100 MB/s
660 */
661 #define INIT_BW (100 << (20 - PAGE_SHIFT))
663 int bdi_init(struct backing_dev_info *bdi)
664 {
665 int i, err;
667 bdi->dev = NULL;
669 bdi->min_ratio = 0;
670 bdi->max_ratio = 100;
671 bdi->max_prop_frac = PROP_FRAC_BASE;
672 spin_lock_init(&bdi->wb_lock);
673 INIT_LIST_HEAD(&bdi->bdi_list);
674 INIT_LIST_HEAD(&bdi->work_list);
676 bdi_wb_init(&bdi->wb, bdi);
678 for (i = 0; i < NR_BDI_STAT_ITEMS; i++) {
679 err = percpu_counter_init(&bdi->bdi_stat[i], 0);
680 if (err)
681 goto err;
682 }
684 bdi->dirty_exceeded = 0;
686 bdi->bw_time_stamp = jiffies;
687 bdi->written_stamp = 0;
689 bdi->balanced_dirty_ratelimit = INIT_BW;
690 bdi->dirty_ratelimit = INIT_BW;
691 bdi->write_bandwidth = INIT_BW;
692 bdi->avg_write_bandwidth = INIT_BW;
694 err = prop_local_init_percpu(&bdi->completions);
696 if (err) {
697 err:
698 while (i--)
699 percpu_counter_destroy(&bdi->bdi_stat[i]);
700 }
702 return err;
703 }
704 EXPORT_SYMBOL(bdi_init);
706 void bdi_destroy(struct backing_dev_info *bdi)
707 {
708 int i;
710 /*
711 * Splice our entries to the default_backing_dev_info, if this
712 * bdi disappears
713 */
714 if (bdi_has_dirty_io(bdi)) {
715 struct bdi_writeback *dst = &default_backing_dev_info.wb;
717 bdi_lock_two(&bdi->wb, dst);
718 list_splice(&bdi->wb.b_dirty, &dst->b_dirty);
719 list_splice(&bdi->wb.b_io, &dst->b_io);
720 list_splice(&bdi->wb.b_more_io, &dst->b_more_io);
721 spin_unlock(&bdi->wb.list_lock);
722 spin_unlock(&dst->list_lock);
723 }
725 bdi_unregister(bdi);
727 /*
728 * If bdi_unregister() had already been called earlier, the
729 * wakeup_timer could still be armed because bdi_prune_sb()
730 * can race with the bdi_wakeup_thread_delayed() calls from
731 * __mark_inode_dirty().
732 */
733 del_timer_sync(&bdi->wb.wakeup_timer);
735 for (i = 0; i < NR_BDI_STAT_ITEMS; i++)
736 percpu_counter_destroy(&bdi->bdi_stat[i]);
738 prop_local_destroy_percpu(&bdi->completions);
739 }
740 EXPORT_SYMBOL(bdi_destroy);
742 /*
743 * For use from filesystems to quickly init and register a bdi associated
744 * with dirty writeback
745 */
746 int bdi_setup_and_register(struct backing_dev_info *bdi, char *name,
747 unsigned int cap)
748 {
749 char tmp[32];
750 int err;
752 bdi->name = name;
753 bdi->capabilities = cap;
754 err = bdi_init(bdi);
755 if (err)
756 return err;
758 sprintf(tmp, "%.28s%s", name, "-%d");
759 err = bdi_register(bdi, NULL, tmp, atomic_long_inc_return(&bdi_seq));
760 if (err) {
761 bdi_destroy(bdi);
762 return err;
763 }
765 return 0;
766 }
767 EXPORT_SYMBOL(bdi_setup_and_register);
769 static wait_queue_head_t congestion_wqh[2] = {
770 __WAIT_QUEUE_HEAD_INITIALIZER(congestion_wqh[0]),
771 __WAIT_QUEUE_HEAD_INITIALIZER(congestion_wqh[1])
772 };
773 static atomic_t nr_bdi_congested[2];
775 void clear_bdi_congested(struct backing_dev_info *bdi, int sync)
776 {
777 enum bdi_state bit;
778 wait_queue_head_t *wqh = &congestion_wqh[sync];
780 bit = sync ? BDI_sync_congested : BDI_async_congested;
781 if (test_and_clear_bit(bit, &bdi->state))
782 atomic_dec(&nr_bdi_congested[sync]);
783 smp_mb__after_clear_bit();
784 if (waitqueue_active(wqh))
785 wake_up(wqh);
786 }
787 EXPORT_SYMBOL(clear_bdi_congested);
789 void set_bdi_congested(struct backing_dev_info *bdi, int sync)
790 {
791 enum bdi_state bit;
793 bit = sync ? BDI_sync_congested : BDI_async_congested;
794 if (!test_and_set_bit(bit, &bdi->state))
795 atomic_inc(&nr_bdi_congested[sync]);
796 }
797 EXPORT_SYMBOL(set_bdi_congested);
799 /**
800 * congestion_wait - wait for a backing_dev to become uncongested
801 * @sync: SYNC or ASYNC IO
802 * @timeout: timeout in jiffies
803 *
804 * Waits for up to @timeout jiffies for a backing_dev (any backing_dev) to exit
805 * write congestion. If no backing_devs are congested then just wait for the
806 * next write to be completed.
807 */
808 long congestion_wait(int sync, long timeout)
809 {
810 long ret;
811 unsigned long start = jiffies;
812 DEFINE_WAIT(wait);
813 wait_queue_head_t *wqh = &congestion_wqh[sync];
815 prepare_to_wait(wqh, &wait, TASK_UNINTERRUPTIBLE);
816 ret = io_schedule_timeout(timeout);
817 finish_wait(wqh, &wait);
819 trace_writeback_congestion_wait(jiffies_to_usecs(timeout),
820 jiffies_to_usecs(jiffies - start));
822 return ret;
823 }
824 EXPORT_SYMBOL(congestion_wait);
826 /**
827 * wait_iff_congested - Conditionally wait for a backing_dev to become uncongested or a zone to complete writes
828 * @zone: A zone to check if it is heavily congested
829 * @sync: SYNC or ASYNC IO
830 * @timeout: timeout in jiffies
831 *
832 * In the event of a congested backing_dev (any backing_dev) and the given
833 * @zone has experienced recent congestion, this waits for up to @timeout
834 * jiffies for either a BDI to exit congestion of the given @sync queue
835 * or a write to complete.
836 *
837 * In the absence of zone congestion, cond_resched() is called to yield
838 * the processor if necessary but otherwise does not sleep.
839 *
840 * The return value is 0 if the sleep is for the full timeout. Otherwise,
841 * it is the number of jiffies that were still remaining when the function
842 * returned. return_value == timeout implies the function did not sleep.
843 */
844 long wait_iff_congested(struct zone *zone, int sync, long timeout)
845 {
846 long ret;
847 unsigned long start = jiffies;
848 DEFINE_WAIT(wait);
849 wait_queue_head_t *wqh = &congestion_wqh[sync];
851 /*
852 * If there is no congestion, or heavy congestion is not being
853 * encountered in the current zone, yield if necessary instead
854 * of sleeping on the congestion queue
855 */
856 if (atomic_read(&nr_bdi_congested[sync]) == 0 ||
857 !zone_is_reclaim_congested(zone)) {
858 cond_resched();
860 /* In case we scheduled, work out time remaining */
861 ret = timeout - (jiffies - start);
862 if (ret < 0)
863 ret = 0;
865 goto out;
866 }
868 /* Sleep until uncongested or a write happens */
869 prepare_to_wait(wqh, &wait, TASK_UNINTERRUPTIBLE);
870 ret = io_schedule_timeout(timeout);
871 finish_wait(wqh, &wait);
873 out:
874 trace_writeback_wait_iff_congested(jiffies_to_usecs(timeout),
875 jiffies_to_usecs(jiffies - start));
877 return ret;
878 }
879 EXPORT_SYMBOL(wait_iff_congested);