]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - mm/dmapool.c
video: da8xx-fb: correct suspend/resume sequence
[sitara-epos/sitara-epos-kernel.git] / mm / dmapool.c
1 /*
2  * DMA Pool allocator
3  *
4  * Copyright 2001 David Brownell
5  * Copyright 2007 Intel Corporation
6  *   Author: Matthew Wilcox <willy@linux.intel.com>
7  *
8  * This software may be redistributed and/or modified under the terms of
9  * the GNU General Public License ("GPL") version 2 as published by the
10  * Free Software Foundation.
11  *
12  * This allocator returns small blocks of a given size which are DMA-able by
13  * the given device.  It uses the dma_alloc_coherent page allocator to get
14  * new pages, then splits them up into blocks of the required size.
15  * Many older drivers still have their own code to do this.
16  *
17  * The current design of this allocator is fairly simple.  The pool is
18  * represented by the 'struct dma_pool' which keeps a doubly-linked list of
19  * allocated pages.  Each page in the page_list is split into blocks of at
20  * least 'size' bytes.  Free blocks are tracked in an unsorted singly-linked
21  * list of free blocks within the page.  Used blocks aren't tracked, but we
22  * keep a count of how many are currently allocated from each page.
23  */
25 #include <linux/device.h>
26 #include <linux/dma-mapping.h>
27 #include <linux/dmapool.h>
28 #include <linux/kernel.h>
29 #include <linux/list.h>
30 #include <linux/export.h>
31 #include <linux/mutex.h>
32 #include <linux/poison.h>
33 #include <linux/sched.h>
34 #include <linux/slab.h>
35 #include <linux/stat.h>
36 #include <linux/spinlock.h>
37 #include <linux/string.h>
38 #include <linux/types.h>
39 #include <linux/wait.h>
41 #if defined(CONFIG_DEBUG_SLAB) || defined(CONFIG_SLUB_DEBUG_ON)
42 #define DMAPOOL_DEBUG 1
43 #endif
45 struct dma_pool {               /* the pool */
46         struct list_head page_list;
47         spinlock_t lock;
48         size_t size;
49         struct device *dev;
50         size_t allocation;
51         size_t boundary;
52         char name[32];
53         wait_queue_head_t waitq;
54         struct list_head pools;
55 };
57 struct dma_page {               /* cacheable header for 'allocation' bytes */
58         struct list_head page_list;
59         void *vaddr;
60         dma_addr_t dma;
61         unsigned int in_use;
62         unsigned int offset;
63 };
65 #define POOL_TIMEOUT_JIFFIES    ((100 /* msec */ * HZ) / 1000)
67 static DEFINE_MUTEX(pools_lock);
69 static ssize_t
70 show_pools(struct device *dev, struct device_attribute *attr, char *buf)
71 {
72         unsigned temp;
73         unsigned size;
74         char *next;
75         struct dma_page *page;
76         struct dma_pool *pool;
78         next = buf;
79         size = PAGE_SIZE;
81         temp = scnprintf(next, size, "poolinfo - 0.1\n");
82         size -= temp;
83         next += temp;
85         mutex_lock(&pools_lock);
86         list_for_each_entry(pool, &dev->dma_pools, pools) {
87                 unsigned pages = 0;
88                 unsigned blocks = 0;
90                 spin_lock_irq(&pool->lock);
91                 list_for_each_entry(page, &pool->page_list, page_list) {
92                         pages++;
93                         blocks += page->in_use;
94                 }
95                 spin_unlock_irq(&pool->lock);
97                 /* per-pool info, no real statistics yet */
98                 temp = scnprintf(next, size, "%-16s %4u %4Zu %4Zu %2u\n",
99                                  pool->name, blocks,
100                                  pages * (pool->allocation / pool->size),
101                                  pool->size, pages);
102                 size -= temp;
103                 next += temp;
104         }
105         mutex_unlock(&pools_lock);
107         return PAGE_SIZE - size;
110 static DEVICE_ATTR(pools, S_IRUGO, show_pools, NULL);
112 /**
113  * dma_pool_create - Creates a pool of consistent memory blocks, for dma.
114  * @name: name of pool, for diagnostics
115  * @dev: device that will be doing the DMA
116  * @size: size of the blocks in this pool.
117  * @align: alignment requirement for blocks; must be a power of two
118  * @boundary: returned blocks won't cross this power of two boundary
119  * Context: !in_interrupt()
120  *
121  * Returns a dma allocation pool with the requested characteristics, or
122  * null if one can't be created.  Given one of these pools, dma_pool_alloc()
123  * may be used to allocate memory.  Such memory will all have "consistent"
124  * DMA mappings, accessible by the device and its driver without using
125  * cache flushing primitives.  The actual size of blocks allocated may be
126  * larger than requested because of alignment.
127  *
128  * If @boundary is nonzero, objects returned from dma_pool_alloc() won't
129  * cross that size boundary.  This is useful for devices which have
130  * addressing restrictions on individual DMA transfers, such as not crossing
131  * boundaries of 4KBytes.
132  */
133 struct dma_pool *dma_pool_create(const char *name, struct device *dev,
134                                  size_t size, size_t align, size_t boundary)
136         struct dma_pool *retval;
137         size_t allocation;
139         if (align == 0) {
140                 align = 1;
141         } else if (align & (align - 1)) {
142                 return NULL;
143         }
145         if (size == 0) {
146                 return NULL;
147         } else if (size < 4) {
148                 size = 4;
149         }
151         if ((size % align) != 0)
152                 size = ALIGN(size, align);
154         allocation = max_t(size_t, size, PAGE_SIZE);
156         if (!boundary) {
157                 boundary = allocation;
158         } else if ((boundary < size) || (boundary & (boundary - 1))) {
159                 return NULL;
160         }
162         retval = kmalloc_node(sizeof(*retval), GFP_KERNEL, dev_to_node(dev));
163         if (!retval)
164                 return retval;
166         strlcpy(retval->name, name, sizeof(retval->name));
168         retval->dev = dev;
170         INIT_LIST_HEAD(&retval->page_list);
171         spin_lock_init(&retval->lock);
172         retval->size = size;
173         retval->boundary = boundary;
174         retval->allocation = allocation;
175         init_waitqueue_head(&retval->waitq);
177         if (dev) {
178                 int ret;
180                 mutex_lock(&pools_lock);
181                 if (list_empty(&dev->dma_pools))
182                         ret = device_create_file(dev, &dev_attr_pools);
183                 else
184                         ret = 0;
185                 /* note:  not currently insisting "name" be unique */
186                 if (!ret)
187                         list_add(&retval->pools, &dev->dma_pools);
188                 else {
189                         kfree(retval);
190                         retval = NULL;
191                 }
192                 mutex_unlock(&pools_lock);
193         } else
194                 INIT_LIST_HEAD(&retval->pools);
196         return retval;
198 EXPORT_SYMBOL(dma_pool_create);
200 static void pool_initialise_page(struct dma_pool *pool, struct dma_page *page)
202         unsigned int offset = 0;
203         unsigned int next_boundary = pool->boundary;
205         do {
206                 unsigned int next = offset + pool->size;
207                 if (unlikely((next + pool->size) >= next_boundary)) {
208                         next = next_boundary;
209                         next_boundary += pool->boundary;
210                 }
211                 *(int *)(page->vaddr + offset) = next;
212                 offset = next;
213         } while (offset < pool->allocation);
216 static struct dma_page *pool_alloc_page(struct dma_pool *pool, gfp_t mem_flags)
218         struct dma_page *page;
220         page = kmalloc(sizeof(*page), mem_flags);
221         if (!page)
222                 return NULL;
223         page->vaddr = dma_alloc_coherent(pool->dev, pool->allocation,
224                                          &page->dma, mem_flags);
225         if (page->vaddr) {
226 #ifdef  DMAPOOL_DEBUG
227                 memset(page->vaddr, POOL_POISON_FREED, pool->allocation);
228 #endif
229                 pool_initialise_page(pool, page);
230                 list_add(&page->page_list, &pool->page_list);
231                 page->in_use = 0;
232                 page->offset = 0;
233         } else {
234                 kfree(page);
235                 page = NULL;
236         }
237         return page;
240 static inline int is_page_busy(struct dma_page *page)
242         return page->in_use != 0;
245 static void pool_free_page(struct dma_pool *pool, struct dma_page *page)
247         dma_addr_t dma = page->dma;
249 #ifdef  DMAPOOL_DEBUG
250         memset(page->vaddr, POOL_POISON_FREED, pool->allocation);
251 #endif
252         dma_free_coherent(pool->dev, pool->allocation, page->vaddr, dma);
253         list_del(&page->page_list);
254         kfree(page);
257 /**
258  * dma_pool_destroy - destroys a pool of dma memory blocks.
259  * @pool: dma pool that will be destroyed
260  * Context: !in_interrupt()
261  *
262  * Caller guarantees that no more memory from the pool is in use,
263  * and that nothing will try to use the pool after this call.
264  */
265 void dma_pool_destroy(struct dma_pool *pool)
267         mutex_lock(&pools_lock);
268         list_del(&pool->pools);
269         if (pool->dev && list_empty(&pool->dev->dma_pools))
270                 device_remove_file(pool->dev, &dev_attr_pools);
271         mutex_unlock(&pools_lock);
273         while (!list_empty(&pool->page_list)) {
274                 struct dma_page *page;
275                 page = list_entry(pool->page_list.next,
276                                   struct dma_page, page_list);
277                 if (is_page_busy(page)) {
278                         if (pool->dev)
279                                 dev_err(pool->dev,
280                                         "dma_pool_destroy %s, %p busy\n",
281                                         pool->name, page->vaddr);
282                         else
283                                 printk(KERN_ERR
284                                        "dma_pool_destroy %s, %p busy\n",
285                                        pool->name, page->vaddr);
286                         /* leak the still-in-use consistent memory */
287                         list_del(&page->page_list);
288                         kfree(page);
289                 } else
290                         pool_free_page(pool, page);
291         }
293         kfree(pool);
295 EXPORT_SYMBOL(dma_pool_destroy);
297 /**
298  * dma_pool_alloc - get a block of consistent memory
299  * @pool: dma pool that will produce the block
300  * @mem_flags: GFP_* bitmask
301  * @handle: pointer to dma address of block
302  *
303  * This returns the kernel virtual address of a currently unused block,
304  * and reports its dma address through the handle.
305  * If such a memory block can't be allocated, %NULL is returned.
306  */
307 void *dma_pool_alloc(struct dma_pool *pool, gfp_t mem_flags,
308                      dma_addr_t *handle)
310         unsigned long flags;
311         struct dma_page *page;
312         size_t offset;
313         void *retval;
315         might_sleep_if(mem_flags & __GFP_WAIT);
317         spin_lock_irqsave(&pool->lock, flags);
318  restart:
319         list_for_each_entry(page, &pool->page_list, page_list) {
320                 if (page->offset < pool->allocation)
321                         goto ready;
322         }
323         page = pool_alloc_page(pool, GFP_ATOMIC);
324         if (!page) {
325                 if (mem_flags & __GFP_WAIT) {
326                         DECLARE_WAITQUEUE(wait, current);
328                         __set_current_state(TASK_UNINTERRUPTIBLE);
329                         __add_wait_queue(&pool->waitq, &wait);
330                         spin_unlock_irqrestore(&pool->lock, flags);
332                         schedule_timeout(POOL_TIMEOUT_JIFFIES);
334                         spin_lock_irqsave(&pool->lock, flags);
335                         __remove_wait_queue(&pool->waitq, &wait);
336                         goto restart;
337                 }
338                 retval = NULL;
339                 goto done;
340         }
342  ready:
343         page->in_use++;
344         offset = page->offset;
345         page->offset = *(int *)(page->vaddr + offset);
346         retval = offset + page->vaddr;
347         *handle = offset + page->dma;
348 #ifdef  DMAPOOL_DEBUG
349         memset(retval, POOL_POISON_ALLOCATED, pool->size);
350 #endif
351  done:
352         spin_unlock_irqrestore(&pool->lock, flags);
353         return retval;
355 EXPORT_SYMBOL(dma_pool_alloc);
357 static struct dma_page *pool_find_page(struct dma_pool *pool, dma_addr_t dma)
359         struct dma_page *page;
361         list_for_each_entry(page, &pool->page_list, page_list) {
362                 if (dma < page->dma)
363                         continue;
364                 if (dma < (page->dma + pool->allocation))
365                         return page;
366         }
367         return NULL;
370 /**
371  * dma_pool_free - put block back into dma pool
372  * @pool: the dma pool holding the block
373  * @vaddr: virtual address of block
374  * @dma: dma address of block
375  *
376  * Caller promises neither device nor driver will again touch this block
377  * unless it is first re-allocated.
378  */
379 void dma_pool_free(struct dma_pool *pool, void *vaddr, dma_addr_t dma)
381         struct dma_page *page;
382         unsigned long flags;
383         unsigned int offset;
385         spin_lock_irqsave(&pool->lock, flags);
386         page = pool_find_page(pool, dma);
387         if (!page) {
388                 spin_unlock_irqrestore(&pool->lock, flags);
389                 if (pool->dev)
390                         dev_err(pool->dev,
391                                 "dma_pool_free %s, %p/%lx (bad dma)\n",
392                                 pool->name, vaddr, (unsigned long)dma);
393                 else
394                         printk(KERN_ERR "dma_pool_free %s, %p/%lx (bad dma)\n",
395                                pool->name, vaddr, (unsigned long)dma);
396                 return;
397         }
399         offset = vaddr - page->vaddr;
400 #ifdef  DMAPOOL_DEBUG
401         if ((dma - page->dma) != offset) {
402                 spin_unlock_irqrestore(&pool->lock, flags);
403                 if (pool->dev)
404                         dev_err(pool->dev,
405                                 "dma_pool_free %s, %p (bad vaddr)/%Lx\n",
406                                 pool->name, vaddr, (unsigned long long)dma);
407                 else
408                         printk(KERN_ERR
409                                "dma_pool_free %s, %p (bad vaddr)/%Lx\n",
410                                pool->name, vaddr, (unsigned long long)dma);
411                 return;
412         }
413         {
414                 unsigned int chain = page->offset;
415                 while (chain < pool->allocation) {
416                         if (chain != offset) {
417                                 chain = *(int *)(page->vaddr + chain);
418                                 continue;
419                         }
420                         spin_unlock_irqrestore(&pool->lock, flags);
421                         if (pool->dev)
422                                 dev_err(pool->dev, "dma_pool_free %s, dma %Lx "
423                                         "already free\n", pool->name,
424                                         (unsigned long long)dma);
425                         else
426                                 printk(KERN_ERR "dma_pool_free %s, dma %Lx "
427                                         "already free\n", pool->name,
428                                         (unsigned long long)dma);
429                         return;
430                 }
431         }
432         memset(vaddr, POOL_POISON_FREED, pool->size);
433 #endif
435         page->in_use--;
436         *(int *)vaddr = page->offset;
437         page->offset = offset;
438         if (waitqueue_active(&pool->waitq))
439                 wake_up_locked(&pool->waitq);
440         /*
441          * Resist a temptation to do
442          *    if (!is_page_busy(page)) pool_free_page(pool, page);
443          * Better have a few empty pages hang around.
444          */
445         spin_unlock_irqrestore(&pool->lock, flags);
447 EXPORT_SYMBOL(dma_pool_free);
449 /*
450  * Managed DMA pool
451  */
452 static void dmam_pool_release(struct device *dev, void *res)
454         struct dma_pool *pool = *(struct dma_pool **)res;
456         dma_pool_destroy(pool);
459 static int dmam_pool_match(struct device *dev, void *res, void *match_data)
461         return *(struct dma_pool **)res == match_data;
464 /**
465  * dmam_pool_create - Managed dma_pool_create()
466  * @name: name of pool, for diagnostics
467  * @dev: device that will be doing the DMA
468  * @size: size of the blocks in this pool.
469  * @align: alignment requirement for blocks; must be a power of two
470  * @allocation: returned blocks won't cross this boundary (or zero)
471  *
472  * Managed dma_pool_create().  DMA pool created with this function is
473  * automatically destroyed on driver detach.
474  */
475 struct dma_pool *dmam_pool_create(const char *name, struct device *dev,
476                                   size_t size, size_t align, size_t allocation)
478         struct dma_pool **ptr, *pool;
480         ptr = devres_alloc(dmam_pool_release, sizeof(*ptr), GFP_KERNEL);
481         if (!ptr)
482                 return NULL;
484         pool = *ptr = dma_pool_create(name, dev, size, align, allocation);
485         if (pool)
486                 devres_add(dev, ptr);
487         else
488                 devres_free(ptr);
490         return pool;
492 EXPORT_SYMBOL(dmam_pool_create);
494 /**
495  * dmam_pool_destroy - Managed dma_pool_destroy()
496  * @pool: dma pool that will be destroyed
497  *
498  * Managed dma_pool_destroy().
499  */
500 void dmam_pool_destroy(struct dma_pool *pool)
502         struct device *dev = pool->dev;
504         WARN_ON(devres_destroy(dev, dmam_pool_release, dmam_pool_match, pool));
505         dma_pool_destroy(pool);
507 EXPORT_SYMBOL(dmam_pool_destroy);