]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - samples/Kconfig
Merge branch 'v4l_for_linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mchehab...
[sitara-epos/sitara-epos-kernel.git] / samples / Kconfig
1 menuconfig SAMPLES
2         bool "Sample kernel code"
3         help
4           You can build and test sample kernel code here.
6 if SAMPLES
8 config SAMPLE_TRACEPOINTS
9         tristate "Build tracepoints examples -- loadable modules only"
10         depends on TRACEPOINTS && m
11         help
12           This build tracepoints example modules.
14 config SAMPLE_TRACE_EVENTS
15         tristate "Build trace_events examples -- loadable modules only"
16         depends on EVENT_TRACING && m
17         help
18           This build trace event example modules.
20 config SAMPLE_KOBJECT
21         tristate "Build kobject examples -- loadable modules only"
22         depends on m
23         help
24           This config option will allow you to build a number of
25           different kobject sample modules showing how to use kobjects,
26           ksets, and ktypes properly.
28           If in doubt, say "N" here.
30 config SAMPLE_KPROBES
31         tristate "Build kprobes examples -- loadable modules only"
32         depends on KPROBES && m
33         help
34           This build several kprobes example modules.
36 config SAMPLE_KRETPROBES
37         tristate "Build kretprobes example -- loadable modules only"
38         default m
39         depends on SAMPLE_KPROBES && KRETPROBES
41 config SAMPLE_HW_BREAKPOINT
42         tristate "Build kernel hardware breakpoint examples -- loadable module only"
43         depends on HAVE_HW_BREAKPOINT && m
44         help
45           This builds kernel hardware breakpoint example modules.
47 config SAMPLE_KFIFO
48         tristate "Build kfifo examples -- loadable modules only"
49         depends on m
50         help
51           This config option will allow you to build a number of
52           different kfifo sample modules showing how to use the
53           generic kfifo API.
55           If in doubt, say "N" here.
57 config SAMPLE_KDB
58         tristate "Build kdb command example -- loadable modules only"
59         depends on KGDB_KDB && m
60         help
61           Build an example of how to dynamically add the hello
62           command to the kdb shell.
64 endif # SAMPLES