]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - scripts/patch-kernel
arm:omap:am33xx: Reverting gigabit disabling support
[sitara-epos/sitara-epos-kernel.git] / scripts / patch-kernel
1 #! /bin/sh
2 # Script to apply kernel patches.
3 #   usage: patch-kernel [ sourcedir [ patchdir [ stopversion ] [ -acxx ] ] ]
4 #     The source directory defaults to /usr/src/linux, and the patch
5 #     directory defaults to the current directory.
6 # e.g.
7 #   scripts/patch-kernel . ..
8 #      Update the kernel tree in the current directory using patches in the
9 #      directory above to the latest Linus kernel
10 #   scripts/patch-kernel . .. -ac
11 #      Get the latest Linux kernel and patch it with the latest ac patch
12 #   scripts/patch-kernel . .. 2.4.9
13 #      Gets standard kernel 2.4.9
14 #   scripts/patch-kernel . .. 2.4.9 -ac
15 #      Gets 2.4.9 with latest ac patches
16 #   scripts/patch-kernel . .. 2.4.9 -ac11
17 #      Gets 2.4.9 with ac patch ac11
18 #   Note: It uses the patches relative to the Linus kernels, not the
19 #   ac to ac relative patches
20 #
21 # It determines the current kernel version from the top-level Makefile.
22 # It then looks for patches for the next sublevel in the patch directory.
23 # This is applied using "patch -p1 -s" from within the kernel directory.
24 # A check is then made for "*.rej" files to see if the patch was
25 # successful.  If it is, then all of the "*.orig" files are removed.
26 #
27 #       Nick Holloway <Nick.Holloway@alfie.demon.co.uk>, 2nd January 1995.
28 #
29 # Added support for handling multiple types of compression. What includes
30 # gzip, bzip, bzip2, zip, compress, and plaintext. 
31 #
32 #       Adam Sulmicki <adam@cfar.umd.edu>, 1st January 1997.
33 #
34 # Added ability to stop at a given version number
35 # Put the full version number (i.e. 2.3.31) as the last parameter
36 #       Dave Gilbert <linux@treblig.org>, 11th December 1999.
38 # Fixed previous patch so that if we are already at the correct version
39 # not to patch up.
40 #
41 # Added -ac option, use -ac or -ac9 (say) to stop at a particular version
42 #       Dave Gilbert <linux@treblig.org>, 29th September 2001.
43 #
44 # Add support for (use of) EXTRAVERSION (to support 2.6.8.x, e.g.);
45 # update usage message;
46 # fix some whitespace damage;
47 # be smarter about stopping when current version is larger than requested;
48 #       Randy Dunlap <rdunlap@xenotime.net>, 2004-AUG-18.
49 #
50 # Add better support for (non-incremental) 2.6.x.y patches;
51 # If an ending version number if not specified, the script automatically
52 # increments the SUBLEVEL (x in 2.6.x.y) until no more patch files are found;
53 # however, EXTRAVERSION (y in 2.6.x.y) is never automatically incremented
54 # but must be specified fully.
55 #
56 # patch-kernel does not normally support reverse patching, but does so when
57 # applying EXTRAVERSION (x.y) patches, so that moving from 2.6.11.y to 2.6.11.z
58 # is easy and handled by the script (reverse 2.6.11.y and apply 2.6.11.z).
59 #       Randy Dunlap <rdunlap@xenotime.net>, 2005-APR-08.
61 PNAME=patch-kernel
63 # Set directories from arguments, or use defaults.
64 sourcedir=${1-/usr/src/linux}
65 patchdir=${2-.}
66 stopvers=${3-default}
68 if [ "$1" = -h -o "$1" = --help -o ! -r "$sourcedir/Makefile" ]; then
69 cat << USAGE
70 usage: $PNAME [-h] [ sourcedir [ patchdir [ stopversion ] [ -acxx ] ] ]
71   source directory defaults to /usr/src/linux,
72   patch directory defaults to the current directory,
73   stopversion defaults to <all in patchdir>.
74 USAGE
75 exit 1
76 fi
78 # See if we have any -ac options
79 for PARM in $*
80 do
81   case $PARM in
82           -ac*)
83                   gotac=$PARM;
85         esac;
86 done
88 # ---------------------------------------------------------------------------
89 # arg1 is filename
90 noFile () {
91         echo "cannot find patch file: ${patch}"
92         exit 1
93 }
95 # ---------------------------------------------------------------------------
96 backwards () {
97         echo "$PNAME does not support reverse patching"
98         exit 1
99 }
101 # ---------------------------------------------------------------------------
102 # Find a file, first parameter is basename of file
103 # it tries many compression mechanisms and sets variables to say how to get it
104 findFile () {
105   filebase=$1;
107   if [ -r ${filebase}.gz ]; then
108                 ext=".gz"
109                 name="gzip"
110                 uncomp="gunzip -dc"
111   elif [ -r ${filebase}.bz  ]; then
112                 ext=".bz"
113                 name="bzip"
114                 uncomp="bunzip -dc"
115   elif [ -r ${filebase}.bz2 ]; then
116                 ext=".bz2"
117                 name="bzip2"
118                 uncomp="bunzip2 -dc"
119   elif [ -r ${filebase}.zip ]; then
120                 ext=".zip"
121                 name="zip"
122                 uncomp="unzip -d"
123   elif [ -r ${filebase}.Z ]; then
124                 ext=".Z"
125                 name="uncompress"
126                 uncomp="uncompress -c"
127   elif [ -r ${filebase} ]; then
128                 ext=""
129                 name="plaintext"
130                 uncomp="cat"
131   else
132         return 1;
133   fi
135   return 0;
138 # ---------------------------------------------------------------------------
139 # Apply a patch and check it goes in cleanly
140 # First param is patch name (e.g. patch-2.4.9-ac5) - without path or extension
142 applyPatch () {
143   echo -n "Applying $1 (${name})... "
144   if $uncomp ${patchdir}/$1${ext} | patch -p1 -s -N -E -d $sourcedir
145   then
146     echo "done."
147   else
148     echo "failed.  Clean up yourself."
149     return 1;
150   fi
151   if [ "`find $sourcedir/ '(' -name '*.rej' -o -name '.*.rej' ')' -print`" ]
152   then
153     echo "Aborting.  Reject files found."
154     return 1;
155   fi
156   # Remove backup files
157   find $sourcedir/ '(' -name '*.orig' -o -name '.*.orig' ')' -exec rm -f {} \;
158  
159   return 0;
162 # ---------------------------------------------------------------------------
163 # arg1 is patch filename
164 reversePatch () {
165         echo -n "Reversing $1 (${name}) ... "
166         if $uncomp ${patchdir}/"$1"${ext} | patch -p1 -Rs -N -E -d $sourcedir
167         then
168                 echo "done."
169         else
170                 echo "failed.  Clean it up."
171                 exit 1
172         fi
173         if [ "`find $sourcedir/ '(' -name '*.rej' -o -name '.*.rej' ')' -print`" ]
174         then
175                 echo "Aborting.  Reject files found."
176                 return 1
177         fi
178         # Remove backup files
179         find $sourcedir/ '(' -name '*.orig' -o -name '.*.orig' ')' -exec rm -f {} \;
181         return 0
184 # set current VERSION, PATCHLEVEL, SUBLEVEL, EXTRAVERSION
185 # force $TMPFILEs below to be in local directory: a slash character prevents
186 # the dot command from using the search path.
187 TMPFILE=`mktemp ./.tmpver.XXXXXX` || { echo "cannot make temp file" ; exit 1; }
188 grep -E "^(VERSION|PATCHLEVEL|SUBLEVEL|EXTRAVERSION)" $sourcedir/Makefile > $TMPFILE
189 tr -d [:blank:] < $TMPFILE > $TMPFILE.1
190 . $TMPFILE.1
191 rm -f $TMPFILE*
192 if [ -z "$VERSION" -o -z "$PATCHLEVEL" -o -z "$SUBLEVEL" ]
193 then
194     echo "unable to determine current kernel version" >&2
195     exit 1
196 fi
198 NAME=`grep ^NAME $sourcedir/Makefile`
199 NAME=${NAME##*=}
201 echo "Current kernel version is $VERSION.$PATCHLEVEL.$SUBLEVEL${EXTRAVERSION} ($NAME)"
203 # strip EXTRAVERSION to just a number (drop leading '.' and trailing additions)
204 EXTRAVER=
205 if [ x$EXTRAVERSION != "x" ]
206 then
207         EXTRAVER=${EXTRAVERSION#.}
208         EXTRAVER=${EXTRAVER%%[[:punct:]]*}
209         #echo "$PNAME: changing EXTRAVERSION from $EXTRAVERSION to $EXTRAVER"
210 fi
212 #echo "stopvers=$stopvers"
213 if [ $stopvers != "default" ]; then
214         STOPSUBLEVEL=`echo $stopvers | cut -d. -f3`
215         STOPEXTRA=`echo $stopvers | cut -d. -f4`
216         STOPFULLVERSION=${stopvers%%.$STOPEXTRA}
217         #echo "#___STOPSUBLEVEL=/$STOPSUBLEVEL/, STOPEXTRA=/$STOPEXTRA/"
218 else
219         STOPSUBLEVEL=9999
220         STOPEXTRA=9999
221 fi
223 # This all assumes a 2.6.x[.y] kernel tree.
224 # Don't allow backwards/reverse patching.
225 if [ $STOPSUBLEVEL -lt $SUBLEVEL ]; then
226         backwards
227 fi
229 if [ x$EXTRAVER != "x" ]; then
230         CURRENTFULLVERSION="$VERSION.$PATCHLEVEL.$SUBLEVEL.$EXTRAVER"
231 else
232         CURRENTFULLVERSION="$VERSION.$PATCHLEVEL.$SUBLEVEL"
233 fi
235 if [ x$EXTRAVER != "x" ]; then
236         echo "backing up to: $VERSION.$PATCHLEVEL.$SUBLEVEL"
237         patch="patch-${CURRENTFULLVERSION}"
238         findFile $patchdir/${patch} || noFile ${patch}
239         reversePatch ${patch} || exit 1
240 fi
242 # now current is 2.6.x, with no EXTRA applied,
243 # so update to target SUBLEVEL (2.6.SUBLEVEL)
244 # and then to target EXTRAVER (2.6.SUB.EXTRAVER) if requested.
245 # If not ending sublevel is specified, it is incremented until
246 # no further sublevels are found.
248 if [ $STOPSUBLEVEL -gt $SUBLEVEL ]; then
249 while :                         # incrementing SUBLEVEL (s in v.p.s)
250 do
251     CURRENTFULLVERSION="$VERSION.$PATCHLEVEL.$SUBLEVEL"
252     EXTRAVER=
253     if [ x$STOPFULLVERSION = x$CURRENTFULLVERSION ]; then
254         echo "Stopping at $CURRENTFULLVERSION base as requested."
255         break
256     fi
258     SUBLEVEL=$(($SUBLEVEL + 1))
259     FULLVERSION="$VERSION.$PATCHLEVEL.$SUBLEVEL"
260     #echo "#___ trying $FULLVERSION ___"
262     if [ $(($SUBLEVEL)) -gt $(($STOPSUBLEVEL)) ]; then
263         echo "Stopping since sublevel ($SUBLEVEL) is beyond stop-sublevel ($STOPSUBLEVEL)"
264         exit 1
265     fi
267     patch=patch-$FULLVERSION
268     # See if the file exists and find extension
269     findFile $patchdir/${patch} || noFile ${patch}
271     # Apply the patch and check all is OK
272     applyPatch $patch || break
273 done
274 #echo "#___sublevel all done"
275 fi
277 # There is no incremental searching for extraversion...
278 if [ "$STOPEXTRA" != "" ]; then
279 while :                         # just to allow break
280 do
281 # apply STOPEXTRA directly (not incrementally) (x in v.p.s.x)
282         FULLVERSION="$VERSION.$PATCHLEVEL.$SUBLEVEL.$STOPEXTRA"
283         #echo "#... trying $FULLVERSION ..."
284         patch=patch-$FULLVERSION
286         # See if the file exists and find extension
287         findFile $patchdir/${patch} || noFile ${patch}
289         # Apply the patch and check all is OK
290         applyPatch $patch || break
291         #echo "#___extraver all done"
292         break
293 done
294 fi
296 if [ x$gotac != x ]; then
297   # Out great user wants the -ac patches
298         # They could have done -ac (get latest) or -acxx where xx=version they want
299         if [ $gotac = "-ac" ]; then
300           # They want the latest version
301                 HIGHESTPATCH=0
302                 for PATCHNAMES in $patchdir/patch-${CURRENTFULLVERSION}-ac*\.*
303                 do
304                         ACVALUE=`echo $PATCHNAMES | sed -e 's/^.*patch-[0-9.]*-ac\([0-9]*\).*/\1/'`
305                         # Check it is actually a recognised patch type
306                         findFile $patchdir/patch-${CURRENTFULLVERSION}-ac${ACVALUE} || break
308                   if [ $ACVALUE -gt $HIGHESTPATCH ]; then
309                           HIGHESTPATCH=$ACVALUE
310                   fi
311                 done
313                 if [ $HIGHESTPATCH -ne 0 ]; then
314                         findFile $patchdir/patch-${CURRENTFULLVERSION}-ac${HIGHESTPATCH} || break
315                         applyPatch patch-${CURRENTFULLVERSION}-ac${HIGHESTPATCH}
316                 else
317                   echo "No -ac patches found"
318                 fi
319         else
320           # They want an exact version
321                 findFile $patchdir/patch-${CURRENTFULLVERSION}${gotac} || {
322                   echo "Sorry, I couldn't find the $gotac patch for $CURRENTFULLVERSION.  Hohum."
323                         exit 1
324                 }
325                 applyPatch patch-${CURRENTFULLVERSION}${gotac}
326         fi
327 fi