1 /* Common capabilities, needed by capability.o.
2 *
3 * This program is free software; you can redistribute it and/or modify
4 * it under the terms of the GNU General Public License as published by
5 * the Free Software Foundation; either version 2 of the License, or
6 * (at your option) any later version.
7 *
8 */
10 #include <linux/capability.h>
11 #include <linux/audit.h>
12 #include <linux/module.h>
13 #include <linux/init.h>
14 #include <linux/kernel.h>
15 #include <linux/security.h>
16 #include <linux/file.h>
17 #include <linux/mm.h>
18 #include <linux/mman.h>
19 #include <linux/pagemap.h>
20 #include <linux/swap.h>
21 #include <linux/skbuff.h>
22 #include <linux/netlink.h>
23 #include <linux/ptrace.h>
24 #include <linux/xattr.h>
25 #include <linux/hugetlb.h>
26 #include <linux/mount.h>
27 #include <linux/sched.h>
28 #include <linux/prctl.h>
29 #include <linux/securebits.h>
30 #include <linux/user_namespace.h>
32 /*
33 * If a non-root user executes a setuid-root binary in
34 * !secure(SECURE_NOROOT) mode, then we raise capabilities.
35 * However if fE is also set, then the intent is for only
36 * the file capabilities to be applied, and the setuid-root
37 * bit is left on either to change the uid (plausible) or
38 * to get full privilege on a kernel without file capabilities
39 * support. So in that case we do not raise capabilities.
40 *
41 * Warn if that happens, once per boot.
42 */
43 static void warn_setuid_and_fcaps_mixed(const char *fname)
44 {
45 static int warned;
46 if (!warned) {
47 printk(KERN_INFO "warning: `%s' has both setuid-root and"
48 " effective capabilities. Therefore not raising all"
49 " capabilities.\n", fname);
50 warned = 1;
51 }
52 }
54 int cap_netlink_send(struct sock *sk, struct sk_buff *skb)
55 {
56 return 0;
57 }
59 int cap_netlink_recv(struct sk_buff *skb, int cap)
60 {
61 if (!cap_raised(current_cap(), cap))
62 return -EPERM;
63 return 0;
64 }
65 EXPORT_SYMBOL(cap_netlink_recv);
67 /**
68 * cap_capable - Determine whether a task has a particular effective capability
69 * @tsk: The task to query
70 * @cred: The credentials to use
71 * @ns: The user namespace in which we need the capability
72 * @cap: The capability to check for
73 * @audit: Whether to write an audit message or not
74 *
75 * Determine whether the nominated task has the specified capability amongst
76 * its effective set, returning 0 if it does, -ve if it does not.
77 *
78 * NOTE WELL: cap_has_capability() cannot be used like the kernel's capable()
79 * and has_capability() functions. That is, it has the reverse semantics:
80 * cap_has_capability() returns 0 when a task has a capability, but the
81 * kernel's capable() and has_capability() returns 1 for this case.
82 */
83 int cap_capable(struct task_struct *tsk, const struct cred *cred,
84 struct user_namespace *targ_ns, int cap, int audit)
85 {
86 for (;;) {
87 /* The creator of the user namespace has all caps. */
88 if (targ_ns != &init_user_ns && targ_ns->creator == cred->user)
89 return 0;
91 /* Do we have the necessary capabilities? */
92 if (targ_ns == cred->user->user_ns)
93 return cap_raised(cred->cap_effective, cap) ? 0 : -EPERM;
95 /* Have we tried all of the parent namespaces? */
96 if (targ_ns == &init_user_ns)
97 return -EPERM;
99 /*
100 *If you have a capability in a parent user ns, then you have
101 * it over all children user namespaces as well.
102 */
103 targ_ns = targ_ns->creator->user_ns;
104 }
106 /* We never get here */
107 }
109 /**
110 * cap_settime - Determine whether the current process may set the system clock
111 * @ts: The time to set
112 * @tz: The timezone to set
113 *
114 * Determine whether the current process may set the system clock and timezone
115 * information, returning 0 if permission granted, -ve if denied.
116 */
117 int cap_settime(const struct timespec *ts, const struct timezone *tz)
118 {
119 if (!capable(CAP_SYS_TIME))
120 return -EPERM;
121 return 0;
122 }
124 /**
125 * cap_ptrace_access_check - Determine whether the current process may access
126 * another
127 * @child: The process to be accessed
128 * @mode: The mode of attachment.
129 *
130 * If we are in the same or an ancestor user_ns and have all the target
131 * task's capabilities, then ptrace access is allowed.
132 * If we have the ptrace capability to the target user_ns, then ptrace
133 * access is allowed.
134 * Else denied.
135 *
136 * Determine whether a process may access another, returning 0 if permission
137 * granted, -ve if denied.
138 */
139 int cap_ptrace_access_check(struct task_struct *child, unsigned int mode)
140 {
141 int ret = 0;
142 const struct cred *cred, *child_cred;
144 rcu_read_lock();
145 cred = current_cred();
146 child_cred = __task_cred(child);
147 if (cred->user->user_ns == child_cred->user->user_ns &&
148 cap_issubset(child_cred->cap_permitted, cred->cap_permitted))
149 goto out;
150 if (ns_capable(child_cred->user->user_ns, CAP_SYS_PTRACE))
151 goto out;
152 ret = -EPERM;
153 out:
154 rcu_read_unlock();
155 return ret;
156 }
158 /**
159 * cap_ptrace_traceme - Determine whether another process may trace the current
160 * @parent: The task proposed to be the tracer
161 *
162 * If parent is in the same or an ancestor user_ns and has all current's
163 * capabilities, then ptrace access is allowed.
164 * If parent has the ptrace capability to current's user_ns, then ptrace
165 * access is allowed.
166 * Else denied.
167 *
168 * Determine whether the nominated task is permitted to trace the current
169 * process, returning 0 if permission is granted, -ve if denied.
170 */
171 int cap_ptrace_traceme(struct task_struct *parent)
172 {
173 int ret = 0;
174 const struct cred *cred, *child_cred;
176 rcu_read_lock();
177 cred = __task_cred(parent);
178 child_cred = current_cred();
179 if (cred->user->user_ns == child_cred->user->user_ns &&
180 cap_issubset(child_cred->cap_permitted, cred->cap_permitted))
181 goto out;
182 if (has_ns_capability(parent, child_cred->user->user_ns, CAP_SYS_PTRACE))
183 goto out;
184 ret = -EPERM;
185 out:
186 rcu_read_unlock();
187 return ret;
188 }
190 /**
191 * cap_capget - Retrieve a task's capability sets
192 * @target: The task from which to retrieve the capability sets
193 * @effective: The place to record the effective set
194 * @inheritable: The place to record the inheritable set
195 * @permitted: The place to record the permitted set
196 *
197 * This function retrieves the capabilities of the nominated task and returns
198 * them to the caller.
199 */
200 int cap_capget(struct task_struct *target, kernel_cap_t *effective,
201 kernel_cap_t *inheritable, kernel_cap_t *permitted)
202 {
203 const struct cred *cred;
205 /* Derived from kernel/capability.c:sys_capget. */
206 rcu_read_lock();
207 cred = __task_cred(target);
208 *effective = cred->cap_effective;
209 *inheritable = cred->cap_inheritable;
210 *permitted = cred->cap_permitted;
211 rcu_read_unlock();
212 return 0;
213 }
215 /*
216 * Determine whether the inheritable capabilities are limited to the old
217 * permitted set. Returns 1 if they are limited, 0 if they are not.
218 */
219 static inline int cap_inh_is_capped(void)
220 {
222 /* they are so limited unless the current task has the CAP_SETPCAP
223 * capability
224 */
225 if (cap_capable(current, current_cred(),
226 current_cred()->user->user_ns, CAP_SETPCAP,
227 SECURITY_CAP_AUDIT) == 0)
228 return 0;
229 return 1;
230 }
232 /**
233 * cap_capset - Validate and apply proposed changes to current's capabilities
234 * @new: The proposed new credentials; alterations should be made here
235 * @old: The current task's current credentials
236 * @effective: A pointer to the proposed new effective capabilities set
237 * @inheritable: A pointer to the proposed new inheritable capabilities set
238 * @permitted: A pointer to the proposed new permitted capabilities set
239 *
240 * This function validates and applies a proposed mass change to the current
241 * process's capability sets. The changes are made to the proposed new
242 * credentials, and assuming no error, will be committed by the caller of LSM.
243 */
244 int cap_capset(struct cred *new,
245 const struct cred *old,
246 const kernel_cap_t *effective,
247 const kernel_cap_t *inheritable,
248 const kernel_cap_t *permitted)
249 {
250 if (cap_inh_is_capped() &&
251 !cap_issubset(*inheritable,
252 cap_combine(old->cap_inheritable,
253 old->cap_permitted)))
254 /* incapable of using this inheritable set */
255 return -EPERM;
257 if (!cap_issubset(*inheritable,
258 cap_combine(old->cap_inheritable,
259 old->cap_bset)))
260 /* no new pI capabilities outside bounding set */
261 return -EPERM;
263 /* verify restrictions on target's new Permitted set */
264 if (!cap_issubset(*permitted, old->cap_permitted))
265 return -EPERM;
267 /* verify the _new_Effective_ is a subset of the _new_Permitted_ */
268 if (!cap_issubset(*effective, *permitted))
269 return -EPERM;
271 new->cap_effective = *effective;
272 new->cap_inheritable = *inheritable;
273 new->cap_permitted = *permitted;
274 return 0;
275 }
277 /*
278 * Clear proposed capability sets for execve().
279 */
280 static inline void bprm_clear_caps(struct linux_binprm *bprm)
281 {
282 cap_clear(bprm->cred->cap_permitted);
283 bprm->cap_effective = false;
284 }
286 /**
287 * cap_inode_need_killpriv - Determine if inode change affects privileges
288 * @dentry: The inode/dentry in being changed with change marked ATTR_KILL_PRIV
289 *
290 * Determine if an inode having a change applied that's marked ATTR_KILL_PRIV
291 * affects the security markings on that inode, and if it is, should
292 * inode_killpriv() be invoked or the change rejected?
293 *
294 * Returns 0 if granted; +ve if granted, but inode_killpriv() is required; and
295 * -ve to deny the change.
296 */
297 int cap_inode_need_killpriv(struct dentry *dentry)
298 {
299 struct inode *inode = dentry->d_inode;
300 int error;
302 if (!inode->i_op->getxattr)
303 return 0;
305 error = inode->i_op->getxattr(dentry, XATTR_NAME_CAPS, NULL, 0);
306 if (error <= 0)
307 return 0;
308 return 1;
309 }
311 /**
312 * cap_inode_killpriv - Erase the security markings on an inode
313 * @dentry: The inode/dentry to alter
314 *
315 * Erase the privilege-enhancing security markings on an inode.
316 *
317 * Returns 0 if successful, -ve on error.
318 */
319 int cap_inode_killpriv(struct dentry *dentry)
320 {
321 struct inode *inode = dentry->d_inode;
323 if (!inode->i_op->removexattr)
324 return 0;
326 return inode->i_op->removexattr(dentry, XATTR_NAME_CAPS);
327 }
329 /*
330 * Calculate the new process capability sets from the capability sets attached
331 * to a file.
332 */
333 static inline int bprm_caps_from_vfs_caps(struct cpu_vfs_cap_data *caps,
334 struct linux_binprm *bprm,
335 bool *effective,
336 bool *has_cap)
337 {
338 struct cred *new = bprm->cred;
339 unsigned i;
340 int ret = 0;
342 if (caps->magic_etc & VFS_CAP_FLAGS_EFFECTIVE)
343 *effective = true;
345 if (caps->magic_etc & VFS_CAP_REVISION_MASK)
346 *has_cap = true;
348 CAP_FOR_EACH_U32(i) {
349 __u32 permitted = caps->permitted.cap[i];
350 __u32 inheritable = caps->inheritable.cap[i];
352 /*
353 * pP' = (X & fP) | (pI & fI)
354 */
355 new->cap_permitted.cap[i] =
356 (new->cap_bset.cap[i] & permitted) |
357 (new->cap_inheritable.cap[i] & inheritable);
359 if (permitted & ~new->cap_permitted.cap[i])
360 /* insufficient to execute correctly */
361 ret = -EPERM;
362 }
364 /*
365 * For legacy apps, with no internal support for recognizing they
366 * do not have enough capabilities, we return an error if they are
367 * missing some "forced" (aka file-permitted) capabilities.
368 */
369 return *effective ? ret : 0;
370 }
372 /*
373 * Extract the on-exec-apply capability sets for an executable file.
374 */
375 int get_vfs_caps_from_disk(const struct dentry *dentry, struct cpu_vfs_cap_data *cpu_caps)
376 {
377 struct inode *inode = dentry->d_inode;
378 __u32 magic_etc;
379 unsigned tocopy, i;
380 int size;
381 struct vfs_cap_data caps;
383 memset(cpu_caps, 0, sizeof(struct cpu_vfs_cap_data));
385 if (!inode || !inode->i_op->getxattr)
386 return -ENODATA;
388 size = inode->i_op->getxattr((struct dentry *)dentry, XATTR_NAME_CAPS, &caps,
389 XATTR_CAPS_SZ);
390 if (size == -ENODATA || size == -EOPNOTSUPP)
391 /* no data, that's ok */
392 return -ENODATA;
393 if (size < 0)
394 return size;
396 if (size < sizeof(magic_etc))
397 return -EINVAL;
399 cpu_caps->magic_etc = magic_etc = le32_to_cpu(caps.magic_etc);
401 switch (magic_etc & VFS_CAP_REVISION_MASK) {
402 case VFS_CAP_REVISION_1:
403 if (size != XATTR_CAPS_SZ_1)
404 return -EINVAL;
405 tocopy = VFS_CAP_U32_1;
406 break;
407 case VFS_CAP_REVISION_2:
408 if (size != XATTR_CAPS_SZ_2)
409 return -EINVAL;
410 tocopy = VFS_CAP_U32_2;
411 break;
412 default:
413 return -EINVAL;
414 }
416 CAP_FOR_EACH_U32(i) {
417 if (i >= tocopy)
418 break;
419 cpu_caps->permitted.cap[i] = le32_to_cpu(caps.data[i].permitted);
420 cpu_caps->inheritable.cap[i] = le32_to_cpu(caps.data[i].inheritable);
421 }
423 return 0;
424 }
426 /*
427 * Attempt to get the on-exec apply capability sets for an executable file from
428 * its xattrs and, if present, apply them to the proposed credentials being
429 * constructed by execve().
430 */
431 static int get_file_caps(struct linux_binprm *bprm, bool *effective, bool *has_cap)
432 {
433 struct dentry *dentry;
434 int rc = 0;
435 struct cpu_vfs_cap_data vcaps;
437 bprm_clear_caps(bprm);
439 if (!file_caps_enabled)
440 return 0;
442 if (bprm->file->f_vfsmnt->mnt_flags & MNT_NOSUID)
443 return 0;
445 dentry = dget(bprm->file->f_dentry);
447 rc = get_vfs_caps_from_disk(dentry, &vcaps);
448 if (rc < 0) {
449 if (rc == -EINVAL)
450 printk(KERN_NOTICE "%s: get_vfs_caps_from_disk returned %d for %s\n",
451 __func__, rc, bprm->filename);
452 else if (rc == -ENODATA)
453 rc = 0;
454 goto out;
455 }
457 rc = bprm_caps_from_vfs_caps(&vcaps, bprm, effective, has_cap);
458 if (rc == -EINVAL)
459 printk(KERN_NOTICE "%s: cap_from_disk returned %d for %s\n",
460 __func__, rc, bprm->filename);
462 out:
463 dput(dentry);
464 if (rc)
465 bprm_clear_caps(bprm);
467 return rc;
468 }
470 /**
471 * cap_bprm_set_creds - Set up the proposed credentials for execve().
472 * @bprm: The execution parameters, including the proposed creds
473 *
474 * Set up the proposed credentials for a new execution context being
475 * constructed by execve(). The proposed creds in @bprm->cred is altered,
476 * which won't take effect immediately. Returns 0 if successful, -ve on error.
477 */
478 int cap_bprm_set_creds(struct linux_binprm *bprm)
479 {
480 const struct cred *old = current_cred();
481 struct cred *new = bprm->cred;
482 bool effective, has_cap = false;
483 int ret;
485 effective = false;
486 ret = get_file_caps(bprm, &effective, &has_cap);
487 if (ret < 0)
488 return ret;
490 if (!issecure(SECURE_NOROOT)) {
491 /*
492 * If the legacy file capability is set, then don't set privs
493 * for a setuid root binary run by a non-root user. Do set it
494 * for a root user just to cause least surprise to an admin.
495 */
496 if (has_cap && new->uid != 0 && new->euid == 0) {
497 warn_setuid_and_fcaps_mixed(bprm->filename);
498 goto skip;
499 }
500 /*
501 * To support inheritance of root-permissions and suid-root
502 * executables under compatibility mode, we override the
503 * capability sets for the file.
504 *
505 * If only the real uid is 0, we do not set the effective bit.
506 */
507 if (new->euid == 0 || new->uid == 0) {
508 /* pP' = (cap_bset & ~0) | (pI & ~0) */
509 new->cap_permitted = cap_combine(old->cap_bset,
510 old->cap_inheritable);
511 }
512 if (new->euid == 0)
513 effective = true;
514 }
515 skip:
517 /* Don't let someone trace a set[ug]id/setpcap binary with the revised
518 * credentials unless they have the appropriate permit
519 */
520 if ((new->euid != old->uid ||
521 new->egid != old->gid ||
522 !cap_issubset(new->cap_permitted, old->cap_permitted)) &&
523 bprm->unsafe & ~LSM_UNSAFE_PTRACE_CAP) {
524 /* downgrade; they get no more than they had, and maybe less */
525 if (!capable(CAP_SETUID)) {
526 new->euid = new->uid;
527 new->egid = new->gid;
528 }
529 new->cap_permitted = cap_intersect(new->cap_permitted,
530 old->cap_permitted);
531 }
533 new->suid = new->fsuid = new->euid;
534 new->sgid = new->fsgid = new->egid;
536 if (effective)
537 new->cap_effective = new->cap_permitted;
538 else
539 cap_clear(new->cap_effective);
540 bprm->cap_effective = effective;
542 /*
543 * Audit candidate if current->cap_effective is set
544 *
545 * We do not bother to audit if 3 things are true:
546 * 1) cap_effective has all caps
547 * 2) we are root
548 * 3) root is supposed to have all caps (SECURE_NOROOT)
549 * Since this is just a normal root execing a process.
550 *
551 * Number 1 above might fail if you don't have a full bset, but I think
552 * that is interesting information to audit.
553 */
554 if (!cap_isclear(new->cap_effective)) {
555 if (!cap_issubset(CAP_FULL_SET, new->cap_effective) ||
556 new->euid != 0 || new->uid != 0 ||
557 issecure(SECURE_NOROOT)) {
558 ret = audit_log_bprm_fcaps(bprm, new, old);
559 if (ret < 0)
560 return ret;
561 }
562 }
564 new->securebits &= ~issecure_mask(SECURE_KEEP_CAPS);
565 return 0;
566 }
568 /**
569 * cap_bprm_secureexec - Determine whether a secure execution is required
570 * @bprm: The execution parameters
571 *
572 * Determine whether a secure execution is required, return 1 if it is, and 0
573 * if it is not.
574 *
575 * The credentials have been committed by this point, and so are no longer
576 * available through @bprm->cred.
577 */
578 int cap_bprm_secureexec(struct linux_binprm *bprm)
579 {
580 const struct cred *cred = current_cred();
582 if (cred->uid != 0) {
583 if (bprm->cap_effective)
584 return 1;
585 if (!cap_isclear(cred->cap_permitted))
586 return 1;
587 }
589 return (cred->euid != cred->uid ||
590 cred->egid != cred->gid);
591 }
593 /**
594 * cap_inode_setxattr - Determine whether an xattr may be altered
595 * @dentry: The inode/dentry being altered
596 * @name: The name of the xattr to be changed
597 * @value: The value that the xattr will be changed to
598 * @size: The size of value
599 * @flags: The replacement flag
600 *
601 * Determine whether an xattr may be altered or set on an inode, returning 0 if
602 * permission is granted, -ve if denied.
603 *
604 * This is used to make sure security xattrs don't get updated or set by those
605 * who aren't privileged to do so.
606 */
607 int cap_inode_setxattr(struct dentry *dentry, const char *name,
608 const void *value, size_t size, int flags)
609 {
610 if (!strcmp(name, XATTR_NAME_CAPS)) {
611 if (!capable(CAP_SETFCAP))
612 return -EPERM;
613 return 0;
614 }
616 if (!strncmp(name, XATTR_SECURITY_PREFIX,
617 sizeof(XATTR_SECURITY_PREFIX) - 1) &&
618 !capable(CAP_SYS_ADMIN))
619 return -EPERM;
620 return 0;
621 }
623 /**
624 * cap_inode_removexattr - Determine whether an xattr may be removed
625 * @dentry: The inode/dentry being altered
626 * @name: The name of the xattr to be changed
627 *
628 * Determine whether an xattr may be removed from an inode, returning 0 if
629 * permission is granted, -ve if denied.
630 *
631 * This is used to make sure security xattrs don't get removed by those who
632 * aren't privileged to remove them.
633 */
634 int cap_inode_removexattr(struct dentry *dentry, const char *name)
635 {
636 if (!strcmp(name, XATTR_NAME_CAPS)) {
637 if (!capable(CAP_SETFCAP))
638 return -EPERM;
639 return 0;
640 }
642 if (!strncmp(name, XATTR_SECURITY_PREFIX,
643 sizeof(XATTR_SECURITY_PREFIX) - 1) &&
644 !capable(CAP_SYS_ADMIN))
645 return -EPERM;
646 return 0;
647 }
649 /*
650 * cap_emulate_setxuid() fixes the effective / permitted capabilities of
651 * a process after a call to setuid, setreuid, or setresuid.
652 *
653 * 1) When set*uiding _from_ one of {r,e,s}uid == 0 _to_ all of
654 * {r,e,s}uid != 0, the permitted and effective capabilities are
655 * cleared.
656 *
657 * 2) When set*uiding _from_ euid == 0 _to_ euid != 0, the effective
658 * capabilities of the process are cleared.
659 *
660 * 3) When set*uiding _from_ euid != 0 _to_ euid == 0, the effective
661 * capabilities are set to the permitted capabilities.
662 *
663 * fsuid is handled elsewhere. fsuid == 0 and {r,e,s}uid!= 0 should
664 * never happen.
665 *
666 * -astor
667 *
668 * cevans - New behaviour, Oct '99
669 * A process may, via prctl(), elect to keep its capabilities when it
670 * calls setuid() and switches away from uid==0. Both permitted and
671 * effective sets will be retained.
672 * Without this change, it was impossible for a daemon to drop only some
673 * of its privilege. The call to setuid(!=0) would drop all privileges!
674 * Keeping uid 0 is not an option because uid 0 owns too many vital
675 * files..
676 * Thanks to Olaf Kirch and Peter Benie for spotting this.
677 */
678 static inline void cap_emulate_setxuid(struct cred *new, const struct cred *old)
679 {
680 if ((old->uid == 0 || old->euid == 0 || old->suid == 0) &&
681 (new->uid != 0 && new->euid != 0 && new->suid != 0) &&
682 !issecure(SECURE_KEEP_CAPS)) {
683 cap_clear(new->cap_permitted);
684 cap_clear(new->cap_effective);
685 }
686 if (old->euid == 0 && new->euid != 0)
687 cap_clear(new->cap_effective);
688 if (old->euid != 0 && new->euid == 0)
689 new->cap_effective = new->cap_permitted;
690 }
692 /**
693 * cap_task_fix_setuid - Fix up the results of setuid() call
694 * @new: The proposed credentials
695 * @old: The current task's current credentials
696 * @flags: Indications of what has changed
697 *
698 * Fix up the results of setuid() call before the credential changes are
699 * actually applied, returning 0 to grant the changes, -ve to deny them.
700 */
701 int cap_task_fix_setuid(struct cred *new, const struct cred *old, int flags)
702 {
703 switch (flags) {
704 case LSM_SETID_RE:
705 case LSM_SETID_ID:
706 case LSM_SETID_RES:
707 /* juggle the capabilities to follow [RES]UID changes unless
708 * otherwise suppressed */
709 if (!issecure(SECURE_NO_SETUID_FIXUP))
710 cap_emulate_setxuid(new, old);
711 break;
713 case LSM_SETID_FS:
714 /* juggle the capabilties to follow FSUID changes, unless
715 * otherwise suppressed
716 *
717 * FIXME - is fsuser used for all CAP_FS_MASK capabilities?
718 * if not, we might be a bit too harsh here.
719 */
720 if (!issecure(SECURE_NO_SETUID_FIXUP)) {
721 if (old->fsuid == 0 && new->fsuid != 0)
722 new->cap_effective =
723 cap_drop_fs_set(new->cap_effective);
725 if (old->fsuid != 0 && new->fsuid == 0)
726 new->cap_effective =
727 cap_raise_fs_set(new->cap_effective,
728 new->cap_permitted);
729 }
730 break;
732 default:
733 return -EINVAL;
734 }
736 return 0;
737 }
739 /*
740 * Rationale: code calling task_setscheduler, task_setioprio, and
741 * task_setnice, assumes that
742 * . if capable(cap_sys_nice), then those actions should be allowed
743 * . if not capable(cap_sys_nice), but acting on your own processes,
744 * then those actions should be allowed
745 * This is insufficient now since you can call code without suid, but
746 * yet with increased caps.
747 * So we check for increased caps on the target process.
748 */
749 static int cap_safe_nice(struct task_struct *p)
750 {
751 int is_subset;
753 rcu_read_lock();
754 is_subset = cap_issubset(__task_cred(p)->cap_permitted,
755 current_cred()->cap_permitted);
756 rcu_read_unlock();
758 if (!is_subset && !capable(CAP_SYS_NICE))
759 return -EPERM;
760 return 0;
761 }
763 /**
764 * cap_task_setscheduler - Detemine if scheduler policy change is permitted
765 * @p: The task to affect
766 *
767 * Detemine if the requested scheduler policy change is permitted for the
768 * specified task, returning 0 if permission is granted, -ve if denied.
769 */
770 int cap_task_setscheduler(struct task_struct *p)
771 {
772 return cap_safe_nice(p);
773 }
775 /**
776 * cap_task_ioprio - Detemine if I/O priority change is permitted
777 * @p: The task to affect
778 * @ioprio: The I/O priority to set
779 *
780 * Detemine if the requested I/O priority change is permitted for the specified
781 * task, returning 0 if permission is granted, -ve if denied.
782 */
783 int cap_task_setioprio(struct task_struct *p, int ioprio)
784 {
785 return cap_safe_nice(p);
786 }
788 /**
789 * cap_task_ioprio - Detemine if task priority change is permitted
790 * @p: The task to affect
791 * @nice: The nice value to set
792 *
793 * Detemine if the requested task priority change is permitted for the
794 * specified task, returning 0 if permission is granted, -ve if denied.
795 */
796 int cap_task_setnice(struct task_struct *p, int nice)
797 {
798 return cap_safe_nice(p);
799 }
801 /*
802 * Implement PR_CAPBSET_DROP. Attempt to remove the specified capability from
803 * the current task's bounding set. Returns 0 on success, -ve on error.
804 */
805 static long cap_prctl_drop(struct cred *new, unsigned long cap)
806 {
807 if (!capable(CAP_SETPCAP))
808 return -EPERM;
809 if (!cap_valid(cap))
810 return -EINVAL;
812 cap_lower(new->cap_bset, cap);
813 return 0;
814 }
816 /**
817 * cap_task_prctl - Implement process control functions for this security module
818 * @option: The process control function requested
819 * @arg2, @arg3, @arg4, @arg5: The argument data for this function
820 *
821 * Allow process control functions (sys_prctl()) to alter capabilities; may
822 * also deny access to other functions not otherwise implemented here.
823 *
824 * Returns 0 or +ve on success, -ENOSYS if this function is not implemented
825 * here, other -ve on error. If -ENOSYS is returned, sys_prctl() and other LSM
826 * modules will consider performing the function.
827 */
828 int cap_task_prctl(int option, unsigned long arg2, unsigned long arg3,
829 unsigned long arg4, unsigned long arg5)
830 {
831 struct cred *new;
832 long error = 0;
834 new = prepare_creds();
835 if (!new)
836 return -ENOMEM;
838 switch (option) {
839 case PR_CAPBSET_READ:
840 error = -EINVAL;
841 if (!cap_valid(arg2))
842 goto error;
843 error = !!cap_raised(new->cap_bset, arg2);
844 goto no_change;
846 case PR_CAPBSET_DROP:
847 error = cap_prctl_drop(new, arg2);
848 if (error < 0)
849 goto error;
850 goto changed;
852 /*
853 * The next four prctl's remain to assist with transitioning a
854 * system from legacy UID=0 based privilege (when filesystem
855 * capabilities are not in use) to a system using filesystem
856 * capabilities only - as the POSIX.1e draft intended.
857 *
858 * Note:
859 *
860 * PR_SET_SECUREBITS =
861 * issecure_mask(SECURE_KEEP_CAPS_LOCKED)
862 * | issecure_mask(SECURE_NOROOT)
863 * | issecure_mask(SECURE_NOROOT_LOCKED)
864 * | issecure_mask(SECURE_NO_SETUID_FIXUP)
865 * | issecure_mask(SECURE_NO_SETUID_FIXUP_LOCKED)
866 *
867 * will ensure that the current process and all of its
868 * children will be locked into a pure
869 * capability-based-privilege environment.
870 */
871 case PR_SET_SECUREBITS:
872 error = -EPERM;
873 if ((((new->securebits & SECURE_ALL_LOCKS) >> 1)
874 & (new->securebits ^ arg2)) /*[1]*/
875 || ((new->securebits & SECURE_ALL_LOCKS & ~arg2)) /*[2]*/
876 || (arg2 & ~(SECURE_ALL_LOCKS | SECURE_ALL_BITS)) /*[3]*/
877 || (cap_capable(current, current_cred(),
878 current_cred()->user->user_ns, CAP_SETPCAP,
879 SECURITY_CAP_AUDIT) != 0) /*[4]*/
880 /*
881 * [1] no changing of bits that are locked
882 * [2] no unlocking of locks
883 * [3] no setting of unsupported bits
884 * [4] doing anything requires privilege (go read about
885 * the "sendmail capabilities bug")
886 */
887 )
888 /* cannot change a locked bit */
889 goto error;
890 new->securebits = arg2;
891 goto changed;
893 case PR_GET_SECUREBITS:
894 error = new->securebits;
895 goto no_change;
897 case PR_GET_KEEPCAPS:
898 if (issecure(SECURE_KEEP_CAPS))
899 error = 1;
900 goto no_change;
902 case PR_SET_KEEPCAPS:
903 error = -EINVAL;
904 if (arg2 > 1) /* Note, we rely on arg2 being unsigned here */
905 goto error;
906 error = -EPERM;
907 if (issecure(SECURE_KEEP_CAPS_LOCKED))
908 goto error;
909 if (arg2)
910 new->securebits |= issecure_mask(SECURE_KEEP_CAPS);
911 else
912 new->securebits &= ~issecure_mask(SECURE_KEEP_CAPS);
913 goto changed;
915 default:
916 /* No functionality available - continue with default */
917 error = -ENOSYS;
918 goto error;
919 }
921 /* Functionality provided */
922 changed:
923 return commit_creds(new);
925 no_change:
926 error:
927 abort_creds(new);
928 return error;
929 }
931 /**
932 * cap_vm_enough_memory - Determine whether a new virtual mapping is permitted
933 * @mm: The VM space in which the new mapping is to be made
934 * @pages: The size of the mapping
935 *
936 * Determine whether the allocation of a new virtual mapping by the current
937 * task is permitted, returning 0 if permission is granted, -ve if not.
938 */
939 int cap_vm_enough_memory(struct mm_struct *mm, long pages)
940 {
941 int cap_sys_admin = 0;
943 if (cap_capable(current, current_cred(), &init_user_ns, CAP_SYS_ADMIN,
944 SECURITY_CAP_NOAUDIT) == 0)
945 cap_sys_admin = 1;
946 return __vm_enough_memory(mm, pages, cap_sys_admin);
947 }
949 /*
950 * cap_file_mmap - check if able to map given addr
951 * @file: unused
952 * @reqprot: unused
953 * @prot: unused
954 * @flags: unused
955 * @addr: address attempting to be mapped
956 * @addr_only: unused
957 *
958 * If the process is attempting to map memory below dac_mmap_min_addr they need
959 * CAP_SYS_RAWIO. The other parameters to this function are unused by the
960 * capability security module. Returns 0 if this mapping should be allowed
961 * -EPERM if not.
962 */
963 int cap_file_mmap(struct file *file, unsigned long reqprot,
964 unsigned long prot, unsigned long flags,
965 unsigned long addr, unsigned long addr_only)
966 {
967 int ret = 0;
969 if (addr < dac_mmap_min_addr) {
970 ret = cap_capable(current, current_cred(), &init_user_ns, CAP_SYS_RAWIO,
971 SECURITY_CAP_AUDIT);
972 /* set PF_SUPERPRIV if it turns out we allow the low mmap */
973 if (ret == 0)
974 current->flags |= PF_SUPERPRIV;
975 }
976 return ret;
977 }