1 /*
2 * inode.c - securityfs
3 *
4 * Copyright (C) 2005 Greg Kroah-Hartman <gregkh@suse.de>
5 *
6 * This program is free software; you can redistribute it and/or
7 * modify it under the terms of the GNU General Public License version
8 * 2 as published by the Free Software Foundation.
9 *
10 * Based on fs/debugfs/inode.c which had the following copyright notice:
11 * Copyright (C) 2004 Greg Kroah-Hartman <greg@kroah.com>
12 * Copyright (C) 2004 IBM Inc.
13 */
15 /* #define DEBUG */
16 #include <linux/module.h>
17 #include <linux/fs.h>
18 #include <linux/mount.h>
19 #include <linux/pagemap.h>
20 #include <linux/init.h>
21 #include <linux/namei.h>
22 #include <linux/security.h>
23 #include <linux/magic.h>
25 static struct vfsmount *mount;
26 static int mount_count;
28 /*
29 * TODO:
30 * I think I can get rid of these default_file_ops, but not quite sure...
31 */
32 static ssize_t default_read_file(struct file *file, char __user *buf,
33 size_t count, loff_t *ppos)
34 {
35 return 0;
36 }
38 static ssize_t default_write_file(struct file *file, const char __user *buf,
39 size_t count, loff_t *ppos)
40 {
41 return count;
42 }
44 static int default_open(struct inode *inode, struct file *file)
45 {
46 if (inode->i_private)
47 file->private_data = inode->i_private;
49 return 0;
50 }
52 static const struct file_operations default_file_ops = {
53 .read = default_read_file,
54 .write = default_write_file,
55 .open = default_open,
56 .llseek = noop_llseek,
57 };
59 static struct inode *get_inode(struct super_block *sb, int mode, dev_t dev)
60 {
61 struct inode *inode = new_inode(sb);
63 if (inode) {
64 inode->i_ino = get_next_ino();
65 inode->i_mode = mode;
66 inode->i_atime = inode->i_mtime = inode->i_ctime = CURRENT_TIME;
67 switch (mode & S_IFMT) {
68 default:
69 init_special_inode(inode, mode, dev);
70 break;
71 case S_IFREG:
72 inode->i_fop = &default_file_ops;
73 break;
74 case S_IFDIR:
75 inode->i_op = &simple_dir_inode_operations;
76 inode->i_fop = &simple_dir_operations;
78 /* directory inodes start off with i_nlink == 2 (for "." entry) */
79 inc_nlink(inode);
80 break;
81 }
82 }
83 return inode;
84 }
86 /* SMP-safe */
87 static int mknod(struct inode *dir, struct dentry *dentry,
88 int mode, dev_t dev)
89 {
90 struct inode *inode;
91 int error = -ENOMEM;
93 if (dentry->d_inode)
94 return -EEXIST;
96 inode = get_inode(dir->i_sb, mode, dev);
97 if (inode) {
98 d_instantiate(dentry, inode);
99 dget(dentry);
100 error = 0;
101 }
102 return error;
103 }
105 static int mkdir(struct inode *dir, struct dentry *dentry, int mode)
106 {
107 int res;
109 mode = (mode & (S_IRWXUGO | S_ISVTX)) | S_IFDIR;
110 res = mknod(dir, dentry, mode, 0);
111 if (!res)
112 inc_nlink(dir);
113 return res;
114 }
116 static int create(struct inode *dir, struct dentry *dentry, int mode)
117 {
118 mode = (mode & S_IALLUGO) | S_IFREG;
119 return mknod(dir, dentry, mode, 0);
120 }
122 static inline int positive(struct dentry *dentry)
123 {
124 return dentry->d_inode && !d_unhashed(dentry);
125 }
127 static int fill_super(struct super_block *sb, void *data, int silent)
128 {
129 static struct tree_descr files[] = {{""}};
131 return simple_fill_super(sb, SECURITYFS_MAGIC, files);
132 }
134 static struct dentry *get_sb(struct file_system_type *fs_type,
135 int flags, const char *dev_name,
136 void *data)
137 {
138 return mount_single(fs_type, flags, data, fill_super);
139 }
141 static struct file_system_type fs_type = {
142 .owner = THIS_MODULE,
143 .name = "securityfs",
144 .mount = get_sb,
145 .kill_sb = kill_litter_super,
146 };
148 static int create_by_name(const char *name, mode_t mode,
149 struct dentry *parent,
150 struct dentry **dentry)
151 {
152 int error = 0;
154 *dentry = NULL;
156 /* If the parent is not specified, we create it in the root.
157 * We need the root dentry to do this, which is in the super
158 * block. A pointer to that is in the struct vfsmount that we
159 * have around.
160 */
161 if (!parent)
162 parent = mount->mnt_sb->s_root;
164 mutex_lock(&parent->d_inode->i_mutex);
165 *dentry = lookup_one_len(name, parent, strlen(name));
166 if (!IS_ERR(*dentry)) {
167 if ((mode & S_IFMT) == S_IFDIR)
168 error = mkdir(parent->d_inode, *dentry, mode);
169 else
170 error = create(parent->d_inode, *dentry, mode);
171 if (error)
172 dput(*dentry);
173 } else
174 error = PTR_ERR(*dentry);
175 mutex_unlock(&parent->d_inode->i_mutex);
177 return error;
178 }
180 /**
181 * securityfs_create_file - create a file in the securityfs filesystem
182 *
183 * @name: a pointer to a string containing the name of the file to create.
184 * @mode: the permission that the file should have
185 * @parent: a pointer to the parent dentry for this file. This should be a
186 * directory dentry if set. If this parameter is %NULL, then the
187 * file will be created in the root of the securityfs filesystem.
188 * @data: a pointer to something that the caller will want to get to later
189 * on. The inode.i_private pointer will point to this value on
190 * the open() call.
191 * @fops: a pointer to a struct file_operations that should be used for
192 * this file.
193 *
194 * This is the basic "create a file" function for securityfs. It allows for a
195 * wide range of flexibility in creating a file, or a directory (if you
196 * want to create a directory, the securityfs_create_dir() function is
197 * recommended to be used instead).
198 *
199 * This function returns a pointer to a dentry if it succeeds. This
200 * pointer must be passed to the securityfs_remove() function when the file is
201 * to be removed (no automatic cleanup happens if your module is unloaded,
202 * you are responsible here). If an error occurs, the function will return
203 * the erorr value (via ERR_PTR).
204 *
205 * If securityfs is not enabled in the kernel, the value %-ENODEV is
206 * returned.
207 */
208 struct dentry *securityfs_create_file(const char *name, mode_t mode,
209 struct dentry *parent, void *data,
210 const struct file_operations *fops)
211 {
212 struct dentry *dentry = NULL;
213 int error;
215 pr_debug("securityfs: creating file '%s'\n",name);
217 error = simple_pin_fs(&fs_type, &mount, &mount_count);
218 if (error) {
219 dentry = ERR_PTR(error);
220 goto exit;
221 }
223 error = create_by_name(name, mode, parent, &dentry);
224 if (error) {
225 dentry = ERR_PTR(error);
226 simple_release_fs(&mount, &mount_count);
227 goto exit;
228 }
230 if (dentry->d_inode) {
231 if (fops)
232 dentry->d_inode->i_fop = fops;
233 if (data)
234 dentry->d_inode->i_private = data;
235 }
236 exit:
237 return dentry;
238 }
239 EXPORT_SYMBOL_GPL(securityfs_create_file);
241 /**
242 * securityfs_create_dir - create a directory in the securityfs filesystem
243 *
244 * @name: a pointer to a string containing the name of the directory to
245 * create.
246 * @parent: a pointer to the parent dentry for this file. This should be a
247 * directory dentry if set. If this parameter is %NULL, then the
248 * directory will be created in the root of the securityfs filesystem.
249 *
250 * This function creates a directory in securityfs with the given @name.
251 *
252 * This function returns a pointer to a dentry if it succeeds. This
253 * pointer must be passed to the securityfs_remove() function when the file is
254 * to be removed (no automatic cleanup happens if your module is unloaded,
255 * you are responsible here). If an error occurs, %NULL will be returned.
256 *
257 * If securityfs is not enabled in the kernel, the value %-ENODEV is
258 * returned. It is not wise to check for this value, but rather, check for
259 * %NULL or !%NULL instead as to eliminate the need for #ifdef in the calling
260 * code.
261 */
262 struct dentry *securityfs_create_dir(const char *name, struct dentry *parent)
263 {
264 return securityfs_create_file(name,
265 S_IFDIR | S_IRWXU | S_IRUGO | S_IXUGO,
266 parent, NULL, NULL);
267 }
268 EXPORT_SYMBOL_GPL(securityfs_create_dir);
270 /**
271 * securityfs_remove - removes a file or directory from the securityfs filesystem
272 *
273 * @dentry: a pointer to a the dentry of the file or directory to be removed.
274 *
275 * This function removes a file or directory in securityfs that was previously
276 * created with a call to another securityfs function (like
277 * securityfs_create_file() or variants thereof.)
278 *
279 * This function is required to be called in order for the file to be
280 * removed. No automatic cleanup of files will happen when a module is
281 * removed; you are responsible here.
282 */
283 void securityfs_remove(struct dentry *dentry)
284 {
285 struct dentry *parent;
287 if (!dentry || IS_ERR(dentry))
288 return;
290 parent = dentry->d_parent;
291 if (!parent || !parent->d_inode)
292 return;
294 mutex_lock(&parent->d_inode->i_mutex);
295 if (positive(dentry)) {
296 if (dentry->d_inode) {
297 if (S_ISDIR(dentry->d_inode->i_mode))
298 simple_rmdir(parent->d_inode, dentry);
299 else
300 simple_unlink(parent->d_inode, dentry);
301 dput(dentry);
302 }
303 }
304 mutex_unlock(&parent->d_inode->i_mutex);
305 simple_release_fs(&mount, &mount_count);
306 }
307 EXPORT_SYMBOL_GPL(securityfs_remove);
309 static struct kobject *security_kobj;
311 static int __init securityfs_init(void)
312 {
313 int retval;
315 security_kobj = kobject_create_and_add("security", kernel_kobj);
316 if (!security_kobj)
317 return -EINVAL;
319 retval = register_filesystem(&fs_type);
320 if (retval)
321 kobject_put(security_kobj);
322 return retval;
323 }
325 core_initcall(securityfs_init);
326 MODULE_LICENSE("GPL");