1 menuconfig SOUND
2 tristate "Sound card support"
3 depends on HAS_IOMEM
4 help
5 If you have a sound card in your computer, i.e. if it can say more
6 than an occasional beep, say Y. Be sure to have all the information
7 about your sound card and its configuration down (I/O port,
8 interrupt and DMA channel), because you will be asked for it.
10 You want to read the Sound-HOWTO, available from
11 <http://www.tldp.org/docs.html#howto>. General information about
12 the modular sound system is contained in the files
13 <file:Documentation/sound/oss/Introduction>. The file
14 <file:Documentation/sound/oss/README.OSS> contains some slightly
15 outdated but still useful information as well. Newer sound
16 driver documentation is found in <file:Documentation/sound/alsa/*>.
18 If you have a PnP sound card and you want to configure it at boot
19 time using the ISA PnP tools (read
20 <http://www.roestock.demon.co.uk/isapnptools/>), then you need to
21 compile the sound card support as a module and load that module
22 after the PnP configuration is finished. To do this, choose M here
23 and read <file:Documentation/sound/oss/README.modules>; the module
24 will be called soundcore.
26 if SOUND
28 config SOUND_OSS_CORE
29 bool
30 default n
32 config SOUND_OSS_CORE_PRECLAIM
33 bool "Preclaim OSS device numbers"
34 depends on SOUND_OSS_CORE
35 default y
36 help
37 With this option enabled, the kernel will claim all OSS device
38 numbers if any OSS support (native or emulation) is enabled
39 whether the respective module is loaded or not and try to load the
40 appropriate module using sound-slot/service-* and char-major-*
41 module aliases when one of the device numbers is opened. With
42 this option disabled, kernel will only claim actually in-use
43 device numbers and opening a missing device will generate only the
44 standard char-major-* aliases.
46 The only visible difference is use of additional module aliases
47 and whether OSS sound devices appear multiple times in
48 /proc/devices. sound-slot/service-* module aliases are scheduled
49 to be removed (ie. PRECLAIM won't be available) and this option is
50 to make the transition easier. This option can be overridden
51 during boot using the kernel parameter soundcore.preclaim_oss.
53 Disabling this allows alternative OSS implementations.
55 Please read Documentation/feature-removal-schedule.txt for
56 details.
58 If unsure, say Y.
60 source "sound/oss/dmasound/Kconfig"
62 if !M68K && !UML
64 menuconfig SND
65 tristate "Advanced Linux Sound Architecture"
66 help
67 Say 'Y' or 'M' to enable ALSA (Advanced Linux Sound Architecture),
68 the new base sound system.
70 For more information, see <http://www.alsa-project.org/>
72 if SND
74 source "sound/core/Kconfig"
76 source "sound/drivers/Kconfig"
78 source "sound/isa/Kconfig"
80 source "sound/pci/Kconfig"
82 source "sound/ppc/Kconfig"
84 source "sound/aoa/Kconfig"
86 source "sound/arm/Kconfig"
88 source "sound/atmel/Kconfig"
90 source "sound/spi/Kconfig"
92 source "sound/mips/Kconfig"
94 source "sound/sh/Kconfig"
96 # the following will depend on the order of config.
97 # here assuming USB is defined before ALSA
98 source "sound/usb/Kconfig"
100 source "sound/firewire/Kconfig"
102 # the following will depend on the order of config.
103 # here assuming PCMCIA is defined before ALSA
104 source "sound/pcmcia/Kconfig"
106 source "sound/sparc/Kconfig"
108 source "sound/parisc/Kconfig"
110 source "sound/soc/Kconfig"
112 endif # SND
114 menuconfig SOUND_PRIME
115 tristate "Open Sound System (DEPRECATED)"
116 select SOUND_OSS_CORE
117 help
118 Say 'Y' or 'M' to enable Open Sound System drivers.
120 if SOUND_PRIME
122 source "sound/oss/Kconfig"
124 endif # SOUND_PRIME
126 endif # !M68K
128 endif # SOUND
130 # AC97_BUS is used from both sound and ucb1400
131 config AC97_BUS
132 tristate
133 help
134 This is used to avoid config and link hard dependencies between the
135 sound subsystem and other function drivers completely unrelated to
136 sound although they're sharing the AC97 bus. Concerned drivers
137 should "select" this.