]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/blob - tools/hv/hv_kvp_daemon.c
Merge branch 'stable/vmalloc-3.2' of git://git.kernel.org/pub/scm/linux/kernel/git...
[sitara-epos/sitara-epos-kernel.git] / tools / hv / hv_kvp_daemon.c
1 /*
2  * An implementation of key value pair (KVP) functionality for Linux.
3  *
4  *
5  * Copyright (C) 2010, Novell, Inc.
6  * Author : K. Y. Srinivasan <ksrinivasan@novell.com>
7  *
8  * This program is free software; you can redistribute it and/or modify it
9  * under the terms of the GNU General Public License version 2 as published
10  * by the Free Software Foundation.
11  *
12  * This program is distributed in the hope that it will be useful, but
13  * WITHOUT ANY WARRANTY; without even the implied warranty of
14  * MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE, GOOD TITLE or
15  * NON INFRINGEMENT.  See the GNU General Public License for more
16  * details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA.
21  *
22  */
25 #include <sys/types.h>
26 #include <sys/socket.h>
27 #include <sys/poll.h>
28 #include <sys/utsname.h>
29 #include <linux/types.h>
30 #include <stdio.h>
31 #include <stdlib.h>
32 #include <unistd.h>
33 #include <string.h>
34 #include <errno.h>
35 #include <arpa/inet.h>
36 #include <linux/connector.h>
37 #include <linux/netlink.h>
38 #include <ifaddrs.h>
39 #include <netdb.h>
40 #include <syslog.h>
42 /*
43  * KYS: TODO. Need to register these in the kernel.
44  *
45  * The following definitions are shared with the in-kernel component; do not
46  * change any of this without making the corresponding changes in
47  * the KVP kernel component.
48  */
49 #define CN_KVP_IDX              0x9     /* MSFT KVP functionality */
50 #define CN_KVP_VAL              0x1 /* This supports queries from the kernel */
51 #define CN_KVP_USER_VAL         0x2 /* This supports queries from the user  */
53 /*
54  * KVP protocol: The user mode component first registers with the
55  * the kernel component. Subsequently, the kernel component requests, data
56  * for the specified keys. In response to this message the user mode component
57  * fills in the value corresponding to the specified key. We overload the
58  * sequence field in the cn_msg header to define our KVP message types.
59  *
60  * We use this infrastructure for also supporting queries from user mode
61  * application for state that may be maintained in the KVP kernel component.
62  *
63  * XXXKYS: Have a shared header file between the user and kernel (TODO)
64  */
66 enum kvp_op {
67         KVP_REGISTER = 0, /* Register the user mode component*/
68         KVP_KERNEL_GET, /*Kernel is requesting the value for the specified key*/
69         KVP_KERNEL_SET, /*Kernel is providing the value for the specified key*/
70         KVP_USER_GET, /*User is requesting the value for the specified key*/
71         KVP_USER_SET /*User is providing the value for the specified key*/
72 };
74 #define HV_KVP_EXCHANGE_MAX_KEY_SIZE    512
75 #define HV_KVP_EXCHANGE_MAX_VALUE_SIZE  2048
77 struct hv_ku_msg {
78         __u32   kvp_index;
79         __u8  kvp_key[HV_KVP_EXCHANGE_MAX_KEY_SIZE]; /* Key name */
80         __u8  kvp_value[HV_KVP_EXCHANGE_MAX_VALUE_SIZE]; /* Key  value */
81 };
83 enum key_index {
84         FullyQualifiedDomainName = 0,
85         IntegrationServicesVersion, /*This key is serviced in the kernel*/
86         NetworkAddressIPv4,
87         NetworkAddressIPv6,
88         OSBuildNumber,
89         OSName,
90         OSMajorVersion,
91         OSMinorVersion,
92         OSVersion,
93         ProcessorArchitecture
94 };
96 /*
97  * End of shared definitions.
98  */
100 static char kvp_send_buffer[4096];
101 static char kvp_recv_buffer[4096];
102 static struct sockaddr_nl addr;
104 static char *os_name = "";
105 static char *os_major = "";
106 static char *os_minor = "";
107 static char *processor_arch;
108 static char *os_build;
109 static char *lic_version;
110 static struct utsname uts_buf;
112 void kvp_get_os_info(void)
114         FILE    *file;
115         char    *p, buf[512];
117         uname(&uts_buf);
118         os_build = uts_buf.release;
119         processor_arch = uts_buf.machine;
121         /*
122          * The current windows host (win7) expects the build
123          * string to be of the form: x.y.z
124          * Strip additional information we may have.
125          */
126         p = strchr(os_build, '-');
127         if (p)
128                 *p = '\0';
130         file = fopen("/etc/SuSE-release", "r");
131         if (file != NULL)
132                 goto kvp_osinfo_found;
133         file  = fopen("/etc/redhat-release", "r");
134         if (file != NULL)
135                 goto kvp_osinfo_found;
136         /*
137          * Add code for other supported platforms.
138          */
140         /*
141          * We don't have information about the os.
142          */
143         os_name = uts_buf.sysname;
144         return;
146 kvp_osinfo_found:
147         /* up to three lines */
148         p = fgets(buf, sizeof(buf), file);
149         if (p) {
150                 p = strchr(buf, '\n');
151                 if (p)
152                         *p = '\0';
153                 p = strdup(buf);
154                 if (!p)
155                         goto done;
156                 os_name = p;
158                 /* second line */
159                 p = fgets(buf, sizeof(buf), file);
160                 if (p) {
161                         p = strchr(buf, '\n');
162                         if (p)
163                                 *p = '\0';
164                         p = strdup(buf);
165                         if (!p)
166                                 goto done;
167                         os_major = p;
169                         /* third line */
170                         p = fgets(buf, sizeof(buf), file);
171                         if (p)  {
172                                 p = strchr(buf, '\n');
173                                 if (p)
174                                         *p = '\0';
175                                 p = strdup(buf);
176                                 if (p)
177                                         os_minor = p;
178                         }
179                 }
180         }
182 done:
183         fclose(file);
184         return;
187 static int
188 kvp_get_ip_address(int family, char *buffer, int length)
190         struct ifaddrs *ifap;
191         struct ifaddrs *curp;
192         int ipv4_len = strlen("255.255.255.255") + 1;
193         int ipv6_len = strlen("ffff:ffff:ffff:ffff:ffff:ffff:ffff:ffff")+1;
194         int offset = 0;
195         const char *str;
196         char tmp[50];
197         int error = 0;
199         /*
200          * On entry into this function, the buffer is capable of holding the
201          * maximum key value (2048 bytes).
202          */
204         if (getifaddrs(&ifap)) {
205                 strcpy(buffer, "getifaddrs failed\n");
206                 return 1;
207         }
209         curp = ifap;
210         while (curp != NULL) {
211                 if ((curp->ifa_addr != NULL) &&
212                    (curp->ifa_addr->sa_family == family)) {
213                         if (family == AF_INET) {
214                                 struct sockaddr_in *addr =
215                                 (struct sockaddr_in *) curp->ifa_addr;
217                                 str = inet_ntop(family, &addr->sin_addr,
218                                                 tmp, 50);
219                                 if (str == NULL) {
220                                         strcpy(buffer, "inet_ntop failed\n");
221                                         error = 1;
222                                         goto getaddr_done;
223                                 }
224                                 if (offset == 0)
225                                         strcpy(buffer, tmp);
226                                 else
227                                         strcat(buffer, tmp);
228                                 strcat(buffer, ";");
230                                 offset += strlen(str) + 1;
231                                 if ((length - offset) < (ipv4_len + 1))
232                                         goto getaddr_done;
234                         } else {
236                         /*
237                          * We only support AF_INET and AF_INET6
238                          * and the list of addresses is separated by a ";".
239                          */
240                                 struct sockaddr_in6 *addr =
241                                 (struct sockaddr_in6 *) curp->ifa_addr;
243                                 str = inet_ntop(family,
244                                         &addr->sin6_addr.s6_addr,
245                                         tmp, 50);
246                                 if (str == NULL) {
247                                         strcpy(buffer, "inet_ntop failed\n");
248                                         error = 1;
249                                         goto getaddr_done;
250                                 }
251                                 if (offset == 0)
252                                         strcpy(buffer, tmp);
253                                 else
254                                         strcat(buffer, tmp);
255                                 strcat(buffer, ";");
256                                 offset += strlen(str) + 1;
257                                 if ((length - offset) < (ipv6_len + 1))
258                                         goto getaddr_done;
260                         }
262                 }
263                 curp = curp->ifa_next;
264         }
266 getaddr_done:
267         freeifaddrs(ifap);
268         return error;
272 static int
273 kvp_get_domain_name(char *buffer, int length)
275         struct addrinfo hints, *info ;
276         int error = 0;
278         gethostname(buffer, length);
279         memset(&hints, 0, sizeof(hints));
280         hints.ai_family = AF_INET; /*Get only ipv4 addrinfo. */
281         hints.ai_socktype = SOCK_STREAM;
282         hints.ai_flags = AI_CANONNAME;
284         error = getaddrinfo(buffer, NULL, &hints, &info);
285         if (error != 0) {
286                 strcpy(buffer, "getaddrinfo failed\n");
287                 return error;
288         }
289         strcpy(buffer, info->ai_canonname);
290         freeaddrinfo(info);
291         return error;
294 static int
295 netlink_send(int fd, struct cn_msg *msg)
297         struct nlmsghdr *nlh;
298         unsigned int size;
299         struct msghdr message;
300         char buffer[64];
301         struct iovec iov[2];
303         size = NLMSG_SPACE(sizeof(struct cn_msg) + msg->len);
305         nlh = (struct nlmsghdr *)buffer;
306         nlh->nlmsg_seq = 0;
307         nlh->nlmsg_pid = getpid();
308         nlh->nlmsg_type = NLMSG_DONE;
309         nlh->nlmsg_len = NLMSG_LENGTH(size - sizeof(*nlh));
310         nlh->nlmsg_flags = 0;
312         iov[0].iov_base = nlh;
313         iov[0].iov_len = sizeof(*nlh);
315         iov[1].iov_base = msg;
316         iov[1].iov_len = size;
318         memset(&message, 0, sizeof(message));
319         message.msg_name = &addr;
320         message.msg_namelen = sizeof(addr);
321         message.msg_iov = iov;
322         message.msg_iovlen = 2;
324         return sendmsg(fd, &message, 0);
327 int main(void)
329         int fd, len, sock_opt;
330         int error;
331         struct cn_msg *message;
332         struct pollfd pfd;
333         struct nlmsghdr *incoming_msg;
334         struct cn_msg   *incoming_cn_msg;
335         struct hv_ku_msg *hv_msg;
336         char    *p;
337         char    *key_value;
338         char    *key_name;
340         daemon(1, 0);
341         openlog("KVP", 0, LOG_USER);
342         syslog(LOG_INFO, "KVP starting; pid is:%d", getpid());
343         /*
344          * Retrieve OS release information.
345          */
346         kvp_get_os_info();
348         fd = socket(AF_NETLINK, SOCK_DGRAM, NETLINK_CONNECTOR);
349         if (fd < 0) {
350                 syslog(LOG_ERR, "netlink socket creation failed; error:%d", fd);
351                 exit(-1);
352         }
353         addr.nl_family = AF_NETLINK;
354         addr.nl_pad = 0;
355         addr.nl_pid = 0;
356         addr.nl_groups = CN_KVP_IDX;
359         error = bind(fd, (struct sockaddr *)&addr, sizeof(addr));
360         if (error < 0) {
361                 syslog(LOG_ERR, "bind failed; error:%d", error);
362                 close(fd);
363                 exit(-1);
364         }
365         sock_opt = addr.nl_groups;
366         setsockopt(fd, 270, 1, &sock_opt, sizeof(sock_opt));
367         /*
368          * Register ourselves with the kernel.
369          */
370         message = (struct cn_msg *)kvp_send_buffer;
371         message->id.idx = CN_KVP_IDX;
372         message->id.val = CN_KVP_VAL;
373         message->seq = KVP_REGISTER;
374         message->ack = 0;
375         message->len = 0;
377         len = netlink_send(fd, message);
378         if (len < 0) {
379                 syslog(LOG_ERR, "netlink_send failed; error:%d", len);
380                 close(fd);
381                 exit(-1);
382         }
384         pfd.fd = fd;
386         while (1) {
387                 pfd.events = POLLIN;
388                 pfd.revents = 0;
389                 poll(&pfd, 1, -1);
391                 len = recv(fd, kvp_recv_buffer, sizeof(kvp_recv_buffer), 0);
393                 if (len < 0) {
394                         syslog(LOG_ERR, "recv failed; error:%d", len);
395                         close(fd);
396                         return -1;
397                 }
399                 incoming_msg = (struct nlmsghdr *)kvp_recv_buffer;
400                 incoming_cn_msg = (struct cn_msg *)NLMSG_DATA(incoming_msg);
402                 switch (incoming_cn_msg->seq) {
403                 case KVP_REGISTER:
404                         /*
405                          * Driver is registering with us; stash away the version
406                          * information.
407                          */
408                         p = (char *)incoming_cn_msg->data;
409                         lic_version = malloc(strlen(p) + 1);
410                         if (lic_version) {
411                                 strcpy(lic_version, p);
412                                 syslog(LOG_INFO, "KVP LIC Version: %s",
413                                         lic_version);
414                         } else {
415                                 syslog(LOG_ERR, "malloc failed");
416                         }
417                         continue;
419                 case KVP_KERNEL_GET:
420                         break;
421                 default:
422                         continue;
423                 }
425                 hv_msg = (struct hv_ku_msg *)incoming_cn_msg->data;
426                 key_name = (char *)hv_msg->kvp_key;
427                 key_value = (char *)hv_msg->kvp_value;
429                 switch (hv_msg->kvp_index) {
430                 case FullyQualifiedDomainName:
431                         kvp_get_domain_name(key_value,
432                                         HV_KVP_EXCHANGE_MAX_VALUE_SIZE);
433                         strcpy(key_name, "FullyQualifiedDomainName");
434                         break;
435                 case IntegrationServicesVersion:
436                         strcpy(key_name, "IntegrationServicesVersion");
437                         strcpy(key_value, lic_version);
438                         break;
439                 case NetworkAddressIPv4:
440                         kvp_get_ip_address(AF_INET, key_value,
441                                         HV_KVP_EXCHANGE_MAX_VALUE_SIZE);
442                         strcpy(key_name, "NetworkAddressIPv4");
443                         break;
444                 case NetworkAddressIPv6:
445                         kvp_get_ip_address(AF_INET6, key_value,
446                                         HV_KVP_EXCHANGE_MAX_VALUE_SIZE);
447                         strcpy(key_name, "NetworkAddressIPv6");
448                         break;
449                 case OSBuildNumber:
450                         strcpy(key_value, os_build);
451                         strcpy(key_name, "OSBuildNumber");
452                         break;
453                 case OSName:
454                         strcpy(key_value, os_name);
455                         strcpy(key_name, "OSName");
456                         break;
457                 case OSMajorVersion:
458                         strcpy(key_value, os_major);
459                         strcpy(key_name, "OSMajorVersion");
460                         break;
461                 case OSMinorVersion:
462                         strcpy(key_value, os_minor);
463                         strcpy(key_name, "OSMinorVersion");
464                         break;
465                 case OSVersion:
466                         strcpy(key_value, os_build);
467                         strcpy(key_name, "OSVersion");
468                         break;
469                 case ProcessorArchitecture:
470                         strcpy(key_value, processor_arch);
471                         strcpy(key_name, "ProcessorArchitecture");
472                         break;
473                 default:
474                         strcpy(key_value, "Unknown Key");
475                         /*
476                          * We use a null key name to terminate enumeration.
477                          */
478                         strcpy(key_name, "");
479                         break;
480                 }
481                 /*
482                  * Send the value back to the kernel. The response is
483                  * already in the receive buffer. Update the cn_msg header to
484                  * reflect the key value that has been added to the message
485                  */
487                 incoming_cn_msg->id.idx = CN_KVP_IDX;
488                 incoming_cn_msg->id.val = CN_KVP_VAL;
489                 incoming_cn_msg->seq = KVP_USER_SET;
490                 incoming_cn_msg->ack = 0;
491                 incoming_cn_msg->len = sizeof(struct hv_ku_msg);
493                 len = netlink_send(fd, incoming_cn_msg);
494                 if (len < 0) {
495                         syslog(LOG_ERR, "net_link send failed; error:%d", len);
496                         exit(-1);
497                 }
498         }