1 /*
2 * An implementation of key value pair (KVP) functionality for Linux.
3 *
4 *
5 * Copyright (C) 2010, Novell, Inc.
6 * Author : K. Y. Srinivasan <ksrinivasan@novell.com>
7 *
8 * This program is free software; you can redistribute it and/or modify it
9 * under the terms of the GNU General Public License version 2 as published
10 * by the Free Software Foundation.
11 *
12 * This program is distributed in the hope that it will be useful, but
13 * WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE, GOOD TITLE or
15 * NON INFRINGEMENT. See the GNU General Public License for more
16 * details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA.
21 *
22 */
25 #include <sys/types.h>
26 #include <sys/socket.h>
27 #include <sys/poll.h>
28 #include <sys/utsname.h>
29 #include <linux/types.h>
30 #include <stdio.h>
31 #include <stdlib.h>
32 #include <unistd.h>
33 #include <string.h>
34 #include <errno.h>
35 #include <arpa/inet.h>
36 #include <linux/connector.h>
37 #include <linux/netlink.h>
38 #include <ifaddrs.h>
39 #include <netdb.h>
40 #include <syslog.h>
42 /*
43 * KYS: TODO. Need to register these in the kernel.
44 *
45 * The following definitions are shared with the in-kernel component; do not
46 * change any of this without making the corresponding changes in
47 * the KVP kernel component.
48 */
49 #define CN_KVP_IDX 0x9 /* MSFT KVP functionality */
50 #define CN_KVP_VAL 0x1 /* This supports queries from the kernel */
51 #define CN_KVP_USER_VAL 0x2 /* This supports queries from the user */
53 /*
54 * KVP protocol: The user mode component first registers with the
55 * the kernel component. Subsequently, the kernel component requests, data
56 * for the specified keys. In response to this message the user mode component
57 * fills in the value corresponding to the specified key. We overload the
58 * sequence field in the cn_msg header to define our KVP message types.
59 *
60 * We use this infrastructure for also supporting queries from user mode
61 * application for state that may be maintained in the KVP kernel component.
62 *
63 * XXXKYS: Have a shared header file between the user and kernel (TODO)
64 */
66 enum kvp_op {
67 KVP_REGISTER = 0, /* Register the user mode component*/
68 KVP_KERNEL_GET, /*Kernel is requesting the value for the specified key*/
69 KVP_KERNEL_SET, /*Kernel is providing the value for the specified key*/
70 KVP_USER_GET, /*User is requesting the value for the specified key*/
71 KVP_USER_SET /*User is providing the value for the specified key*/
72 };
74 #define HV_KVP_EXCHANGE_MAX_KEY_SIZE 512
75 #define HV_KVP_EXCHANGE_MAX_VALUE_SIZE 2048
77 struct hv_ku_msg {
78 __u32 kvp_index;
79 __u8 kvp_key[HV_KVP_EXCHANGE_MAX_KEY_SIZE]; /* Key name */
80 __u8 kvp_value[HV_KVP_EXCHANGE_MAX_VALUE_SIZE]; /* Key value */
81 };
83 enum key_index {
84 FullyQualifiedDomainName = 0,
85 IntegrationServicesVersion, /*This key is serviced in the kernel*/
86 NetworkAddressIPv4,
87 NetworkAddressIPv6,
88 OSBuildNumber,
89 OSName,
90 OSMajorVersion,
91 OSMinorVersion,
92 OSVersion,
93 ProcessorArchitecture
94 };
96 /*
97 * End of shared definitions.
98 */
100 static char kvp_send_buffer[4096];
101 static char kvp_recv_buffer[4096];
102 static struct sockaddr_nl addr;
104 static char *os_name = "";
105 static char *os_major = "";
106 static char *os_minor = "";
107 static char *processor_arch;
108 static char *os_build;
109 static char *lic_version;
110 static struct utsname uts_buf;
112 void kvp_get_os_info(void)
113 {
114 FILE *file;
115 char *p, buf[512];
117 uname(&uts_buf);
118 os_build = uts_buf.release;
119 processor_arch = uts_buf.machine;
121 /*
122 * The current windows host (win7) expects the build
123 * string to be of the form: x.y.z
124 * Strip additional information we may have.
125 */
126 p = strchr(os_build, '-');
127 if (p)
128 *p = '\0';
130 file = fopen("/etc/SuSE-release", "r");
131 if (file != NULL)
132 goto kvp_osinfo_found;
133 file = fopen("/etc/redhat-release", "r");
134 if (file != NULL)
135 goto kvp_osinfo_found;
136 /*
137 * Add code for other supported platforms.
138 */
140 /*
141 * We don't have information about the os.
142 */
143 os_name = uts_buf.sysname;
144 return;
146 kvp_osinfo_found:
147 /* up to three lines */
148 p = fgets(buf, sizeof(buf), file);
149 if (p) {
150 p = strchr(buf, '\n');
151 if (p)
152 *p = '\0';
153 p = strdup(buf);
154 if (!p)
155 goto done;
156 os_name = p;
158 /* second line */
159 p = fgets(buf, sizeof(buf), file);
160 if (p) {
161 p = strchr(buf, '\n');
162 if (p)
163 *p = '\0';
164 p = strdup(buf);
165 if (!p)
166 goto done;
167 os_major = p;
169 /* third line */
170 p = fgets(buf, sizeof(buf), file);
171 if (p) {
172 p = strchr(buf, '\n');
173 if (p)
174 *p = '\0';
175 p = strdup(buf);
176 if (p)
177 os_minor = p;
178 }
179 }
180 }
182 done:
183 fclose(file);
184 return;
185 }
187 static int
188 kvp_get_ip_address(int family, char *buffer, int length)
189 {
190 struct ifaddrs *ifap;
191 struct ifaddrs *curp;
192 int ipv4_len = strlen("255.255.255.255") + 1;
193 int ipv6_len = strlen("ffff:ffff:ffff:ffff:ffff:ffff:ffff:ffff")+1;
194 int offset = 0;
195 const char *str;
196 char tmp[50];
197 int error = 0;
199 /*
200 * On entry into this function, the buffer is capable of holding the
201 * maximum key value (2048 bytes).
202 */
204 if (getifaddrs(&ifap)) {
205 strcpy(buffer, "getifaddrs failed\n");
206 return 1;
207 }
209 curp = ifap;
210 while (curp != NULL) {
211 if ((curp->ifa_addr != NULL) &&
212 (curp->ifa_addr->sa_family == family)) {
213 if (family == AF_INET) {
214 struct sockaddr_in *addr =
215 (struct sockaddr_in *) curp->ifa_addr;
217 str = inet_ntop(family, &addr->sin_addr,
218 tmp, 50);
219 if (str == NULL) {
220 strcpy(buffer, "inet_ntop failed\n");
221 error = 1;
222 goto getaddr_done;
223 }
224 if (offset == 0)
225 strcpy(buffer, tmp);
226 else
227 strcat(buffer, tmp);
228 strcat(buffer, ";");
230 offset += strlen(str) + 1;
231 if ((length - offset) < (ipv4_len + 1))
232 goto getaddr_done;
234 } else {
236 /*
237 * We only support AF_INET and AF_INET6
238 * and the list of addresses is separated by a ";".
239 */
240 struct sockaddr_in6 *addr =
241 (struct sockaddr_in6 *) curp->ifa_addr;
243 str = inet_ntop(family,
244 &addr->sin6_addr.s6_addr,
245 tmp, 50);
246 if (str == NULL) {
247 strcpy(buffer, "inet_ntop failed\n");
248 error = 1;
249 goto getaddr_done;
250 }
251 if (offset == 0)
252 strcpy(buffer, tmp);
253 else
254 strcat(buffer, tmp);
255 strcat(buffer, ";");
256 offset += strlen(str) + 1;
257 if ((length - offset) < (ipv6_len + 1))
258 goto getaddr_done;
260 }
262 }
263 curp = curp->ifa_next;
264 }
266 getaddr_done:
267 freeifaddrs(ifap);
268 return error;
269 }
272 static int
273 kvp_get_domain_name(char *buffer, int length)
274 {
275 struct addrinfo hints, *info ;
276 int error = 0;
278 gethostname(buffer, length);
279 memset(&hints, 0, sizeof(hints));
280 hints.ai_family = AF_INET; /*Get only ipv4 addrinfo. */
281 hints.ai_socktype = SOCK_STREAM;
282 hints.ai_flags = AI_CANONNAME;
284 error = getaddrinfo(buffer, NULL, &hints, &info);
285 if (error != 0) {
286 strcpy(buffer, "getaddrinfo failed\n");
287 return error;
288 }
289 strcpy(buffer, info->ai_canonname);
290 freeaddrinfo(info);
291 return error;
292 }
294 static int
295 netlink_send(int fd, struct cn_msg *msg)
296 {
297 struct nlmsghdr *nlh;
298 unsigned int size;
299 struct msghdr message;
300 char buffer[64];
301 struct iovec iov[2];
303 size = NLMSG_SPACE(sizeof(struct cn_msg) + msg->len);
305 nlh = (struct nlmsghdr *)buffer;
306 nlh->nlmsg_seq = 0;
307 nlh->nlmsg_pid = getpid();
308 nlh->nlmsg_type = NLMSG_DONE;
309 nlh->nlmsg_len = NLMSG_LENGTH(size - sizeof(*nlh));
310 nlh->nlmsg_flags = 0;
312 iov[0].iov_base = nlh;
313 iov[0].iov_len = sizeof(*nlh);
315 iov[1].iov_base = msg;
316 iov[1].iov_len = size;
318 memset(&message, 0, sizeof(message));
319 message.msg_name = &addr;
320 message.msg_namelen = sizeof(addr);
321 message.msg_iov = iov;
322 message.msg_iovlen = 2;
324 return sendmsg(fd, &message, 0);
325 }
327 int main(void)
328 {
329 int fd, len, sock_opt;
330 int error;
331 struct cn_msg *message;
332 struct pollfd pfd;
333 struct nlmsghdr *incoming_msg;
334 struct cn_msg *incoming_cn_msg;
335 struct hv_ku_msg *hv_msg;
336 char *p;
337 char *key_value;
338 char *key_name;
340 daemon(1, 0);
341 openlog("KVP", 0, LOG_USER);
342 syslog(LOG_INFO, "KVP starting; pid is:%d", getpid());
343 /*
344 * Retrieve OS release information.
345 */
346 kvp_get_os_info();
348 fd = socket(AF_NETLINK, SOCK_DGRAM, NETLINK_CONNECTOR);
349 if (fd < 0) {
350 syslog(LOG_ERR, "netlink socket creation failed; error:%d", fd);
351 exit(-1);
352 }
353 addr.nl_family = AF_NETLINK;
354 addr.nl_pad = 0;
355 addr.nl_pid = 0;
356 addr.nl_groups = CN_KVP_IDX;
359 error = bind(fd, (struct sockaddr *)&addr, sizeof(addr));
360 if (error < 0) {
361 syslog(LOG_ERR, "bind failed; error:%d", error);
362 close(fd);
363 exit(-1);
364 }
365 sock_opt = addr.nl_groups;
366 setsockopt(fd, 270, 1, &sock_opt, sizeof(sock_opt));
367 /*
368 * Register ourselves with the kernel.
369 */
370 message = (struct cn_msg *)kvp_send_buffer;
371 message->id.idx = CN_KVP_IDX;
372 message->id.val = CN_KVP_VAL;
373 message->seq = KVP_REGISTER;
374 message->ack = 0;
375 message->len = 0;
377 len = netlink_send(fd, message);
378 if (len < 0) {
379 syslog(LOG_ERR, "netlink_send failed; error:%d", len);
380 close(fd);
381 exit(-1);
382 }
384 pfd.fd = fd;
386 while (1) {
387 pfd.events = POLLIN;
388 pfd.revents = 0;
389 poll(&pfd, 1, -1);
391 len = recv(fd, kvp_recv_buffer, sizeof(kvp_recv_buffer), 0);
393 if (len < 0) {
394 syslog(LOG_ERR, "recv failed; error:%d", len);
395 close(fd);
396 return -1;
397 }
399 incoming_msg = (struct nlmsghdr *)kvp_recv_buffer;
400 incoming_cn_msg = (struct cn_msg *)NLMSG_DATA(incoming_msg);
402 switch (incoming_cn_msg->seq) {
403 case KVP_REGISTER:
404 /*
405 * Driver is registering with us; stash away the version
406 * information.
407 */
408 p = (char *)incoming_cn_msg->data;
409 lic_version = malloc(strlen(p) + 1);
410 if (lic_version) {
411 strcpy(lic_version, p);
412 syslog(LOG_INFO, "KVP LIC Version: %s",
413 lic_version);
414 } else {
415 syslog(LOG_ERR, "malloc failed");
416 }
417 continue;
419 case KVP_KERNEL_GET:
420 break;
421 default:
422 continue;
423 }
425 hv_msg = (struct hv_ku_msg *)incoming_cn_msg->data;
426 key_name = (char *)hv_msg->kvp_key;
427 key_value = (char *)hv_msg->kvp_value;
429 switch (hv_msg->kvp_index) {
430 case FullyQualifiedDomainName:
431 kvp_get_domain_name(key_value,
432 HV_KVP_EXCHANGE_MAX_VALUE_SIZE);
433 strcpy(key_name, "FullyQualifiedDomainName");
434 break;
435 case IntegrationServicesVersion:
436 strcpy(key_name, "IntegrationServicesVersion");
437 strcpy(key_value, lic_version);
438 break;
439 case NetworkAddressIPv4:
440 kvp_get_ip_address(AF_INET, key_value,
441 HV_KVP_EXCHANGE_MAX_VALUE_SIZE);
442 strcpy(key_name, "NetworkAddressIPv4");
443 break;
444 case NetworkAddressIPv6:
445 kvp_get_ip_address(AF_INET6, key_value,
446 HV_KVP_EXCHANGE_MAX_VALUE_SIZE);
447 strcpy(key_name, "NetworkAddressIPv6");
448 break;
449 case OSBuildNumber:
450 strcpy(key_value, os_build);
451 strcpy(key_name, "OSBuildNumber");
452 break;
453 case OSName:
454 strcpy(key_value, os_name);
455 strcpy(key_name, "OSName");
456 break;
457 case OSMajorVersion:
458 strcpy(key_value, os_major);
459 strcpy(key_name, "OSMajorVersion");
460 break;
461 case OSMinorVersion:
462 strcpy(key_value, os_minor);
463 strcpy(key_name, "OSMinorVersion");
464 break;
465 case OSVersion:
466 strcpy(key_value, os_build);
467 strcpy(key_name, "OSVersion");
468 break;
469 case ProcessorArchitecture:
470 strcpy(key_value, processor_arch);
471 strcpy(key_name, "ProcessorArchitecture");
472 break;
473 default:
474 strcpy(key_value, "Unknown Key");
475 /*
476 * We use a null key name to terminate enumeration.
477 */
478 strcpy(key_name, "");
479 break;
480 }
481 /*
482 * Send the value back to the kernel. The response is
483 * already in the receive buffer. Update the cn_msg header to
484 * reflect the key value that has been added to the message
485 */
487 incoming_cn_msg->id.idx = CN_KVP_IDX;
488 incoming_cn_msg->id.val = CN_KVP_VAL;
489 incoming_cn_msg->seq = KVP_USER_SET;
490 incoming_cn_msg->ack = 0;
491 incoming_cn_msg->len = sizeof(struct hv_ku_msg);
493 len = netlink_send(fd, incoming_cn_msg);
494 if (len < 0) {
495 syslog(LOG_ERR, "net_link send failed; error:%d", len);
496 exit(-1);
497 }
498 }
500 }