The following is a list of files and features that are going to be removed in the kernel source tree. Every entry should contain what exactly is going away, why it is happening, and who is going to be doing the work. When the feature is removed from the kernel, it should also be removed from this file. --------------------------- What: x86 floppy disable_hlt When: 2012 Why: ancient workaround of dubious utility clutters the code used by everybody else. Who: Len Brown --------------------------- What: CONFIG_APM_CPU_IDLE, and its ability to call APM BIOS in idle When: 2012 Why: This optional sub-feature of APM is of dubious reliability, and ancient APM laptops are likely better served by calling HLT. Deleting CONFIG_APM_CPU_IDLE allows x86 to stop exporting the pm_idle function pointer to modules. Who: Len Brown ---------------------------- What: x86_32 "no-hlt" cmdline param When: 2012 Why: remove a branch from idle path, simplify code used by everybody. This option disabled the use of HLT in idle and machine_halt() for hardware that was flakey 15-years ago. Today we have "idle=poll" that removed HLT from idle, and so if such a machine is still running the upstream kernel, "idle=poll" is likely sufficient. Who: Len Brown ---------------------------- What: x86 "idle=mwait" cmdline param When: 2012 Why: simplify x86 idle code Who: Len Brown ---------------------------- What: PRISM54 When: 2.6.34 Why: prism54 FullMAC PCI / Cardbus devices used to be supported only by the prism54 wireless driver. After Intersil stopped selling these devices in preference for the newer more flexible SoftMAC devices a SoftMAC device driver was required and prism54 did not support them. The p54pci driver now exists and has been present in the kernel for a while. This driver supports both SoftMAC devices and FullMAC devices. The main difference between these devices was the amount of memory which could be used for the firmware. The SoftMAC devices support a smaller amount of memory. Because of this the SoftMAC firmware fits into FullMAC devices's memory. p54pci supports not only PCI / Cardbus but also USB and SPI. Since p54pci supports all devices prism54 supports you will have a conflict. I'm not quite sure how distributions are handling this conflict right now. prism54 was kept around due to claims users may experience issues when using the SoftMAC driver. Time has passed users have not reported issues. If you use prism54 and for whatever reason you cannot use p54pci please let us know! E-mail us at: linux-wireless@vger.kernel.org For more information see the p54 wiki page: http://wireless.kernel.org/en/users/Drivers/p54 Who: Luis R. Rodriguez --------------------------- What: IRQF_SAMPLE_RANDOM Check: IRQF_SAMPLE_RANDOM When: July 2009 Why: Many of IRQF_SAMPLE_RANDOM users are technically bogus as entropy sources in the kernel's current entropy model. To resolve this, every input point to the kernel's entropy pool needs to better document the type of entropy source it actually is. This will be replaced with additional add_*_randomness functions in drivers/char/random.c Who: Robin Getz & Matt Mackall --------------------------- What: Deprecated snapshot ioctls When: 2.6.36 Why: The ioctls in kernel/power/user.c were marked as deprecated long time ago. Now they notify users about that so that they need to replace their userspace. After some more time, remove them completely. Who: Jiri Slaby --------------------------- What: The ieee80211_regdom module parameter When: March 2010 / desktop catchup Why: This was inherited by the CONFIG_WIRELESS_OLD_REGULATORY code, and currently serves as an option for users to define an ISO / IEC 3166 alpha2 code for the country they are currently present in. Although there are userspace API replacements for this through nl80211 distributions haven't yet caught up with implementing decent alternatives through standard GUIs. Although available as an option through iw or wpa_supplicant its just a matter of time before distributions pick up good GUI options for this. The ideal solution would actually consist of intelligent designs which would do this for the user automatically even when travelling through different countries. Until then we leave this module parameter as a compromise. When userspace improves with reasonable widely-available alternatives for this we will no longer need this module parameter. This entry hopes that by the super-futuristically looking date of "March 2010" we will have such replacements widely available. Who: Luis R. Rodriguez --------------------------- What: dev->power.power_state When: July 2007 Why: Broken design for runtime control over driver power states, confusing driver-internal runtime power management with: mechanisms to support system-wide sleep state transitions; event codes that distinguish different phases of swsusp "sleep" transitions; and userspace policy inputs. This framework was never widely used, and most attempts to use it were broken. Drivers should instead be exposing domain-specific interfaces either to kernel or to userspace. Who: Pavel Machek --------------------------- What: /proc//oom_adj When: August 2012 Why: /proc//oom_adj allows userspace to influence the oom killer's badness heuristic used to determine which task to kill when the kernel is out of memory. The badness heuristic has since been rewritten since the introduction of this tunable such that its meaning is deprecated. The value was implemented as a bitshift on a score generated by the badness() function that did not have any precise units of measure. With the rewrite, the score is given as a proportion of available memory to the task allocating pages, so using a bitshift which grows the score exponentially is, thus, impossible to tune with fine granularity. A much more powerful interface, /proc//oom_score_adj, was introduced with the oom killer rewrite that allows users to increase or decrease the badness score linearly. This interface will replace /proc//oom_adj. A warning will be emitted to the kernel log if an application uses this deprecated interface. After it is printed once, future warnings will be suppressed until the kernel is rebooted. --------------------------- What: remove EXPORT_SYMBOL(kernel_thread) When: August 2006 Files: arch/*/kernel/*_ksyms.c Check: kernel_thread Why: kernel_thread is a low-level implementation detail. Drivers should use the API instead which shields them from implementation details and provides a higherlevel interface that prevents bugs and code duplication Who: Christoph Hellwig --------------------------- What: Unused EXPORT_SYMBOL/EXPORT_SYMBOL_GPL exports (temporary transition config option provided until then) The transition config option will also be removed at the same time. When: before 2.6.19 Why: Unused symbols are both increasing the size of the kernel binary and are often a sign of "wrong API" Who: Arjan van de Ven --------------------------- What: PHYSDEVPATH, PHYSDEVBUS, PHYSDEVDRIVER in the uevent environment When: October 2008 Why: The stacking of class devices makes these values misleading and inconsistent. Class devices should not carry any of these properties, and bus devices have SUBSYTEM and DRIVER as a replacement. Who: Kay Sievers --------------------------- What: ACPI procfs interface When: July 2008 Why: ACPI sysfs conversion should be finished by January 2008. ACPI procfs interface will be removed in July 2008 so that there is enough time for the user space to catch up. Who: Zhang Rui --------------------------- What: CONFIG_ACPI_PROCFS_POWER When: 2.6.39 Why: sysfs I/F for ACPI power devices, including AC and Battery, has been working in upstream kernel since 2.6.24, Sep 2007. In 2.6.37, we make the sysfs I/F always built in and this option disabled by default. Remove this option and the ACPI power procfs interface in 2.6.39. Who: Zhang Rui --------------------------- What: /proc/acpi/event When: February 2008 Why: /proc/acpi/event has been replaced by events via the input layer and netlink since 2.6.23. Who: Len Brown --------------------------- What: i386/x86_64 bzImage symlinks When: April 2010 Why: The i386/x86_64 merge provides a symlink to the old bzImage location so not yet updated user space tools, e.g. package scripts, do not break. Who: Thomas Gleixner --------------------------- What: GPIO autorequest on gpio_direction_{input,output}() in gpiolib When: February 2010 Why: All callers should use explicit gpio_request()/gpio_free(). The autorequest mechanism in gpiolib was provided mostly as a migration aid for legacy GPIO interfaces (for SOC based GPIOs). Those users have now largely migrated. Platforms implementing the GPIO interfaces without using gpiolib will see no changes. Who: David Brownell --------------------------- What: b43 support for firmware revision < 410 When: The schedule was July 2008, but it was decided that we are going to keep the code as long as there are no major maintanance headaches. So it _could_ be removed _any_ time now, if it conflicts with something new. Why: The support code for the old firmware hurts code readability/maintainability and slightly hurts runtime performance. Bugfixes for the old firmware are not provided by Broadcom anymore. Who: Michael Buesch --------------------------- What: Ability for non root users to shm_get hugetlb pages based on mlock resource limits When: 2.6.31 Why: Non root users need to be part of /proc/sys/vm/hugetlb_shm_group or have CAP_IPC_LOCK to be able to allocate shm segments backed by huge pages. The mlock based rlimit check to allow shm hugetlb is inconsistent with mmap based allocations. Hence it is being deprecated. Who: Ravikiran Thirumalai --------------------------- What: Code that is now under CONFIG_WIRELESS_EXT_SYSFS (in net/core/net-sysfs.c) When: After the only user (hal) has seen a release with the patches for enough time, probably some time in 2010. Why: Over 1K .text/.data size reduction, data is available in other ways (ioctls) Who: Johannes Berg --------------------------- What: sysfs ui for changing p4-clockmod parameters When: September 2009 Why: See commits 129f8ae9b1b5be94517da76009ea956e89104ce8 and e088e4c9cdb618675874becb91b2fd581ee707e6. Removal is subject to fixing any remaining bugs in ACPI which may cause the thermal throttling not to happen at the right time. Who: Dave Jones , Matthew Garrett ----------------------------- What: fakephp and associated sysfs files in /sys/bus/pci/slots/ When: 2011 Why: In 2.6.27, the semantics of /sys/bus/pci/slots was redefined to represent a machine's physical PCI slots. The change in semantics had userspace implications, as the hotplug core no longer allowed drivers to create multiple sysfs files per physical slot (required for multi-function devices, e.g.). fakephp was seen as a developer's tool only, and its interface changed. Too late, we learned that there were some users of the fakephp interface. In 2.6.30, the original fakephp interface was restored. At the same time, the PCI core gained the ability that fakephp provided, namely function-level hot-remove and hot-add. Since the PCI core now provides the same functionality, exposed in: /sys/bus/pci/rescan /sys/bus/pci/devices/.../remove /sys/bus/pci/devices/.../rescan there is no functional reason to maintain fakephp as well. We will keep the existing module so that 'modprobe fakephp' will present the old /sys/bus/pci/slots/... interface for compatibility, but users are urged to migrate their applications to the API above. After a reasonable transition period, we will remove the legacy fakephp interface. Who: Alex Chiang --------------------------- What: CONFIG_RFKILL_INPUT When: 2.6.33 Why: Should be implemented in userspace, policy daemon. Who: Johannes Berg ---------------------------- What: sound-slot/service-* module aliases and related clutters in sound/sound_core.c When: August 2010 Why: OSS sound_core grabs all legacy minors (0-255) of SOUND_MAJOR (14) and requests modules using custom sound-slot/service-* module aliases. The only benefit of doing this is allowing use of custom module aliases which might as well be considered a bug at this point. This preemptive claiming prevents alternative OSS implementations. Till the feature is removed, the kernel will be requesting both sound-slot/service-* and the standard char-major-* module aliases and allow turning off the pre-claiming selectively via CONFIG_SOUND_OSS_CORE_PRECLAIM and soundcore.preclaim_oss kernel parameter. After the transition phase is complete, both the custom module aliases and switches to disable it will go away. This removal will also allow making ALSA OSS emulation independent of sound_core. The dependency will be broken then too. Who: Tejun Heo ---------------------------- What: sysfs-class-rfkill state file When: Feb 2014 Files: net/rfkill/core.c Why: Documented as obsolete since Feb 2010. This file is limited to 3 states while the rfkill drivers can have 4 states. Who: anybody or Florian Mickler ---------------------------- What: sysfs-class-rfkill claim file When: Feb 2012 Files: net/rfkill/core.c Why: It is not possible to claim an rfkill driver since 2007. This is Documented as obsolete since Feb 2010. Who: anybody or Florian Mickler ---------------------------- What: KVM paravirt mmu host support When: January 2011 Why: The paravirt mmu host support is slower than non-paravirt mmu, both on newer and older hardware. It is already not exposed to the guest, and kept only for live migration purposes. Who: Avi Kivity ---------------------------- What: iwlwifi 50XX module parameters When: 3.0 Why: The "..50" modules parameters were used to configure 5000 series and up devices; different set of module parameters also available for 4965 with same functionalities. Consolidate both set into single place in drivers/net/wireless/iwlwifi/iwl-agn.c Who: Wey-Yi Guy ---------------------------- What: iwl4965 alias support When: 3.0 Why: Internal alias support has been present in module-init-tools for some time, the MODULE_ALIAS("iwl4965") boilerplate aliases can be removed with no impact. Who: Wey-Yi Guy --------------------------- What: xt_NOTRACK Files: net/netfilter/xt_NOTRACK.c When: April 2011 Why: Superseded by xt_CT Who: Netfilter developer team ---------------------------- What: IRQF_DISABLED When: 2.6.36 Why: The flag is a NOOP as we run interrupt handlers with interrupts disabled Who: Thomas Gleixner ---------------------------- What: PCI DMA unmap state API When: August 2012 Why: PCI DMA unmap state API (include/linux/pci-dma.h) was replaced with DMA unmap state API (DMA unmap state API can be used for any bus). Who: FUJITA Tomonori ---------------------------- What: iwlwifi disable_hw_scan module parameters When: 3.0 Why: Hareware scan is the prefer method for iwlwifi devices for scanning operation. Remove software scan support for all the iwlwifi devices. Who: Wey-Yi Guy ---------------------------- What: Legacy, non-standard chassis intrusion detection interface. When: June 2011 Why: The adm9240, w83792d and w83793 hardware monitoring drivers have legacy interfaces for chassis intrusion detection. A standard interface has been added to each driver, so the legacy interface can be removed. Who: Jean Delvare ---------------------------- What: xt_connlimit rev 0 When: 2012 Who: Jan Engelhardt Files: net/netfilter/xt_connlimit.c ---------------------------- What: ipt_addrtype match include file When: 2012 Why: superseded by xt_addrtype Who: Florian Westphal Files: include/linux/netfilter_ipv4/ipt_addrtype.h ---------------------------- What: i2c_driver.attach_adapter i2c_driver.detach_adapter When: September 2011 Why: These legacy callbacks should no longer be used as i2c-core offers a variety of preferable alternative ways to instantiate I2C devices. Who: Jean Delvare ---------------------------- What: Support for driver specific ioctls in the pwc driver (everything defined in media/pwc-ioctl.h) When: 3.3 Why: This stems from the v4l1 era, with v4l2 everything can be done with standardized v4l2 API calls Who: Hans de Goede ---------------------------- What: Driver specific sysfs API in the pwc driver When: 3.3 Why: Setting pan/tilt should be done with v4l2 controls, like with other cams. The button is available as a standard input device Who: Hans de Goede ---------------------------- What: Driver specific use of pixfmt.priv in the pwc driver When: 3.3 Why: The .priv field never was intended for this, setting a framerate is support using the standardized S_PARM ioctl Who: Hans de Goede ---------------------------- What: Software emulation of arbritary resolutions in the pwc driver When: 3.3 Why: The pwc driver claims to support any resolution between 160x120 and 640x480, but emulates this by simply drawing a black border around the image. Userspace can draw its own black border if it really wants one. Who: Hans de Goede ---------------------------- What: For VIDIOC_S_FREQUENCY the type field must match the device node's type. If not, return -EINVAL. When: 3.2 Why: It makes no sense to switch the tuner to radio mode by calling VIDIOC_S_FREQUENCY on a video node, or to switch the tuner to tv mode by calling VIDIOC_S_FREQUENCY on a radio node. This is the first step of a move to more consistent handling of tv and radio tuners. Who: Hans Verkuil ---------------------------- What: Opening a radio device node will no longer automatically switch the tuner mode from tv to radio. When: 3.3 Why: Just opening a V4L device should not change the state of the hardware like that. It's very unexpected and against the V4L spec. Instead, you switch to radio mode by calling VIDIOC_S_FREQUENCY. This is the second and last step of the move to consistent handling of tv and radio tuners. Who: Hans Verkuil ---------------------------- What: g_file_storage driver When: 3.8 Why: This driver has been superseded by g_mass_storage. Who: Alan Stern ---------------------------- What: threeg and interface sysfs files in /sys/devices/platform/acer-wmi When: 2012 Why: In 3.0, we can now autodetect internal 3G device and already have the threeg rfkill device. So, we plan to remove threeg sysfs support for it's no longer necessary. We also plan to remove interface sysfs file that exposed which ACPI-WMI interface that was used by acer-wmi driver. It will replaced by information log when acer-wmi initial. Who: Lee, Chun-Yi --------------------------- What: /sys/devices/platform/_UDC_/udc/_UDC_/is_dualspeed file and is_dualspeed line in /sys/devices/platform/ci13xxx_*/udc/device file. When: 3.8 Why: The is_dualspeed file is superseded by maximum_speed in the same directory and is_dualspeed line in device file is superseded by max_speed line in the same file. The maximum_speed/max_speed specifies maximum speed supported by UDC. To check if dualspeeed is supported, check if the value is >= 3. Various possible speeds are defined in . Who: Michal Nazarewicz ---------------------------- What: The XFS nodelaylog mount option When: 3.3 Why: The delaylog mode that has been the default since 2.6.39 has proven stable, and the old code is in the way of additional improvements in the log code. Who: Christoph Hellwig ---------------------------- What: iwlagn alias support When: 3.5 Why: The iwlagn module has been renamed iwlwifi. The alias will be around for backward compatibility for several cycles and then dropped. Who: Don Fry