CONFIG_EXPERIMENTAL=y CONFIG_LOG_BUF_SHIFT=14 CONFIG_EMBEDDED=y # CONFIG_HOTPLUG is not set # CONFIG_ELF_CORE is not set # CONFIG_FUTEX is not set # CONFIG_TIMERFD is not set # CONFIG_VM_EVENT_COUNTERS is not set # CONFIG_COMPAT_BRK is not set CONFIG_SLAB=y # CONFIG_LBDAF is not set # CONFIG_BLK_DEV_BSG is not set # CONFIG_IOSCHED_DEADLINE is not set # CONFIG_IOSCHED_CFQ is not set # CONFIG_MMU is not set CONFIG_ARCH_AT91=y CONFIG_ARCH_AT91X40=y CONFIG_MACH_AT91EB01=y CONFIG_AT91_EARLY_USART0=y CONFIG_CPU_ARM7TDMI=y CONFIG_SET_MEM_PARAM=y CONFIG_DRAM_BASE=0x01000000 CONFIG_DRAM_SIZE=0x00400000 CONFIG_FLASH_MEM_BASE=0x01400000 CONFIG_PROCESSOR_ID=0x14000040 CONFIG_ZBOOT_ROM_TEXT=0x0 CONFIG_ZBOOT_ROM_BSS=0x0 CONFIG_BINFMT_FLAT=y # CONFIG_SUSPEND is not set # CONFIG_FW_LOADER is not set CONFIG_MTD=y CONFIG_MTD_PARTITIONS=y CONFIG_MTD_CHAR=y CONFIG_MTD_BLOCK=y CONFIG_MTD_RAM=y CONFIG_MTD_ROM=y CONFIG_BLK_DEV_RAM=y # CONFIG_INPUT is not set # CONFIG_SERIO is not set # CONFIG_VT is not set # CONFIG_DEVKMEM is not set # CONFIG_HW_RANDOM is not set # CONFIG_HWMON is not set # CONFIG_USB_SUPPORT is not set CONFIG_EXT2_FS=y # CONFIG_DNOTIFY is not set CONFIG_ROMFS_FS=y # CONFIG_ENABLE_MUST_CHECK is not set