/* * OMAP2/3/4 clockdomain framework functions * * Copyright (C) 2008-2011 Texas Instruments, Inc. * Copyright (C) 2008-2011 Nokia Corporation * * Written by Paul Walmsley and Jouni Högander * Added OMAP4 specific support by Abhijit Pagare * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #undef DEBUG #include #include #include #include #include #include #include #include #include #include #include #include #include "clockdomain.h" /* clkdm_list contains all registered struct clockdomains */ static LIST_HEAD(clkdm_list); /* array of clockdomain deps to be added/removed when clkdm in hwsup mode */ static struct clkdm_autodep *autodeps; static struct clkdm_ops *arch_clkdm; /* Private functions */ static struct clockdomain *_clkdm_lookup(const char *name) { struct clockdomain *clkdm, *temp_clkdm; if (!name) return NULL; clkdm = NULL; list_for_each_entry(temp_clkdm, &clkdm_list, node) { if (!strcmp(name, temp_clkdm->name)) { clkdm = temp_clkdm; break; } } return clkdm; } /** * _clkdm_register - register a clockdomain * @clkdm: struct clockdomain * to register * * Adds a clockdomain to the internal clockdomain list. * Returns -EINVAL if given a null pointer, -EEXIST if a clockdomain is * already registered by the provided name, or 0 upon success. */ static int _clkdm_register(struct clockdomain *clkdm) { struct powerdomain *pwrdm; if (!clkdm || !clkdm->name) return -EINVAL; pwrdm = pwrdm_lookup(clkdm->pwrdm.name); if (!pwrdm) { pr_err("clockdomain: %s: powerdomain %s does not exist\n", clkdm->name, clkdm->pwrdm.name); return -EINVAL; } clkdm->pwrdm.ptr = pwrdm; /* Verify that the clockdomain is not already registered */ if (_clkdm_lookup(clkdm->name)) return -EEXIST; list_add(&clkdm->node, &clkdm_list); pwrdm_add_clkdm(pwrdm, clkdm); spin_lock_init(&clkdm->lock); pr_debug("clockdomain: registered %s\n", clkdm->name); return 0; } /* _clkdm_deps_lookup - look up the specified clockdomain in a clkdm list */ static struct clkdm_dep *_clkdm_deps_lookup(struct clockdomain *clkdm, struct clkdm_dep *deps) { struct clkdm_dep *cd; if (!clkdm || !deps) return ERR_PTR(-EINVAL); for (cd = deps; cd->clkdm_name; cd++) { if (!cd->clkdm && cd->clkdm_name) cd->clkdm = _clkdm_lookup(cd->clkdm_name); if (cd->clkdm == clkdm) break; } if (!cd->clkdm_name) return ERR_PTR(-ENOENT); return cd; } /* * _autodep_lookup - resolve autodep clkdm names to clkdm pointers; store * @autodep: struct clkdm_autodep * to resolve * * Resolve autodep clockdomain names to clockdomain pointers via * clkdm_lookup() and store the pointers in the autodep structure. An * "autodep" is a clockdomain sleep/wakeup dependency that is * automatically added and removed whenever clocks in the associated * clockdomain are enabled or disabled (respectively) when the * clockdomain is in hardware-supervised mode. Meant to be called * once at clockdomain layer initialization, since these should remain * fixed for a particular architecture. No return value. * * XXX autodeps are deprecated and should be removed at the earliest * opportunity */ static void _autodep_lookup(struct clkdm_autodep *autodep) { struct clockdomain *clkdm; if (!autodep) return; clkdm = clkdm_lookup(autodep->clkdm.name); if (!clkdm) { pr_err("clockdomain: autodeps: clockdomain %s does not exist\n", autodep->clkdm.name); clkdm = ERR_PTR(-ENOENT); } autodep->clkdm.ptr = clkdm; } /* * _clkdm_add_autodeps - add auto sleepdeps/wkdeps to clkdm upon clock enable * @clkdm: struct clockdomain * * * Add the "autodep" sleep & wakeup dependencies to clockdomain 'clkdm' * in hardware-supervised mode. Meant to be called from clock framework * when a clock inside clockdomain 'clkdm' is enabled. No return value. * * XXX autodeps are deprecated and should be removed at the earliest * opportunity */ void _clkdm_add_autodeps(struct clockdomain *clkdm) { struct clkdm_autodep *autodep; if (!autodeps || clkdm->flags & CLKDM_NO_AUTODEPS) return; for (autodep = autodeps; autodep->clkdm.ptr; autodep++) { if (IS_ERR(autodep->clkdm.ptr)) continue; pr_debug("clockdomain: adding %s sleepdep/wkdep for " "clkdm %s\n", autodep->clkdm.ptr->name, clkdm->name); clkdm_add_sleepdep(clkdm, autodep->clkdm.ptr); clkdm_add_wkdep(clkdm, autodep->clkdm.ptr); } } /* * _clkdm_add_autodeps - remove auto sleepdeps/wkdeps from clkdm * @clkdm: struct clockdomain * * * Remove the "autodep" sleep & wakeup dependencies from clockdomain 'clkdm' * in hardware-supervised mode. Meant to be called from clock framework * when a clock inside clockdomain 'clkdm' is disabled. No return value. * * XXX autodeps are deprecated and should be removed at the earliest * opportunity */ void _clkdm_del_autodeps(struct clockdomain *clkdm) { struct clkdm_autodep *autodep; if (!autodeps || clkdm->flags & CLKDM_NO_AUTODEPS) return; for (autodep = autodeps; autodep->clkdm.ptr; autodep++) { if (IS_ERR(autodep->clkdm.ptr)) continue; pr_debug("clockdomain: removing %s sleepdep/wkdep for " "clkdm %s\n", autodep->clkdm.ptr->name, clkdm->name); clkdm_del_sleepdep(clkdm, autodep->clkdm.ptr); clkdm_del_wkdep(clkdm, autodep->clkdm.ptr); } } /** * _resolve_clkdm_deps() - resolve clkdm_names in @clkdm_deps to clkdms * @clkdm: clockdomain that we are resolving dependencies for * @clkdm_deps: ptr to array of struct clkdm_deps to resolve * * Iterates through @clkdm_deps, looking up the struct clockdomain named by * clkdm_name and storing the clockdomain pointer in the struct clkdm_dep. * No return value. */ static void _resolve_clkdm_deps(struct clockdomain *clkdm, struct clkdm_dep *clkdm_deps) { struct clkdm_dep *cd; for (cd = clkdm_deps; cd && cd->clkdm_name; cd++) { if (cd->clkdm) continue; cd->clkdm = _clkdm_lookup(cd->clkdm_name); WARN(!cd->clkdm, "clockdomain: %s: could not find clkdm %s while resolving dependencies - should never happen", clkdm->name, cd->clkdm_name); } } /* Public functions */ /** * clkdm_register_platform_funcs - register clockdomain implementation fns * @co: func pointers for arch specific implementations * * Register the list of function pointers used to implement the * clockdomain functions on different OMAP SoCs. Should be called * before any other clkdm_register*() function. Returns -EINVAL if * @co is null, -EEXIST if platform functions have already been * registered, or 0 upon success. */ int clkdm_register_platform_funcs(struct clkdm_ops *co) { if (!co) return -EINVAL; if (arch_clkdm) return -EEXIST; arch_clkdm = co; return 0; }; /** * clkdm_register_clkdms - register SoC clockdomains * @cs: pointer to an array of struct clockdomain to register * * Register the clockdomains available on a particular OMAP SoC. Must * be called after clkdm_register_platform_funcs(). May be called * multiple times. Returns -EACCES if called before * clkdm_register_platform_funcs(); -EINVAL if the argument @cs is * null; or 0 upon success. */ int clkdm_register_clkdms(struct clockdomain **cs) { struct clockdomain **c = NULL; if (!arch_clkdm) return -EACCES; if (!cs) return -EINVAL; for (c = cs; *c; c++) _clkdm_register(*c); return 0; } /** * clkdm_register_autodeps - register autodeps (if required) * @ia: pointer to a static array of struct clkdm_autodep to register * * Register clockdomain "automatic dependencies." These are * clockdomain wakeup and sleep dependencies that are automatically * added whenever the first clock inside a clockdomain is enabled, and * removed whenever the last clock inside a clockdomain is disabled. * These are currently only used on OMAP3 devices, and are deprecated, * since they waste energy. However, until the OMAP2/3 IP block * enable/disable sequence can be converted to match the OMAP4 * sequence, they are needed. * * Must be called only after all of the SoC clockdomains are * registered, since the function will resolve autodep clockdomain * names into clockdomain pointers. * * The struct clkdm_autodep @ia array must be static, as this function * does not copy the array elements. * * Returns -EACCES if called before any clockdomains have been * registered, -EINVAL if called with a null @ia argument, -EEXIST if * autodeps have already been registered, or 0 upon success. */ int clkdm_register_autodeps(struct clkdm_autodep *ia) { struct clkdm_autodep *a = NULL; if (list_empty(&clkdm_list)) return -EACCES; if (!ia) return -EINVAL; if (autodeps) return -EEXIST; autodeps = ia; for (a = autodeps; a->clkdm.ptr; a++) _autodep_lookup(a); return 0; } /** * clkdm_complete_init - set up the clockdomain layer * * Put all clockdomains into software-supervised mode; PM code should * later enable hardware-supervised mode as appropriate. Must be * called after clkdm_register_clkdms(). Returns -EACCES if called * before clkdm_register_clkdms(), or 0 upon success. */ int clkdm_complete_init(void) { struct clockdomain *clkdm; if (list_empty(&clkdm_list)) return -EACCES; list_for_each_entry(clkdm, &clkdm_list, node) { if (clkdm->flags & CLKDM_CAN_FORCE_WAKEUP) clkdm_wakeup(clkdm); else if (clkdm->flags & CLKDM_CAN_DISABLE_AUTO) clkdm_deny_idle(clkdm); _resolve_clkdm_deps(clkdm, clkdm->wkdep_srcs); clkdm_clear_all_wkdeps(clkdm); _resolve_clkdm_deps(clkdm, clkdm->sleepdep_srcs); clkdm_clear_all_sleepdeps(clkdm); } return 0; } /** * clkdm_lookup - look up a clockdomain by name, return a pointer * @name: name of clockdomain * * Find a registered clockdomain by its name @name. Returns a pointer * to the struct clockdomain if found, or NULL otherwise. */ struct clockdomain *clkdm_lookup(const char *name) { struct clockdomain *clkdm, *temp_clkdm; if (!name) return NULL; clkdm = NULL; list_for_each_entry(temp_clkdm, &clkdm_list, node) { if (!strcmp(name, temp_clkdm->name)) { clkdm = temp_clkdm; break; } } return clkdm; } /** * clkdm_for_each - call function on each registered clockdomain * @fn: callback function * * * Call the supplied function @fn for each registered clockdomain. * The callback function @fn can return anything but 0 to bail * out early from the iterator. The callback function is called with * the clkdm_mutex held, so no clockdomain structure manipulation * functions should be called from the callback, although hardware * clockdomain control functions are fine. Returns the last return * value of the callback function, which should be 0 for success or * anything else to indicate failure; or -EINVAL if the function pointer * is null. */ int clkdm_for_each(int (*fn)(struct clockdomain *clkdm, void *user), void *user) { struct clockdomain *clkdm; int ret = 0; if (!fn) return -EINVAL; list_for_each_entry(clkdm, &clkdm_list, node) { ret = (*fn)(clkdm, user); if (ret) break; } return ret; } /** * clkdm_get_pwrdm - return a ptr to the pwrdm that this clkdm resides in * @clkdm: struct clockdomain * * * Return a pointer to the struct powerdomain that the specified clockdomain * @clkdm exists in, or returns NULL if @clkdm is NULL. */ struct powerdomain *clkdm_get_pwrdm(struct clockdomain *clkdm) { if (!clkdm) return NULL; return clkdm->pwrdm.ptr; } /* Hardware clockdomain control */ /** * clkdm_add_wkdep - add a wakeup dependency from clkdm2 to clkdm1 * @clkdm1: wake this struct clockdomain * up (dependent) * @clkdm2: when this struct clockdomain * wakes up (source) * * When the clockdomain represented by @clkdm2 wakes up, wake up * @clkdm1. Implemented in hardware on the OMAP, this feature is * designed to reduce wakeup latency of the dependent clockdomain @clkdm1. * Returns -EINVAL if presented with invalid clockdomain pointers, * -ENOENT if @clkdm2 cannot wake up clkdm1 in hardware, or 0 upon * success. */ int clkdm_add_wkdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2) { struct clkdm_dep *cd; int ret = 0; if (!clkdm1 || !clkdm2) return -EINVAL; cd = _clkdm_deps_lookup(clkdm2, clkdm1->wkdep_srcs); if (IS_ERR(cd)) ret = PTR_ERR(cd); if (!arch_clkdm || !arch_clkdm->clkdm_add_wkdep) ret = -EINVAL; if (ret) { pr_debug("clockdomain: hardware cannot set/clear wake up of " "%s when %s wakes up\n", clkdm1->name, clkdm2->name); return ret; } if (atomic_inc_return(&cd->wkdep_usecount) == 1) { pr_debug("clockdomain: hardware will wake up %s when %s wakes " "up\n", clkdm1->name, clkdm2->name); ret = arch_clkdm->clkdm_add_wkdep(clkdm1, clkdm2); } return ret; } /** * clkdm_del_wkdep - remove a wakeup dependency from clkdm2 to clkdm1 * @clkdm1: wake this struct clockdomain * up (dependent) * @clkdm2: when this struct clockdomain * wakes up (source) * * Remove a wakeup dependency causing @clkdm1 to wake up when @clkdm2 * wakes up. Returns -EINVAL if presented with invalid clockdomain * pointers, -ENOENT if @clkdm2 cannot wake up clkdm1 in hardware, or * 0 upon success. */ int clkdm_del_wkdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2) { struct clkdm_dep *cd; int ret = 0; if (!clkdm1 || !clkdm2) return -EINVAL; cd = _clkdm_deps_lookup(clkdm2, clkdm1->wkdep_srcs); if (IS_ERR(cd)) ret = PTR_ERR(cd); if (!arch_clkdm || !arch_clkdm->clkdm_del_wkdep) ret = -EINVAL; if (ret) { pr_debug("clockdomain: hardware cannot set/clear wake up of " "%s when %s wakes up\n", clkdm1->name, clkdm2->name); return ret; } if (atomic_dec_return(&cd->wkdep_usecount) == 0) { pr_debug("clockdomain: hardware will no longer wake up %s " "after %s wakes up\n", clkdm1->name, clkdm2->name); ret = arch_clkdm->clkdm_del_wkdep(clkdm1, clkdm2); } return ret; } /** * clkdm_read_wkdep - read wakeup dependency state from clkdm2 to clkdm1 * @clkdm1: wake this struct clockdomain * up (dependent) * @clkdm2: when this struct clockdomain * wakes up (source) * * Return 1 if a hardware wakeup dependency exists wherein @clkdm1 will be * awoken when @clkdm2 wakes up; 0 if dependency is not set; -EINVAL * if either clockdomain pointer is invalid; or -ENOENT if the hardware * is incapable. * * REVISIT: Currently this function only represents software-controllable * wakeup dependencies. Wakeup dependencies fixed in hardware are not * yet handled here. */ int clkdm_read_wkdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2) { struct clkdm_dep *cd; int ret = 0; if (!clkdm1 || !clkdm2) return -EINVAL; cd = _clkdm_deps_lookup(clkdm2, clkdm1->wkdep_srcs); if (IS_ERR(cd)) ret = PTR_ERR(cd); if (!arch_clkdm || !arch_clkdm->clkdm_read_wkdep) ret = -EINVAL; if (ret) { pr_debug("clockdomain: hardware cannot set/clear wake up of " "%s when %s wakes up\n", clkdm1->name, clkdm2->name); return ret; } /* XXX It's faster to return the atomic wkdep_usecount */ return arch_clkdm->clkdm_read_wkdep(clkdm1, clkdm2); } /** * clkdm_clear_all_wkdeps - remove all wakeup dependencies from target clkdm * @clkdm: struct clockdomain * to remove all wakeup dependencies from * * Remove all inter-clockdomain wakeup dependencies that could cause * @clkdm to wake. Intended to be used during boot to initialize the * PRCM to a known state, after all clockdomains are put into swsup idle * and woken up. Returns -EINVAL if @clkdm pointer is invalid, or * 0 upon success. */ int clkdm_clear_all_wkdeps(struct clockdomain *clkdm) { if (!clkdm) return -EINVAL; if (!arch_clkdm || !arch_clkdm->clkdm_clear_all_wkdeps) return -EINVAL; return arch_clkdm->clkdm_clear_all_wkdeps(clkdm); } /** * clkdm_add_sleepdep - add a sleep dependency from clkdm2 to clkdm1 * @clkdm1: prevent this struct clockdomain * from sleeping (dependent) * @clkdm2: when this struct clockdomain * is active (source) * * Prevent @clkdm1 from automatically going inactive (and then to * retention or off) if @clkdm2 is active. Returns -EINVAL if * presented with invalid clockdomain pointers or called on a machine * that does not support software-configurable hardware sleep * dependencies, -ENOENT if the specified dependency cannot be set in * hardware, or 0 upon success. */ int clkdm_add_sleepdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2) { struct clkdm_dep *cd; int ret = 0; if (!clkdm1 || !clkdm2) return -EINVAL; cd = _clkdm_deps_lookup(clkdm2, clkdm1->sleepdep_srcs); if (IS_ERR(cd)) ret = PTR_ERR(cd); if (!arch_clkdm || !arch_clkdm->clkdm_add_sleepdep) ret = -EINVAL; if (ret) { pr_debug("clockdomain: hardware cannot set/clear sleep " "dependency affecting %s from %s\n", clkdm1->name, clkdm2->name); return ret; } if (atomic_inc_return(&cd->sleepdep_usecount) == 1) { pr_debug("clockdomain: will prevent %s from sleeping if %s " "is active\n", clkdm1->name, clkdm2->name); ret = arch_clkdm->clkdm_add_sleepdep(clkdm1, clkdm2); } return ret; } /** * clkdm_del_sleepdep - remove a sleep dependency from clkdm2 to clkdm1 * @clkdm1: prevent this struct clockdomain * from sleeping (dependent) * @clkdm2: when this struct clockdomain * is active (source) * * Allow @clkdm1 to automatically go inactive (and then to retention or * off), independent of the activity state of @clkdm2. Returns -EINVAL * if presented with invalid clockdomain pointers or called on a machine * that does not support software-configurable hardware sleep dependencies, * -ENOENT if the specified dependency cannot be cleared in hardware, or * 0 upon success. */ int clkdm_del_sleepdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2) { struct clkdm_dep *cd; int ret = 0; if (!clkdm1 || !clkdm2) return -EINVAL; cd = _clkdm_deps_lookup(clkdm2, clkdm1->sleepdep_srcs); if (IS_ERR(cd)) ret = PTR_ERR(cd); if (!arch_clkdm || !arch_clkdm->clkdm_del_sleepdep) ret = -EINVAL; if (ret) { pr_debug("clockdomain: hardware cannot set/clear sleep " "dependency affecting %s from %s\n", clkdm1->name, clkdm2->name); return ret; } if (atomic_dec_return(&cd->sleepdep_usecount) == 0) { pr_debug("clockdomain: will no longer prevent %s from " "sleeping if %s is active\n", clkdm1->name, clkdm2->name); ret = arch_clkdm->clkdm_del_sleepdep(clkdm1, clkdm2); } return ret; } /** * clkdm_read_sleepdep - read sleep dependency state from clkdm2 to clkdm1 * @clkdm1: prevent this struct clockdomain * from sleeping (dependent) * @clkdm2: when this struct clockdomain * is active (source) * * Return 1 if a hardware sleep dependency exists wherein @clkdm1 will * not be allowed to automatically go inactive if @clkdm2 is active; * 0 if @clkdm1's automatic power state inactivity transition is independent * of @clkdm2's; -EINVAL if either clockdomain pointer is invalid or called * on a machine that does not support software-configurable hardware sleep * dependencies; or -ENOENT if the hardware is incapable. * * REVISIT: Currently this function only represents software-controllable * sleep dependencies. Sleep dependencies fixed in hardware are not * yet handled here. */ int clkdm_read_sleepdep(struct clockdomain *clkdm1, struct clockdomain *clkdm2) { struct clkdm_dep *cd; int ret = 0; if (!clkdm1 || !clkdm2) return -EINVAL; cd = _clkdm_deps_lookup(clkdm2, clkdm1->sleepdep_srcs); if (IS_ERR(cd)) ret = PTR_ERR(cd); if (!arch_clkdm || !arch_clkdm->clkdm_read_sleepdep) ret = -EINVAL; if (ret) { pr_debug("clockdomain: hardware cannot set/clear sleep " "dependency affecting %s from %s\n", clkdm1->name, clkdm2->name); return ret; } /* XXX It's faster to return the atomic sleepdep_usecount */ return arch_clkdm->clkdm_read_sleepdep(clkdm1, clkdm2); } /** * clkdm_clear_all_sleepdeps - remove all sleep dependencies from target clkdm * @clkdm: struct clockdomain * to remove all sleep dependencies from * * Remove all inter-clockdomain sleep dependencies that could prevent * @clkdm from idling. Intended to be used during boot to initialize the * PRCM to a known state, after all clockdomains are put into swsup idle * and woken up. Returns -EINVAL if @clkdm pointer is invalid, or * 0 upon success. */ int clkdm_clear_all_sleepdeps(struct clockdomain *clkdm) { if (!clkdm) return -EINVAL; if (!arch_clkdm || !arch_clkdm->clkdm_clear_all_sleepdeps) return -EINVAL; return arch_clkdm->clkdm_clear_all_sleepdeps(clkdm); } /** * clkdm_sleep - force clockdomain sleep transition * @clkdm: struct clockdomain * * * Instruct the CM to force a sleep transition on the specified * clockdomain @clkdm. Returns -EINVAL if @clkdm is NULL or if * clockdomain does not support software-initiated sleep; 0 upon * success. */ int clkdm_sleep(struct clockdomain *clkdm) { int ret; unsigned long flags; if (!clkdm) return -EINVAL; if (!(clkdm->flags & CLKDM_CAN_FORCE_SLEEP)) { pr_debug("clockdomain: %s does not support forcing " "sleep via software\n", clkdm->name); return -EINVAL; } if (!arch_clkdm || !arch_clkdm->clkdm_sleep) return -EINVAL; pr_debug("clockdomain: forcing sleep on %s\n", clkdm->name); spin_lock_irqsave(&clkdm->lock, flags); clkdm->_flags &= ~_CLKDM_FLAG_HWSUP_ENABLED; ret = arch_clkdm->clkdm_sleep(clkdm); spin_unlock_irqrestore(&clkdm->lock, flags); return ret; } /** * clkdm_wakeup - force clockdomain wakeup transition * @clkdm: struct clockdomain * * * Instruct the CM to force a wakeup transition on the specified * clockdomain @clkdm. Returns -EINVAL if @clkdm is NULL or if the * clockdomain does not support software-controlled wakeup; 0 upon * success. */ int clkdm_wakeup(struct clockdomain *clkdm) { int ret; unsigned long flags; if (!clkdm) return -EINVAL; if (!(clkdm->flags & CLKDM_CAN_FORCE_WAKEUP)) { pr_debug("clockdomain: %s does not support forcing " "wakeup via software\n", clkdm->name); return -EINVAL; } if (!arch_clkdm || !arch_clkdm->clkdm_wakeup) return -EINVAL; pr_debug("clockdomain: forcing wakeup on %s\n", clkdm->name); spin_lock_irqsave(&clkdm->lock, flags); clkdm->_flags &= ~_CLKDM_FLAG_HWSUP_ENABLED; ret = arch_clkdm->clkdm_wakeup(clkdm); ret |= pwrdm_state_switch(clkdm->pwrdm.ptr); spin_unlock_irqrestore(&clkdm->lock, flags); return ret; } /** * clkdm_allow_idle - enable hwsup idle transitions for clkdm * @clkdm: struct clockdomain * * * Allow the hardware to automatically switch the clockdomain @clkdm into * active or idle states, as needed by downstream clocks. If the * clockdomain has any downstream clocks enabled in the clock * framework, wkdep/sleepdep autodependencies are added; this is so * device drivers can read and write to the device. No return value. */ void clkdm_allow_idle(struct clockdomain *clkdm) { unsigned long flags; if (!clkdm) return; if (!(clkdm->flags & CLKDM_CAN_ENABLE_AUTO)) { pr_debug("clock: automatic idle transitions cannot be enabled " "on clockdomain %s\n", clkdm->name); return; } if (!arch_clkdm || !arch_clkdm->clkdm_allow_idle) return; pr_debug("clockdomain: enabling automatic idle transitions for %s\n", clkdm->name); spin_lock_irqsave(&clkdm->lock, flags); clkdm->_flags |= _CLKDM_FLAG_HWSUP_ENABLED; arch_clkdm->clkdm_allow_idle(clkdm); pwrdm_clkdm_state_switch(clkdm); spin_unlock_irqrestore(&clkdm->lock, flags); } /** * clkdm_deny_idle - disable hwsup idle transitions for clkdm * @clkdm: struct clockdomain * * * Prevent the hardware from automatically switching the clockdomain * @clkdm into inactive or idle states. If the clockdomain has * downstream clocks enabled in the clock framework, wkdep/sleepdep * autodependencies are removed. No return value. */ void clkdm_deny_idle(struct clockdomain *clkdm) { unsigned long flags; if (!clkdm) return; if (!(clkdm->flags & CLKDM_CAN_DISABLE_AUTO)) { pr_debug("clockdomain: automatic idle transitions cannot be " "disabled on %s\n", clkdm->name); return; } if (!arch_clkdm || !arch_clkdm->clkdm_deny_idle) return; pr_debug("clockdomain: disabling automatic idle transitions for %s\n", clkdm->name); spin_lock_irqsave(&clkdm->lock, flags); clkdm->_flags &= ~_CLKDM_FLAG_HWSUP_ENABLED; arch_clkdm->clkdm_deny_idle(clkdm); pwrdm_state_switch(clkdm->pwrdm.ptr); spin_unlock_irqrestore(&clkdm->lock, flags); } /** * clkdm_in_hwsup - is clockdomain @clkdm have hardware-supervised idle enabled? * @clkdm: struct clockdomain * * * Returns true if clockdomain @clkdm currently has * hardware-supervised idle enabled, or false if it does not or if * @clkdm is NULL. It is only valid to call this function after * clkdm_init() has been called. This function does not actually read * bits from the hardware; it instead tests an in-memory flag that is * changed whenever the clockdomain code changes the auto-idle mode. */ bool clkdm_in_hwsup(struct clockdomain *clkdm) { bool ret; unsigned long flags; if (!clkdm) return false; spin_lock_irqsave(&clkdm->lock, flags); ret = (clkdm->_flags & _CLKDM_FLAG_HWSUP_ENABLED) ? true : false; spin_unlock_irqrestore(&clkdm->lock, flags); return ret; } /* Clockdomain-to-clock/hwmod framework interface code */ static int _clkdm_clk_hwmod_enable(struct clockdomain *clkdm) { unsigned long flags; if (!clkdm || !arch_clkdm || !arch_clkdm->clkdm_clk_enable) return -EINVAL; /* * For arch's with no autodeps, clkcm_clk_enable * should be called for every clock instance or hwmod that is * enabled, so the clkdm can be force woken up. */ if ((atomic_inc_return(&clkdm->usecount) > 1) && autodeps) return 0; spin_lock_irqsave(&clkdm->lock, flags); arch_clkdm->clkdm_clk_enable(clkdm); pwrdm_wait_transition(clkdm->pwrdm.ptr); pwrdm_clkdm_state_switch(clkdm); spin_unlock_irqrestore(&clkdm->lock, flags); pr_debug("clockdomain: clkdm %s: enabled\n", clkdm->name); return 0; } static int _clkdm_clk_hwmod_disable(struct clockdomain *clkdm) { unsigned long flags; if (!clkdm || !arch_clkdm || !arch_clkdm->clkdm_clk_disable) return -EINVAL; if (atomic_read(&clkdm->usecount) == 0) { WARN_ON(1); /* underflow */ return -ERANGE; } if (atomic_dec_return(&clkdm->usecount) > 0) return 0; spin_lock_irqsave(&clkdm->lock, flags); arch_clkdm->clkdm_clk_disable(clkdm); pwrdm_clkdm_state_switch(clkdm); spin_unlock_irqrestore(&clkdm->lock, flags); pr_debug("clockdomain: clkdm %s: disabled\n", clkdm->name); return 0; } /** * clkdm_clk_enable - add an enabled downstream clock to this clkdm * @clkdm: struct clockdomain * * @clk: struct clk * of the enabled downstream clock * * Increment the usecount of the clockdomain @clkdm and ensure that it * is awake before @clk is enabled. Intended to be called by * clk_enable() code. If the clockdomain is in software-supervised * idle mode, force the clockdomain to wake. If the clockdomain is in * hardware-supervised idle mode, add clkdm-pwrdm autodependencies, to * ensure that devices in the clockdomain can be read from/written to * by on-chip processors. Returns -EINVAL if passed null pointers; * returns 0 upon success or if the clockdomain is in hwsup idle mode. */ int clkdm_clk_enable(struct clockdomain *clkdm, struct clk *clk) { /* * XXX Rewrite this code to maintain a list of enabled * downstream clocks for debugging purposes? */ if (!clk) return -EINVAL; return _clkdm_clk_hwmod_enable(clkdm); } /** * clkdm_clk_disable - remove an enabled downstream clock from this clkdm * @clkdm: struct clockdomain * * @clk: struct clk * of the disabled downstream clock * * Decrement the usecount of this clockdomain @clkdm when @clk is * disabled. Intended to be called by clk_disable() code. If the * clockdomain usecount goes to 0, put the clockdomain to sleep * (software-supervised mode) or remove the clkdm autodependencies * (hardware-supervised mode). Returns -EINVAL if passed null * pointers; -ERANGE if the @clkdm usecount underflows; or returns 0 * upon success or if the clockdomain is in hwsup idle mode. */ int clkdm_clk_disable(struct clockdomain *clkdm, struct clk *clk) { /* * XXX Rewrite this code to maintain a list of enabled * downstream clocks for debugging purposes? */ if (!clk) return -EINVAL; return _clkdm_clk_hwmod_disable(clkdm); } /** * clkdm_hwmod_enable - add an enabled downstream hwmod to this clkdm * @clkdm: struct clockdomain * * @oh: struct omap_hwmod * of the enabled downstream hwmod * * Increment the usecount of the clockdomain @clkdm and ensure that it * is awake before @oh is enabled. Intended to be called by * module_enable() code. * If the clockdomain is in software-supervised idle mode, force the * clockdomain to wake. If the clockdomain is in hardware-supervised idle * mode, add clkdm-pwrdm autodependencies, to ensure that devices in the * clockdomain can be read from/written to by on-chip processors. * Returns -EINVAL if passed null pointers; * returns 0 upon success or if the clockdomain is in hwsup idle mode. */ int clkdm_hwmod_enable(struct clockdomain *clkdm, struct omap_hwmod *oh) { /* The clkdm attribute does not exist yet prior OMAP4 */ if (cpu_is_omap24xx() || cpu_is_omap34xx()) return 0; /* * XXX Rewrite this code to maintain a list of enabled * downstream hwmods for debugging purposes? */ if (!oh) return -EINVAL; return _clkdm_clk_hwmod_enable(clkdm); } /** * clkdm_hwmod_disable - remove an enabled downstream hwmod from this clkdm * @clkdm: struct clockdomain * * @oh: struct omap_hwmod * of the disabled downstream hwmod * * Decrement the usecount of this clockdomain @clkdm when @oh is * disabled. Intended to be called by module_disable() code. * If the clockdomain usecount goes to 0, put the clockdomain to sleep * (software-supervised mode) or remove the clkdm autodependencies * (hardware-supervised mode). * Returns -EINVAL if passed null pointers; -ERANGE if the @clkdm usecount * underflows; or returns 0 upon success or if the clockdomain is in hwsup * idle mode. */ int clkdm_hwmod_disable(struct clockdomain *clkdm, struct omap_hwmod *oh) { /* The clkdm attribute does not exist yet prior OMAP4 */ if (cpu_is_omap24xx() || cpu_is_omap34xx()) return 0; /* * XXX Rewrite this code to maintain a list of enabled * downstream hwmods for debugging purposes? */ if (!oh) return -EINVAL; return _clkdm_clk_hwmod_disable(clkdm); }