/* * opp2420_data.c - old-style "OPP" table for OMAP2420 * * Copyright (C) 2005-2009 Texas Instruments, Inc. * Copyright (C) 2004-2009 Nokia Corporation * * Richard Woodruff * * The OMAP2 processor can be run at several discrete 'PRCM configurations'. * These configurations are characterized by voltage and speed for clocks. * The device is only validated for certain combinations. One way to express * these combinations is via the 'ratios' which the clocks operate with * respect to each other. These ratio sets are for a given voltage/DPLL * setting. All configurations can be described by a DPLL setting and a ratio. * * XXX Missing voltage data. * XXX Missing 19.2MHz sys_clk rate sets (needed for N800/N810) * * THe format described in this file is deprecated. Once a reasonable * OPP API exists, the data in this file should be converted to use it. * * This is technically part of the OMAP2xxx clock code. * * Considerable work is still needed to fully support dynamic frequency * changes on OMAP2xxx-series chips. Readers interested in such a * project are encouraged to review the Maemo Diablo RX-34 and RX-44 * kernel source at: * http://repository.maemo.org/pool/diablo/free/k/kernel-source-diablo/ */ #include "opp2xxx.h" #include "sdrc.h" #include "clock.h" /* * Key dividers which make up a PRCM set. Ratios for a PRCM are mandated. * xtal_speed, dpll_speed, mpu_speed, CM_CLKSEL_MPU, * CM_CLKSEL_DSP, CM_CLKSEL_GFX, CM_CLKSEL1_CORE, CM_CLKSEL1_PLL, * CM_CLKSEL2_PLL, CM_CLKSEL_MDM * * Filling in table based on H4 boards available. There are quite a * few more rate combinations which could be defined. * * When multiple values are defined the start up will try and choose * the fastest one. If a 'fast' value is defined, then automatically, * the /2 one should be included as it can be used. Generally having * more than one fast set does not make sense, as static timings need * to be changed to change the set. The exception is the bypass * setting which is available for low power bypass. * * Note: This table needs to be sorted, fastest to slowest. **/ const struct prcm_config omap2420_rate_table[] = { /* PRCM I - FAST */ {S12M, S660M, S330M, RI_CM_CLKSEL_MPU_VAL, /* 330MHz ARM */ RI_CM_CLKSEL_DSP_VAL, RI_CM_CLKSEL_GFX_VAL, RI_CM_CLKSEL1_CORE_VAL, MI_CM_CLKSEL1_PLL_12_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_165MHz, RATE_IN_242X}, /* PRCM II - FAST */ {S12M, S600M, S300M, RII_CM_CLKSEL_MPU_VAL, /* 300MHz ARM */ RII_CM_CLKSEL_DSP_VAL, RII_CM_CLKSEL_GFX_VAL, RII_CM_CLKSEL1_CORE_VAL, MII_CM_CLKSEL1_PLL_12_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_100MHz, RATE_IN_242X}, {S13M, S600M, S300M, RII_CM_CLKSEL_MPU_VAL, /* 300MHz ARM */ RII_CM_CLKSEL_DSP_VAL, RII_CM_CLKSEL_GFX_VAL, RII_CM_CLKSEL1_CORE_VAL, MII_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_100MHz, RATE_IN_242X}, /* PRCM III - FAST */ {S12M, S532M, S266M, RIII_CM_CLKSEL_MPU_VAL, /* 266MHz ARM */ RIII_CM_CLKSEL_DSP_VAL, RIII_CM_CLKSEL_GFX_VAL, RIII_CM_CLKSEL1_CORE_VAL, MIII_CM_CLKSEL1_PLL_12_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_133MHz, RATE_IN_242X}, {S13M, S532M, S266M, RIII_CM_CLKSEL_MPU_VAL, /* 266MHz ARM */ RIII_CM_CLKSEL_DSP_VAL, RIII_CM_CLKSEL_GFX_VAL, RIII_CM_CLKSEL1_CORE_VAL, MIII_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_133MHz, RATE_IN_242X}, /* PRCM II - SLOW */ {S12M, S300M, S150M, RII_CM_CLKSEL_MPU_VAL, /* 150MHz ARM */ RII_CM_CLKSEL_DSP_VAL, RII_CM_CLKSEL_GFX_VAL, RII_CM_CLKSEL1_CORE_VAL, MII_CM_CLKSEL1_PLL_12_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_100MHz, RATE_IN_242X}, {S13M, S300M, S150M, RII_CM_CLKSEL_MPU_VAL, /* 150MHz ARM */ RII_CM_CLKSEL_DSP_VAL, RII_CM_CLKSEL_GFX_VAL, RII_CM_CLKSEL1_CORE_VAL, MII_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_100MHz, RATE_IN_242X}, /* PRCM III - SLOW */ {S12M, S266M, S133M, RIII_CM_CLKSEL_MPU_VAL, /* 133MHz ARM */ RIII_CM_CLKSEL_DSP_VAL, RIII_CM_CLKSEL_GFX_VAL, RIII_CM_CLKSEL1_CORE_VAL, MIII_CM_CLKSEL1_PLL_12_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_133MHz, RATE_IN_242X}, {S13M, S266M, S133M, RIII_CM_CLKSEL_MPU_VAL, /* 133MHz ARM */ RIII_CM_CLKSEL_DSP_VAL, RIII_CM_CLKSEL_GFX_VAL, RIII_CM_CLKSEL1_CORE_VAL, MIII_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_133MHz, RATE_IN_242X}, /* PRCM-VII (boot-bypass) */ {S12M, S12M, S12M, RVII_CM_CLKSEL_MPU_VAL, /* 12MHz ARM*/ RVII_CM_CLKSEL_DSP_VAL, RVII_CM_CLKSEL_GFX_VAL, RVII_CM_CLKSEL1_CORE_VAL, MVII_CM_CLKSEL1_PLL_12_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_BYPASS, RATE_IN_242X}, /* PRCM-VII (boot-bypass) */ {S13M, S13M, S13M, RVII_CM_CLKSEL_MPU_VAL, /* 13MHz ARM */ RVII_CM_CLKSEL_DSP_VAL, RVII_CM_CLKSEL_GFX_VAL, RVII_CM_CLKSEL1_CORE_VAL, MVII_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, 0, SDRC_RFR_CTRL_BYPASS, RATE_IN_242X}, { 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0}, };