/* * opp2430_data.c - old-style "OPP" table for OMAP2430 * * Copyright (C) 2005-2009 Texas Instruments, Inc. * Copyright (C) 2004-2009 Nokia Corporation * * Richard Woodruff * * The OMAP2 processor can be run at several discrete 'PRCM configurations'. * These configurations are characterized by voltage and speed for clocks. * The device is only validated for certain combinations. One way to express * these combinations is via the 'ratios' which the clocks operate with * respect to each other. These ratio sets are for a given voltage/DPLL * setting. All configurations can be described by a DPLL setting and a ratio. * * 2430 differs from 2420 in that there are no more phase synchronizers used. * They both have a slightly different clock domain setup. 2420(iva1,dsp) vs * 2430 (iva2.1, NOdsp, mdm) * * XXX Missing voltage data. * XXX Missing 19.2MHz sys_clk rate sets. * * THe format described in this file is deprecated. Once a reasonable * OPP API exists, the data in this file should be converted to use it. * * This is technically part of the OMAP2xxx clock code. */ #include "opp2xxx.h" #include "sdrc.h" #include "clock.h" /* * Key dividers which make up a PRCM set. Ratios for a PRCM are mandated. * xtal_speed, dpll_speed, mpu_speed, CM_CLKSEL_MPU, * CM_CLKSEL_DSP, CM_CLKSEL_GFX, CM_CLKSEL1_CORE, CM_CLKSEL1_PLL, * CM_CLKSEL2_PLL, CM_CLKSEL_MDM * * Filling in table based on 2430-SDPs variants available. There are * quite a few more rate combinations which could be defined. * * When multiple values are defined the start up will try and choose * the fastest one. If a 'fast' value is defined, then automatically, * the /2 one should be included as it can be used. Generally having * more than one fast set does not make sense, as static timings need * to be changed to change the set. The exception is the bypass * setting which is available for low power bypass. * * Note: This table needs to be sorted, fastest to slowest. */ const struct prcm_config omap2430_rate_table[] = { /* PRCM #4 - ratio2 (ES2.1) - FAST */ {S13M, S798M, S399M, R2_CM_CLKSEL_MPU_VAL, /* 399MHz ARM */ R2_CM_CLKSEL_DSP_VAL, R2_CM_CLKSEL_GFX_VAL, R2_CM_CLKSEL1_CORE_VAL, M4_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, R2_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_133MHz, RATE_IN_243X}, /* PRCM #2 - ratio1 (ES2) - FAST */ {S13M, S658M, S329M, R1_CM_CLKSEL_MPU_VAL, /* 330MHz ARM */ R1_CM_CLKSEL_DSP_VAL, R1_CM_CLKSEL_GFX_VAL, R1_CM_CLKSEL1_CORE_VAL, M2_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, R1_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_165MHz, RATE_IN_243X}, /* PRCM #5a - ratio1 - FAST */ {S13M, S532M, S266M, R1_CM_CLKSEL_MPU_VAL, /* 266MHz ARM */ R1_CM_CLKSEL_DSP_VAL, R1_CM_CLKSEL_GFX_VAL, R1_CM_CLKSEL1_CORE_VAL, M5A_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, R1_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_133MHz, RATE_IN_243X}, /* PRCM #5b - ratio1 - FAST */ {S13M, S400M, S200M, R1_CM_CLKSEL_MPU_VAL, /* 200MHz ARM */ R1_CM_CLKSEL_DSP_VAL, R1_CM_CLKSEL_GFX_VAL, R1_CM_CLKSEL1_CORE_VAL, M5B_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, R1_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_100MHz, RATE_IN_243X}, /* PRCM #4 - ratio1 (ES2.1) - SLOW */ {S13M, S399M, S199M, R2_CM_CLKSEL_MPU_VAL, /* 200MHz ARM */ R2_CM_CLKSEL_DSP_VAL, R2_CM_CLKSEL_GFX_VAL, R2_CM_CLKSEL1_CORE_VAL, M4_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_1x_VAL, R2_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_133MHz, RATE_IN_243X}, /* PRCM #2 - ratio1 (ES2) - SLOW */ {S13M, S329M, S164M, R1_CM_CLKSEL_MPU_VAL, /* 165MHz ARM */ R1_CM_CLKSEL_DSP_VAL, R1_CM_CLKSEL_GFX_VAL, R1_CM_CLKSEL1_CORE_VAL, M2_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_1x_VAL, R1_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_165MHz, RATE_IN_243X}, /* PRCM #5a - ratio1 - SLOW */ {S13M, S266M, S133M, R1_CM_CLKSEL_MPU_VAL, /* 133MHz ARM */ R1_CM_CLKSEL_DSP_VAL, R1_CM_CLKSEL_GFX_VAL, R1_CM_CLKSEL1_CORE_VAL, M5A_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_1x_VAL, R1_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_133MHz, RATE_IN_243X}, /* PRCM #5b - ratio1 - SLOW*/ {S13M, S200M, S100M, R1_CM_CLKSEL_MPU_VAL, /* 100MHz ARM */ R1_CM_CLKSEL_DSP_VAL, R1_CM_CLKSEL_GFX_VAL, R1_CM_CLKSEL1_CORE_VAL, M5B_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_1x_VAL, R1_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_100MHz, RATE_IN_243X}, /* PRCM-boot/bypass */ {S13M, S13M, S13M, RB_CM_CLKSEL_MPU_VAL, /* 13Mhz */ RB_CM_CLKSEL_DSP_VAL, RB_CM_CLKSEL_GFX_VAL, RB_CM_CLKSEL1_CORE_VAL, MB_CM_CLKSEL1_PLL_13_VAL, MX_CLKSEL2_PLL_2x_VAL, RB_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_BYPASS, RATE_IN_243X}, /* PRCM-boot/bypass */ {S12M, S12M, S12M, RB_CM_CLKSEL_MPU_VAL, /* 12Mhz */ RB_CM_CLKSEL_DSP_VAL, RB_CM_CLKSEL_GFX_VAL, RB_CM_CLKSEL1_CORE_VAL, MB_CM_CLKSEL1_PLL_12_VAL, MX_CLKSEL2_PLL_2x_VAL, RB_CM_CLKSEL_MDM_VAL, SDRC_RFR_CTRL_BYPASS, RATE_IN_243X}, { 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0}, };