/* * pm.c - Common OMAP2+ power management-related code * * Copyright (C) 2010 Texas Instruments, Inc. * Copyright (C) 2010 Nokia Corporation * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include #include #include #include #include #include #include #include #include "common.h" #include "voltage.h" #include "powerdomain.h" #include "clockdomain.h" #include "pm.h" #include "twl-common.h" static struct omap_device_pm_latency *pm_lats; static int _init_omap_device(char *name) { struct omap_hwmod *oh; struct platform_device *pdev; oh = omap_hwmod_lookup(name); if (WARN(!oh, "%s: could not find omap_hwmod for %s\n", __func__, name)) return -ENODEV; pdev = omap_device_build(oh->name, 0, oh, NULL, 0, pm_lats, 0, false); if (WARN(IS_ERR(pdev), "%s: could not build omap_device for %s\n", __func__, name)) return -ENODEV; return 0; } /* * Build omap_devices for processors and bus. */ static void omap2_init_processor_devices(void) { _init_omap_device("mpu"); if (omap3_has_iva()) _init_omap_device("iva"); if (cpu_is_omap44xx()) { _init_omap_device("l3_main_1"); _init_omap_device("dsp"); _init_omap_device("iva"); } else { _init_omap_device("l3_main"); } } /* Types of sleep_switch used in omap_set_pwrdm_state */ #define FORCEWAKEUP_SWITCH 0 #define LOWPOWERSTATE_SWITCH 1 /* * This sets pwrdm state (other than mpu & core. Currently only ON & * RET are supported. */ int omap_set_pwrdm_state(struct powerdomain *pwrdm, u32 state) { u32 cur_state; int sleep_switch = -1; int ret = 0; int hwsup = 0; if (pwrdm == NULL || IS_ERR(pwrdm)) return -EINVAL; while (!(pwrdm->pwrsts & (1 << state))) { if (state == PWRDM_POWER_OFF) return ret; state--; } cur_state = pwrdm_read_next_pwrst(pwrdm); if (cur_state == state) return ret; if (pwrdm_read_pwrst(pwrdm) < PWRDM_POWER_ON) { if ((pwrdm_read_pwrst(pwrdm) > state) && (pwrdm->flags & PWRDM_HAS_LOWPOWERSTATECHANGE)) { sleep_switch = LOWPOWERSTATE_SWITCH; } else { hwsup = clkdm_in_hwsup(pwrdm->pwrdm_clkdms[0]); clkdm_wakeup(pwrdm->pwrdm_clkdms[0]); sleep_switch = FORCEWAKEUP_SWITCH; } } ret = pwrdm_set_next_pwrst(pwrdm, state); if (ret) { pr_err("%s: unable to set state of powerdomain: %s\n", __func__, pwrdm->name); goto err; } switch (sleep_switch) { case FORCEWAKEUP_SWITCH: if (hwsup) clkdm_allow_idle(pwrdm->pwrdm_clkdms[0]); else clkdm_sleep(pwrdm->pwrdm_clkdms[0]); break; case LOWPOWERSTATE_SWITCH: pwrdm_set_lowpwrstchange(pwrdm); break; default: return ret; } pwrdm_state_switch(pwrdm); err: return ret; } /* * This API is to be called during init to set the various voltage * domains to the voltage as per the opp table. Typically we boot up * at the nominal voltage. So this function finds out the rate of * the clock associated with the voltage domain, finds out the correct * opp entry and sets the voltage domain to the voltage specified * in the opp entry */ static int __init omap2_set_init_voltage(char *vdd_name, char *clk_name, const char *oh_name) { struct voltagedomain *voltdm; struct clk *clk; struct opp *opp; unsigned long freq, bootup_volt; struct device *dev; if (!vdd_name || !clk_name || !oh_name) { pr_err("%s: invalid parameters\n", __func__); goto exit; } dev = omap_device_get_by_hwmod_name(oh_name); if (IS_ERR(dev)) { pr_err("%s: Unable to get dev pointer for hwmod %s\n", __func__, oh_name); goto exit; } voltdm = voltdm_lookup(vdd_name); if (IS_ERR(voltdm)) { pr_err("%s: unable to get vdd pointer for vdd_%s\n", __func__, vdd_name); goto exit; } clk = clk_get(NULL, clk_name); if (IS_ERR(clk)) { pr_err("%s: unable to get clk %s\n", __func__, clk_name); goto exit; } freq = clk->rate; clk_put(clk); opp = opp_find_freq_ceil(dev, &freq); if (IS_ERR(opp)) { pr_err("%s: unable to find boot up OPP for vdd_%s\n", __func__, vdd_name); goto exit; } bootup_volt = opp_get_voltage(opp); if (!bootup_volt) { pr_err("%s: unable to find voltage corresponding " "to the bootup OPP for vdd_%s\n", __func__, vdd_name); goto exit; } voltdm_scale(voltdm, bootup_volt); return 0; exit: pr_err("%s: unable to set vdd_%s\n", __func__, vdd_name); return -EINVAL; } static void __init omap3_init_voltages(void) { if (!cpu_is_omap34xx()) return; omap2_set_init_voltage("mpu_iva", "dpll1_ck", "mpu"); omap2_set_init_voltage("core", "l3_ick", "l3_main"); } static void __init omap4_init_voltages(void) { if (!cpu_is_omap44xx()) return; omap2_set_init_voltage("mpu", "dpll_mpu_ck", "mpu"); omap2_set_init_voltage("core", "l3_div_ck", "l3_main_1"); omap2_set_init_voltage("iva", "dpll_iva_m5x2_ck", "iva"); } static int __init omap2_common_pm_init(void) { if (!of_have_populated_dt()) omap2_init_processor_devices(); omap_pm_if_init(); return 0; } postcore_initcall(omap2_common_pm_init); static int __init omap2_common_pm_late_init(void) { /* Init the voltage layer */ omap_pmic_late_init(); omap_voltage_late_init(); /* Initialize the voltages */ omap3_init_voltages(); omap4_init_voltages(); /* Smartreflex device init */ omap_devinit_smartreflex(); return 0; } late_initcall(omap2_common_pm_late_init);