/* * OMAP2 Power Management Routines * * Copyright (C) 2005 Texas Instruments, Inc. * Copyright (C) 2006-2008 Nokia Corporation * * Written by: * Richard Woodruff * Tony Lindgren * Juha Yrjola * Amit Kucheria * Igor Stoppa * * Based on pm.c for omap1 * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "common.h" #include "prm2xxx_3xxx.h" #include "prm-regbits-24xx.h" #include "cm2xxx_3xxx.h" #include "cm-regbits-24xx.h" #include "sdrc.h" #include "pm.h" #include "control.h" #include "powerdomain.h" #include "clockdomain.h" #ifdef CONFIG_SUSPEND static suspend_state_t suspend_state = PM_SUSPEND_ON; static inline bool is_suspending(void) { return (suspend_state != PM_SUSPEND_ON); } #else static inline bool is_suspending(void) { return false; } #endif static void (*omap2_sram_idle)(void); static void (*omap2_sram_suspend)(u32 dllctrl, void __iomem *sdrc_dlla_ctrl, void __iomem *sdrc_power); static struct powerdomain *mpu_pwrdm, *core_pwrdm; static struct clockdomain *dsp_clkdm, *mpu_clkdm, *wkup_clkdm, *gfx_clkdm; static struct clk *osc_ck, *emul_ck; static int omap2_fclks_active(void) { u32 f1, f2; f1 = omap2_cm_read_mod_reg(CORE_MOD, CM_FCLKEN1); f2 = omap2_cm_read_mod_reg(CORE_MOD, OMAP24XX_CM_FCLKEN2); /* Ignore UART clocks. These are handled by UART core (serial.c) */ f1 &= ~(OMAP24XX_EN_UART1_MASK | OMAP24XX_EN_UART2_MASK); f2 &= ~OMAP24XX_EN_UART3_MASK; if (f1 | f2) return 1; return 0; } static void omap2_enter_full_retention(void) { u32 l; /* There is 1 reference hold for all children of the oscillator * clock, the following will remove it. If no one else uses the * oscillator itself it will be disabled if/when we enter retention * mode. */ clk_disable(osc_ck); /* Clear old wake-up events */ /* REVISIT: These write to reserved bits? */ omap2_prm_write_mod_reg(0xffffffff, CORE_MOD, PM_WKST1); omap2_prm_write_mod_reg(0xffffffff, CORE_MOD, OMAP24XX_PM_WKST2); omap2_prm_write_mod_reg(0xffffffff, WKUP_MOD, PM_WKST); /* * Set MPU powerdomain's next power state to RETENTION; * preserve logic state during retention */ pwrdm_set_logic_retst(mpu_pwrdm, PWRDM_POWER_RET); pwrdm_set_next_pwrst(mpu_pwrdm, PWRDM_POWER_RET); /* Workaround to kill USB */ l = omap_ctrl_readl(OMAP2_CONTROL_DEVCONF0) | OMAP24XX_USBSTANDBYCTRL; omap_ctrl_writel(l, OMAP2_CONTROL_DEVCONF0); omap2_gpio_prepare_for_idle(0); /* One last check for pending IRQs to avoid extra latency due * to sleeping unnecessarily. */ if (omap_irq_pending()) goto no_sleep; /* Jump to SRAM suspend code */ omap2_sram_suspend(sdrc_read_reg(SDRC_DLLA_CTRL), OMAP_SDRC_REGADDR(SDRC_DLLA_CTRL), OMAP_SDRC_REGADDR(SDRC_POWER)); no_sleep: omap2_gpio_resume_after_idle(); clk_enable(osc_ck); /* clear CORE wake-up events */ omap2_prm_write_mod_reg(0xffffffff, CORE_MOD, PM_WKST1); omap2_prm_write_mod_reg(0xffffffff, CORE_MOD, OMAP24XX_PM_WKST2); /* wakeup domain events - bit 1: GPT1, bit5 GPIO */ omap2_prm_clear_mod_reg_bits(0x4 | 0x1, WKUP_MOD, PM_WKST); /* MPU domain wake events */ l = omap2_prm_read_mod_reg(OCP_MOD, OMAP2_PRCM_IRQSTATUS_MPU_OFFSET); if (l & 0x01) omap2_prm_write_mod_reg(0x01, OCP_MOD, OMAP2_PRCM_IRQSTATUS_MPU_OFFSET); if (l & 0x20) omap2_prm_write_mod_reg(0x20, OCP_MOD, OMAP2_PRCM_IRQSTATUS_MPU_OFFSET); /* Mask future PRCM-to-MPU interrupts */ omap2_prm_write_mod_reg(0x0, OCP_MOD, OMAP2_PRCM_IRQSTATUS_MPU_OFFSET); } static int omap2_i2c_active(void) { u32 l; l = omap2_cm_read_mod_reg(CORE_MOD, CM_FCLKEN1); return l & (OMAP2420_EN_I2C2_MASK | OMAP2420_EN_I2C1_MASK); } static int sti_console_enabled; static int omap2_allow_mpu_retention(void) { u32 l; /* Check for MMC, UART2, UART1, McSPI2, McSPI1 and DSS1. */ l = omap2_cm_read_mod_reg(CORE_MOD, CM_FCLKEN1); if (l & (OMAP2420_EN_MMC_MASK | OMAP24XX_EN_UART2_MASK | OMAP24XX_EN_UART1_MASK | OMAP24XX_EN_MCSPI2_MASK | OMAP24XX_EN_MCSPI1_MASK | OMAP24XX_EN_DSS1_MASK)) return 0; /* Check for UART3. */ l = omap2_cm_read_mod_reg(CORE_MOD, OMAP24XX_CM_FCLKEN2); if (l & OMAP24XX_EN_UART3_MASK) return 0; if (sti_console_enabled) return 0; return 1; } static void omap2_enter_mpu_retention(void) { int only_idle = 0; /* Putting MPU into the WFI state while a transfer is active * seems to cause the I2C block to timeout. Why? Good question. */ if (omap2_i2c_active()) return; /* The peripherals seem not to be able to wake up the MPU when * it is in retention mode. */ if (omap2_allow_mpu_retention()) { /* REVISIT: These write to reserved bits? */ omap2_prm_write_mod_reg(0xffffffff, CORE_MOD, PM_WKST1); omap2_prm_write_mod_reg(0xffffffff, CORE_MOD, OMAP24XX_PM_WKST2); omap2_prm_write_mod_reg(0xffffffff, WKUP_MOD, PM_WKST); /* Try to enter MPU retention */ omap2_prm_write_mod_reg((0x01 << OMAP_POWERSTATE_SHIFT) | OMAP_LOGICRETSTATE_MASK, MPU_MOD, OMAP2_PM_PWSTCTRL); } else { /* Block MPU retention */ omap2_prm_write_mod_reg(OMAP_LOGICRETSTATE_MASK, MPU_MOD, OMAP2_PM_PWSTCTRL); only_idle = 1; } omap2_sram_idle(); } static int omap2_can_sleep(void) { if (omap2_fclks_active()) return 0; if (osc_ck->usecount > 1) return 0; if (omap_dma_running()) return 0; return 1; } static void omap2_pm_idle(void) { local_irq_disable(); local_fiq_disable(); if (!omap2_can_sleep()) { if (omap_irq_pending()) goto out; omap2_enter_mpu_retention(); goto out; } if (omap_irq_pending()) goto out; omap2_enter_full_retention(); out: local_fiq_enable(); local_irq_enable(); } #ifdef CONFIG_SUSPEND static int omap2_pm_begin(suspend_state_t state) { disable_hlt(); suspend_state = state; return 0; } static int omap2_pm_suspend(void) { u32 wken_wkup, mir1; wken_wkup = omap2_prm_read_mod_reg(WKUP_MOD, PM_WKEN); wken_wkup &= ~OMAP24XX_EN_GPT1_MASK; omap2_prm_write_mod_reg(wken_wkup, WKUP_MOD, PM_WKEN); /* Mask GPT1 */ mir1 = omap_readl(0x480fe0a4); omap_writel(1 << 5, 0x480fe0ac); omap2_enter_full_retention(); omap_writel(mir1, 0x480fe0a4); omap2_prm_write_mod_reg(wken_wkup, WKUP_MOD, PM_WKEN); return 0; } static int omap2_pm_enter(suspend_state_t state) { int ret = 0; switch (state) { case PM_SUSPEND_STANDBY: case PM_SUSPEND_MEM: ret = omap2_pm_suspend(); break; default: ret = -EINVAL; } return ret; } static void omap2_pm_end(void) { suspend_state = PM_SUSPEND_ON; enable_hlt(); } static const struct platform_suspend_ops omap_pm_ops = { .begin = omap2_pm_begin, .enter = omap2_pm_enter, .end = omap2_pm_end, .valid = suspend_valid_only_mem, }; #else static const struct platform_suspend_ops __initdata omap_pm_ops; #endif /* CONFIG_SUSPEND */ /* XXX This function should be shareable between OMAP2xxx and OMAP3 */ static int __init clkdms_setup(struct clockdomain *clkdm, void *unused) { if (clkdm->flags & CLKDM_CAN_ENABLE_AUTO) clkdm_allow_idle(clkdm); else if (clkdm->flags & CLKDM_CAN_FORCE_SLEEP && atomic_read(&clkdm->usecount) == 0) clkdm_sleep(clkdm); return 0; } static void __init prcm_setup_regs(void) { int i, num_mem_banks; struct powerdomain *pwrdm; /* * Enable autoidle * XXX This should be handled by hwmod code or PRCM init code */ omap2_prm_write_mod_reg(OMAP24XX_AUTOIDLE_MASK, OCP_MOD, OMAP2_PRCM_SYSCONFIG_OFFSET); /* * Set CORE powerdomain memory banks to retain their contents * during RETENTION */ num_mem_banks = pwrdm_get_mem_bank_count(core_pwrdm); for (i = 0; i < num_mem_banks; i++) pwrdm_set_mem_retst(core_pwrdm, i, PWRDM_POWER_RET); /* Set CORE powerdomain's next power state to RETENTION */ pwrdm_set_next_pwrst(core_pwrdm, PWRDM_POWER_RET); /* * Set MPU powerdomain's next power state to RETENTION; * preserve logic state during retention */ pwrdm_set_logic_retst(mpu_pwrdm, PWRDM_POWER_RET); pwrdm_set_next_pwrst(mpu_pwrdm, PWRDM_POWER_RET); /* Force-power down DSP, GFX powerdomains */ pwrdm = clkdm_get_pwrdm(dsp_clkdm); pwrdm_set_next_pwrst(pwrdm, PWRDM_POWER_OFF); clkdm_sleep(dsp_clkdm); pwrdm = clkdm_get_pwrdm(gfx_clkdm); pwrdm_set_next_pwrst(pwrdm, PWRDM_POWER_OFF); clkdm_sleep(gfx_clkdm); /* Enable hardware-supervised idle for all clkdms */ clkdm_for_each(clkdms_setup, NULL); clkdm_add_wkdep(mpu_clkdm, wkup_clkdm); /* REVISIT: Configure number of 32 kHz clock cycles for sys_clk * stabilisation */ omap2_prm_write_mod_reg(15 << OMAP_SETUP_TIME_SHIFT, OMAP24XX_GR_MOD, OMAP2_PRCM_CLKSSETUP_OFFSET); /* Configure automatic voltage transition */ omap2_prm_write_mod_reg(2 << OMAP_SETUP_TIME_SHIFT, OMAP24XX_GR_MOD, OMAP2_PRCM_VOLTSETUP_OFFSET); omap2_prm_write_mod_reg(OMAP24XX_AUTO_EXTVOLT_MASK | (0x1 << OMAP24XX_SETOFF_LEVEL_SHIFT) | OMAP24XX_MEMRETCTRL_MASK | (0x1 << OMAP24XX_SETRET_LEVEL_SHIFT) | (0x0 << OMAP24XX_VOLT_LEVEL_SHIFT), OMAP24XX_GR_MOD, OMAP2_PRCM_VOLTCTRL_OFFSET); /* Enable wake-up events */ omap2_prm_write_mod_reg(OMAP24XX_EN_GPIOS_MASK | OMAP24XX_EN_GPT1_MASK, WKUP_MOD, PM_WKEN); } static int __init omap2_pm_init(void) { u32 l; if (!cpu_is_omap24xx()) return -ENODEV; printk(KERN_INFO "Power Management for OMAP2 initializing\n"); l = omap2_prm_read_mod_reg(OCP_MOD, OMAP2_PRCM_REVISION_OFFSET); printk(KERN_INFO "PRCM revision %d.%d\n", (l >> 4) & 0x0f, l & 0x0f); /* Look up important powerdomains */ mpu_pwrdm = pwrdm_lookup("mpu_pwrdm"); if (!mpu_pwrdm) pr_err("PM: mpu_pwrdm not found\n"); core_pwrdm = pwrdm_lookup("core_pwrdm"); if (!core_pwrdm) pr_err("PM: core_pwrdm not found\n"); /* Look up important clockdomains */ mpu_clkdm = clkdm_lookup("mpu_clkdm"); if (!mpu_clkdm) pr_err("PM: mpu_clkdm not found\n"); wkup_clkdm = clkdm_lookup("wkup_clkdm"); if (!wkup_clkdm) pr_err("PM: wkup_clkdm not found\n"); dsp_clkdm = clkdm_lookup("dsp_clkdm"); if (!dsp_clkdm) pr_err("PM: dsp_clkdm not found\n"); gfx_clkdm = clkdm_lookup("gfx_clkdm"); if (!gfx_clkdm) pr_err("PM: gfx_clkdm not found\n"); osc_ck = clk_get(NULL, "osc_ck"); if (IS_ERR(osc_ck)) { printk(KERN_ERR "could not get osc_ck\n"); return -ENODEV; } if (cpu_is_omap242x()) { emul_ck = clk_get(NULL, "emul_ck"); if (IS_ERR(emul_ck)) { printk(KERN_ERR "could not get emul_ck\n"); clk_put(osc_ck); return -ENODEV; } } prcm_setup_regs(); /* Hack to prevent MPU retention when STI console is enabled. */ { const struct omap_sti_console_config *sti; sti = omap_get_config(OMAP_TAG_STI_CONSOLE, struct omap_sti_console_config); if (sti != NULL && sti->enable) sti_console_enabled = 1; } /* * We copy the assembler sleep/wakeup routines to SRAM. * These routines need to be in SRAM as that's the only * memory the MPU can see when it wakes up. */ if (cpu_is_omap24xx()) { omap2_sram_idle = omap_sram_push(omap24xx_idle_loop_suspend, omap24xx_idle_loop_suspend_sz); omap2_sram_suspend = omap_sram_push(omap24xx_cpu_suspend, omap24xx_cpu_suspend_sz); } suspend_set_ops(&omap_pm_ops); pm_idle = omap2_pm_idle; return 0; } late_initcall(omap2_pm_init);