/* * OMAP2/3 PRM module functions * * Copyright (C) 2010 Texas Instruments, Inc. * Copyright (C) 2010 Nokia Corporation * BenoƮt Cousson * Paul Walmsley * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include #include #include #include #include "common.h" #include #include #include "vp.h" #include "prm2xxx_3xxx.h" #include "cm2xxx_3xxx.h" #include "prm-regbits-24xx.h" #include "prm-regbits-34xx.h" u32 omap2_prm_read_mod_reg(s16 module, u16 idx) { return __raw_readl(prm_base + module + idx); } void omap2_prm_write_mod_reg(u32 val, s16 module, u16 idx) { __raw_writel(val, prm_base + module + idx); } /* Read-modify-write a register in a PRM module. Caller must lock */ u32 omap2_prm_rmw_mod_reg_bits(u32 mask, u32 bits, s16 module, s16 idx) { u32 v; v = omap2_prm_read_mod_reg(module, idx); v &= ~mask; v |= bits; omap2_prm_write_mod_reg(v, module, idx); return v; } /* Read a PRM register, AND it, and shift the result down to bit 0 */ u32 omap2_prm_read_mod_bits_shift(s16 domain, s16 idx, u32 mask) { u32 v; v = omap2_prm_read_mod_reg(domain, idx); v &= mask; v >>= __ffs(mask); return v; } u32 omap2_prm_set_mod_reg_bits(u32 bits, s16 module, s16 idx) { return omap2_prm_rmw_mod_reg_bits(bits, bits, module, idx); } u32 omap2_prm_clear_mod_reg_bits(u32 bits, s16 module, s16 idx) { return omap2_prm_rmw_mod_reg_bits(bits, 0x0, module, idx); } /** * omap2_prm_is_hardreset_asserted - read the HW reset line state of * submodules contained in the hwmod module * @prm_mod: PRM submodule base (e.g. CORE_MOD) * @shift: register bit shift corresponding to the reset line to check * * Returns 1 if the (sub)module hardreset line is currently asserted, * 0 if the (sub)module hardreset line is not currently asserted, or * -EINVAL if called while running on a non-OMAP2/3 chip. */ int omap2_prm_is_hardreset_asserted(s16 prm_mod, u8 shift) { if (!(cpu_is_omap24xx() || cpu_is_omap34xx())) return -EINVAL; return omap2_prm_read_mod_bits_shift(prm_mod, OMAP2_RM_RSTCTRL, (1 << shift)); } /** * omap2_prm_assert_hardreset - assert the HW reset line of a submodule * @prm_mod: PRM submodule base (e.g. CORE_MOD) * @shift: register bit shift corresponding to the reset line to assert * * Some IPs like dsp or iva contain processors that require an HW * reset line to be asserted / deasserted in order to fully enable the * IP. These modules may have multiple hard-reset lines that reset * different 'submodules' inside the IP block. This function will * place the submodule into reset. Returns 0 upon success or -EINVAL * upon an argument error. */ int omap2_prm_assert_hardreset(s16 prm_mod, u8 shift) { u32 mask; if (!(cpu_is_omap24xx() || cpu_is_omap34xx())) return -EINVAL; mask = 1 << shift; omap2_prm_rmw_mod_reg_bits(mask, mask, prm_mod, OMAP2_RM_RSTCTRL); return 0; } /** * omap2_prm_deassert_hardreset - deassert a submodule hardreset line and wait * @prm_mod: PRM submodule base (e.g. CORE_MOD) * @rst_shift: register bit shift corresponding to the reset line to deassert * @st_shift: register bit shift for the status of the deasserted submodule * * Some IPs like dsp or iva contain processors that require an HW * reset line to be asserted / deasserted in order to fully enable the * IP. These modules may have multiple hard-reset lines that reset * different 'submodules' inside the IP block. This function will * take the submodule out of reset and wait until the PRCM indicates * that the reset has completed before returning. Returns 0 upon success or * -EINVAL upon an argument error, -EEXIST if the submodule was already out * of reset, or -EBUSY if the submodule did not exit reset promptly. */ int omap2_prm_deassert_hardreset(s16 prm_mod, u8 rst_shift, u8 st_shift) { u32 rst, st; int c; if (!(cpu_is_omap24xx() || cpu_is_omap34xx())) return -EINVAL; rst = 1 << rst_shift; st = 1 << st_shift; /* Check the current status to avoid de-asserting the line twice */ if (omap2_prm_read_mod_bits_shift(prm_mod, OMAP2_RM_RSTCTRL, rst) == 0) return -EEXIST; /* Clear the reset status by writing 1 to the status bit */ omap2_prm_rmw_mod_reg_bits(0xffffffff, st, prm_mod, OMAP2_RM_RSTST); /* de-assert the reset control line */ omap2_prm_rmw_mod_reg_bits(rst, 0, prm_mod, OMAP2_RM_RSTCTRL); /* wait the status to be set */ omap_test_timeout(omap2_prm_read_mod_bits_shift(prm_mod, OMAP2_RM_RSTST, st), MAX_MODULE_HARDRESET_WAIT, c); return (c == MAX_MODULE_HARDRESET_WAIT) ? -EBUSY : 0; } /* PRM VP */ /* * struct omap3_vp - OMAP3 VP register access description. * @tranxdone_status: VP_TRANXDONE_ST bitmask in PRM_IRQSTATUS_MPU reg */ struct omap3_vp { u32 tranxdone_status; }; static struct omap3_vp omap3_vp[] = { [OMAP3_VP_VDD_MPU_ID] = { .tranxdone_status = OMAP3430_VP1_TRANXDONE_ST_MASK, }, [OMAP3_VP_VDD_CORE_ID] = { .tranxdone_status = OMAP3430_VP2_TRANXDONE_ST_MASK, }, }; #define MAX_VP_ID ARRAY_SIZE(omap3_vp); u32 omap3_prm_vp_check_txdone(u8 vp_id) { struct omap3_vp *vp = &omap3_vp[vp_id]; u32 irqstatus; irqstatus = omap2_prm_read_mod_reg(OCP_MOD, OMAP3_PRM_IRQSTATUS_MPU_OFFSET); return irqstatus & vp->tranxdone_status; } void omap3_prm_vp_clear_txdone(u8 vp_id) { struct omap3_vp *vp = &omap3_vp[vp_id]; omap2_prm_write_mod_reg(vp->tranxdone_status, OCP_MOD, OMAP3_PRM_IRQSTATUS_MPU_OFFSET); } u32 omap3_prm_vcvp_read(u8 offset) { return omap2_prm_read_mod_reg(OMAP3430_GR_MOD, offset); } void omap3_prm_vcvp_write(u32 val, u8 offset) { omap2_prm_write_mod_reg(val, OMAP3430_GR_MOD, offset); } u32 omap3_prm_vcvp_rmw(u32 mask, u32 bits, u8 offset) { return omap2_prm_rmw_mod_reg_bits(mask, bits, OMAP3430_GR_MOD, offset); }