/* * linux/arch/arm/mach-omap2/sdrc2xxx.c * * SDRAM timing related functions for OMAP2xxx * * Copyright (C) 2005, 2008 Texas Instruments Inc. * Copyright (C) 2005, 2008 Nokia Corporation * * Tony Lindgren * Paul Walmsley * Richard Woodruff * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include #include #include #include #include #include #include #include #include "common.h" #include #include #include "prm2xxx_3xxx.h" #include "clock.h" #include #include "sdrc.h" /* Memory timing, DLL mode flags */ #define M_DDR 1 #define M_LOCK_CTRL (1 << 2) #define M_UNLOCK 0 #define M_LOCK 1 static struct memory_timings mem_timings; static u32 curr_perf_level = CORE_CLK_SRC_DPLL_X2; static u32 omap2xxx_sdrc_get_slow_dll_ctrl(void) { return mem_timings.slow_dll_ctrl; } static u32 omap2xxx_sdrc_get_fast_dll_ctrl(void) { return mem_timings.fast_dll_ctrl; } static u32 omap2xxx_sdrc_get_type(void) { return mem_timings.m_type; } /* * Check the DLL lock state, and return tue if running in unlock mode. * This is needed to compensate for the shifted DLL value in unlock mode. */ u32 omap2xxx_sdrc_dll_is_unlocked(void) { /* dlla and dllb are a set */ u32 dll_state = sdrc_read_reg(SDRC_DLLA_CTRL); if ((dll_state & (1 << 2)) == (1 << 2)) return 1; else return 0; } /* * 'level' is the value to store to CM_CLKSEL2_PLL.CORE_CLK_SRC. * Practical values are CORE_CLK_SRC_DPLL (for CORE_CLK = DPLL_CLK) or * CORE_CLK_SRC_DPLL_X2 (for CORE_CLK = * DPLL_CLK * 2) * * Used by the clock framework during CORE DPLL changes */ u32 omap2xxx_sdrc_reprogram(u32 level, u32 force) { u32 dll_ctrl, m_type; u32 prev = curr_perf_level; unsigned long flags; if ((curr_perf_level == level) && !force) return prev; if (level == CORE_CLK_SRC_DPLL) dll_ctrl = omap2xxx_sdrc_get_slow_dll_ctrl(); else if (level == CORE_CLK_SRC_DPLL_X2) dll_ctrl = omap2xxx_sdrc_get_fast_dll_ctrl(); else return prev; m_type = omap2xxx_sdrc_get_type(); local_irq_save(flags); /* * XXX These calls should be abstracted out through a * prm2xxx.c function */ if (cpu_is_omap2420()) __raw_writel(0xffff, OMAP2420_PRCM_VOLTSETUP); else __raw_writel(0xffff, OMAP2430_PRCM_VOLTSETUP); omap2_sram_reprogram_sdrc(level, dll_ctrl, m_type); curr_perf_level = level; local_irq_restore(flags); return prev; } /* Used by the clock framework during CORE DPLL changes */ void omap2xxx_sdrc_init_params(u32 force_lock_to_unlock_mode) { unsigned long dll_cnt; u32 fast_dll = 0; /* DDR = 1, SDR = 0 */ mem_timings.m_type = !((sdrc_read_reg(SDRC_MR_0) & 0x3) == 0x1); /* 2422 es2.05 and beyond has a single SIP DDR instead of 2 like others. * In the case of 2422, its ok to use CS1 instead of CS0. */ if (cpu_is_omap2422()) mem_timings.base_cs = 1; else mem_timings.base_cs = 0; if (mem_timings.m_type != M_DDR) return; /* With DDR we need to determine the low frequency DLL value */ if (((mem_timings.fast_dll_ctrl & (1 << 2)) == M_LOCK_CTRL)) mem_timings.dll_mode = M_UNLOCK; else mem_timings.dll_mode = M_LOCK; if (mem_timings.base_cs == 0) { fast_dll = sdrc_read_reg(SDRC_DLLA_CTRL); dll_cnt = sdrc_read_reg(SDRC_DLLA_STATUS) & 0xff00; } else { fast_dll = sdrc_read_reg(SDRC_DLLB_CTRL); dll_cnt = sdrc_read_reg(SDRC_DLLB_STATUS) & 0xff00; } if (force_lock_to_unlock_mode) { fast_dll &= ~0xff00; fast_dll |= dll_cnt; /* Current lock mode */ } /* set fast timings with DLL filter disabled */ mem_timings.fast_dll_ctrl = (fast_dll | (3 << 8)); /* No disruptions, DDR will be offline & C-ABI not followed */ omap2_sram_ddr_init(&mem_timings.slow_dll_ctrl, mem_timings.fast_dll_ctrl, mem_timings.base_cs, force_lock_to_unlock_mode); mem_timings.slow_dll_ctrl &= 0xff00; /* Keep lock value */ /* Turn status into unlock ctrl */ mem_timings.slow_dll_ctrl |= ((mem_timings.fast_dll_ctrl & 0xF) | (1 << 2)); /* 90 degree phase for anything below 133Mhz + disable DLL filter */ mem_timings.slow_dll_ctrl |= ((1 << 1) | (3 << 8)); }