/* * linux/arch/arm/mach-omap2/sleep.S * * (C) Copyright 2004 * Texas Instruments, * Richard Woodruff * * (C) Copyright 2006 Nokia Corporation * Fixed idle loop sleep * Igor Stoppa * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License as * published by the Free Software Foundation; either version 2 of * the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR /PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, * MA 02111-1307 USA */ #include #include #include #include #include "sdrc.h" /* First address of reserved address space? apparently valid for OMAP2 & 3 */ #define A_SDRC0_V (0xC0000000) .text /* * Forces OMAP into idle state * * omap24xx_idle_loop_suspend() - This bit of code just executes the WFI * for normal idles. * * Note: This code get's copied to internal SRAM at boot. When the OMAP * wakes up it continues execution at the point it went to sleep. */ .align 3 ENTRY(omap24xx_idle_loop_suspend) stmfd sp!, {r0, lr} @ save registers on stack mov r0, #0 @ clear for mcr setup mcr p15, 0, r0, c7, c0, 4 @ wait for interrupt ldmfd sp!, {r0, pc} @ restore regs and return ENTRY(omap24xx_idle_loop_suspend_sz) .word . - omap24xx_idle_loop_suspend /* * omap24xx_cpu_suspend() - Forces OMAP into deep sleep state by completing * SDRC shutdown then ARM shutdown. Upon wake MPU is back on so just restore * SDRC. * * Input: * R0 : DLL ctrl value pre-Sleep * R1 : SDRC_DLLA_CTRL * R2 : SDRC_POWER * * The if the DPLL is going to AutoIdle. It seems like the DPLL may be back on * when we get called, but the DLL probably isn't. We will wait a bit more in * case the DPLL isn't quite there yet. The code will wait on DLL for DDR even * if in unlocked mode. * * For less than 242x-ES2.2 upon wake from a sleep mode where the external * oscillator was stopped, a timing bug exists where a non-stabilized 12MHz * clock can pass into the PRCM can cause problems at DSP and IVA. * To work around this the code will switch to the 32kHz source prior to sleep. * Post sleep we will shift back to using the DPLL. Apparently, * CM_IDLEST_CLKGEN does not reflect the full clock change so you need to wait * 3x12MHz + 3x32kHz clocks for a full switch. * * The DLL load value is not kept in RETENTION or OFF. It needs to be restored * at wake */ .align 3 ENTRY(omap24xx_cpu_suspend) stmfd sp!, {r0 - r12, lr} @ save registers on stack mov r3, #0x0 @ clear for mcr call mcr p15, 0, r3, c7, c10, 4 @ memory barrier, hope SDR/DDR finished nop nop ldr r4, [r2] @ read SDRC_POWER orr r4, r4, #0x40 @ enable self refresh on idle req mov r5, #0x2000 @ set delay (DPLL relock + DLL relock) str r4, [r2] @ make it so nop mcr p15, 0, r3, c7, c0, 4 @ wait for interrupt nop loop: subs r5, r5, #0x1 @ awake, wait just a bit bne loop /* The DPLL has to be on before we take the DDR out of self refresh */ bic r4, r4, #0x40 @ now clear self refresh bit. str r4, [r2] @ write to SDRC_POWER ldr r4, A_SDRC0 @ make a clock happen ldr r4, [r4] @ read A_SDRC0 nop @ start auto refresh only after clk ok movs r0, r0 @ see if DDR or SDR strne r0, [r1] @ rewrite DLLA to force DLL reload addne r1, r1, #0x8 @ move to DLLB strne r0, [r1] @ rewrite DLLB to force DLL reload mov r5, #0x1000 loop2: subs r5, r5, #0x1 bne loop2 /* resume*/ ldmfd sp!, {r0 - r12, pc} @ restore regs and return A_SDRC0: .word A_SDRC0_V ENTRY(omap24xx_cpu_suspend_sz) .word . - omap24xx_cpu_suspend