/* * OMAP Voltage Controller (VC) interface * * Copyright (C) 2011 Texas Instruments, Inc. * * This file is licensed under the terms of the GNU General Public * License version 2. This program is licensed "as is" without any * warranty of any kind, whether express or implied. */ #include #include #include #include #include "voltage.h" #include "vc.h" #include "prm-regbits-34xx.h" #include "prm-regbits-44xx.h" #include "prm44xx.h" /** * struct omap_vc_channel_cfg - describe the cfg_channel bitfield * @sa: bit for slave address * @rav: bit for voltage configuration register * @rac: bit for command configuration register * @racen: enable bit for RAC * @cmd: bit for command value set selection * * Channel configuration bits, common for OMAP3+ * OMAP3 register: PRM_VC_CH_CONF * OMAP4 register: PRM_VC_CFG_CHANNEL * OMAP5 register: PRM_VC_SMPS__CONFIG */ struct omap_vc_channel_cfg { u8 sa; u8 rav; u8 rac; u8 racen; u8 cmd; }; static struct omap_vc_channel_cfg vc_default_channel_cfg = { .sa = BIT(0), .rav = BIT(1), .rac = BIT(2), .racen = BIT(3), .cmd = BIT(4), }; /* * On OMAP3+, all VC channels have the above default bitfield * configuration, except the OMAP4 MPU channel. This appears * to be a freak accident as every other VC channel has the * default configuration, thus creating a mutant channel config. */ static struct omap_vc_channel_cfg vc_mutant_channel_cfg = { .sa = BIT(0), .rav = BIT(2), .rac = BIT(3), .racen = BIT(4), .cmd = BIT(1), }; static struct omap_vc_channel_cfg *vc_cfg_bits; #define CFG_CHANNEL_MASK 0x1f /** * omap_vc_config_channel - configure VC channel to PMIC mappings * @voltdm: pointer to voltagdomain defining the desired VC channel * * Configures the VC channel to PMIC mappings for the following * PMIC settings * - i2c slave address (SA) * - voltage configuration address (RAV) * - command configuration address (RAC) and enable bit (RACEN) * - command values for ON, ONLP, RET and OFF (CMD) * * This function currently only allows flexible configuration of the * non-default channel. Starting with OMAP4, there are more than 2 * channels, with one defined as the default (on OMAP4, it's MPU.) * Only the non-default channel can be configured. */ static int omap_vc_config_channel(struct voltagedomain *voltdm) { struct omap_vc_channel *vc = voltdm->vc; /* * For default channel, the only configurable bit is RACEN. * All others must stay at zero (see function comment above.) */ if (vc->flags & OMAP_VC_CHANNEL_DEFAULT) vc->cfg_channel &= vc_cfg_bits->racen; voltdm->rmw(CFG_CHANNEL_MASK << vc->cfg_channel_sa_shift, vc->cfg_channel << vc->cfg_channel_sa_shift, vc->cfg_channel_reg); return 0; } /* Voltage scale and accessory APIs */ int omap_vc_pre_scale(struct voltagedomain *voltdm, unsigned long target_volt, u8 *target_vsel, u8 *current_vsel) { struct omap_vc_channel *vc = voltdm->vc; u32 vc_cmdval; /* Check if sufficient pmic info is available for this vdd */ if (!voltdm->pmic) { pr_err("%s: Insufficient pmic info to scale the vdd_%s\n", __func__, voltdm->name); return -EINVAL; } if (!voltdm->pmic->uv_to_vsel) { pr_err("%s: PMIC function to convert voltage in uV to" "vsel not registered. Hence unable to scale voltage" "for vdd_%s\n", __func__, voltdm->name); return -ENODATA; } if (!voltdm->read || !voltdm->write) { pr_err("%s: No read/write API for accessing vdd_%s regs\n", __func__, voltdm->name); return -EINVAL; } *target_vsel = voltdm->pmic->uv_to_vsel(target_volt); *current_vsel = voltdm->pmic->uv_to_vsel(voltdm->nominal_volt); /* Setting the ON voltage to the new target voltage */ vc_cmdval = voltdm->read(vc->cmdval_reg); vc_cmdval &= ~vc->common->cmd_on_mask; vc_cmdval |= (*target_vsel << vc->common->cmd_on_shift); voltdm->write(vc_cmdval, vc->cmdval_reg); omap_vp_update_errorgain(voltdm, target_volt); return 0; } void omap_vc_post_scale(struct voltagedomain *voltdm, unsigned long target_volt, u8 target_vsel, u8 current_vsel) { u32 smps_steps = 0, smps_delay = 0; smps_steps = abs(target_vsel - current_vsel); /* SMPS slew rate / step size. 2us added as buffer. */ smps_delay = ((smps_steps * voltdm->pmic->step_size) / voltdm->pmic->slew_rate) + 2; udelay(smps_delay); } /* vc_bypass_scale - VC bypass method of voltage scaling */ int omap_vc_bypass_scale(struct voltagedomain *voltdm, unsigned long target_volt) { struct omap_vc_channel *vc = voltdm->vc; u32 loop_cnt = 0, retries_cnt = 0; u32 vc_valid, vc_bypass_val_reg, vc_bypass_value; u8 target_vsel, current_vsel; int ret; ret = omap_vc_pre_scale(voltdm, target_volt, &target_vsel, ¤t_vsel); if (ret) return ret; vc_valid = vc->common->valid; vc_bypass_val_reg = vc->common->bypass_val_reg; vc_bypass_value = (target_vsel << vc->common->data_shift) | (vc->volt_reg_addr << vc->common->regaddr_shift) | (vc->i2c_slave_addr << vc->common->slaveaddr_shift); voltdm->write(vc_bypass_value, vc_bypass_val_reg); voltdm->write(vc_bypass_value | vc_valid, vc_bypass_val_reg); vc_bypass_value = voltdm->read(vc_bypass_val_reg); /* * Loop till the bypass command is acknowledged from the SMPS. * NOTE: This is legacy code. The loop count and retry count needs * to be revisited. */ while (!(vc_bypass_value & vc_valid)) { loop_cnt++; if (retries_cnt > 10) { pr_warning("%s: Retry count exceeded\n", __func__); return -ETIMEDOUT; } if (loop_cnt > 50) { retries_cnt++; loop_cnt = 0; udelay(10); } vc_bypass_value = voltdm->read(vc_bypass_val_reg); } omap_vc_post_scale(voltdm, target_volt, target_vsel, current_vsel); return 0; } static void __init omap3_vfsm_init(struct voltagedomain *voltdm) { /* * Voltage Manager FSM parameters init * XXX This data should be passed in from the board file */ voltdm->write(OMAP3_CLKSETUP, OMAP3_PRM_CLKSETUP_OFFSET); voltdm->write(OMAP3_VOLTOFFSET, OMAP3_PRM_VOLTOFFSET_OFFSET); voltdm->write(OMAP3_VOLTSETUP2, OMAP3_PRM_VOLTSETUP2_OFFSET); } static void __init omap3_vc_init_channel(struct voltagedomain *voltdm) { static bool is_initialized; if (is_initialized) return; omap3_vfsm_init(voltdm); is_initialized = true; } /* OMAP4 specific voltage init functions */ static void __init omap4_vc_init_channel(struct voltagedomain *voltdm) { static bool is_initialized; u32 vc_val; if (is_initialized) return; /* XXX These are magic numbers and do not belong! */ vc_val = (0x60 << OMAP4430_SCLL_SHIFT | 0x26 << OMAP4430_SCLH_SHIFT); voltdm->write(vc_val, OMAP4_PRM_VC_CFG_I2C_CLK_OFFSET); is_initialized = true; } /** * omap_vc_i2c_init - initialize I2C interface to PMIC * @voltdm: voltage domain containing VC data * * Use PMIC supplied seetings for I2C high-speed mode and * master code (if set) and program the VC I2C configuration * register. * * The VC I2C configuration is common to all VC channels, * so this function only configures I2C for the first VC * channel registers. All other VC channels will use the * same configuration. */ static void __init omap_vc_i2c_init(struct voltagedomain *voltdm) { struct omap_vc_channel *vc = voltdm->vc; static bool initialized; static bool i2c_high_speed; u8 mcode; if (initialized) { if (voltdm->pmic->i2c_high_speed != i2c_high_speed) pr_warn("%s: I2C config for all channels must match.", __func__); return; } i2c_high_speed = voltdm->pmic->i2c_high_speed; if (i2c_high_speed) voltdm->rmw(vc->common->i2c_cfg_hsen_mask, vc->common->i2c_cfg_hsen_mask, vc->common->i2c_cfg_reg); mcode = voltdm->pmic->i2c_mcode; if (mcode) voltdm->rmw(vc->common->i2c_mcode_mask, mcode << __ffs(vc->common->i2c_mcode_mask), vc->common->i2c_cfg_reg); initialized = true; } void __init omap_vc_init_channel(struct voltagedomain *voltdm) { struct omap_vc_channel *vc = voltdm->vc; u8 on_vsel, onlp_vsel, ret_vsel, off_vsel; u32 val; if (!voltdm->pmic || !voltdm->pmic->uv_to_vsel) { pr_err("%s: missing PMIC for vdd_%s.\n", __func__, voltdm->name); return; } if (!voltdm->read || !voltdm->write) { pr_err("%s: No read/write API for accessing vdd_%s regs\n", __func__, voltdm->name); return; } vc->cfg_channel = 0; if (vc->flags & OMAP_VC_CHANNEL_CFG_MUTANT) vc_cfg_bits = &vc_mutant_channel_cfg; else vc_cfg_bits = &vc_default_channel_cfg; /* get PMIC/board specific settings */ vc->i2c_slave_addr = voltdm->pmic->i2c_slave_addr; vc->volt_reg_addr = voltdm->pmic->volt_reg_addr; vc->cmd_reg_addr = voltdm->pmic->cmd_reg_addr; vc->setup_time = voltdm->pmic->volt_setup_time; /* Configure the i2c slave address for this VC */ voltdm->rmw(vc->smps_sa_mask, vc->i2c_slave_addr << __ffs(vc->smps_sa_mask), vc->smps_sa_reg); vc->cfg_channel |= vc_cfg_bits->sa; /* * Configure the PMIC register addresses. */ voltdm->rmw(vc->smps_volra_mask, vc->volt_reg_addr << __ffs(vc->smps_volra_mask), vc->smps_volra_reg); vc->cfg_channel |= vc_cfg_bits->rav; if (vc->cmd_reg_addr) { voltdm->rmw(vc->smps_cmdra_mask, vc->cmd_reg_addr << __ffs(vc->smps_cmdra_mask), vc->smps_cmdra_reg); vc->cfg_channel |= vc_cfg_bits->rac | vc_cfg_bits->racen; } /* Set up the on, inactive, retention and off voltage */ on_vsel = voltdm->pmic->uv_to_vsel(voltdm->pmic->on_volt); onlp_vsel = voltdm->pmic->uv_to_vsel(voltdm->pmic->onlp_volt); ret_vsel = voltdm->pmic->uv_to_vsel(voltdm->pmic->ret_volt); off_vsel = voltdm->pmic->uv_to_vsel(voltdm->pmic->off_volt); val = ((on_vsel << vc->common->cmd_on_shift) | (onlp_vsel << vc->common->cmd_onlp_shift) | (ret_vsel << vc->common->cmd_ret_shift) | (off_vsel << vc->common->cmd_off_shift)); voltdm->write(val, vc->cmdval_reg); vc->cfg_channel |= vc_cfg_bits->cmd; /* Channel configuration */ omap_vc_config_channel(voltdm); /* Configure the setup times */ voltdm->rmw(voltdm->vfsm->voltsetup_mask, vc->setup_time << __ffs(voltdm->vfsm->voltsetup_mask), voltdm->vfsm->voltsetup_reg); omap_vc_i2c_init(voltdm); if (cpu_is_omap34xx()) omap3_vc_init_channel(voltdm); else if (cpu_is_omap44xx()) omap4_vc_init_channel(voltdm); }