/* * arch/arm/plat-omap/include/mach/gpio.h * * OMAP GPIO handling defines and functions * * Copyright (C) 2003-2005 Nokia Corporation * * Written by Juha Yrjölä * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA * */ #ifndef __ASM_ARCH_OMAP_GPIO_H #define __ASM_ARCH_OMAP_GPIO_H #include #include #include #define OMAP1_MPUIO_BASE 0xfffb5000 /* * These are the omap15xx/16xx offsets. The omap7xx offset are * OMAP_MPUIO_ / 2 offsets below. */ #define OMAP_MPUIO_INPUT_LATCH 0x00 #define OMAP_MPUIO_OUTPUT 0x04 #define OMAP_MPUIO_IO_CNTL 0x08 #define OMAP_MPUIO_KBR_LATCH 0x10 #define OMAP_MPUIO_KBC 0x14 #define OMAP_MPUIO_GPIO_EVENT_MODE 0x18 #define OMAP_MPUIO_GPIO_INT_EDGE 0x1c #define OMAP_MPUIO_KBD_INT 0x20 #define OMAP_MPUIO_GPIO_INT 0x24 #define OMAP_MPUIO_KBD_MASKIT 0x28 #define OMAP_MPUIO_GPIO_MASKIT 0x2c #define OMAP_MPUIO_GPIO_DEBOUNCING 0x30 #define OMAP_MPUIO_LATCH 0x34 #define OMAP34XX_NR_GPIOS 6 /* * OMAP1510 GPIO registers */ #define OMAP1510_GPIO_DATA_INPUT 0x00 #define OMAP1510_GPIO_DATA_OUTPUT 0x04 #define OMAP1510_GPIO_DIR_CONTROL 0x08 #define OMAP1510_GPIO_INT_CONTROL 0x0c #define OMAP1510_GPIO_INT_MASK 0x10 #define OMAP1510_GPIO_INT_STATUS 0x14 #define OMAP1510_GPIO_PIN_CONTROL 0x18 #define OMAP1510_IH_GPIO_BASE 64 /* * OMAP1610 specific GPIO registers */ #define OMAP1610_GPIO_REVISION 0x0000 #define OMAP1610_GPIO_SYSCONFIG 0x0010 #define OMAP1610_GPIO_SYSSTATUS 0x0014 #define OMAP1610_GPIO_IRQSTATUS1 0x0018 #define OMAP1610_GPIO_IRQENABLE1 0x001c #define OMAP1610_GPIO_WAKEUPENABLE 0x0028 #define OMAP1610_GPIO_DATAIN 0x002c #define OMAP1610_GPIO_DATAOUT 0x0030 #define OMAP1610_GPIO_DIRECTION 0x0034 #define OMAP1610_GPIO_EDGE_CTRL1 0x0038 #define OMAP1610_GPIO_EDGE_CTRL2 0x003c #define OMAP1610_GPIO_CLEAR_IRQENABLE1 0x009c #define OMAP1610_GPIO_CLEAR_WAKEUPENA 0x00a8 #define OMAP1610_GPIO_CLEAR_DATAOUT 0x00b0 #define OMAP1610_GPIO_SET_IRQENABLE1 0x00dc #define OMAP1610_GPIO_SET_WAKEUPENA 0x00e8 #define OMAP1610_GPIO_SET_DATAOUT 0x00f0 /* * OMAP7XX specific GPIO registers */ #define OMAP7XX_GPIO_DATA_INPUT 0x00 #define OMAP7XX_GPIO_DATA_OUTPUT 0x04 #define OMAP7XX_GPIO_DIR_CONTROL 0x08 #define OMAP7XX_GPIO_INT_CONTROL 0x0c #define OMAP7XX_GPIO_INT_MASK 0x10 #define OMAP7XX_GPIO_INT_STATUS 0x14 /* * omap2+ specific GPIO registers */ #define OMAP24XX_GPIO_REVISION 0x0000 #define OMAP24XX_GPIO_IRQSTATUS1 0x0018 #define OMAP24XX_GPIO_IRQSTATUS2 0x0028 #define OMAP24XX_GPIO_IRQENABLE2 0x002c #define OMAP24XX_GPIO_IRQENABLE1 0x001c #define OMAP24XX_GPIO_WAKE_EN 0x0020 #define OMAP24XX_GPIO_CTRL 0x0030 #define OMAP24XX_GPIO_OE 0x0034 #define OMAP24XX_GPIO_DATAIN 0x0038 #define OMAP24XX_GPIO_DATAOUT 0x003c #define OMAP24XX_GPIO_LEVELDETECT0 0x0040 #define OMAP24XX_GPIO_LEVELDETECT1 0x0044 #define OMAP24XX_GPIO_RISINGDETECT 0x0048 #define OMAP24XX_GPIO_FALLINGDETECT 0x004c #define OMAP24XX_GPIO_DEBOUNCE_EN 0x0050 #define OMAP24XX_GPIO_DEBOUNCE_VAL 0x0054 #define OMAP24XX_GPIO_CLEARIRQENABLE1 0x0060 #define OMAP24XX_GPIO_SETIRQENABLE1 0x0064 #define OMAP24XX_GPIO_CLEARWKUENA 0x0080 #define OMAP24XX_GPIO_SETWKUENA 0x0084 #define OMAP24XX_GPIO_CLEARDATAOUT 0x0090 #define OMAP24XX_GPIO_SETDATAOUT 0x0094 #define OMAP4_GPIO_REVISION 0x0000 #define OMAP4_GPIO_EOI 0x0020 #define OMAP4_GPIO_IRQSTATUSRAW0 0x0024 #define OMAP4_GPIO_IRQSTATUSRAW1 0x0028 #define OMAP4_GPIO_IRQSTATUS0 0x002c #define OMAP4_GPIO_IRQSTATUS1 0x0030 #define OMAP4_GPIO_IRQSTATUSSET0 0x0034 #define OMAP4_GPIO_IRQSTATUSSET1 0x0038 #define OMAP4_GPIO_IRQSTATUSCLR0 0x003c #define OMAP4_GPIO_IRQSTATUSCLR1 0x0040 #define OMAP4_GPIO_IRQWAKEN0 0x0044 #define OMAP4_GPIO_IRQWAKEN1 0x0048 #define OMAP4_GPIO_IRQENABLE1 0x011c #define OMAP4_GPIO_WAKE_EN 0x0120 #define OMAP4_GPIO_IRQSTATUS2 0x0128 #define OMAP4_GPIO_IRQENABLE2 0x012c #define OMAP4_GPIO_CTRL 0x0130 #define OMAP4_GPIO_OE 0x0134 #define OMAP4_GPIO_DATAIN 0x0138 #define OMAP4_GPIO_DATAOUT 0x013c #define OMAP4_GPIO_LEVELDETECT0 0x0140 #define OMAP4_GPIO_LEVELDETECT1 0x0144 #define OMAP4_GPIO_RISINGDETECT 0x0148 #define OMAP4_GPIO_FALLINGDETECT 0x014c #define OMAP4_GPIO_DEBOUNCENABLE 0x0150 #define OMAP4_GPIO_DEBOUNCINGTIME 0x0154 #define OMAP4_GPIO_CLEARIRQENABLE1 0x0160 #define OMAP4_GPIO_SETIRQENABLE1 0x0164 #define OMAP4_GPIO_CLEARWKUENA 0x0180 #define OMAP4_GPIO_SETWKUENA 0x0184 #define OMAP4_GPIO_CLEARDATAOUT 0x0190 #define OMAP4_GPIO_SETDATAOUT 0x0194 #define OMAP_MPUIO(nr) (OMAP_MAX_GPIO_LINES + (nr)) #define OMAP_GPIO_IS_MPUIO(nr) ((nr) >= OMAP_MAX_GPIO_LINES) #define OMAP_GPIO_IRQ(nr) (OMAP_GPIO_IS_MPUIO(nr) ? \ IH_MPUIO_BASE + ((nr) & 0x0f) : \ IH_GPIO_BASE + (nr)) #define METHOD_MPUIO 0 #define METHOD_GPIO_1510 1 #define METHOD_GPIO_1610 2 #define METHOD_GPIO_7XX 3 #define METHOD_GPIO_24XX 5 #define METHOD_GPIO_44XX 6 struct omap_gpio_dev_attr { int bank_width; /* GPIO bank width */ bool dbck_flag; /* dbck required or not - True for OMAP3&4 */ }; struct omap_gpio_reg_offs { u16 revision; u16 direction; u16 datain; u16 dataout; u16 set_dataout; u16 clr_dataout; u16 irqstatus; u16 irqstatus2; u16 irqenable; u16 set_irqenable; u16 clr_irqenable; u16 debounce; u16 debounce_en; bool irqenable_inv; }; struct omap_gpio_platform_data { u16 virtual_irq_start; int bank_type; int bank_width; /* GPIO bank width */ int bank_stride; /* Only needed for omap1 MPUIO */ bool dbck_flag; /* dbck required or not - True for OMAP3&4 */ struct omap_gpio_reg_offs *regs; }; /* TODO: Analyze removing gpio_bank_count usage from driver code */ extern int gpio_bank_count; extern void omap2_gpio_prepare_for_idle(int off_mode); extern void omap2_gpio_resume_after_idle(void); extern void omap_set_gpio_debounce(int gpio, int enable); extern void omap_set_gpio_debounce_time(int gpio, int enable); extern void omap_gpio_save_context(void); extern void omap_gpio_restore_context(void); /*-------------------------------------------------------------------------*/ /* Wrappers for "new style" GPIO calls, using the new infrastructure * which lets us plug in FPGA, I2C, and other implementations. * * * The original OMAP-specific calls should eventually be removed. */ #include #include static inline int irq_to_gpio(unsigned irq) { int tmp; /* omap1 SOC mpuio */ if (cpu_class_is_omap1() && (irq < (IH_MPUIO_BASE + 16))) return (irq - IH_MPUIO_BASE) + OMAP_MAX_GPIO_LINES; /* SOC gpio */ tmp = irq - IH_GPIO_BASE; if (tmp < OMAP_MAX_GPIO_LINES) return tmp; /* we don't supply reverse mappings for non-SOC gpios */ return -EIO; } #endif