/* * omap-pm.h - OMAP power management interface * * Copyright (C) 2008-2010 Texas Instruments, Inc. * Copyright (C) 2008-2010 Nokia Corporation * Paul Walmsley * * Interface developed by (in alphabetical order): Karthik Dasu, Jouni * Högander, Tony Lindgren, Rajendra Nayak, Sakari Poussa, * Veeramanikandan Raju, Anand Sawant, Igor Stoppa, Paul Walmsley, * Richard Woodruff */ #ifndef ASM_ARM_ARCH_OMAP_OMAP_PM_H #define ASM_ARM_ARCH_OMAP_OMAP_PM_H #include #include #include #include /* * agent_id values for use with omap_pm_set_min_bus_tput(): * * OCP_INITIATOR_AGENT is only valid for devices that can act as * initiators -- it represents the device's L3 interconnect * connection. OCP_TARGET_AGENT represents the device's L4 * interconnect connection. */ #define OCP_TARGET_AGENT 1 #define OCP_INITIATOR_AGENT 2 /** * omap_pm_if_early_init - OMAP PM init code called before clock fw init * @mpu_opp_table: array ptr to struct omap_opp for MPU * @dsp_opp_table: array ptr to struct omap_opp for DSP * @l3_opp_table : array ptr to struct omap_opp for CORE * * Initialize anything that must be configured before the clock * framework starts. The "_if_" is to avoid name collisions with the * PM idle-loop code. */ int __init omap_pm_if_early_init(void); /** * omap_pm_if_init - OMAP PM init code called after clock fw init * * The main initialization code. OPP tables are passed in here. The * "_if_" is to avoid name collisions with the PM idle-loop code. */ int __init omap_pm_if_init(void); /** * omap_pm_if_exit - OMAP PM exit code * * Exit code; currently unused. The "_if_" is to avoid name * collisions with the PM idle-loop code. */ void omap_pm_if_exit(void); /* * Device-driver-originated constraints (via board-*.c files, platform_data) */ /** * omap_pm_set_max_mpu_wakeup_lat - set the maximum MPU wakeup latency * @dev: struct device * requesting the constraint * @t: maximum MPU wakeup latency in microseconds * * Request that the maximum interrupt latency for the MPU to be no * greater than @t microseconds. "Interrupt latency" in this case is * defined as the elapsed time from the occurrence of a hardware or * timer interrupt to the time when the device driver's interrupt * service routine has been entered by the MPU. * * It is intended that underlying PM code will use this information to * determine what power state to put the MPU powerdomain into, and * possibly the CORE powerdomain as well, since interrupt handling * code currently runs from SDRAM. Advanced PM or board*.c code may * also configure interrupt controller priorities, OCP bus priorities, * CPU speed(s), etc. * * This function will not affect device wakeup latency, e.g., time * elapsed from when a device driver enables a hardware device with * clk_enable(), to when the device is ready for register access or * other use. To control this device wakeup latency, use * omap_pm_set_max_dev_wakeup_lat() * * Multiple calls to omap_pm_set_max_mpu_wakeup_lat() will replace the * previous t value. To remove the latency target for the MPU, call * with t = -1. * * XXX This constraint will be deprecated soon in favor of the more * general omap_pm_set_max_dev_wakeup_lat() * * Returns -EINVAL for an invalid argument, -ERANGE if the constraint * is not satisfiable, or 0 upon success. */ int omap_pm_set_max_mpu_wakeup_lat(struct device *dev, long t); /** * omap_pm_set_min_bus_tput - set minimum bus throughput needed by device * @dev: struct device * requesting the constraint * @tbus_id: interconnect to operate on (OCP_{INITIATOR,TARGET}_AGENT) * @r: minimum throughput (in KiB/s) * * Request that the minimum data throughput on the OCP interconnect * attached to device @dev interconnect agent @tbus_id be no less * than @r KiB/s. * * It is expected that the OMAP PM or bus code will use this * information to set the interconnect clock to run at the lowest * possible speed that satisfies all current system users. The PM or * bus code will adjust the estimate based on its model of the bus, so * device driver authors should attempt to specify an accurate * quantity for their device use case, and let the PM or bus code * overestimate the numbers as necessary to handle request/response * latency, other competing users on the system, etc. On OMAP2/3, if * a driver requests a minimum L4 interconnect speed constraint, the * code will also need to add an minimum L3 interconnect speed * constraint, * * Multiple calls to omap_pm_set_min_bus_tput() will replace the * previous rate value for this device. To remove the interconnect * throughput restriction for this device, call with r = 0. * * Returns -EINVAL for an invalid argument, -ERANGE if the constraint * is not satisfiable, or 0 upon success. */ int omap_pm_set_min_bus_tput(struct device *dev, u8 agent_id, unsigned long r); /** * omap_pm_set_max_dev_wakeup_lat - set the maximum device enable latency * @req_dev: struct device * requesting the constraint, or NULL if none * @dev: struct device * to set the constraint one * @t: maximum device wakeup latency in microseconds * * Request that the maximum amount of time necessary for a device @dev * to become accessible after its clocks are enabled should be no * greater than @t microseconds. Specifically, this represents the * time from when a device driver enables device clocks with * clk_enable(), to when the register reads and writes on the device * will succeed. This function should be called before clk_disable() * is called, since the power state transition decision may be made * during clk_disable(). * * It is intended that underlying PM code will use this information to * determine what power state to put the powerdomain enclosing this * device into. * * Multiple calls to omap_pm_set_max_dev_wakeup_lat() will replace the * previous wakeup latency values for this device. To remove the * wakeup latency restriction for this device, call with t = -1. * * Returns -EINVAL for an invalid argument, -ERANGE if the constraint * is not satisfiable, or 0 upon success. */ int omap_pm_set_max_dev_wakeup_lat(struct device *req_dev, struct device *dev, long t); /** * omap_pm_set_max_sdma_lat - set the maximum system DMA transfer start latency * @dev: struct device * * @t: maximum DMA transfer start latency in microseconds * * Request that the maximum system DMA transfer start latency for this * device 'dev' should be no greater than 't' microseconds. "DMA * transfer start latency" here is defined as the elapsed time from * when a device (e.g., McBSP) requests that a system DMA transfer * start or continue, to the time at which data starts to flow into * that device from the system DMA controller. * * It is intended that underlying PM code will use this information to * determine what power state to put the CORE powerdomain into. * * Since system DMA transfers may not involve the MPU, this function * will not affect MPU wakeup latency. Use set_max_cpu_lat() to do * so. Similarly, this function will not affect device wakeup latency * -- use set_max_dev_wakeup_lat() to affect that. * * Multiple calls to set_max_sdma_lat() will replace the previous t * value for this device. To remove the maximum DMA latency for this * device, call with t = -1. * * Returns -EINVAL for an invalid argument, -ERANGE if the constraint * is not satisfiable, or 0 upon success. */ int omap_pm_set_max_sdma_lat(struct device *dev, long t); /** * omap_pm_set_min_clk_rate - set minimum clock rate requested by @dev * @dev: struct device * requesting the constraint * @clk: struct clk * to set the minimum rate constraint on * @r: minimum rate in Hz * * Request that the minimum clock rate on the device @dev's clk @clk * be no less than @r Hz. * * It is expected that the OMAP PM code will use this information to * find an OPP or clock setting that will satisfy this clock rate * constraint, along with any other applicable system constraints on * the clock rate or corresponding voltage, etc. * * omap_pm_set_min_clk_rate() differs from the clock code's * clk_set_rate() in that it considers other constraints before taking * any hardware action, and may change a system OPP rather than just a * clock rate. clk_set_rate() is intended to be a low-level * interface. * * omap_pm_set_min_clk_rate() is easily open to abuse. A better API * would be something like "omap_pm_set_min_dev_performance()"; * however, there is no easily-generalizable concept of performance * that applies to all devices. Only a device (and possibly the * device subsystem) has both the subsystem-specific knowledge, and * the hardware IP block-specific knowledge, to translate a constraint * on "touchscreen sampling accuracy" or "number of pixels or polygons * rendered per second" to a clock rate. This translation can be * dependent on the hardware IP block's revision, or firmware version, * and the driver is the only code on the system that has this * information and can know how to translate that into a clock rate. * * The intended use-case for this function is for userspace or other * kernel code to communicate a particular performance requirement to * a subsystem; then for the subsystem to communicate that requirement * to something that is meaningful to the device driver; then for the * device driver to convert that requirement to a clock rate, and to * then call omap_pm_set_min_clk_rate(). * * Users of this function (such as device drivers) should not simply * call this function with some high clock rate to ensure "high * performance." Rather, the device driver should take a performance * constraint from its subsystem, such as "render at least X polygons * per second," and use some formula or table to convert that into a * clock rate constraint given the hardware type and hardware * revision. Device drivers or subsystems should not assume that they * know how to make a power/performance tradeoff - some device use * cases may tolerate a lower-fidelity device function for lower power * consumption; others may demand a higher-fidelity device function, * no matter what the power consumption. * * Multiple calls to omap_pm_set_min_clk_rate() will replace the * previous rate value for the device @dev. To remove the minimum clock * rate constraint for the device, call with r = 0. * * Returns -EINVAL for an invalid argument, -ERANGE if the constraint * is not satisfiable, or 0 upon success. */ int omap_pm_set_min_clk_rate(struct device *dev, struct clk *c, long r); /* * DSP Bridge-specific constraints */ /** * omap_pm_dsp_get_opp_table - get OPP->DSP clock frequency table * * Intended for use by DSPBridge. Returns an array of OPP->DSP clock * frequency entries. The final item in the array should have .rate = * .opp_id = 0. */ const struct omap_opp *omap_pm_dsp_get_opp_table(void); /** * omap_pm_dsp_set_min_opp - receive desired OPP target ID from DSP Bridge * @opp_id: target DSP OPP ID * * Set a minimum OPP ID for the DSP. This is intended to be called * only from the DSP Bridge MPU-side driver. Unfortunately, the only * information that code receives from the DSP/BIOS load estimator is the * target OPP ID; hence, this interface. No return value. */ void omap_pm_dsp_set_min_opp(u8 opp_id); /** * omap_pm_dsp_get_opp - report the current DSP OPP ID * * Report the current OPP for the DSP. Since on OMAP3, the DSP and * MPU share a single voltage domain, the OPP ID returned back may * represent a higher DSP speed than the OPP requested via * omap_pm_dsp_set_min_opp(). * * Returns the current VDD1 OPP ID, or 0 upon error. */ u8 omap_pm_dsp_get_opp(void); /* * CPUFreq-originated constraint * * In the future, this should be handled by custom OPP clocktype * functions. */ /** * omap_pm_cpu_get_freq_table - return a cpufreq_frequency_table array ptr * * Provide a frequency table usable by CPUFreq for the current chip/board. * Returns a pointer to a struct cpufreq_frequency_table array or NULL * upon error. */ struct cpufreq_frequency_table **omap_pm_cpu_get_freq_table(void); /** * omap_pm_cpu_set_freq - set the current minimum MPU frequency * @f: MPU frequency in Hz * * Set the current minimum CPU frequency. The actual CPU frequency * used could end up higher if the DSP requested a higher OPP. * Intended to be called by plat-omap/cpu_omap.c:omap_target(). No * return value. */ void omap_pm_cpu_set_freq(unsigned long f); /** * omap_pm_cpu_get_freq - report the current CPU frequency * * Returns the current MPU frequency, or 0 upon error. */ unsigned long omap_pm_cpu_get_freq(void); /* * Device context loss tracking */ /** * omap_pm_get_dev_context_loss_count - return count of times dev has lost ctx * @dev: struct device * * * This function returns the number of times that the device @dev has * lost its internal context. This generally occurs on a powerdomain * transition to OFF. Drivers use this as an optimization to avoid restoring * context if the device hasn't lost it. To use, drivers should initially * call this in their context save functions and store the result. Early in * the driver's context restore function, the driver should call this function * again, and compare the result to the stored counter. If they differ, the * driver must restore device context. If the number of context losses * exceeds the maximum positive integer, the function will wrap to 0 and * continue counting. Returns the number of context losses for this device, * or negative value upon error. */ int omap_pm_get_dev_context_loss_count(struct device *dev); void omap_pm_enable_off_mode(void); void omap_pm_disable_off_mode(void); #endif