/* * omap_hwmod macros, structures * * Copyright (C) 2009-2011 Nokia Corporation * Copyright (C) 2011 Texas Instruments, Inc. * Paul Walmsley * * Created in collaboration with (alphabetical order): BenoƮt Cousson, * Kevin Hilman, Tony Lindgren, Rajendra Nayak, Vikram Pandita, Sakari * Poussa, Anand Sawant, Santosh Shilimkar, Richard Woodruff * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * * These headers and macros are used to define OMAP on-chip module * data and their integration with other OMAP modules and Linux. * Copious documentation and references can also be found in the * omap_hwmod code, in arch/arm/mach-omap2/omap_hwmod.c (as of this * writing). * * To do: * - add interconnect error log structures * - add pinmuxing * - init_conn_id_bit (CONNID_BIT_VECTOR) * - implement default hwmod SMS/SDRC flags? * - move Linux-specific data ("non-ROM data") out * */ #ifndef __ARCH_ARM_PLAT_OMAP_INCLUDE_MACH_OMAP_HWMOD_H #define __ARCH_ARM_PLAT_OMAP_INCLUDE_MACH_OMAP_HWMOD_H #include #include #include #include #include #include struct omap_device; extern struct omap_hwmod_sysc_fields omap_hwmod_sysc_type1; extern struct omap_hwmod_sysc_fields omap_hwmod_sysc_type2; /* * OCP SYSCONFIG bit shifts/masks TYPE1. These are for IPs compliant * with the original PRCM protocol defined for OMAP2420 */ #define SYSC_TYPE1_MIDLEMODE_SHIFT 12 #define SYSC_TYPE1_MIDLEMODE_MASK (0x3 << SYSC_MIDLEMODE_SHIFT) #define SYSC_TYPE1_CLOCKACTIVITY_SHIFT 8 #define SYSC_TYPE1_CLOCKACTIVITY_MASK (0x3 << SYSC_CLOCKACTIVITY_SHIFT) #define SYSC_TYPE1_SIDLEMODE_SHIFT 3 #define SYSC_TYPE1_SIDLEMODE_MASK (0x3 << SYSC_SIDLEMODE_SHIFT) #define SYSC_TYPE1_ENAWAKEUP_SHIFT 2 #define SYSC_TYPE1_ENAWAKEUP_MASK (1 << SYSC_ENAWAKEUP_SHIFT) #define SYSC_TYPE1_SOFTRESET_SHIFT 1 #define SYSC_TYPE1_SOFTRESET_MASK (1 << SYSC_SOFTRESET_SHIFT) #define SYSC_TYPE1_AUTOIDLE_SHIFT 0 #define SYSC_TYPE1_AUTOIDLE_MASK (1 << SYSC_AUTOIDLE_SHIFT) /* * OCP SYSCONFIG bit shifts/masks TYPE2. These are for IPs compliant * with the new PRCM protocol defined for new OMAP4 IPs. */ #define SYSC_TYPE2_SOFTRESET_SHIFT 0 #define SYSC_TYPE2_SOFTRESET_MASK (1 << SYSC_TYPE2_SOFTRESET_SHIFT) #define SYSC_TYPE2_SIDLEMODE_SHIFT 2 #define SYSC_TYPE2_SIDLEMODE_MASK (0x3 << SYSC_TYPE2_SIDLEMODE_SHIFT) #define SYSC_TYPE2_MIDLEMODE_SHIFT 4 #define SYSC_TYPE2_MIDLEMODE_MASK (0x3 << SYSC_TYPE2_MIDLEMODE_SHIFT) /* OCP SYSSTATUS bit shifts/masks */ #define SYSS_RESETDONE_SHIFT 0 #define SYSS_RESETDONE_MASK (1 << SYSS_RESETDONE_SHIFT) /* Master standby/slave idle mode flags */ #define HWMOD_IDLEMODE_FORCE (1 << 0) #define HWMOD_IDLEMODE_NO (1 << 1) #define HWMOD_IDLEMODE_SMART (1 << 2) #define HWMOD_IDLEMODE_SMART_WKUP (1 << 3) /* modulemode control type (SW or HW) */ #define MODULEMODE_HWCTRL 1 #define MODULEMODE_SWCTRL 2 /** * struct omap_hwmod_mux_info - hwmod specific mux configuration * @pads: array of omap_device_pad entries * @nr_pads: number of omap_device_pad entries * * Note that this is currently built during init as needed. */ struct omap_hwmod_mux_info { int nr_pads; struct omap_device_pad *pads; int nr_pads_dynamic; struct omap_device_pad **pads_dynamic; bool enabled; }; /** * struct omap_hwmod_irq_info - MPU IRQs used by the hwmod * @name: name of the IRQ channel (module local name) * @irq: IRQ channel ID (should be non-negative except -1 = terminator) * * @name should be something short, e.g., "tx" or "rx". It is for use * by platform_get_resource_byname(). It is defined locally to the * hwmod. */ struct omap_hwmod_irq_info { const char *name; s16 irq; }; /** * struct omap_hwmod_dma_info - DMA channels used by the hwmod * @name: name of the DMA channel (module local name) * @dma_req: DMA request ID (should be non-negative except -1 = terminator) * * @name should be something short, e.g., "tx" or "rx". It is for use * by platform_get_resource_byname(). It is defined locally to the * hwmod. */ struct omap_hwmod_dma_info { const char *name; s16 dma_req; }; /** * struct omap_hwmod_rst_info - IPs reset lines use by hwmod * @name: name of the reset line (module local name) * @rst_shift: Offset of the reset bit * @st_shift: Offset of the reset status bit (OMAP2/3 only) * * @name should be something short, e.g., "cpu0" or "rst". It is defined * locally to the hwmod. */ struct omap_hwmod_rst_info { const char *name; u8 rst_shift; u8 st_shift; }; /** * struct omap_hwmod_opt_clk - optional clocks used by this hwmod * @role: "sys", "32k", "tv", etc -- for use in clk_get() * @clk: opt clock: OMAP clock name * @_clk: pointer to the struct clk (filled in at runtime) * * The module's interface clock and main functional clock should not * be added as optional clocks. */ struct omap_hwmod_opt_clk { const char *role; const char *clk; struct clk *_clk; }; /* omap_hwmod_omap2_firewall.flags bits */ #define OMAP_FIREWALL_L3 (1 << 0) #define OMAP_FIREWALL_L4 (1 << 1) /** * struct omap_hwmod_omap2_firewall - OMAP2/3 device firewall data * @l3_perm_bit: bit shift for L3_PM_*_PERMISSION_* * @l4_fw_region: L4 firewall region ID * @l4_prot_group: L4 protection group ID * @flags: (see omap_hwmod_omap2_firewall.flags macros above) */ struct omap_hwmod_omap2_firewall { u8 l3_perm_bit; u8 l4_fw_region; u8 l4_prot_group; u8 flags; }; /* * omap_hwmod_addr_space.flags bits * * ADDR_MAP_ON_INIT: Map this address space during omap_hwmod init. * ADDR_TYPE_RT: Address space contains module register target data. */ #define ADDR_MAP_ON_INIT (1 << 0) /* XXX does not belong */ #define ADDR_TYPE_RT (1 << 1) /** * struct omap_hwmod_addr_space - address space handled by the hwmod * @name: name of the address space * @pa_start: starting physical address * @pa_end: ending physical address * @flags: (see omap_hwmod_addr_space.flags macros above) * * Address space doesn't necessarily follow physical interconnect * structure. GPMC is one example. */ struct omap_hwmod_addr_space { const char *name; u32 pa_start; u32 pa_end; u8 flags; }; /* * omap_hwmod_ocp_if.user bits: these indicate the initiators that use this * interface to interact with the hwmod. Used to add sleep dependencies * when the module is enabled or disabled. */ #define OCP_USER_MPU (1 << 0) #define OCP_USER_SDMA (1 << 1) /* omap_hwmod_ocp_if.flags bits */ #define OCPIF_SWSUP_IDLE (1 << 0) #define OCPIF_CAN_BURST (1 << 1) /** * struct omap_hwmod_ocp_if - OCP interface data * @master: struct omap_hwmod that initiates OCP transactions on this link * @slave: struct omap_hwmod that responds to OCP transactions on this link * @addr: address space associated with this link * @clk: interface clock: OMAP clock name * @_clk: pointer to the interface struct clk (filled in at runtime) * @fw: interface firewall data * @width: OCP data width * @user: initiators using this interface (see OCP_USER_* macros above) * @flags: OCP interface flags (see OCPIF_* macros above) * * It may also be useful to add a tag_cnt field for OCP2.x devices. * * Parameter names beginning with an underscore are managed internally by * the omap_hwmod code and should not be set during initialization. */ struct omap_hwmod_ocp_if { struct omap_hwmod *master; struct omap_hwmod *slave; struct omap_hwmod_addr_space *addr; const char *clk; struct clk *_clk; union { struct omap_hwmod_omap2_firewall omap2; } fw; u8 width; u8 user; u8 flags; }; /* Macros for use in struct omap_hwmod_sysconfig */ /* Flags for use in omap_hwmod_sysconfig.idlemodes */ #define MASTER_STANDBY_SHIFT 4 #define SLAVE_IDLE_SHIFT 0 #define SIDLE_FORCE (HWMOD_IDLEMODE_FORCE << SLAVE_IDLE_SHIFT) #define SIDLE_NO (HWMOD_IDLEMODE_NO << SLAVE_IDLE_SHIFT) #define SIDLE_SMART (HWMOD_IDLEMODE_SMART << SLAVE_IDLE_SHIFT) #define SIDLE_SMART_WKUP (HWMOD_IDLEMODE_SMART_WKUP << SLAVE_IDLE_SHIFT) #define MSTANDBY_FORCE (HWMOD_IDLEMODE_FORCE << MASTER_STANDBY_SHIFT) #define MSTANDBY_NO (HWMOD_IDLEMODE_NO << MASTER_STANDBY_SHIFT) #define MSTANDBY_SMART (HWMOD_IDLEMODE_SMART << MASTER_STANDBY_SHIFT) #define MSTANDBY_SMART_WKUP (HWMOD_IDLEMODE_SMART_WKUP << MASTER_STANDBY_SHIFT) /* omap_hwmod_sysconfig.sysc_flags capability flags */ #define SYSC_HAS_AUTOIDLE (1 << 0) #define SYSC_HAS_SOFTRESET (1 << 1) #define SYSC_HAS_ENAWAKEUP (1 << 2) #define SYSC_HAS_EMUFREE (1 << 3) #define SYSC_HAS_CLOCKACTIVITY (1 << 4) #define SYSC_HAS_SIDLEMODE (1 << 5) #define SYSC_HAS_MIDLEMODE (1 << 6) #define SYSS_HAS_RESET_STATUS (1 << 7) #define SYSC_NO_CACHE (1 << 8) /* XXX SW flag, belongs elsewhere */ #define SYSC_HAS_RESET_STATUS (1 << 9) /* omap_hwmod_sysconfig.clockact flags */ #define CLOCKACT_TEST_BOTH 0x0 #define CLOCKACT_TEST_MAIN 0x1 #define CLOCKACT_TEST_ICLK 0x2 #define CLOCKACT_TEST_NONE 0x3 /** * struct omap_hwmod_sysc_fields - hwmod OCP_SYSCONFIG register field offsets. * @midle_shift: Offset of the midle bit * @clkact_shift: Offset of the clockactivity bit * @sidle_shift: Offset of the sidle bit * @enwkup_shift: Offset of the enawakeup bit * @srst_shift: Offset of the softreset bit * @autoidle_shift: Offset of the autoidle bit */ struct omap_hwmod_sysc_fields { u8 midle_shift; u8 clkact_shift; u8 sidle_shift; u8 enwkup_shift; u8 srst_shift; u8 autoidle_shift; }; /** * struct omap_hwmod_class_sysconfig - hwmod class OCP_SYS* data * @rev_offs: IP block revision register offset (from module base addr) * @sysc_offs: OCP_SYSCONFIG register offset (from module base addr) * @syss_offs: OCP_SYSSTATUS register offset (from module base addr) * @idlemodes: One or more of {SIDLE,MSTANDBY}_{OFF,FORCE,SMART} * @sysc_flags: SYS{C,S}_HAS* flags indicating SYSCONFIG bits supported * @clockact: the default value of the module CLOCKACTIVITY bits * * @clockact describes to the module which clocks are likely to be * disabled when the PRCM issues its idle request to the module. Some * modules have separate clockdomains for the interface clock and main * functional clock, and can check whether they should acknowledge the * idle request based on the internal module functionality that has * been associated with the clocks marked in @clockact. This field is * only used if HWMOD_SET_DEFAULT_CLOCKACT is set (see below) * * @sysc_fields: structure containing the offset positions of various bits in * SYSCONFIG register. This can be populated using omap_hwmod_sysc_type1 or * omap_hwmod_sysc_type2 defined in omap_hwmod_common_data.c depending on * whether the device ip is compliant with the original PRCM protocol * defined for OMAP2420 or the new PRCM protocol for new OMAP4 IPs. * If the device follows a different scheme for the sysconfig register , * then this field has to be populated with the correct offset structure. */ struct omap_hwmod_class_sysconfig { u16 rev_offs; u16 sysc_offs; u16 syss_offs; u16 sysc_flags; u8 idlemodes; u8 clockact; struct omap_hwmod_sysc_fields *sysc_fields; }; /** * struct omap_hwmod_omap2_prcm - OMAP2/3-specific PRCM data * @module_offs: PRCM submodule offset from the start of the PRM/CM * @prcm_reg_id: PRCM register ID (e.g., 3 for CM_AUTOIDLE3) * @module_bit: register bit shift for AUTOIDLE, WKST, WKEN, GRPSEL regs * @idlest_reg_id: IDLEST register ID (e.g., 3 for CM_IDLEST3) * @idlest_idle_bit: register bit shift for CM_IDLEST slave idle bit * @idlest_stdby_bit: register bit shift for CM_IDLEST master standby bit * * @prcm_reg_id and @module_bit are specific to the AUTOIDLE, WKST, * WKEN, GRPSEL registers. In an ideal world, no extra information * would be needed for IDLEST information, but alas, there are some * exceptions, so @idlest_reg_id, @idlest_idle_bit, @idlest_stdby_bit * are needed for the IDLEST registers (c.f. 2430 I2CHS, 3430 USBHOST) */ struct omap_hwmod_omap2_prcm { s16 module_offs; u8 prcm_reg_id; u8 module_bit; u8 idlest_reg_id; u8 idlest_idle_bit; u8 idlest_stdby_bit; }; /** * struct omap_hwmod_omap4_prcm - OMAP4-specific PRCM data * @clkctrl_reg: PRCM address of the clock control register * @rstctrl_reg: address of the XXX_RSTCTRL register located in the PRM * @submodule_wkdep_bit: bit shift of the WKDEP range */ struct omap_hwmod_omap4_prcm { u16 clkctrl_offs; u16 rstctrl_offs; u16 context_offs; u8 submodule_wkdep_bit; u8 modulemode; }; /* * omap_hwmod.flags definitions * * HWMOD_SWSUP_SIDLE: omap_hwmod code should manually bring module in and out * of idle, rather than relying on module smart-idle * HWMOD_SWSUP_MSTDBY: omap_hwmod code should manually bring module in and out * of standby, rather than relying on module smart-standby * HWMOD_INIT_NO_RESET: don't reset this module at boot - important for * SDRAM controller, etc. XXX probably belongs outside the main hwmod file * XXX Should be HWMOD_SETUP_NO_RESET * HWMOD_INIT_NO_IDLE: don't idle this module at boot - important for SDRAM * controller, etc. XXX probably belongs outside the main hwmod file * XXX Should be HWMOD_SETUP_NO_IDLE * HWMOD_NO_OCP_AUTOIDLE: disable module autoidle (OCP_SYSCONFIG.AUTOIDLE) * when module is enabled, rather than the default, which is to * enable autoidle * HWMOD_SET_DEFAULT_CLOCKACT: program CLOCKACTIVITY bits at startup * HWMOD_NO_IDLEST: this module does not have idle status - this is the case * only for few initiator modules on OMAP2 & 3. * HWMOD_CONTROL_OPT_CLKS_IN_RESET: Enable all optional clocks during reset. * This is needed for devices like DSS that require optional clocks enabled * in order to complete the reset. Optional clocks will be disabled * again after the reset. * HWMOD_16BIT_REG: Module has 16bit registers */ #define HWMOD_SWSUP_SIDLE (1 << 0) #define HWMOD_SWSUP_MSTANDBY (1 << 1) #define HWMOD_INIT_NO_RESET (1 << 2) #define HWMOD_INIT_NO_IDLE (1 << 3) #define HWMOD_NO_OCP_AUTOIDLE (1 << 4) #define HWMOD_SET_DEFAULT_CLOCKACT (1 << 5) #define HWMOD_NO_IDLEST (1 << 6) #define HWMOD_CONTROL_OPT_CLKS_IN_RESET (1 << 7) #define HWMOD_16BIT_REG (1 << 8) /* * omap_hwmod._int_flags definitions * These are for internal use only and are managed by the omap_hwmod code. * * _HWMOD_NO_MPU_PORT: no path exists for the MPU to write to this module * _HWMOD_WAKEUP_ENABLED: set when the omap_hwmod code has enabled ENAWAKEUP * _HWMOD_SYSCONFIG_LOADED: set when the OCP_SYSCONFIG value has been cached */ #define _HWMOD_NO_MPU_PORT (1 << 0) #define _HWMOD_WAKEUP_ENABLED (1 << 1) #define _HWMOD_SYSCONFIG_LOADED (1 << 2) /* * omap_hwmod._state definitions * * INITIALIZED: reset (optionally), initialized, enabled, disabled * (optionally) * * */ #define _HWMOD_STATE_UNKNOWN 0 #define _HWMOD_STATE_REGISTERED 1 #define _HWMOD_STATE_CLKS_INITED 2 #define _HWMOD_STATE_INITIALIZED 3 #define _HWMOD_STATE_ENABLED 4 #define _HWMOD_STATE_IDLE 5 #define _HWMOD_STATE_DISABLED 6 /** * struct omap_hwmod_class - the type of an IP block * @name: name of the hwmod_class * @sysc: device SYSCONFIG/SYSSTATUS register data * @rev: revision of the IP class * @pre_shutdown: ptr to fn to be executed immediately prior to device shutdown * @reset: ptr to fn to be executed in place of the standard hwmod reset fn * * Represent the class of a OMAP hardware "modules" (e.g. timer, * smartreflex, gpio, uart...) * * @pre_shutdown is a function that will be run immediately before * hwmod clocks are disabled, etc. It is intended for use for hwmods * like the MPU watchdog, which cannot be disabled with the standard * omap_hwmod_shutdown(). The function should return 0 upon success, * or some negative error upon failure. Returning an error will cause * omap_hwmod_shutdown() to abort the device shutdown and return an * error. * * If @reset is defined, then the function it points to will be * executed in place of the standard hwmod _reset() code in * mach-omap2/omap_hwmod.c. This is needed for IP blocks which have * unusual reset sequences - usually processor IP blocks like the IVA. */ struct omap_hwmod_class { const char *name; struct omap_hwmod_class_sysconfig *sysc; u32 rev; int (*pre_shutdown)(struct omap_hwmod *oh); int (*reset)(struct omap_hwmod *oh); }; /** * struct omap_hwmod - integration data for OMAP hardware "modules" (IP blocks) * @name: name of the hwmod * @class: struct omap_hwmod_class * to the class of this hwmod * @od: struct omap_device currently associated with this hwmod (internal use) * @mpu_irqs: ptr to an array of MPU IRQs * @sdma_reqs: ptr to an array of System DMA request IDs * @prcm: PRCM data pertaining to this hwmod * @main_clk: main clock: OMAP clock name * @_clk: pointer to the main struct clk (filled in at runtime) * @opt_clks: other device clocks that drivers can request (0..*) * @vdd_name: voltage domain name * @voltdm: pointer to voltage domain (filled in at runtime) * @masters: ptr to array of OCP ifs that this hwmod can initiate on * @slaves: ptr to array of OCP ifs that this hwmod can respond on * @dev_attr: arbitrary device attributes that can be passed to the driver * @_sysc_cache: internal-use hwmod flags * @_mpu_rt_va: cached register target start address (internal use) * @_mpu_port_index: cached MPU register target slave ID (internal use) * @opt_clks_cnt: number of @opt_clks * @master_cnt: number of @master entries * @slaves_cnt: number of @slave entries * @response_lat: device OCP response latency (in interface clock cycles) * @_int_flags: internal-use hwmod flags * @_state: internal-use hwmod state * @_postsetup_state: internal-use state to leave the hwmod in after _setup() * @flags: hwmod flags (documented below) * @_lock: spinlock serializing operations on this hwmod * @node: list node for hwmod list (internal use) * * @main_clk refers to this module's "main clock," which for our * purposes is defined as "the functional clock needed for register * accesses to complete." Modules may not have a main clock if the * interface clock also serves as a main clock. * * Parameter names beginning with an underscore are managed internally by * the omap_hwmod code and should not be set during initialization. */ struct omap_hwmod { const char *name; struct omap_hwmod_class *class; struct omap_device *od; struct omap_hwmod_mux_info *mux; struct omap_hwmod_irq_info *mpu_irqs; struct omap_hwmod_dma_info *sdma_reqs; struct omap_hwmod_rst_info *rst_lines; union { struct omap_hwmod_omap2_prcm omap2; struct omap_hwmod_omap4_prcm omap4; } prcm; const char *main_clk; struct clk *_clk; struct omap_hwmod_opt_clk *opt_clks; char *clkdm_name; struct clockdomain *clkdm; char *vdd_name; struct omap_hwmod_ocp_if **masters; /* connect to *_IA */ struct omap_hwmod_ocp_if **slaves; /* connect to *_TA */ void *dev_attr; u32 _sysc_cache; void __iomem *_mpu_rt_va; spinlock_t _lock; struct list_head node; u16 flags; u8 _mpu_port_index; u8 response_lat; u8 rst_lines_cnt; u8 opt_clks_cnt; u8 masters_cnt; u8 slaves_cnt; u8 hwmods_cnt; u8 _int_flags; u8 _state; u8 _postsetup_state; }; int omap_hwmod_register(struct omap_hwmod **ohs); struct omap_hwmod *omap_hwmod_lookup(const char *name); int omap_hwmod_for_each(int (*fn)(struct omap_hwmod *oh, void *data), void *data); int __init omap_hwmod_setup_one(const char *name); int omap_hwmod_enable(struct omap_hwmod *oh); int _omap_hwmod_enable(struct omap_hwmod *oh); int omap_hwmod_idle(struct omap_hwmod *oh); int _omap_hwmod_idle(struct omap_hwmod *oh); int omap_hwmod_shutdown(struct omap_hwmod *oh); int omap_hwmod_assert_hardreset(struct omap_hwmod *oh, const char *name); int omap_hwmod_deassert_hardreset(struct omap_hwmod *oh, const char *name); int omap_hwmod_read_hardreset(struct omap_hwmod *oh, const char *name); int omap_hwmod_enable_clocks(struct omap_hwmod *oh); int omap_hwmod_disable_clocks(struct omap_hwmod *oh); int omap_hwmod_set_slave_idlemode(struct omap_hwmod *oh, u8 idlemode); int omap_hwmod_set_ocp_autoidle(struct omap_hwmod *oh, u8 autoidle); int omap_hwmod_reset(struct omap_hwmod *oh); void omap_hwmod_ocp_barrier(struct omap_hwmod *oh); void omap_hwmod_write(u32 v, struct omap_hwmod *oh, u16 reg_offs); u32 omap_hwmod_read(struct omap_hwmod *oh, u16 reg_offs); int omap_hwmod_softreset(struct omap_hwmod *oh); int omap_hwmod_count_resources(struct omap_hwmod *oh); int omap_hwmod_fill_resources(struct omap_hwmod *oh, struct resource *res); struct powerdomain *omap_hwmod_get_pwrdm(struct omap_hwmod *oh); void __iomem *omap_hwmod_get_mpu_rt_va(struct omap_hwmod *oh); int omap_hwmod_add_initiator_dep(struct omap_hwmod *oh, struct omap_hwmod *init_oh); int omap_hwmod_del_initiator_dep(struct omap_hwmod *oh, struct omap_hwmod *init_oh); int omap_hwmod_set_clockact_both(struct omap_hwmod *oh); int omap_hwmod_set_clockact_main(struct omap_hwmod *oh); int omap_hwmod_set_clockact_iclk(struct omap_hwmod *oh); int omap_hwmod_set_clockact_none(struct omap_hwmod *oh); int omap_hwmod_enable_wakeup(struct omap_hwmod *oh); int omap_hwmod_disable_wakeup(struct omap_hwmod *oh); int omap_hwmod_for_each_by_class(const char *classname, int (*fn)(struct omap_hwmod *oh, void *user), void *user); int omap_hwmod_set_postsetup_state(struct omap_hwmod *oh, u8 state); u32 omap_hwmod_get_context_loss_count(struct omap_hwmod *oh); int omap_hwmod_no_setup_reset(struct omap_hwmod *oh); /* * Chip variant-specific hwmod init routines - XXX should be converted * to use initcalls once the initial boot ordering is straightened out */ extern int omap2420_hwmod_init(void); extern int omap2430_hwmod_init(void); extern int omap3xxx_hwmod_init(void); extern int omap44xx_hwmod_init(void); #endif