# # Ethernet LAN device configuration # menuconfig ETHERNET bool "Ethernet driver support" depends on NET default y ---help--- This section contains all the Ethernet device drivers. if ETHERNET config MDIO tristate config SUNGEM_PHY tristate source "drivers/net/ethernet/3com/Kconfig" source "drivers/net/ethernet/adaptec/Kconfig" source "drivers/net/ethernet/aeroflex/Kconfig" source "drivers/net/ethernet/alteon/Kconfig" source "drivers/net/ethernet/amd/Kconfig" source "drivers/net/ethernet/apple/Kconfig" source "drivers/net/ethernet/atheros/Kconfig" source "drivers/net/ethernet/cadence/Kconfig" source "drivers/net/ethernet/adi/Kconfig" source "drivers/net/ethernet/broadcom/Kconfig" source "drivers/net/ethernet/brocade/Kconfig" source "drivers/net/ethernet/chelsio/Kconfig" source "drivers/net/ethernet/cirrus/Kconfig" source "drivers/net/ethernet/cisco/Kconfig" source "drivers/net/ethernet/davicom/Kconfig" config DNET tristate "Dave ethernet support (DNET)" depends on HAS_IOMEM select PHYLIB ---help--- The Dave ethernet interface (DNET) is found on Qong Board FPGA. Say Y to include support for the DNET chip. To compile this driver as a module, choose M here: the module will be called dnet. source "drivers/net/ethernet/dec/Kconfig" source "drivers/net/ethernet/dlink/Kconfig" source "drivers/net/ethernet/emulex/Kconfig" source "drivers/net/ethernet/neterion/Kconfig" source "drivers/net/ethernet/faraday/Kconfig" source "drivers/net/ethernet/freescale/Kconfig" source "drivers/net/ethernet/fujitsu/Kconfig" source "drivers/net/ethernet/hp/Kconfig" source "drivers/net/ethernet/ibm/Kconfig" source "drivers/net/ethernet/intel/Kconfig" source "drivers/net/ethernet/i825xx/Kconfig" source "drivers/net/ethernet/xscale/Kconfig" source "drivers/net/ethernet/icplus/Kconfig" config JME tristate "JMicron(R) PCI-Express Gigabit Ethernet support" depends on PCI select CRC32 select NET_CORE select MII ---help--- This driver supports the PCI-Express gigabit ethernet adapters based on JMicron JMC250 chipset. To compile this driver as a module, choose M here. The module will be called jme. config KORINA tristate "Korina (IDT RC32434) Ethernet support" depends on MIKROTIK_RB532 ---help--- If you have a Mikrotik RouterBoard 500 or IDT RC32434 based system say Y. Otherwise say N. config LANTIQ_ETOP tristate "Lantiq SoC ETOP driver" depends on SOC_TYPE_XWAY ---help--- Support for the MII0 inside the Lantiq SoC source "drivers/net/ethernet/marvell/Kconfig" source "drivers/net/ethernet/mellanox/Kconfig" source "drivers/net/ethernet/micrel/Kconfig" source "drivers/net/ethernet/microchip/Kconfig" config MIPS_SIM_NET tristate "MIPS simulator Network device" depends on MIPS_SIM ---help--- The MIPSNET device is a simple Ethernet network device which is emulated by the MIPS Simulator. If you are not using a MIPSsim or are unsure, say N. source "drivers/net/ethernet/myricom/Kconfig" config FEALNX tristate "Myson MTD-8xx PCI Ethernet support" depends on PCI select CRC32 select NET_CORE select MII ---help--- Say Y here to support the Myson MTD-800 family of PCI-based Ethernet cards. source "drivers/net/ethernet/natsemi/Kconfig" source "drivers/net/ethernet/8390/Kconfig" config NET_NETX tristate "NetX Ethernet support" select NET_CORE select MII depends on ARCH_NETX ---help--- This is support for the Hilscher netX builtin Ethernet ports To compile this driver as a module, choose M here. The module will be called netx-eth. source "drivers/net/ethernet/nuvoton/Kconfig" source "drivers/net/ethernet/nvidia/Kconfig" source "drivers/net/ethernet/octeon/Kconfig" source "drivers/net/ethernet/oki-semi/Kconfig" config ETHOC tristate "OpenCores 10/100 Mbps Ethernet MAC support" depends on HAS_IOMEM && HAS_DMA select NET_CORE select MII select PHYLIB select CRC32 select BITREVERSE ---help--- Say Y here if you want to use the OpenCores 10/100 Mbps Ethernet MAC. source "drivers/net/ethernet/packetengines/Kconfig" source "drivers/net/ethernet/pasemi/Kconfig" source "drivers/net/ethernet/qlogic/Kconfig" source "drivers/net/ethernet/racal/Kconfig" source "drivers/net/ethernet/realtek/Kconfig" source "drivers/net/ethernet/renesas/Kconfig" source "drivers/net/ethernet/rdc/Kconfig" config S6GMAC tristate "S6105 GMAC ethernet support" depends on XTENSA_VARIANT_S6000 select PHYLIB ---help--- This driver supports the on chip ethernet device on the S6105 xtensa processor. To compile this driver as a module, choose M here. The module will be called s6gmac. source "drivers/net/ethernet/seeq/Kconfig" source "drivers/net/ethernet/silan/Kconfig" source "drivers/net/ethernet/sis/Kconfig" source "drivers/net/ethernet/sfc/Kconfig" source "drivers/net/ethernet/sgi/Kconfig" source "drivers/net/ethernet/smsc/Kconfig" source "drivers/net/ethernet/stmicro/Kconfig" source "drivers/net/ethernet/sun/Kconfig" source "drivers/net/ethernet/tehuti/Kconfig" source "drivers/net/ethernet/ti/Kconfig" source "drivers/net/ethernet/tile/Kconfig" source "drivers/net/ethernet/toshiba/Kconfig" source "drivers/net/ethernet/tundra/Kconfig" source "drivers/net/ethernet/via/Kconfig" source "drivers/net/ethernet/xilinx/Kconfig" source "drivers/net/ethernet/xircom/Kconfig" endif # ETHERNET