/* * Texas Instruments TI81XX "usb platform glue layer" * * Copyright (c) 2008, MontaVista Software, Inc. * * Based on the DaVinci "glue layer" code. * Copyright (C) 2005-2006 by Texas Instruments * * This file is part of the Inventra Controller Driver for Linux. * * The Inventra Controller Driver for Linux is free software; you * can redistribute it and/or modify it under the terms of the GNU * General Public License version 2 as published by the Free Software * Foundation. * * The Inventra Controller Driver for Linux is distributed in * the hope that it will be useful, but WITHOUT ANY WARRANTY; * without even the implied warranty of MERCHANTABILITY or * FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public * License for more details. * * You should have received a copy of the GNU General Public License * along with The Inventra Controller Driver for Linux ; if not, * write to the Free Software Foundation, Inc., 59 Temple Place, * Suite 330, Boston, MA 02111-1307 USA * */ #include #include #include #include #include #include #include #include "cppi41.h" #include "ti81xx.h" #include "musb_core.h" #include "cppi41_dma.h" struct ti81xx_glue { struct device *dev; struct clk *ick; /* common usbss interface clk */ struct clk *fck; /* common usbss functional clk */ struct resource *mem_pa; /* usbss memory resource */ void *mem_va; /* ioremapped virtual address */ struct platform_device *musb[2];/* child musb pdevs */ u8 irq; /* usbss irq */ }; static u64 musb_dmamask = DMA_BIT_MASK(32); static void *usbss_virt_base; static u8 usbss_init_done; struct musb *gmusb[2]; u8 usbid_sw_ctrl; #undef USB_TI81XX_DEBUG #ifdef USB_TI81XX_DEBUG #define dprintk(x, ...) printk(x, ## __VA_ARGS__) #else #define dprintk(x, ...) #endif #ifdef CONFIG_USB_TI_CPPI41_DMA static irqreturn_t cppi41dma_Interrupt(int irq, void *hci); static u8 cppi41_init_done; static void *cppi41_dma_base; #define CPPI41_ADDR(offs) ((void *)((u32)cppi41_dma_base + (offs - 0x2000))) #endif extern void omap_ctrl_writel(u32 val, u16 offset); extern u32 omap_ctrl_readl(u16 offset); static inline u32 usbss_read(u32 offset) { if (!usbss_init_done) return 0; return __raw_readl(usbss_virt_base + offset); } static inline void usbss_write(u32 offset, u32 data) { if (!usbss_init_done) return ; __raw_writel(data, usbss_virt_base + offset); } static void usbotg_ss_init(void) { if (!usbss_init_done) { /* reset the usbss for usb0/usb1 */ usbss_write(USBSS_SYSCONFIG, usbss_read(USBSS_SYSCONFIG) | USB_SOFT_RESET_MASK); /* clear any USBSS interrupts */ usbss_write(USBSS_IRQ_EOI, 0); usbss_write(USBSS_IRQ_STATUS, usbss_read(USBSS_IRQ_STATUS)); usbss_init_done = 1; } } static void usbotg_ss_uninit(void) { if (usbss_init_done) { usbss_init_done = 0; usbss_virt_base = 0; } } void set_frame_threshold(struct musb *musb, u8 is_tx, u8 epnum, u8 value, u8 en_intr) { u32 base, reg_val, frame_intr = 0, frame_base = 0; u32 offs = epnum/4*4; u8 indx = (epnum % 4) * 8; if (is_tx) base = musb->id ? USBSS_IRQ_FRAME_THRESHOLD_TX1 : USBSS_IRQ_FRAME_THRESHOLD_TX0; else base = musb->id ? USBSS_IRQ_FRAME_THRESHOLD_RX1 : USBSS_IRQ_FRAME_THRESHOLD_RX0; reg_val = usbss_read(base + offs); reg_val &= ~(0xFF << indx); reg_val |= (value << indx); usbss_write(base + offs, reg_val); if (en_intr) { frame_base = musb->id ? USBSS_IRQ_FRAME_ENABLE_1 : USBSS_IRQ_FRAME_ENABLE_0; frame_intr = musb->id ? usbss_read(USBSS_IRQ_FRAME_ENABLE_0) : usbss_read(USBSS_IRQ_FRAME_ENABLE_1); frame_intr |= is_tx ? (1 << epnum) : (1 << (16 + epnum)); usbss_write(frame_base, frame_intr); dev_dbg(musb->controller, "%s: framebase=%x, frame_intr=%x\n", is_tx ? "tx" : "rx", frame_base, frame_intr); } } void set_dma_threshold(struct musb *musb, u8 is_tx, u8 epnum, u8 value) { u32 base, reg_val; u32 offs = epnum/4*4; u8 indx = (epnum % 4) * 8; if (musb->id == 0) base = is_tx ? USBSS_IRQ_DMA_THRESHOLD_TX0 : USBSS_IRQ_DMA_THRESHOLD_RX0; else base = is_tx ? USBSS_IRQ_DMA_THRESHOLD_TX1 : USBSS_IRQ_DMA_THRESHOLD_RX1; reg_val = usbss_read(base + offs); reg_val &= ~(0xFF << indx); reg_val |= (value << indx); dev_dbg(musb->controller, "base=%x, offs=%x, indx=%d, reg_val = (%x)%x\n", base, offs, indx, reg_val, usbss_read(base + offs)); usbss_write(base + offs, reg_val); } /* ti81xx specific read/write functions */ u16 ti81xx_musb_readw(const void __iomem *addr, unsigned offset) { u32 tmp; u16 val; tmp = __raw_readl(addr + (offset & ~3)); switch (offset & 0x3) { case 0: val = (tmp & 0xffff); break; case 1: val = (tmp >> 8) & 0xffff; break; case 2: case 3: default: val = (tmp >> 16) & 0xffff; break; } return val; } void ti81xx_musb_writew(void __iomem *addr, unsigned offset, u16 data) { __raw_writew(data, addr + offset); } u8 ti81xx_musb_readb(const void __iomem *addr, unsigned offset) { u32 tmp; u8 val; tmp = __raw_readl(addr + (offset & ~3)); switch (offset & 0x3) { case 0: val = tmp & 0xff; break; case 1: val = (tmp >> 8); break; case 2: val = (tmp >> 16); break; case 3: default: val = (tmp >> 24); break; } return val; } void ti81xx_musb_writeb(void __iomem *addr, unsigned offset, u8 data) { __raw_writeb(data, addr + offset); } #ifdef CONFIG_USB_TI_CPPI41_DMA /* * CPPI 4.1 resources used for USB OTG controller module: * tx/rx completion queues for usb0 */ static u16 tx_comp_q[] = {93, 94, 95, 96, 97, 98, 99, 100, 101, 102, 103, 104, 105, 106, 107 }; static u16 rx_comp_q[] = {109, 110, 111, 112, 113, 114, 115, 116, 117, 118, 119, 120, 121, 122, 123 }; /* tx/rx completion queues for usb1 */ static u16 tx_comp_q1[] = {125, 126, 127, 128, 129, 130, 131, 132, 133, 134, 135, 136, 137, 138, 139 }; static u16 rx_comp_q1[] = {141, 142, 143, 144, 145, 146, 147, 148, 149, 150, 151, 152, 153, 154, 155 }; /* Fair scheduling */ u32 dma_sched_table[] = { 0x81018000, 0x83038202, 0x85058404, 0x87078606, 0x89098808, 0x8b0b8a0a, 0x8d0d8c0c, 0x8f0f8e0e, 0x91119010, 0x93139212, 0x95159414, 0x97179616, 0x99199818, 0x9b1b9a1a, 0x9d1d9c1c, 0x00009e1e, }; /* cppi41 dma tx channel info */ static const struct cppi41_tx_ch tx_ch_info[] = { [0] = { .port_num = 1, .num_tx_queue = 2, .tx_queue = { {0, 32} , {0, 33} } }, [1] = { .port_num = 2, .num_tx_queue = 2, .tx_queue = { {0, 34} , {0, 35} } }, [2] = { .port_num = 3, .num_tx_queue = 2, .tx_queue = { {0, 36} , {0, 37} } }, [3] = { .port_num = 4, .num_tx_queue = 2, .tx_queue = { {0, 38} , {0, 39} } }, [4] = { .port_num = 5, .num_tx_queue = 2, .tx_queue = { {0, 40} , {0, 41} } }, [5] = { .port_num = 6, .num_tx_queue = 2, .tx_queue = { {0, 42} , {0, 43} } }, [6] = { .port_num = 7, .num_tx_queue = 2, .tx_queue = { {0, 44} , {0, 45} } }, [7] = { .port_num = 8, .num_tx_queue = 2, .tx_queue = { {0, 46} , {0, 47} } }, [8] = { .port_num = 9, .num_tx_queue = 2, .tx_queue = { {0, 48} , {0, 49} } }, [9] = { .port_num = 10, .num_tx_queue = 2, .tx_queue = { {0, 50} , {0, 51} } }, [10] = { .port_num = 11, .num_tx_queue = 2, .tx_queue = { {0, 52} , {0, 53} } }, [11] = { .port_num = 12, .num_tx_queue = 2, .tx_queue = { {0, 54} , {0, 55} } }, [12] = { .port_num = 13, .num_tx_queue = 2, .tx_queue = { {0, 56} , {0, 57} } }, [13] = { .port_num = 14, .num_tx_queue = 2, .tx_queue = { {0, 58} , {0, 59} } }, [14] = { .port_num = 15, .num_tx_queue = 2, .tx_queue = { {0, 60} , {0, 61} } }, [15] = { .port_num = 1, .num_tx_queue = 2, .tx_queue = { {0, 62} , {0, 63} } }, [16] = { .port_num = 2, .num_tx_queue = 2, .tx_queue = { {0, 64} , {0, 65} } }, [17] = { .port_num = 3, .num_tx_queue = 2, .tx_queue = { {0, 66} , {0, 67} } }, [18] = { .port_num = 4, .num_tx_queue = 2, .tx_queue = { {0, 68} , {0, 69} } }, [19] = { .port_num = 5, .num_tx_queue = 2, .tx_queue = { {0, 70} , {0, 71} } }, [20] = { .port_num = 6, .num_tx_queue = 2, .tx_queue = { {0, 72} , {0, 73} } }, [21] = { .port_num = 7, .num_tx_queue = 2, .tx_queue = { {0, 74} , {0, 75} } }, [22] = { .port_num = 8, .num_tx_queue = 2, .tx_queue = { {0, 76} , {0, 77} } }, [23] = { .port_num = 9, .num_tx_queue = 2, .tx_queue = { {0, 78} , {0, 79} } }, [24] = { .port_num = 10, .num_tx_queue = 2, .tx_queue = { {0, 80} , {0, 81} } }, [25] = { .port_num = 11, .num_tx_queue = 2, .tx_queue = { {0, 82} , {0, 83} } }, [26] = { .port_num = 12, .num_tx_queue = 2, .tx_queue = { {0, 84} , {0, 85} } }, [27] = { .port_num = 13, .num_tx_queue = 2, .tx_queue = { {0, 86} , {0, 87} } }, [28] = { .port_num = 14, .num_tx_queue = 2, .tx_queue = { {0, 88} , {0, 89} } }, [29] = { .port_num = 15, .num_tx_queue = 2, .tx_queue = { {0, 90} , {0, 91} } } }; /* Queues 0 to 66 are pre-assigned, others are spare */ static const u32 assigned_queues[] = { 0xffffffff, /* queue 0..31 */ 0xffffffff, /* queue 32..63 */ 0xffffffff, /* queue 64..95 */ 0xffffffff, /* queue 96..127 */ 0x0fffffff /* queue 128..155 */ }; int __devinit cppi41_init(u8 id, u8 irq, int num_instances) { struct usb_cppi41_info *cppi_info = &usb_cppi41_info[id]; u16 numch, blknum, order; u32 i; /* init cppi info structure */ cppi_info->dma_block = 0; for (i = 0 ; i < USB_CPPI41_NUM_CH ; i++) cppi_info->ep_dma_ch[i] = i + (15 * id); cppi_info->q_mgr = 0; cppi_info->num_tx_comp_q = 15; cppi_info->num_rx_comp_q = 15; cppi_info->tx_comp_q = id ? tx_comp_q1 : tx_comp_q; cppi_info->rx_comp_q = id ? rx_comp_q1 : rx_comp_q; cppi_info->bd_intr_ctrl = 1; if (cppi41_init_done) return 0; blknum = cppi_info->dma_block; /* Queue manager information */ cppi41_queue_mgr[0].num_queue = 159; cppi41_queue_mgr[0].queue_types = CPPI41_FREE_DESC_BUF_QUEUE | CPPI41_UNASSIGNED_QUEUE; cppi41_queue_mgr[0].base_fdbq_num = 0; cppi41_queue_mgr[0].assigned = assigned_queues; /* init DMA block */ cppi41_dma_block[0].num_tx_ch = 30; cppi41_dma_block[0].num_rx_ch = 30; cppi41_dma_block[0].tx_ch_info = tx_ch_info; /* initilize cppi41 dma & Qmgr address */ cppi41_dma_base = ioremap(TI81XX_USB_CPPIDMA_BASE, TI81XX_USB_CPPIDMA_LEN); cppi41_queue_mgr[0].q_mgr_rgn_base = CPPI41_ADDR(QMGR_RGN_OFFS); cppi41_queue_mgr[0].desc_mem_rgn_base = CPPI41_ADDR(QMRG_DESCRGN_OFFS); cppi41_queue_mgr[0].q_mgmt_rgn_base = CPPI41_ADDR(QMGR_REG_OFFS); cppi41_queue_mgr[0].q_stat_rgn_base = CPPI41_ADDR(QMGR_STAT_OFFS); cppi41_dma_block[0].global_ctrl_base = CPPI41_ADDR(DMA_GLBCTRL_OFFS); cppi41_dma_block[0].ch_ctrl_stat_base = CPPI41_ADDR(DMA_CHCTRL_OFFS); cppi41_dma_block[0].sched_ctrl_base = CPPI41_ADDR(DMA_SCHED_OFFS); cppi41_dma_block[0].sched_table_base = CPPI41_ADDR(DMA_SCHEDTBL_OFFS); /* Initialize for Linking RAM region 0 alone */ cppi41_queue_mgr_init(cppi_info->q_mgr, 0, 0x3fff); numch = USB_CPPI41_NUM_CH * 2 * num_instances; cppi41_dma_block[0].num_max_ch = numch; order = get_count_order(numch); /* TODO: check two teardown desc per channel (5 or 7 ?)*/ if (order < 5) order = 5; cppi41_dma_block_init(blknum, cppi_info->q_mgr, order, dma_sched_table, numch); /* attach to the IRQ */ if (request_irq(irq, cppi41dma_Interrupt, 0, "cppi41_dma", 0)) printk(KERN_INFO "request_irq %d failed!\n", irq); else printk(KERN_INFO "registerd cppi-dma Intr @ IRQ %d\n", irq); cppi41_init_done = 1; printk(KERN_INFO "Cppi41 Init Done Qmgr-base(%p) dma-base(%p)\n", cppi41_queue_mgr[0].q_mgr_rgn_base, cppi41_dma_block[0].global_ctrl_base); /* enable all usbss the interrupts */ usbss_write(USBSS_IRQ_EOI, 0); usbss_write(USBSS_IRQ_ENABLE_SET, USBSS_INTR_FLAGS); usbss_write(USBSS_IRQ_DMA_ENABLE_0, 0xFFFeFFFe); printk(KERN_INFO "Cppi41 Init Done\n"); return 0; } void cppi41_free(void) { u32 numch, blknum, order; struct usb_cppi41_info *cppi_info = &usb_cppi41_info[0]; if (!cppi41_init_done) return ; numch = cppi41_dma_block[0].num_max_ch; order = get_count_order(numch); blknum = cppi_info->dma_block; cppi41_dma_block_uninit(blknum, cppi_info->q_mgr, order, dma_sched_table, numch); cppi41_queue_mgr_uninit(cppi_info->q_mgr); iounmap(cppi41_dma_base); cppi41_dma_base = 0; cppi41_init_done = 0; } int cppi41_disable_sched_rx(void) { cppi41_dma_sched_tbl_init(0, 0, dma_sched_table, 30); return 0; } int cppi41_enable_sched_rx(void) { cppi41_dma_sched_tbl_init(0, 0, dma_sched_table, 30); return 0; } #endif /* CONFIG_USB_TI_CPPI41_DMA */ /* * Because we don't set CTRL.UINT, it's "important" to: * - not read/write INTRUSB/INTRUSBE (except during * initial setup, as a workaround); * - use INTSET/INTCLR instead. */ /** * ti81xx_musb_enable - enable interrupts */ void ti81xx_musb_enable(struct musb *musb) { void __iomem *reg_base = musb->ctrl_base; u32 epmask, coremask; /* Workaround: setup IRQs through both register sets. */ epmask = ((musb->epmask & USB_TX_EP_MASK) << USB_INTR_TX_SHIFT) | ((musb->epmask & USB_RX_EP_MASK) << USB_INTR_RX_SHIFT); coremask = (0x01ff << USB_INTR_USB_SHIFT); coremask &= ~MUSB_INTR_SOF; musb_writel(reg_base, USB_EP_INTR_SET_REG, epmask); musb_writel(reg_base, USB_CORE_INTR_SET_REG, coremask); /* Force the DRVVBUS IRQ so we can start polling for ID change. */ if (is_otg_enabled(musb)) musb_writel(reg_base, USB_CORE_INTR_SET_REG, USB_INTR_DRVVBUS << USB_INTR_USB_SHIFT); } /** * ti81xx_musb_disable - disable HDRC and flush interrupts */ void ti81xx_musb_disable(struct musb *musb) { void __iomem *reg_base = musb->ctrl_base; musb_writel(reg_base, USB_CORE_INTR_CLEAR_REG, USB_INTR_USB_MASK); musb_writel(reg_base, USB_EP_INTR_CLEAR_REG, USB_TX_INTR_MASK | USB_RX_INTR_MASK); musb_writeb(musb->mregs, MUSB_DEVCTL, 0); musb_writel(reg_base, USB_IRQ_EOI, 0); } #define POLL_SECONDS 2 static void otg_timer(unsigned long _musb) { struct musb *musb = (void *)_musb; void __iomem *mregs = musb->mregs; u8 devctl; unsigned long flags; /* We poll because DaVinci's won't expose several OTG-critical * status change events (from the transceiver) otherwise. */ devctl = musb_readb(mregs, MUSB_DEVCTL); dev_dbg(musb->controller, "Poll devctl %02x (%s)\n", devctl, otg_state_string(musb->xceiv->state)); spin_lock_irqsave(&musb->lock, flags); switch (musb->xceiv->state) { case OTG_STATE_A_WAIT_BCON: devctl &= ~MUSB_DEVCTL_SESSION; musb_writeb(musb->mregs, MUSB_DEVCTL, devctl); devctl = musb_readb(musb->mregs, MUSB_DEVCTL); if (devctl & MUSB_DEVCTL_BDEVICE) { musb->xceiv->state = OTG_STATE_B_IDLE; MUSB_DEV_MODE(musb); } else { musb->xceiv->state = OTG_STATE_A_IDLE; MUSB_HST_MODE(musb); } break; case OTG_STATE_A_WAIT_VFALL: /* * Wait till VBUS falls below SessionEnd (~0.2 V); the 1.3 * RTL seems to mis-handle session "start" otherwise (or in * our case "recover"), in routine "VBUS was valid by the time * VBUSERR got reported during enumeration" cases. */ if (devctl & MUSB_DEVCTL_VBUS) { mod_timer(&musb->otg_workaround, jiffies + POLL_SECONDS * HZ); break; } musb->xceiv->state = OTG_STATE_A_WAIT_VRISE; musb_writel(musb->ctrl_base, USB_CORE_INTR_SET_REG, MUSB_INTR_VBUSERROR << USB_INTR_USB_SHIFT); break; case OTG_STATE_B_IDLE: if (!is_peripheral_enabled(musb)) break; /* * There's no ID-changed IRQ, so we have no good way to tell * when to switch to the A-Default state machine (by setting * the DEVCTL.SESSION flag). * * Workaround: whenever we're in B_IDLE, try setting the * session flag every few seconds. If it works, ID was * grounded and we're now in the A-Default state machine. * * NOTE: setting the session flag is _supposed_ to trigger * SRP but clearly it doesn't. */ devctl = musb_readb(mregs, MUSB_DEVCTL); if (devctl & MUSB_DEVCTL_BDEVICE) mod_timer(&musb->otg_workaround, jiffies + POLL_SECONDS * HZ); else musb->xceiv->state = OTG_STATE_A_IDLE; break; default: break; } spin_unlock_irqrestore(&musb->lock, flags); } void ti81xx_musb_try_idle(struct musb *musb, unsigned long timeout) { if (!is_otg_enabled(musb)) return; if (timeout == 0) timeout = jiffies + msecs_to_jiffies(3); /* Never idle if active, or when VBUS timeout is not set as host */ if (musb->is_active || (musb->a_wait_bcon == 0 && musb->xceiv->state == OTG_STATE_A_WAIT_BCON)) { dev_dbg(musb->controller, "%s active, deleting timer\n", otg_state_string(musb->xceiv->state)); del_timer(&musb->otg_workaround); musb->last_timer = jiffies; return; } if (time_after(musb->last_timer, timeout) && timer_pending(&musb->otg_workaround)) { dev_dbg(musb->controller, "Longer idle timer already pending, ignoring...\n"); return; } musb->last_timer = timeout; dev_dbg(musb->controller, "%s inactive, starting idle timer for %u ms\n", otg_state_string(musb->xceiv->state), jiffies_to_msecs(timeout - jiffies)); mod_timer(&musb->otg_workaround, timeout); } #ifdef CONFIG_USB_TI_CPPI41_DMA static irqreturn_t cppi41dma_Interrupt(int irq, void *hci) { struct musb *musb = hci; u32 intr_status; irqreturn_t ret = IRQ_NONE; u32 q_cmpl_status_0, q_cmpl_status_1, q_cmpl_status_2; u32 usb0_tx_intr, usb0_rx_intr; u32 usb1_tx_intr, usb1_rx_intr; void *q_mgr_base = cppi41_queue_mgr[0].q_mgr_rgn_base; unsigned long flags; musb = hci; /* * CPPI 4.1 interrupts share the same IRQ and the EOI register but * don't get reflected in the interrupt source/mask registers. */ /* * Check for the interrupts from Tx/Rx completion queues; they * are level-triggered and will stay asserted until the queues * are emptied. We're using the queue pending register 0 as a * substitute for the interrupt status register and reading it * directly for speed. */ intr_status = usbss_read(USBSS_IRQ_STATUS); if (intr_status) usbss_write(USBSS_IRQ_STATUS, intr_status); else printk(KERN_DEBUG "spurious usbss intr\n"); q_cmpl_status_0 = musb_readl(q_mgr_base, CPPI41_QSTATUS_REG2); q_cmpl_status_1 = musb_readl(q_mgr_base, CPPI41_QSTATUS_REG3); q_cmpl_status_2 = musb_readl(q_mgr_base, CPPI41_QSTATUS_REG4); /* USB0 tx/rx completion */ /* usb0 tx completion interrupt for ep1..15 */ usb0_tx_intr = (q_cmpl_status_0 >> 29) | ((q_cmpl_status_1 & 0xFFF) << 3); usb0_rx_intr = ((q_cmpl_status_1 & 0x07FFe000) >> 13); usb1_tx_intr = (q_cmpl_status_1 >> 29) | ((q_cmpl_status_2 & 0xFFF) << 3); usb1_rx_intr = ((q_cmpl_status_2 & 0x0fffe000) >> 13); /* get proper musb handle based usb0/usb1 ctrl-id */ dev_dbg(musb->controller, "CPPI 4.1 IRQ: Tx %x, Rx %x\n", usb0_tx_intr, usb0_rx_intr); if (gmusb[0] && (usb0_tx_intr || usb0_rx_intr)) { spin_lock_irqsave(&gmusb[0]->lock, flags); cppi41_completion(gmusb[0], usb0_rx_intr, usb0_tx_intr); spin_unlock_irqrestore(&gmusb[0]->lock, flags); ret = IRQ_HANDLED; } dev_dbg(musb->controller, "CPPI 4.1 IRQ: Tx %x, Rx %x\n", usb1_tx_intr, usb1_rx_intr); if (gmusb[1] && (usb1_rx_intr || usb1_tx_intr)) { spin_lock_irqsave(&gmusb[1]->lock, flags); cppi41_completion(gmusb[1], usb1_rx_intr, usb1_tx_intr); spin_unlock_irqrestore(&gmusb[1]->lock, flags); ret = IRQ_HANDLED; } usbss_write(USBSS_IRQ_EOI, 0); return ret; } #endif int musb_simulate_babble(struct musb *musb) { void __iomem *reg_base = musb->ctrl_base; void __iomem *mbase = musb->mregs; u8 reg; /* during babble condition musb controller * remove the session */ reg = musb_readb(mbase, MUSB_DEVCTL); reg &= ~MUSB_DEVCTL_SESSION; musb_writeb(mbase, MUSB_DEVCTL, reg); mdelay(100); /* generate s/w babble interrupt */ musb_writel(reg_base, USB_IRQ_STATUS_RAW_1, MUSB_INTR_BABBLE); return 0; } EXPORT_SYMBOL(musb_simulate_babble); void musb_babble_workaround(struct musb *musb) { void __iomem *reg_base = musb->ctrl_base; struct device *dev = musb->controller; struct musb_hdrc_platform_data *plat = dev->platform_data; struct omap_musb_board_data *data = plat->board_data; /* Reset the controller */ musb_writel(reg_base, USB_CTRL_REG, USB_SOFT_RESET_MASK); udelay(100); /* Shutdown the on-chip PHY and its PLL. */ if (data->set_phy_power) data->set_phy_power(0); udelay(100); musb_platform_set_mode(musb, MUSB_HOST); udelay(100); /* enable the usbphy */ if (data->set_phy_power) data->set_phy_power(1); mdelay(100); /* save the usbotgss register contents */ musb_platform_enable(musb); musb_start(musb); } static void evm_deferred_musb_restart(struct work_struct *work) { struct musb *musb = container_of(work, struct musb, work); ERR("deferred musb restart musbid(%d)\n", musb->id); musb_babble_workaround(musb); } static irqreturn_t ti81xx_interrupt(int irq, void *hci) { struct musb *musb = hci; void __iomem *reg_base = musb->ctrl_base; unsigned long flags; irqreturn_t ret = IRQ_NONE; u32 pend1 = 0, pend2 = 0; u32 epintr, usbintr; u8 is_babble = 0; spin_lock_irqsave(&musb->lock, flags); /* Acknowledge and handle non-CPPI interrupts */ /* Get endpoint interrupts */ epintr = musb_readl(reg_base, USB_EP_INTR_STATUS_REG); musb->int_rx = (epintr & USB_RX_INTR_MASK) >> USB_INTR_RX_SHIFT; musb->int_tx = (epintr & USB_TX_INTR_MASK) >> USB_INTR_TX_SHIFT; if (epintr) musb_writel(reg_base, USB_EP_INTR_STATUS_REG, epintr); /* Get usb core interrupts */ usbintr = musb_readl(reg_base, USB_CORE_INTR_STATUS_REG); if (!usbintr && !epintr) { dev_dbg(musb->controller, "sprious interrupt\n"); goto eoi; } if (usbintr) musb_writel(reg_base, USB_CORE_INTR_STATUS_REG, usbintr); musb->int_usb = (usbintr & USB_INTR_USB_MASK) >> USB_INTR_USB_SHIFT; dev_dbg(musb->controller, "usbintr (%x) epintr(%x)\n", usbintr, epintr); /* * DRVVBUS IRQs are the only proxy we have (a very poor one!) for * AM3517's missing ID change IRQ. We need an ID change IRQ to * switch appropriately between halves of the OTG state machine. * Managing DEVCTL.SESSION per Mentor docs requires that we know its * value but DEVCTL.BDEVICE is invalid without DEVCTL.SESSION set. * Also, DRVVBUS pulses for SRP (but not at 5V) ... */ if ((usbintr & MUSB_INTR_BABBLE) && is_otg_enabled(musb) && (musb->xceiv->state == OTG_STATE_A_HOST)) is_babble = 1; else if ((usbintr & MUSB_INTR_BABBLE) && !is_otg_enabled(musb) && is_host_enabled(musb)) is_babble = 1; if (is_babble) { if (musb->enable_babble_work) musb->int_usb |= MUSB_INTR_DISCONNECT; ERR("CAUTION: musb%d: Babble Interrupt Occured\n", musb->id); ERR("Please issue long reset to make usb functional !!\n"); } if (usbintr & (USB_INTR_DRVVBUS << USB_INTR_USB_SHIFT)) { int drvvbus = musb_readl(reg_base, USB_STAT_REG); void __iomem *mregs = musb->mregs; u8 devctl = musb_readb(mregs, MUSB_DEVCTL); int err; err = is_host_enabled(musb) && (musb->int_usb & MUSB_INTR_VBUSERROR); if (err) { /* * The Mentor core doesn't debounce VBUS as needed * to cope with device connect current spikes. This * means it's not uncommon for bus-powered devices * to get VBUS errors during enumeration. * * This is a workaround, but newer RTL from Mentor * seems to allow a better one: "re"-starting sessions * without waiting for VBUS to stop registering in * devctl. */ musb->int_usb &= ~MUSB_INTR_VBUSERROR; musb->xceiv->state = OTG_STATE_A_WAIT_VFALL; mod_timer(&musb->otg_workaround, jiffies + POLL_SECONDS * HZ); WARNING("VBUS error workaround (delay coming)\n"); } else if (is_host_enabled(musb) && drvvbus) { musb->is_active = 1; MUSB_HST_MODE(musb); musb->xceiv->default_a = 1; musb->xceiv->state = OTG_STATE_A_WAIT_VRISE; del_timer(&musb->otg_workaround); } else { musb->is_active = 0; MUSB_DEV_MODE(musb); musb->xceiv->default_a = 0; musb->xceiv->state = OTG_STATE_B_IDLE; } /* NOTE: this must complete power-on within 100 ms. */ dev_dbg(musb->controller, "VBUS %s (%s)%s, devctl %02x\n", drvvbus ? "on" : "off", otg_state_string(musb->xceiv->state), err ? " ERROR" : "", devctl); ret = IRQ_HANDLED; } if (musb->int_tx || musb->int_rx || musb->int_usb) ret |= musb_interrupt(musb); eoi: /* EOI needs to be written for the IRQ to be re-asserted. */ if (ret == IRQ_HANDLED || epintr || usbintr) { /* write EOI */ musb_writel(reg_base, USB_IRQ_EOI, 1); } /* Poll for ID change */ if (is_otg_enabled(musb) && musb->xceiv->state == OTG_STATE_B_IDLE) mod_timer(&musb->otg_workaround, jiffies + POLL_SECONDS * HZ); spin_unlock_irqrestore(&musb->lock, flags); if (ret != IRQ_HANDLED) { if (epintr || usbintr) /* * We sometimes get unhandled IRQs in the peripheral * mode from EP0 and SOF... */ dev_dbg(musb->controller, "Unhandled USB IRQ %08x-%08x\n", epintr, usbintr); else if (printk_ratelimit()) /* * We've seen series of spurious interrupts in the * peripheral mode after USB reset and then after some * time a real interrupt storm starting... */ dev_dbg(musb->controller, "Spurious IRQ, CPPI 4.1 status %08x, %08x\n", pend1, pend2); } if (is_babble) { if (!musb->enable_babble_work) { musb_writeb(musb->mregs, MUSB_DEVCTL, musb_readb(musb->mregs, MUSB_DEVCTL) | MUSB_DEVCTL_SESSION); } else { ERR("Babble: devtcl(%x)Restarting musb....\n", musb_readb(musb->mregs, MUSB_DEVCTL)); schedule_work(&musb->work); } } return ret; } int ti81xx_musb_set_mode(struct musb *musb, u8 musb_mode) { void __iomem *reg_base = musb->ctrl_base; u32 regval; /* TODO: implement this using CONF0 */ if (musb_mode == MUSB_HOST) { regval = musb_readl(reg_base, USB_MODE_REG); regval &= ~USBMODE_USBID_HIGH; if (usbid_sw_ctrl && cpu_is_ti816x()) regval |= USBMODE_USBID_MUXSEL; musb_writel(reg_base, USB_MODE_REG, regval); musb_writel(musb->ctrl_base, USB_PHY_UTMI_REG, 0x02); dev_dbg(musb->controller, "host: value of mode reg=%x regval(%x)\n", musb_readl(reg_base, USB_MODE_REG), regval); } else if (musb_mode == MUSB_PERIPHERAL) { /* TODO commmented writing 8 to USB_MODE_REG device mode is not working */ regval = musb_readl(reg_base, USB_MODE_REG); regval |= USBMODE_USBID_HIGH; if (usbid_sw_ctrl && cpu_is_ti816x()) regval |= USBMODE_USBID_MUXSEL; musb_writel(reg_base, USB_MODE_REG, regval); dev_dbg(musb->controller, "device: value of mode reg=%x regval(%x)\n", musb_readl(reg_base, USB_MODE_REG), regval); } else if (musb_mode == MUSB_OTG) { musb_writel(musb->ctrl_base, USB_PHY_UTMI_REG, 0x02); } else return -EIO; return 0; } int ti81xx_musb_init(struct musb *musb) { void __iomem *reg_base = musb->ctrl_base; struct device *dev = musb->controller; struct musb_hdrc_platform_data *plat = dev->platform_data; struct omap_musb_board_data *data = plat->board_data; u32 rev, status = 0; u8 mode; if (musb->id < 2) gmusb[musb->id] = musb; usb_nop_xceiv_register(musb->id); musb->xceiv = otg_get_transceiver(musb->id); if (!musb->xceiv) return -ENODEV; status = pm_runtime_get_sync(dev); if (status < 0) { dev_err(dev, "pm_runtime_get_sync FAILED"); goto err1; } /* mentor is at offset of 0x400 in am3517/ti81xx */ musb->mregs += USB_MENTOR_CORE_OFFSET; /* Returns zero if e.g. not clocked */ rev = musb_readl(reg_base, USB_REVISION_REG); if (!rev) return -ENODEV; if (is_host_enabled(musb)) setup_timer(&musb->otg_workaround, otg_timer, (unsigned long) musb); /* Reset the controller */ musb_writel(reg_base, USB_CTRL_REG, USB_SOFT_RESET_MASK); /* wait till reset bit clears */ while ((musb_readl(reg_base, USB_CTRL_REG) & 0x1)) cpu_relax(); /* Start the on-chip PHY and its PLL. */ if (data->set_phy_power) data->set_phy_power(1); musb->a_wait_bcon = A_WAIT_BCON_TIMEOUT; musb->isr = ti81xx_interrupt; if (cpu_is_ti816x()) usbid_sw_ctrl = 1; if (is_otg_enabled(musb)) { /* if usb-id contolled through software for ti816x then * configure the usb0 in peripheral mode and usb1 in * host mode */ if (usbid_sw_ctrl && cpu_is_ti816x()) mode = musb->id ? MUSB_HOST : MUSB_PERIPHERAL; else mode = MUSB_OTG; } else /* set musb controller to host mode */ mode = is_host_enabled(musb) ? MUSB_HOST : MUSB_PERIPHERAL; /* set musb controller to host mode */ musb_platform_set_mode(musb, mode); /* enable babble workaround */ INIT_WORK(&musb->work, evm_deferred_musb_restart); musb->enable_babble_work = 0; musb_writel(reg_base, USB_IRQ_EOI, 0); return 0; err1: pm_runtime_disable(dev); return status; } /* TI81xx supports only 32bit read operation */ void ti81xx_musb_read_fifo(struct musb_hw_ep *hw_ep, u16 len, u8 *dst) { void __iomem *fifo = hw_ep->fifo; u32 val; int i; /* Read for 32bit-aligned destination address */ if (likely((0x03 & (unsigned long) dst) == 0) && len >= 4) { readsl(fifo, dst, len >> 2); dst += len & ~0x03; len &= 0x03; } /* * Now read the remaining 1 to 3 byte or complete length if * unaligned address. */ if (len > 4) { for (i = 0; i < (len >> 2); i++) { *(u32 *) dst = musb_readl(fifo, 0); dst += 4; } len &= 0x03; } if (len > 0) { val = musb_readl(fifo, 0); memcpy(dst, &val, len); } } int ti81xx_musb_exit(struct musb *musb) { struct device *dev = musb->controller; struct musb_hdrc_platform_data *plat = dev->platform_data; struct omap_musb_board_data *data = plat->board_data; if (is_host_enabled(musb)) del_timer_sync(&musb->otg_workaround); /* Shutdown the on-chip PHY and its PLL. */ if (data->set_phy_power) data->set_phy_power(0); otg_put_transceiver(musb->xceiv); usb_nop_xceiv_unregister(musb->id); return 0; } static struct musb_platform_ops ti81xx_ops = { .fifo_mode = 4, .flags = MUSB_GLUE_EP_ADDR_FLAT_MAPPING | MUSB_GLUE_DMA_CPPI41, .init = ti81xx_musb_init, .exit = ti81xx_musb_exit, .enable = ti81xx_musb_enable, .disable = ti81xx_musb_disable, .try_idle = ti81xx_musb_try_idle, .set_mode = ti81xx_musb_set_mode, .read_fifo = ti81xx_musb_read_fifo, .write_fifo = musb_write_fifo, .dma_controller_create = cppi41_dma_controller_create, .dma_controller_destroy = cppi41_dma_controller_destroy, .simulate_babble_intr = musb_simulate_babble, }; static void __devexit ti81xx_delete_musb_pdev(struct ti81xx_glue *glue, u8 id) { platform_device_del(glue->musb[id]); platform_device_put(glue->musb[id]); } static int __devinit ti81xx_create_musb_pdev(struct ti81xx_glue *glue, u8 id) { struct device *dev = glue->dev; struct platform_device *pdev = to_platform_device(dev); struct musb_hdrc_platform_data *pdata = dev->platform_data; struct platform_device *musb; struct resource *res; struct resource resources[2]; char res_name[10]; int ret = 0; /* get memory resource */ sprintf(res_name, "musb%d", id); res = platform_get_resource_byname(pdev, IORESOURCE_MEM, res_name); if (!res) { dev_err(dev, "%s get mem resource failed\n", res_name); ret = -ENODEV; goto err0; } res->parent = NULL; resources[0] = *res; /* get irq resource */ sprintf(res_name, "musb%d-irq", id); res = platform_get_resource_byname(pdev, IORESOURCE_IRQ, res_name); if (!res) { dev_err(dev, "%s get irq resource failed\n", res_name); ret = -ENODEV; goto err0; } res->parent = NULL; resources[1] = *res; /* allocate the child platform device */ musb = platform_device_alloc("musb-hdrc", id); if (!musb) { dev_err(dev, "failed to allocate musb device\n"); goto err0; } musb->id = id; musb->dev.parent = dev; musb->dev.dma_mask = &musb_dmamask; musb->dev.coherent_dma_mask = musb_dmamask; glue->musb[id] = musb; pdata->platform_ops = &ti81xx_ops; ret = platform_device_add_resources(musb, resources, 2); if (ret) { dev_err(dev, "failed to add resources\n"); goto err1; } ret = platform_device_add_data(musb, pdata, sizeof(*pdata)); if (ret) { dev_err(dev, "failed to add platform_data\n"); goto err1; } ret = platform_device_add(musb); if (ret) { dev_err(dev, "failed to register musb device\n"); goto err1; } return 0; err1: platform_device_put(musb); err0: return ret; } static int __init ti81xx_probe(struct platform_device *pdev) { struct ti81xx_glue *glue; struct device *dev = &pdev->dev; struct musb_hdrc_platform_data *plat = dev->platform_data; struct omap_musb_board_data *data = plat->board_data; int ret = 0, i; struct resource *res; /* allocate glue */ glue = kzalloc(sizeof(*glue), GFP_KERNEL); if (!glue) { dev_err(&pdev->dev, "unable to allocate glue memory\n"); ret = -ENOMEM; goto err0; } /* interface clock needs to be enabled for usbss register programming */ glue->ick = clk_get(&pdev->dev, "usbotg_ick"); if (IS_ERR(glue->ick)) { dev_err(&pdev->dev, "unable to get usbss interface clock\n"); ret = PTR_ERR(glue->ick); goto err1; } /* functional clock needs to be enabled for usbss register programming */ glue->fck = clk_get(&pdev->dev, "usbotg_fck"); if (IS_ERR(glue->fck)) { dev_err(&pdev->dev, "unable to get usbss functional clock\n"); ret = PTR_ERR(glue->fck); goto err2; } /* get memory resource */ glue->mem_pa = platform_get_resource(pdev, IORESOURCE_MEM, 0); if (!glue->mem_pa) { dev_err(&pdev->dev, "failed to get usbss mem resourse\n"); ret = -ENODEV; goto err3; } /* get memory resource */ res = platform_get_resource_byname(pdev, IORESOURCE_IRQ, "usbss-irq"); if (!res) { dev_err(&pdev->dev, "failed to get usbss irq resourse\n"); ret = -ENODEV; goto err3; } glue->irq = res->start; /* enable interface clock */ ret = clk_enable(glue->ick); if (ret) { dev_err(&pdev->dev, "failed to enable usbss interface clock\n"); goto err3; } /* enable functional clock */ ret = clk_enable(glue->fck); if (ret) { dev_err(&pdev->dev, "failed to enable usbss functional clock\n"); goto err4; } /* iomap for usbss mem space */ glue->mem_va = ioremap(glue->mem_pa->start, resource_size(glue->mem_pa)); if (!glue->mem_va) { dev_err(&pdev->dev, "usbss ioremap failed\n"); ret = -ENOMEM; goto err5; } usbss_virt_base = glue->mem_va; glue->dev = &pdev->dev; platform_set_drvdata(pdev, glue); /* usb subsystem init */ usbotg_ss_init(); /* clear any USBSS interrupts */ __raw_writel(0, glue->mem_va + USBSS_IRQ_EOI); __raw_writel(__raw_readl(glue->mem_va + USBSS_IRQ_STATUS), glue->mem_va + USBSS_IRQ_STATUS); /* create the child platform device for mulitple instances of musb */ for (i = 0; i <= data->instances; ++i) { #ifdef CONFIG_USB_TI_CPPI41_DMA /* initialize the cppi41dma init */ cppi41_init(i, glue->irq, data->instances+1); #endif ret = ti81xx_create_musb_pdev(glue, i); if (ret != 0) goto err6; } return 0; err6: iounmap(glue->mem_va); err5: clk_disable(glue->fck); err4: clk_disable(glue->ick); err3: clk_put(glue->fck); err2: clk_put(glue->ick); err1: kfree(glue); err0: return ret; } static int __exit ti81xx_remove(struct platform_device *pdev) { struct ti81xx_glue *glue = platform_get_drvdata(pdev); struct device *dev = &pdev->dev; struct musb_hdrc_platform_data *plat = dev->platform_data; struct omap_musb_board_data *data = plat->board_data; int i; /* delete the child platform device for mulitple instances of musb */ for (i = 0; i <= data->instances; ++i) ti81xx_delete_musb_pdev(glue, i); #ifdef CONFIG_USB_TI_CPPI41_DMA cppi41_free(); #endif /* iounmap */ iounmap(glue->mem_va); usbotg_ss_uninit(); /* disable common usbss functional clock */ clk_disable(glue->fck); clk_put(glue->fck); /* disable common usbss interface clock */ clk_disable(glue->ick); clk_put(glue->ick); kfree(glue); return 0; } #ifdef CONFIG_PM static int ti81xx_suspend(struct device *dev) { struct ti81xx_glue *glue = dev_get_drvdata(dev); struct musb_hdrc_platform_data *plat = dev->platform_data; struct omap_musb_board_data *data = plat->board_data; int i; /* Shutdown the on-chip PHY and its PLL. */ for (i = 0; i <= data->instances; ++i) { if (data->set_phy_power) data->set_phy_power(i); } /* disable the common usbss functional clock */ clk_disable(glue->fck); /* disable the common usbss interface clock */ clk_disable(glue->ick); return 0; } static int ti81xx_resume(struct device *dev) { struct ti81xx_glue *glue = dev_get_drvdata(dev); struct musb_hdrc_platform_data *plat = dev->platform_data; struct omap_musb_board_data *data = plat->board_data; int ret, i; /* Start the on-chip PHY and its PLL. */ for (i = 0; i <= data->instances; ++i) { if (data->set_phy_power) data->set_phy_power(i); } /* enable the common usbss interface clock */ ret = clk_enable(glue->ick); if (ret) { dev_err(dev, "failed to enable iclock\n"); return ret; } /* enable the common usbss functional clock */ ret = clk_enable(glue->fck); if (ret) { dev_err(dev, "failed to enable fclock\n"); return ret; } return 0; } static const struct dev_pm_ops ti81xx_pm_ops = { .suspend = ti81xx_suspend, .resume = ti81xx_resume, }; #define DEV_PM_OPS (&ti81xx_pm_ops) #else #define DEV_PM_OPS NULL #endif static struct platform_driver ti81xx_musb_driver = { .remove = __exit_p(ti81xx_remove), .driver = { .name = "musb-ti81xx", .pm = DEV_PM_OPS, }, }; MODULE_AUTHOR("Felipe Balbi "); MODULE_DESCRIPTION("AM35x MUSB Glue Layer"); MODULE_LICENSE("GPL v2"); static int __init ti81xx_glue_init(void) { return platform_driver_probe(&ti81xx_musb_driver, ti81xx_probe); } subsys_initcall(ti81xx_glue_init); static void __exit ti81xx_glue_exit(void) { #ifdef CONFIG_USB_TI_CPPI41_DMA /* free the usbss irq */ free_irq(TI81XX_IRQ_USBSS, 0); #endif /* disable the interrupts */ usbss_write(USBSS_IRQ_EOI, 0); usbss_write(USBSS_IRQ_ENABLE_SET, 0); usbss_write(USBSS_IRQ_DMA_ENABLE_0, 0); /* unregister platform driver */ platform_driver_unregister(&ti81xx_musb_driver); } module_exit(ti81xx_glue_exit); #ifdef CONFIG_PM void musb_platform_save_context(struct musb *musb, struct musb_context_registers *musb_context) { /* Save CPPI41 DMA related registers */ } void musb_platform_restore_context(struct musb *musb, struct musb_context_registers *musb_context) { /* Restore CPPI41 DMA related registers */ } #endif