/* Rewritten by Rusty Russell, on the backs of many others... Copyright (C) 2001 Rusty Russell, 2002 Rusty Russell IBM. This program is free software; you can redistribute it and/or modify it under the terms of the GNU General Public License as published by the Free Software Foundation; either version 2 of the License, or (at your option) any later version. This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details. You should have received a copy of the GNU General Public License along with this program; if not, write to the Free Software Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA */ #include #include #include #include #include #include #include /* * mutex protecting text section modification (dynamic code patching). * some users need to sleep (allocating memory...) while they hold this lock. * * NOT exported to modules - patching kernel text is a really delicate matter. */ DEFINE_MUTEX(text_mutex); extern struct exception_table_entry __start___ex_table[]; extern struct exception_table_entry __stop___ex_table[]; /* Sort the kernel's built-in exception table */ void __init sort_main_extable(void) { sort_extable(__start___ex_table, __stop___ex_table); } /* Given an address, look for it in the exception tables. */ const struct exception_table_entry *search_exception_tables(unsigned long addr) { const struct exception_table_entry *e; e = search_extable(__start___ex_table, __stop___ex_table-1, addr); if (!e) e = search_module_extables(addr); return e; } static inline int init_kernel_text(unsigned long addr) { if (addr >= (unsigned long)_sinittext && addr <= (unsigned long)_einittext) return 1; return 0; } int core_kernel_text(unsigned long addr) { if (addr >= (unsigned long)_stext && addr <= (unsigned long)_etext) return 1; if (system_state == SYSTEM_BOOTING && init_kernel_text(addr)) return 1; return 0; } /** * core_kernel_data - tell if addr points to kernel data * @addr: address to test * * Returns true if @addr passed in is from the core kernel data * section. * * Note: On some archs it may return true for core RODATA, and false * for others. But will always be true for core RW data. */ int core_kernel_data(unsigned long addr) { if (addr >= (unsigned long)_sdata && addr < (unsigned long)_edata) return 1; return 0; } int __kernel_text_address(unsigned long addr) { if (core_kernel_text(addr)) return 1; if (is_module_text_address(addr)) return 1; /* * There might be init symbols in saved stacktraces. * Give those symbols a chance to be printed in * backtraces (such as lockdep traces). * * Since we are after the module-symbols check, there's * no danger of address overlap: */ if (init_kernel_text(addr)) return 1; return 0; } int kernel_text_address(unsigned long addr) { if (core_kernel_text(addr)) return 1; return is_module_text_address(addr); } /* * On some architectures (PPC64, IA64) function pointers * are actually only tokens to some data that then holds the * real function address. As a result, to find if a function * pointer is part of the kernel text, we need to do some * special dereferencing first. */ int func_ptr_is_kernel_text(void *ptr) { unsigned long addr; addr = (unsigned long) dereference_function_descriptor(ptr); if (core_kernel_text(addr)) return 1; return is_module_text_address(addr); }