/* * Generic Timer-queue * * Manages a simple queue of timers, ordered by expiration time. * Uses rbtrees for quick list adds and expiration. * * NOTE: All of the following functions need to be serialized * to avoid races. No locking is done by this library code. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA */ #include #include #include /** * timerqueue_add - Adds timer to timerqueue. * * @head: head of timerqueue * @node: timer node to be added * * Adds the timer node to the timerqueue, sorted by the * node's expires value. */ void timerqueue_add(struct timerqueue_head *head, struct timerqueue_node *node) { struct rb_node **p = &head->head.rb_node; struct rb_node *parent = NULL; struct timerqueue_node *ptr; /* Make sure we don't add nodes that are already added */ WARN_ON_ONCE(!RB_EMPTY_NODE(&node->node)); while (*p) { parent = *p; ptr = rb_entry(parent, struct timerqueue_node, node); if (node->expires.tv64 < ptr->expires.tv64) p = &(*p)->rb_left; else p = &(*p)->rb_right; } rb_link_node(&node->node, parent, p); rb_insert_color(&node->node, &head->head); if (!head->next || node->expires.tv64 < head->next->expires.tv64) head->next = node; } EXPORT_SYMBOL_GPL(timerqueue_add); /** * timerqueue_del - Removes a timer from the timerqueue. * * @head: head of timerqueue * @node: timer node to be removed * * Removes the timer node from the timerqueue. */ void timerqueue_del(struct timerqueue_head *head, struct timerqueue_node *node) { WARN_ON_ONCE(RB_EMPTY_NODE(&node->node)); /* update next pointer */ if (head->next == node) { struct rb_node *rbn = rb_next(&node->node); head->next = rbn ? rb_entry(rbn, struct timerqueue_node, node) : NULL; } rb_erase(&node->node, &head->head); RB_CLEAR_NODE(&node->node); } EXPORT_SYMBOL_GPL(timerqueue_del); /** * timerqueue_iterate_next - Returns the timer after the provided timer * * @node: Pointer to a timer. * * Provides the timer that is after the given node. This is used, when * necessary, to iterate through the list of timers in a timer list * without modifying the list. */ struct timerqueue_node *timerqueue_iterate_next(struct timerqueue_node *node) { struct rb_node *next; if (!node) return NULL; next = rb_next(&node->node); if (!next) return NULL; return container_of(next, struct timerqueue_node, node); } EXPORT_SYMBOL_GPL(timerqueue_iterate_next);