/* * An implementation of key value pair (KVP) functionality for Linux. * * * Copyright (C) 2010, Novell, Inc. * Author : K. Y. Srinivasan * * This program is free software; you can redistribute it and/or modify it * under the terms of the GNU General Public License version 2 as published * by the Free Software Foundation. * * This program is distributed in the hope that it will be useful, but * WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE, GOOD TITLE or * NON INFRINGEMENT. See the GNU General Public License for more * details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA. * */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include /* * KYS: TODO. Need to register these in the kernel. * * The following definitions are shared with the in-kernel component; do not * change any of this without making the corresponding changes in * the KVP kernel component. */ #define CN_KVP_IDX 0x9 /* MSFT KVP functionality */ #define CN_KVP_VAL 0x1 /* This supports queries from the kernel */ #define CN_KVP_USER_VAL 0x2 /* This supports queries from the user */ /* * KVP protocol: The user mode component first registers with the * the kernel component. Subsequently, the kernel component requests, data * for the specified keys. In response to this message the user mode component * fills in the value corresponding to the specified key. We overload the * sequence field in the cn_msg header to define our KVP message types. * * We use this infrastructure for also supporting queries from user mode * application for state that may be maintained in the KVP kernel component. * * XXXKYS: Have a shared header file between the user and kernel (TODO) */ enum kvp_op { KVP_REGISTER = 0, /* Register the user mode component*/ KVP_KERNEL_GET, /*Kernel is requesting the value for the specified key*/ KVP_KERNEL_SET, /*Kernel is providing the value for the specified key*/ KVP_USER_GET, /*User is requesting the value for the specified key*/ KVP_USER_SET /*User is providing the value for the specified key*/ }; #define HV_KVP_EXCHANGE_MAX_KEY_SIZE 512 #define HV_KVP_EXCHANGE_MAX_VALUE_SIZE 2048 struct hv_ku_msg { __u32 kvp_index; __u8 kvp_key[HV_KVP_EXCHANGE_MAX_KEY_SIZE]; /* Key name */ __u8 kvp_value[HV_KVP_EXCHANGE_MAX_VALUE_SIZE]; /* Key value */ }; enum key_index { FullyQualifiedDomainName = 0, IntegrationServicesVersion, /*This key is serviced in the kernel*/ NetworkAddressIPv4, NetworkAddressIPv6, OSBuildNumber, OSName, OSMajorVersion, OSMinorVersion, OSVersion, ProcessorArchitecture }; /* * End of shared definitions. */ static char kvp_send_buffer[4096]; static char kvp_recv_buffer[4096]; static struct sockaddr_nl addr; static char *os_name = ""; static char *os_major = ""; static char *os_minor = ""; static char *processor_arch; static char *os_build; static char *lic_version; static struct utsname uts_buf; void kvp_get_os_info(void) { FILE *file; char *p, buf[512]; uname(&uts_buf); os_build = uts_buf.release; processor_arch = uts_buf.machine; /* * The current windows host (win7) expects the build * string to be of the form: x.y.z * Strip additional information we may have. */ p = strchr(os_build, '-'); if (p) *p = '\0'; file = fopen("/etc/SuSE-release", "r"); if (file != NULL) goto kvp_osinfo_found; file = fopen("/etc/redhat-release", "r"); if (file != NULL) goto kvp_osinfo_found; /* * Add code for other supported platforms. */ /* * We don't have information about the os. */ os_name = uts_buf.sysname; return; kvp_osinfo_found: /* up to three lines */ p = fgets(buf, sizeof(buf), file); if (p) { p = strchr(buf, '\n'); if (p) *p = '\0'; p = strdup(buf); if (!p) goto done; os_name = p; /* second line */ p = fgets(buf, sizeof(buf), file); if (p) { p = strchr(buf, '\n'); if (p) *p = '\0'; p = strdup(buf); if (!p) goto done; os_major = p; /* third line */ p = fgets(buf, sizeof(buf), file); if (p) { p = strchr(buf, '\n'); if (p) *p = '\0'; p = strdup(buf); if (p) os_minor = p; } } } done: fclose(file); return; } static int kvp_get_ip_address(int family, char *buffer, int length) { struct ifaddrs *ifap; struct ifaddrs *curp; int ipv4_len = strlen("255.255.255.255") + 1; int ipv6_len = strlen("ffff:ffff:ffff:ffff:ffff:ffff:ffff:ffff")+1; int offset = 0; const char *str; char tmp[50]; int error = 0; /* * On entry into this function, the buffer is capable of holding the * maximum key value (2048 bytes). */ if (getifaddrs(&ifap)) { strcpy(buffer, "getifaddrs failed\n"); return 1; } curp = ifap; while (curp != NULL) { if ((curp->ifa_addr != NULL) && (curp->ifa_addr->sa_family == family)) { if (family == AF_INET) { struct sockaddr_in *addr = (struct sockaddr_in *) curp->ifa_addr; str = inet_ntop(family, &addr->sin_addr, tmp, 50); if (str == NULL) { strcpy(buffer, "inet_ntop failed\n"); error = 1; goto getaddr_done; } if (offset == 0) strcpy(buffer, tmp); else strcat(buffer, tmp); strcat(buffer, ";"); offset += strlen(str) + 1; if ((length - offset) < (ipv4_len + 1)) goto getaddr_done; } else { /* * We only support AF_INET and AF_INET6 * and the list of addresses is separated by a ";". */ struct sockaddr_in6 *addr = (struct sockaddr_in6 *) curp->ifa_addr; str = inet_ntop(family, &addr->sin6_addr.s6_addr, tmp, 50); if (str == NULL) { strcpy(buffer, "inet_ntop failed\n"); error = 1; goto getaddr_done; } if (offset == 0) strcpy(buffer, tmp); else strcat(buffer, tmp); strcat(buffer, ";"); offset += strlen(str) + 1; if ((length - offset) < (ipv6_len + 1)) goto getaddr_done; } } curp = curp->ifa_next; } getaddr_done: freeifaddrs(ifap); return error; } static int kvp_get_domain_name(char *buffer, int length) { struct addrinfo hints, *info ; int error = 0; gethostname(buffer, length); memset(&hints, 0, sizeof(hints)); hints.ai_family = AF_INET; /*Get only ipv4 addrinfo. */ hints.ai_socktype = SOCK_STREAM; hints.ai_flags = AI_CANONNAME; error = getaddrinfo(buffer, NULL, &hints, &info); if (error != 0) { strcpy(buffer, "getaddrinfo failed\n"); return error; } strcpy(buffer, info->ai_canonname); freeaddrinfo(info); return error; } static int netlink_send(int fd, struct cn_msg *msg) { struct nlmsghdr *nlh; unsigned int size; struct msghdr message; char buffer[64]; struct iovec iov[2]; size = NLMSG_SPACE(sizeof(struct cn_msg) + msg->len); nlh = (struct nlmsghdr *)buffer; nlh->nlmsg_seq = 0; nlh->nlmsg_pid = getpid(); nlh->nlmsg_type = NLMSG_DONE; nlh->nlmsg_len = NLMSG_LENGTH(size - sizeof(*nlh)); nlh->nlmsg_flags = 0; iov[0].iov_base = nlh; iov[0].iov_len = sizeof(*nlh); iov[1].iov_base = msg; iov[1].iov_len = size; memset(&message, 0, sizeof(message)); message.msg_name = &addr; message.msg_namelen = sizeof(addr); message.msg_iov = iov; message.msg_iovlen = 2; return sendmsg(fd, &message, 0); } int main(void) { int fd, len, sock_opt; int error; struct cn_msg *message; struct pollfd pfd; struct nlmsghdr *incoming_msg; struct cn_msg *incoming_cn_msg; struct hv_ku_msg *hv_msg; char *p; char *key_value; char *key_name; daemon(1, 0); openlog("KVP", 0, LOG_USER); syslog(LOG_INFO, "KVP starting; pid is:%d", getpid()); /* * Retrieve OS release information. */ kvp_get_os_info(); fd = socket(AF_NETLINK, SOCK_DGRAM, NETLINK_CONNECTOR); if (fd < 0) { syslog(LOG_ERR, "netlink socket creation failed; error:%d", fd); exit(-1); } addr.nl_family = AF_NETLINK; addr.nl_pad = 0; addr.nl_pid = 0; addr.nl_groups = CN_KVP_IDX; error = bind(fd, (struct sockaddr *)&addr, sizeof(addr)); if (error < 0) { syslog(LOG_ERR, "bind failed; error:%d", error); close(fd); exit(-1); } sock_opt = addr.nl_groups; setsockopt(fd, 270, 1, &sock_opt, sizeof(sock_opt)); /* * Register ourselves with the kernel. */ message = (struct cn_msg *)kvp_send_buffer; message->id.idx = CN_KVP_IDX; message->id.val = CN_KVP_VAL; message->seq = KVP_REGISTER; message->ack = 0; message->len = 0; len = netlink_send(fd, message); if (len < 0) { syslog(LOG_ERR, "netlink_send failed; error:%d", len); close(fd); exit(-1); } pfd.fd = fd; while (1) { pfd.events = POLLIN; pfd.revents = 0; poll(&pfd, 1, -1); len = recv(fd, kvp_recv_buffer, sizeof(kvp_recv_buffer), 0); if (len < 0) { syslog(LOG_ERR, "recv failed; error:%d", len); close(fd); return -1; } incoming_msg = (struct nlmsghdr *)kvp_recv_buffer; incoming_cn_msg = (struct cn_msg *)NLMSG_DATA(incoming_msg); switch (incoming_cn_msg->seq) { case KVP_REGISTER: /* * Driver is registering with us; stash away the version * information. */ p = (char *)incoming_cn_msg->data; lic_version = malloc(strlen(p) + 1); if (lic_version) { strcpy(lic_version, p); syslog(LOG_INFO, "KVP LIC Version: %s", lic_version); } else { syslog(LOG_ERR, "malloc failed"); } continue; case KVP_KERNEL_GET: break; default: continue; } hv_msg = (struct hv_ku_msg *)incoming_cn_msg->data; key_name = (char *)hv_msg->kvp_key; key_value = (char *)hv_msg->kvp_value; switch (hv_msg->kvp_index) { case FullyQualifiedDomainName: kvp_get_domain_name(key_value, HV_KVP_EXCHANGE_MAX_VALUE_SIZE); strcpy(key_name, "FullyQualifiedDomainName"); break; case IntegrationServicesVersion: strcpy(key_name, "IntegrationServicesVersion"); strcpy(key_value, lic_version); break; case NetworkAddressIPv4: kvp_get_ip_address(AF_INET, key_value, HV_KVP_EXCHANGE_MAX_VALUE_SIZE); strcpy(key_name, "NetworkAddressIPv4"); break; case NetworkAddressIPv6: kvp_get_ip_address(AF_INET6, key_value, HV_KVP_EXCHANGE_MAX_VALUE_SIZE); strcpy(key_name, "NetworkAddressIPv6"); break; case OSBuildNumber: strcpy(key_value, os_build); strcpy(key_name, "OSBuildNumber"); break; case OSName: strcpy(key_value, os_name); strcpy(key_name, "OSName"); break; case OSMajorVersion: strcpy(key_value, os_major); strcpy(key_name, "OSMajorVersion"); break; case OSMinorVersion: strcpy(key_value, os_minor); strcpy(key_name, "OSMinorVersion"); break; case OSVersion: strcpy(key_value, os_build); strcpy(key_name, "OSVersion"); break; case ProcessorArchitecture: strcpy(key_value, processor_arch); strcpy(key_name, "ProcessorArchitecture"); break; default: strcpy(key_value, "Unknown Key"); /* * We use a null key name to terminate enumeration. */ strcpy(key_name, ""); break; } /* * Send the value back to the kernel. The response is * already in the receive buffer. Update the cn_msg header to * reflect the key value that has been added to the message */ incoming_cn_msg->id.idx = CN_KVP_IDX; incoming_cn_msg->id.val = CN_KVP_VAL; incoming_cn_msg->seq = KVP_USER_SET; incoming_cn_msg->ack = 0; incoming_cn_msg->len = sizeof(struct hv_ku_msg); len = netlink_send(fd, incoming_cn_msg); if (len < 0) { syslog(LOG_ERR, "net_link send failed; error:%d", len); exit(-1); } } }